Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
Image of Trinamic TMC6200-Slide9 1st 2nd

The given BOM is dimensioned for 48V peak motor supply voltage, while offering a tiny footprint. It is realized on the TMC6200-BOB breakout board. It uses compact dual MOSFETs and dual 1206 sense resistors. The resulting value of 16 mΩ is designed for a maximum current of up to 10ARMS phase current at 5 times amplification. The actual RMS current can be adapted to lower settings by initialization via software. For the best sense resistors to match different motor currents, see the calculation formula.

PTM Published on: 2019-08-08