Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
Image of ROHM Semiconductor Low IQ DC/DC Converters - Slide5

As mentioned on the previous slide, the BD83070GWL is a highly efficient DC/DC buck-boost switching converter. The BD83070GWL can provide up to 92% efficiency at very low 100µA of output current, and as shown here in the efficiency graph, as high as 97% at high current. Currently, the BD83070GWL provides one of the best efficiencies when compared to other competitor parts in this category.

PTM Published on: 2019-11-26