Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
Image of ROHM Semiconductor Low IQ DC/DC Converters - Slide2

Most battery powered applications, including wearables, are seeking to extend the operation time while extending the time between charges or replacement of the battery. Therefore, quiescent current of a device becomes very important to address this requirement. Quiescent current (IQ) is the current that is consumed by a device when it is not switching or providing any current to the output. It usually represents a power loss. ROHM has introduced power regulators with very Low IQ to address this need.

PTM Published on: 2019-11-26