TivaWare™ for C Series is an extensive suite of software designed to simplify and speed up embedded application development when using Tiva C Series MCUs. TivaWare for C Series includes the Peripheral Driver Library, Graphics Library, USB Library and Sensor Library, which include several APIs to configure and initialize different peripherals of the Tiva C Series MCUs.
These libraries come with the source code which is mostly in C. They are pre compiled for use 'as-is' and can also be adapted as desired. TivaWare for C Series also includes boot loader, several code examples and third party packages that allow the user to focus on their application development and not so much on 'how to set up the MCU’.