Maker.io main logo

How to Crack a Safe's Combination ‎with a Robotic Auto Dialer - Part 2

829

2023-02-06 | By Zach Hipps

License: See Original Project Adafruit Feather

My brother-in-law, Levy, has a safe and he doesn’t remember the combination. He ‎called and asked me to see if it was possible to build a robot that could crack the safe ‎combination, so of course I told him I would give it a shot. If you haven’t read part 1 of ‎this build series I would suggest starting there.

project_1

The way I’m approaching this problem is to try something, fail, and iterate as quickly as ‎possible. I’m not trying to build the perfect solution right from the start. This is a ‎prototype that will be refined as I progress toward the goal of opening Levy’s safe. I ‎hope to publish my CAD files, code, and other design documentation as open source. I ‎would love for this project to grow beyond my abilities and skills.‎

At this point, I have a stepper motor with a motor driver attached to it. The motor driver ‎can detect the load on the motor shaft which can be monitored for motor stalls. I’m ‎using a PD57-2-1076 stepper motor with a 24V power supply. To send step and ‎direction signals and control the motor driver, I’m using an Adafruit Feather Huzzah ‎ESP8266 Wi-Fi microcontroller. Why did I choose a microcontroller with Wi-Fi? ‎Because I would like to have a web or mobile app interface for this device. I would like ‎to monitor the progress of the safe cracking session from my phone and have the ‎correct combination sent to my phone when it’s done. The ESP8266 has a 128x32 ‎OLED display which can display a lot of useful information, but screen real estate is ‎limited, and using that to configure the device and change settings could be a little ‎difficult. I also looked at professional safe auto-dialers and designed an adjustable ‎chuck that attaches to the motor shaft. I 3D printed flexible “fingers” for the chuck jaws ‎to grab onto the safe dial. The chuck can be adjusted, and various flexible fingers can ‎be attached to accommodate safe dials with diameters that vary from around 1.5” to 4”. ‎Right now, I can hold this crude assembly up to a safe by hand and have the motor ‎spin the dial. I bought a cheap “practice” safe to test my prototype. I know the ‎combination to this new safe, so I hardcoded the combination into my microcontroller ‎and held up the auto dialer to a mixed-up combination dial. The motor was able to turn ‎the dial with a pretty good balance of precision and speed and aligned all three gates. ‎With the gates all aligned, I opened the safe latch by hand. The results are pretty ‎promising, and it gives me the confidence to keep moving in this direction.‎

frame_2

I have a 3D model of a simple frame structure that will hold the motor to the door of the ‎safe. It consists of two aluminum plates held about 4 inches apart with aluminum ‎tubes. The tubes have threads tapped into the ends and the whole assembly is ‎fastened together with ¼-20 countersunk screws. I used a laser cutting service to cut ‎the two plates from ¼” aluminum and had them countersink the holes where the ‎screws go. Finally, they gave it a nice matte black anodized finish. I cut the aluminum ‎tubes to the right length and tapped the ends with a ¼-20 thread. Next, I mounted the ‎stepper motor to the upper plate using some M5 screws and nuts and fastened the two ‎plates together. The plan was to embed some neodymium magnets into the base plate. ‎I even designed some 15mm holes around the base plate for this purpose. I hoped they ‎would be strong enough to hold the whole device to the metal door of the safe. I ‎stacked several 15mm diameter magnets into each of the eight holes and it was pretty ‎clear right away that these would not be strong enough to hold the assembly to the ‎door. I need to come up with a better solution. The quick and dirty way is to just get a ‎huge magnet and use that as some extra holding power. I 3D printed a little mounting ‎bracket for the new magnet and that did the trick. I don’t like how this looks, so I’ll be ‎revisiting this problem in the future. ‎

mount_3

The next problem on the docket is the microcontroller. As I said earlier, I chose a ‎feather huzzah ESP8266 with a small OLED display next to it. This would work fine, ‎but I was already maxing out the number of GPIO pins on that board, and the screen ‎was a bit too small to read from a distance. I found this new ESP32-S2 TFT Feather ‎board, and since it also uses the feather board footprint, it was a drop-in replacement ‎for the ESP8266. It has a much larger 240x135 pixel color TFT display built right onto ‎the same PCB as the ESP32 chip. It has more GPIO pins and native USB built in. ‎Overall, I think this is a much better choice for this project in the long run. I used a ‎featherwing board that breaks out every pin to a screw terminal block which is very ‎handy when prototyping. I can move things around without worrying about soldering ‎the connections. I also added a rotary encoder with a push button for navigating and ‎selecting items in the controller menu I plan to write. At this point, I am ready to set the ‎device onto the safe and write a bunch of code to solve the combination. ‎

code_4

The only problem with the “practice safe” I bought is that it doesn’t allow the user to ‎change the combination. I think it would be much better to have a safe combination ‎that could be changed and updated as I test my code, so I found a replacement dial ‎mechanism that does just that. I designed a mock-up safe door with the proper ‎threaded holes for this new dial. Again, I used a laser cutting service to cut the pieces ‎out of ¼” steel plate and had them drill and tap the holes for me. I mounted the new dial ‎onto the mock-up door and changed the combination to a new one. This mock-up safe ‎door makes it easy to see the inner workings of the dial wheels and see when the ‎gates are aligned.‎

dial_5

These safe combinations usually have 3 numbers with 100 possible numbers to ‎choose from. That means that there are potentially 100*100*100 or 1 million possible ‎combinations. I’m trying to make my auto dialer spin the dial and test each combination ‎as quickly as possible, so for argument’s sake let’s pretend that I can try one ‎combination per second. That would mean to try all combinations it would take 1 ‎million seconds or 11.57 days! So, statistically, it would take me about half that time to ‎find the right combination and stop trying any further combinations.‎

dial_6

This is longer than I want, so there are a few things I can do to make this task much ‎easier. First, on cheap safes the disk for the third number is divided up into 12 indented ‎segments. 11 of those indentations are “false gates” that, I think, are meant to trick a ‎would-be safecracker. The result is that it narrows down the possibilities significantly of ‎a brute force attack which is great for me! Instead of the third number having 100 ‎possibilities I now only have to try 12, so now the total number is 100*100*12 which is ‎only 120,000 combinations to try (1.4 days)! This is a great start, but let’s see if there is ‎anything else I can do to keep reducing that total number. I’ve read that the indents of ‎the 11 false gates are slightly different from the indent of the actual correct third gate. ‎This is something I can feel by turning the handle at one of the false gates and seeing ‎how many degrees I can turn the dial. If I spend a few minutes and test all 12 indents ‎I’m hoping that one of them will let me turn the dial just slightly more (or slightly less), ‎while the other 11 will be the same. This will tell me exactly what the third number is, ‎reducing the total number of combinations to 100*100*1 which equals 10,000. ‎Furthermore, the dial tolerance isn’t perfect which means I don’t have to land perfectly ‎on the correct number for the latch to slide into the gate. Depending on the quality of ‎manufacturing and design tolerance I could be off by a half number above and below ‎the correct number and still be able to open the latch. This again reduces the total ‎number to 50*50*1 which equals 2,500 total combinations which would only take about ‎‎20 minutes on average to find the right one. This is a 99.75% reduction in the total ‎number of combinations I need to try, and I haven’t even put the device on the safe yet! ‎Yeah science! I’m also told that certain manufacturers suggest not using certain ‎numbers for the last digit due to the spacing and interference of the gate pins so I ‎could reduce this down even further if I wanted to get manufacturer specific, but this is ‎good enough for me. I suppose it wouldn’t be that hard to add “profiles” of make and ‎model numbers to a user interface if I wanted to take advantage of these further quirks.‎

It’s time. I’m ready to attach my auto dialer to the mock-up door safe and try to crack my ‎first safe combination. Unfortunately, this mock-up door safe doesn’t have the “false ‎gate” exploit like the cheap safe so I’ll have to try more combinations. I set the dial to its ‎starting point of zero and press the button to start the safe cracking session. The auto ‎dialer makes quick work of testing all the various combinations and after several ‎minutes finds the right combination! Success! I use the change key to set a random ‎combination and run it again just to make sure it wasn’t a fluke. Now that I’ve got a ‎prototype working, it’s time to bring this device over to my brother-in-law’s house and ‎see if I can get his locked safe open! That will be part 3 (and hopefully the concluding ‎part) of this build series.‎

 

Recommended Reading

メーカー品番 PD57-2-1076
STEPPER MOTOR HYBRID BIPOLAR 24V
Analog Devices Inc./Maxim Integrated
メーカー品番 L6R48-240
AC/DC WALL MOUNT ADAPTER 24V 48W
Tri-Mag, LLC
メーカー品番 3213
ESP8266 FEATHER HUZZAH STACK HDR
Adafruit Industries LLC
メーカー品番 3045
ASSEMBLED ADAFRUIT FEATHERWING O
Adafruit Industries LLC
メーカー品番 5300
ESP32-S2 TFT FEATHER PCB ANT
Adafruit Industries LLC
メーカー品番 2926
TERMINAL BLOCK BREAKOUT FEATHERW
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.