Maker.io main logo

Why and How to Build a 6502 Microprocessor-Based Breadboard Computer

1,443

2020-03-25 | By Clive Maxfield

Breadboards Wearables

Why would anyone want to build a 6502 microprocessor-based breadboard computer? Well, that’s just what we do. How can someone build such a beast? Read on...

Engineers are makers by nature. It is their natural inclination to create things in the domain of their choice—mechanical, electronic, fluidic, hardware, software, it really doesn’t matter. Also, although typically not known for their gregarious nature (there's an old joke that you know if an engineer is an extrovert if he looks at your shoes when he's talking to you rather than his own), engineers are almost invariably interested to hear what other engineers are doing engineering-wise, irrespective of whether it's on a professional or personal (hobby) basis.

Ever since I was around 14 years old, I've been building electronic "stuff." During the course of my career, I've designed everything from silicon chips to circuit boards. In the case of my own hobby projects, I've built a range of weird and wonderful things, from brainwave amplifiers to Awesome Audio-Reactive Artifacts to Countdown Timers to Steampunk Prognostication Engines (don't ask). Some of them even worked.

I remember the excitement when the first microprocessors appeared on the scene, starting with the 8-bit Intel 8080 in April 1974, a device that many consider to be the first true general-purpose microprocessor. Although it contained only around 4,500 transistors and could perform only 200,000 operations per second, the 8080 was destined for fame as the central processor of many early home computers. Following the 8080, the microprocessor field exploded with devices such as the 6800 from Motorola in August 1974, the 6502 from MOS Technology in 1975, and the Z80 from Zilog in 1976 (to name but a few).

The 6502, in particular, holds a special place in many people's hearts. When it was introduced in 1975, the 6502 was, by a considerable margin, the least expensive microprocessor on the market. As a result, the 6502 (or variations thereof) formed the heart of many popular video game consoles and computers, such as the Atari 2600, Atari 8-bit family, Apple II, Nintendo Entertainment System, Commodore 64, Atari Lynx, BBC Micro, and others. In fact, a company called Retro Games is poised to launch a retro reboot of the Commodore 64 called THEC64.

I think of the 1970s and 1980s as being the heyday of DIY electronics. As the years passed, however, it seemed as though fewer and fewer people were interested in building electronic projects. By the early 2000s, electronics hobbyist magazines were starting to fail, and I had come to believe that there weren't many of us techno dweebs left. Then, suddenly, circa 2005, MAKE magazine launched, the Arduino appeared on the scene, the Maker Movement started to rock and roll, and Hackerspaces and Maker Faires started to pop up all over the place. "Thank goodness," I thought, "I am not alone!" DigiKey now also has its own must-see DIY site: Maker.io.

These days, I bill myself as an engineer, writer, and communicator. As part of my technical consulting, I run across a lot of leading-edge companies creating next-generation technologies. This is complemented by my interest in DIY, through which I get introduced to all sorts of folks, including masterful makers. Take the aptly named Nick Bild, for example.

Say "Hello" to Nick Bild

Nick is an interesting character whose formal education and experience has all been on the software side of the fence. Nick has degrees in computer science and bioinformatics, and he's spent 15 years as a software engineer. Until relatively recently, however, Nick knew next to nothing about the hardware side of things.

Why and How to Build a 6502 Microprocessor-Based Breadboard Computer

Figure 1: Nick Bild started on the software side of the fence knowing almost nothing about hardware. Now, just one year after deciding to become a maker, his projects include hardware, software, and artificial intelligence. (Image source: Nick Bild)

Nick tells me that, as long as he can remember, he's been interested in understanding how things work, and he's dreamed of coming up with ways of improving devices and technologies. About a year ago, he had the epiphany, "Why don't I just do it? Why can't I be the one to make something new and interesting?"

Initially, Nick wasn't sure how to start, but he says that there are so many educational resources available on the internet that he was able to break down his ideas into a series of steps, do some research, and devise methods to complete each step.

Amazingly enough, the first project Nick set out to design and build was a programmable 6502 CPU-based breadboard computer he called the Vectron 64.

Why and How to Build a 6502 Microprocessor-Based Breadboard Computer

Figure 2: The Vectron 64 breadboard computer comprises an 8-bit 6502 CPU, 32 Kbytes of RAM, and 32 Kbytes of ROM, along with a PS/2 keyboard and an LCD display for input and output. (Image source: Nick Bild)

When Nick commenced the Vectron 64 project, he knew almost nothing about hardware, so his first step was to learn the difference between voltage and current. A few months later, he had a custom-built computer with an 8-bit 6502 CPU, 32 Kbytes of RAM, and 32 Kbytes of ROM, along with a PS/2 keyboard and an LCD display for input and output.

All of the files associated with this project are available on GitHub. Most of the parts Nick used are available from DigiKey. A 99% full BOM with part numbers available from DigiKey is shown at the bottom of this blog: visit Github for a comprehensive BOM. [Note to reviewer: Some parts are not available from DigiKey so are not shown or mentioned here (including the 6502 processor) – they are listed on the Github BOM.]

Since I'm a hardware design engineer by trade (I putter around on the software side of things), I can only imagine how difficult it would be to learn all this stuff from scratch. I can also only imagine the sense of satisfaction Nick must have felt when his first "Hello" message appeared on the Vectron 64's LCD (Figure 3).

Why and How to Build a 6502 Microprocessor-Based Breadboard Computer

Figure 3: After months of work, the Vectron 64 LCD displayed its first "Hello" message. (Image source: Nick Bild)

The Vectron 64 is an incredible achievement for a software developer's first hardware project. Amazingly enough, this only whet Nick's appetite for more. For his next project, Nick decided to make his Vectron 64 do something unexpected or improbable. After some thought, he decided that augmenting it with a homemade virtual reality (VR) headset would be fun.

In fact, Nick has been busily building all sorts of things, including augmented reality sunglasses that can tell you when a baseball is good to hit or not, in real time as you’re prepped to swing.

We will be looking at a variety of these projects in a series of future blogs. In the meantime, what do you think of Nick's Vectron 64? What do you like the most about it? Are you tempted to build one of your own? And is there anything you would do differently if you were to build one for yourself?

Why and How to Build a 6502 Microprocessor-Based Breadboard Computer

Links

KEMET - 399-9859-2-ND

Nichicon - 493-13277-1-ND

United Chemi-Con - 565-4258-1-ND

Panasonic Electronic Components - P13560-ND

KEMET - 399-13913-1-ND

Texas Instruments - 296-1570-5-ND

Texas Instruments - 296-2131-5-ND

Texas Instruments - 296-1646-5-ND

Texas Instruments - 296-1653-5-ND

Texas Instruments - 296-1566-5-ND

STMicroelectronics - <497-1443-5-ND

Microchip Technology - AT28C256-15PU-ND

Cypress Semiconductor Corp - 428-1069-ND

Texas Instruments - 296-1658-5-ND

Lumex Opto/Components Inc. - 67-1781-ND

onsemi - MPSA29-D26ZCT-ND

Stackpole Electronics Inc - CF14JT10K0CT-ND

Vishay/Dale - 1135-1619-ND

Stackpole Electronics Inc - CF14JT3K30CT-ND

C&K - 401-1967-ND

Texas Instruments - 296-1600-5-ND

E-Switch - EG2355-ND

Bourns Inc. - 3362R-104LF-ND

Renesas Electronics America Inc. - 631-1317-1-ND

Adafruit Industries LLC - 1528-2143-ND

メーカー品番 L7805CV
IC REG LINEAR 5V 1.5A TO220
STMicroelectronics
メーカー品番 LCM-S01602DTR/M
LCD MOD 32 DIG 16 X 2 REFLECTIVE
Lumex Opto/Components Inc.
メーカー品番 CF14JT10K0
RES 10K OHM 5% 1/4W AXIAL
Stackpole Electronics Inc
メーカー品番 2143
RASPBERRY PI CAMERA CABLE 1M
Adafruit Industries LLC
メーカー品番 C315C104M5U5TA7303
CAP CER 0.1UF 50V Z5U RADIAL
KEMET
メーカー品番 UCS2C221MHD1TN
CAP ALUM 220UF 20% 160V RADIAL
ニチコン
メーカー品番 EKY-101ETD470MJC5S
CAP ALUM 47UF 20% 100V RADIAL TH
Chemi-Con
メーカー品番 EEU-ED2W220S
CAP ALUM 22UF 20% 450V RADIAL TH
Panasonic Industry
メーカー品番 C315C102K1R5TA7301
CAP CER 1000PF 100V X7R RADIAL
KEMET
メーカー品番 SN74HC08N
IC GATE AND 4CH 2-INP 14DIP
Texas Instruments
メーカー品番 CD74HCT688E
IC ID COMPARATOR 8BIT 20-PDIP
Texas Instruments
メーカー品番 SN74LS161AN
IC BINARY COUNTER 4-BIT 16DIP
Texas Instruments
メーカー品番 SN74LS244N
IC BUFF 4.75V/5.25V 20-PDIP
Texas Instruments
メーカー品番 SN74HC04N
IC INVERTER 6CH 1-INP 14DIP
Texas Instruments
メーカー品番 AT28C256-15PU
IC EEPROM 256KBIT PARALLEL 28DIP
Microchip Technology
メーカー品番 SN74LS32N
IC GATE OR 4CH 2-INP 14DIP
Texas Instruments
メーカー品番 SN74HC595N
IC SR TRI-STATE 8BIT 16-PDIP
Texas Instruments
メーカー品番 MPSA29-D26Z
TRANS NPN DARL 100V 0.8A TO-92-3
onsemi
メーカー品番 CF14JT3K30
RES 3.3K OHM 5% 1/4W AXIAL
Stackpole Electronics Inc
メーカー品番 D6C50 F1 LFS
SWITCH PUSH SPST-NO 0.1A 32V
C&K
メーカー品番 100SP1T1B4M2QE
SWITCH TOGGLE SPDT 5A 120V
E-Switch
メーカー品番 3362R-1-104LF
TRIMMER 100K OHM 0.5W PC PIN TOP
Bourns Inc.
メーカー品番 XLH536001.000000I
XTAL OSC XO 1.0000MHZ HCMOS SMD
Renesas Electronics Corporation
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.