Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Slide 16
Slide 17
Slide 18
Slide 19
Slide 20
Slide 21
Slide 22
Slide 23
Slide 24
Slide 25
Slide 26
Slide 27
Slide 28
Slide 29
Slide 30
Slide 31
Slide 32
Product List
With every new generation of POL converters, OmniOn Power consolidated more components to perform the functions of multiple predecessors. This allows customers to consolidate and simplify designs. Another important feature is that these products are designed to be part of an interchangeable variety of solutions. The DOSA solutions are part of a dual-footprint capability. This means that the PICO and the MICRO, for example, use a dual footprint that allows the user to move quickly between one size and the next, and the same with the MICRO and the MEGA. This allows the ability to move up to a quick cost reduction, or to scale up with a dual footprint. OmniOn Power also licenses their products along with their patented tunable loop technology to alternate vendors such as BelFuse and Murata Power Solutions in order to mitigate the level of risk for the customer.
PTM Published on: 2011-10-26