Maker.io main logo

SparkFun QwiicBus Hookup Guide

221

2025-08-01 | By SparkFun Electronics

Arduino Qwiic

Courtesy of SparkFun

Guide by El Duderino, Englandsaurus

Introduction

Introducing the SparkFun QwiicBus system! The QwiicBus is a fast and easy way to extend the range of your I2C bus. The QwiicBus system features two boards: the SparkFun QwiicBus EndPoint and the SparkFun QwiicBus MidPoint. SparkFun also offers the QwiicBus Kit that includes two EndPoints, one MidPoint and two Ethernet cables to get you started with the QwiicBus.

Using NXP's PCA9615 differential I2C bus buffer IC, the QwiicBus converts the two default I2C signals into four differential signals (two for SCL and two for SDA). The differential signals are sent over an Ethernet cable, which attaches to the EndPoint or MidPoint through the on-board RJ-45 connectors. Differential signaling allows the I2C signals to reach distances of over 100 feet while still maintaining their signal integrity. In our testing using two EndPoints, four MidPoints, at least one Qwiic device on each node and over 200 feet of Ethernet cable, we were able to use all devices with nearly no signal integrity loss!

The EndPoint acts as the starting and ending points of the QwiicBus and the MidPoint allows you to add a drop-in I2C connection to your long-distance differential I2C chain wherever you would like.

These boards grew out of a collaboration with FarmHand Automation. While developing autonomous micro-tractors to help small farmers grow their business, Farmhand realized they needed a low cost, open-source CAN/Modbus alternative. FarmHand founder, Alex Jones said, "We knew the sensors we wanted to use, but as soon as you need to communicate over long distances in noisy environments things get complicated. The Qwiic Midpoint is going to solve a lot of that headache." The QwiicBus MidPoint and QwiicBus EndPoint are ideal for applications that require long-range communication over Ethernet, such as agricultural technology or data collection/monitoring in rural/remote areas.

Whether you have a robot with multiple I2C devices throughout it like FarmHand, a sensor network project with multiple sensors over a large area or other I2C projects you can think of that require a wired signal transmission over long distances, the QwiicBus makes that communication a breeze!

Required Materials

If you are using the QwiicBus Kit, you'll have the required boards and Ethernet cables to assemble your QwiicBus circuit. Otherwise, you'll want to pick up two EndPoints and however many MidPoints your project needs.

Along with the QwiicBus boards, you will need the following materials to follow along with this tutorial. You may not need everything though depending on what you have. Add it to your cart, read through the guide, and adjust the cart, as necessary.

A microcontroller is needed to control any I2C devices attached to your QwiicBus. Below are a few options that come Qwiic-enabled out of the box:

If you would prefer to use a single-board computer (SBC) like a Raspberry Pi or Jetson Nano as your controller, the products below will also work with the QwiicBus:

If your favorite microcontroller or single board computer is not already Qwiic-enabled, you can add that functionality with one or more of the following items:

You will also probably want a few Qwiic cables to connect your devices on your I2C bus:

Finally, if you are not using the QwiicBus Kit you'll need at least one straight through Ethernet cable.

Optional Extras for Alternate QwiicBus Power Configurations

The QwiicBus offers multiple power configurations intended for applications where many devices need to be powered over the QwiicBus. We cover these configurations in more detail in the Hardware Overview and Hardware Assembly. To use these configurations, you will need some extra hardware and tools. Click the button below to view some recommended products for alternate power configurations.

Additional Hardware & Tools for Alternate QwiicBus Power Configurations

 

You'll want a dedicated power supply capable of supplying 5-36V with adequate Amperage depending on your project's needs along with some wire to connect it to your QwiicBus:

  • Power Supply - 5V, 4A
  • Mean Well LED Switching Power Supply - 5VDC, 5A
  • Mean Well Switching Power Supply - 12VDC, 12.5A
  • Mean Well Switching Power Supply - 5VDC, 18A

You'll also need a soldering iron and solder to assemble your power circuit:

Suggested Reading

If you aren't familiar with the Qwiic system, we recommend reading here for an overview.

SparkFun QwiicBus Hookup Guide Qwiic Connect System

We would also recommend taking a look at the following tutorials if you aren't familiar with the topics they cover.

  • Logic Levels: Learn the difference between 3.3V and 5V devices and logic levels.
  • Electric Power: An overview of electric power, the rate of energy transfer. We'll talk definition of power, watts, equations, and power ratings. 1.21 gigawatts of tutorial fun!
  • I2C: An introduction to I2C, one of the main embedded communications protocols in use today.
  • How to Work with Jumper Pads and PCB Traces: Handling PCB jumper pads and traces is an essential skill. Learn how to cut a PCB trace, add a solder jumper between pads to reroute connections, and repair a trace with the green wire method if a trace is damaged.

Hardware Overview

The simplicity of the QwiicBus is one of its biggest appeals as all you really need to get started is the QwiicBus boards, Ethernet and Qwiic cables and a controller (either development board or SBC). Other I2C communication methods require packetizing I2C communication into another protocol, be it RS-485 or 1-Wire. However, the PCA9615 keeps the I2C protocol by utilizing a differential transceiver. In this section, we'll take a closer look at the QwiicBus boards and the hardware present on them to better understand how they work.

PCA9615 Bus Buffer IC

Let's take a quick look at the PCA9615 IC at the heart of the MidPoint and EndPoint. The PCA9615 acts as a bridge that translates a standard two-wire I2C bus to a four-wire differential I2C bus. Translating to a differential bus helps prevent signal disruption in noisy environments as well as extending the signal over long-distance transmissions. For detailed information about the full functionality and feature set of the PCA9615 review the datasheet.

SparkFun QwiicBus Hookup Guide

SparkFun QwiicBus Hookup Guide

The PCA9615 has two supply voltage rails: VDDA and VDDB. VDDA acts primarily as the I2C-bus side power supply and VDDB primarily is used for the differential side power supply. While the two power supplies have slightly different operating ranges (VDDA supply voltage range: 2.3-5.5V. VDDB supply voltage range: 3.0-5.5V), both the EndPoint and MidPoint default to net both voltages together at 3.3V.

The PCA9615 supports I2C clock speeds up to 1MHz though the maximum cable length is inversely related to the clock speed. At max speed, the max rated cable length is listed at 3m but can be increased at lower clock speeds. For example, in our testing of the QwiicBus with over 200 feet of Ethernet cable we observed no significant signal loss while running at the standard clock speed for the Arduino Wire Library (100KHz).

We've designed the QwiicBus MidPoint and EndPoint to have multiple configuration options for powering your QwiicBus so there is a bit to take note of before powering everything up. We cover the different power configurations further down in the Solder Jumpers sub section as well as in the Hardware Assembly section so read on for more information.

The QwiicBus boards also break out the Enable (EN) pin to a PTH header if you would like to control the PCA9615 manually. By default, it is pulled to VDDA via an internal resistor. Refer to section 7.3 of the PCA9615 datasheet for more information on using this pin.

Finally, the PCA9615 requires terminating resistors on both ends of the bus to function properly. The EndPoint includes these resistors but as the MidPoint's name suggests, it is intended to only act as a node (middle point) and therefore does not have terminating resistors. As a result, controllers must be connected to the EndPoint and will not work properly when connected to the MidPoint.

Qwiic and I2C Interface

As a large portion of you readers have come to expect, the I2C pins are broken out to two Qwiic connectors so you can easily connect your QwiicBus boards to other Qwiic devices. We've also broken out the four I2C pins to standard 0.1"-spaced PTH header pins for users who prefer the standard plated through-hole connection.

SparkFun QwiicBus Hookup Guide

SparkFun QwiicBus Hookup Guide

Differential Output and RJ-45 Connectors

The EndPoint has a single RJ-45 to send the differential signal out to another EndPoint or to your MidPoint nodes. The MidPoint comes with two RJ-45 connectors so you can easily integrate it into your existing bus.

SparkFun QwiicBus Hookup Guide

SparkFun QwiicBus Hookup Guide

Depending on your project's power needs, the unused Green and Blue twisted pairs in the Ethernet cable can be used to send 5V over the Blue pair (Ethernet pins 4 and 5) or 3.8V to 36V over the Green pair (Ethernet pins 3 and 6). On the EndPoint, the Blue pair is broken out to PTH pins labeled VCC1 and GND and the Green pair is broken out to PTH pins labeled VCC2 and GND2.

We've also broken out the VCC2 and GND2 lines to a pair of PTH pins on the MidPoint if users would like to use them for powering peripherals or running the voltage over the QwiicBus chain on separate wires.

SparkFun QwiicBus Hookup Guide

SparkFun QwiicBus Hookup Guide

VCC1 is tied to both VDDA and VDDB on the PCA9615 so long as the 0-1 jumper is CLOSED (more on that in the following sections). VCC2 and GND2 are connected to the Ethernet Green pair intended for powering the buck regulator on any attached MidPoint(s). If users are powering the QwiicBus through either of these voltage inputs, the Bypass jumper on all MidPoints must be OPENED. Using the Green or Blue pair to provide voltage to the QwiicBus requires the proper power configuration covered in the Hardware Assembly section.

Lastly, you may notice the VCC2 and GND2 PTH pins on the EndPoint are labeled GRN and GRNW when viewed from the top. The Green pair can be used as an isolated signal line in the default (System @3.3V) and Alternate 1 (VCC@5V) configurations. Note, when using the Green pair in this way, make sure the GND2 jumper(s) on any attached MidPoints are opened and the PSEL jumper on any MidPoints are either completely OPEN (Default) or set to "1".

Buck Regulator - MidPoint Only

The MidPoint includes the LMR33630 Simple Switcher® variable buck regulator from Texas Instruments®. The regulator accepts an input voltage between 3.8V to 36V so you can send higher voltages over the Ethernet cable to render any voltage drop over long cables negligable and the 3A@3.3V output provides a larger current source for any devices attached to the MidPoint. The LMR33630 has a variable voltage output that the MidPoint design sets to 3.3V.

SparkFun QwiicBus Hookup Guide

The buck regulator is not powered by default, but the design features a dual jumper labeled PSEL users can adjust to enable the buck regulator to power the MidPoint(s) from a higher voltage (5V or 3.8V to 36V) via the Blue and Green pair pins broken out on the EndPoint and MidPoint. Read on to the Solder Jumpers sub-section below and the Hardware Assembly section for more information on how to use these alternate power configurations.

Note: While the buck regulator is rated for 3A, sourcing max current through the regulator continuously will cause it to heat up and decrease its efficiency. Running max current through the regulator for an extended period of time can also damage the IC and is not recommended.

Solder Jumpers

If you have never worked with solder jumpers and PCB traces before or would like a quick refresher, check out our How to Work with Solder Jumpers and PCB Traces tutorial for detailed instructions and tips.

In this section we'll cover the jumpers found on both QwiicBus boards and their functionality, default state and a few things to take note of prior to adjusting them.

Since this guide covers both QwiicBus boards (EndPoint and MidPoint) we'll denote which jumpers are found on both boards as well as board-specific jumpers. The EndPoint's five jumpers are labeled: I2C, PWR, VDDA, GND and 0-1. The six MidPoint jumpers are labeled: I2C, PWR, BP, PSEL, GND1 and GND2.

SparkFun QwiicBus Hookup Guide QwiicBus EndPoint Solder Jumpers - Top

SparkFun QwiicBus Hookup Guide QwiicBus EndPoint Solder Jumpers - Bottom

SparkFun QwiicBus Hookup Guide QwiicBus MidPoint Solder Jumpers - Top

SparkFun QwiicBus Hookup Guide QwiicBus MidPoint Solder Jumpers - Bottom

I2C Pull-Up Jumper - EndPoint and MidPoint

This jumper connects the SDA and SCL lines to VDDA of the PCA9615 (normally 3.3V) via a pair of 4.7kΩ resistors. The jumper's default state is CLOSED. To disable the pull-up resistors, open the jumper by severing the trace between the three pads.

Note: Each MidPoint will need its own set of pull-up resistors on the I2C side of the PCA9615. We recommend disabling any pull-up resistors on devices connected to the MidPoint's Qwiic connectors or the SDA/SCL pins since if multiple devices have their pull-up resistors enabled, the parallel equivalent resistance can create too strong of a pull-up for the bus to operate correctly.

Power (PWR) LED Jumper - EndPoint and MidPoint

This jumper connects the Power LED's cathode to 3.3V via a 1kΩ resistor. The jumper is CLOSED by default. Open the jumper by severing the trace between the two pads to disable the power LED on either QwiicBus board.

VDDA and GND Jumpers - EndPoint

The VDDA and GND jumpers connect VDDA (if the 0-1 jumper is closed) and Ground to the Blue twisted pair on the RJ-45 jacks and Ethernet cable. Their default state is CLOSED. If users do not need the Blue pair for a power input, these jumpers can be opened so that pair is available for other data lines or redundant power connections. Most users will want to leave these jumpers alone. If using the Blue pair as an independent signal, make sure the GND2 jumper on any MidPoints is OPEN.

0-1 Jumper - EndPoint

The 0-1 jumper nets VDDA and VDDB on the PCA9615 together. By default, this jumper is CLOSED to power both VDDA and VDDB with the same supply voltage (3.3V in the default power configuration). Open this jumper if using two separate voltages for VDDA (VCC) and VDDB (VCC1). If using separate voltages, make sure they fall within the voltage ranges for VDDA (2.3V-5.5V) and VDDB (3.0V-5.5V).

Heads Up! When using any of the alternate power configurations, the 0-1 jumper on the primary / first EndPoint should be OPEN but the 0-1 jumper on the terminating / last should be CLOSED to avoid leaving VDDB on the terminating EndPoint floating. Take note that with the 0-1 jumper CLOSED, 5V is sent to the Qwiic connectors and 3.3V PTH pin on the terminating EndPoint.

Bypass (BP) Jumper - MidPoint

The Bypass jumper (labeled BP on the board) nets VCC1 with the 3.3V rail on the MidPoint. By default, this jumper is CLOSED. When the QwiicBus system is powered at 3.3V, this jumper can remain closed but if the PSEL jumper is adjusted to use anything over 3.3V to power the QwiicBus, this jumper must be OPEN.

Power Select (PSEL) Jumper - MidPoint

This dual jumper selects which voltage supplies the input voltage for the MidPoint buck regulator. The Power Select jumper defaults to all open and the buck regulator is unpowered. In this default setting, power for each EndPoint is 3.3V and provided over the Blue pair of the Ethernet cable from the microcontroller/SBC or dedicated 3.3V power supply.

If using the 5V power configuration, this jumper should be closed to set it to the "1" side. When set to "1", the input voltage is still provided over the Blue pair of the Ethernet cable but at 5V.

If using the 3.8V-36V power configuration, close the jumper to set it to the "2" side. When set to "2", input voltage is provided over the Green pair of the Ethernet cable.

Important! If either alternate setting of the PSEL Jumper is used, the Bypass Jumper must be OPEN.

GND1 and GND2 Jumpers - MidPoint

The GND1 and GND2 jumpers net both input voltages to a common ground. Both jumpers are CLOSED by default. In advanced-use cases, users can open one or both of these jumpers to reduce noise and/or prevent ground loops on QwiicBus boards further down the chain. Most users will want to leave these jumpers alone.

Board Dimensions

The QwiicBus EndPoint PCB measures identically to the Differential I2C Breakout at 1.75in x 1.00in (44.45mm x 25.40mm). The MidPoint measures 1.80in x 1in (45.72mm x 25.40mm) and is flared to 1.10in (27.94mm) wide at the RJ-45 end. The RJ-45 connectors extend roughly 0.30in (7.62mm) from the edge of the PCB on both boards.

SparkFun QwiicBus Hookup Guide

SparkFun QwiicBus Hookup Guide

Hardware Assembly

In this section we'll go over configuring your QwiicBus EndPoint and MidPoint as how to assemble the QwiicBus circuit. Before we start connecting anything there are a couple of things to take note of.

Ethernet Cables

Make sure your Ethernet cables are straight-through (i.e., Pin 1 on one end of the cable is connected to Pin 1 on the other end) and not crossover. Most Ethernet cables sold are straight-through, so you probably have nothing to worry about here. If you're not sure what type of Ethernet cable you have, you can test for pin continuity with a digital multimeter.

Also take the voltage drop over the Ethernet cables into account. For longer chains or for circuits with many devices on multiple MidPoints, consider using one of the alternate power configurations so the voltage drop is negligible. The formula below can help you calculate the voltage drop at different lengths of CAT-6/Ethernet cable and whether or not you will need to consider one of the alternate power options:

SparkFun QwiicBus Hookup Guide

In this formula, I is the current through the object in Amperes and R is the resistance of the wires in Ohms. Most CAT-6/Ethernet cable will have 24AWG internal wires and depending on the quality of the cable will be either copper or aluminum. Refer to a table like this one from PowerStream to determine the resistance in Ω/1000ft or Ω/km to help calculate the approximate voltage drop.

I2C Pull-Up Resistors

Take time to note which devices you will have connected to your EndPoint and MidPoint's I2C bus side have their pull-up resistors enabled and what voltage they are tied to. Almost all Qwiic products have pull-up resistors enabled by default that pull the SDA/SCL lines connected directly to the I2C bus to 3.3V.

PCA9615 requires pull-up resistors on the two-wire I2C bus so each EndPoint and MidPoint must have at least one pair of pull-up resistors enabled on the two-wire side. The pull-up resistors do not translate through to the differential side of the PCA9615. To help make things a bit simpler, each QwiicBus EndPoint and MidPoint come with pull-up resistors on both SDA and SCL lines tied to VDDA. Normally, VDDA is 3.3V but can be as high as 5V on the EndPoint depending on the power configuration settings.

Note: If multiple devices are connected and you have a single device with pull-up resistors, make sure the voltage they are netted to is within the operating voltage range of all other I2C devices on the bus (normally 3.3V for Qwiic devices). If needed, you can shift the voltage to safe levels with a level shifter or voltage divider. If you're not familiar with logic levels and how to shift them, take a read through this tutorial.

Power Configuration Settings

As we mentioned in the Hardware Overview section of this guide, both QwiicBus boards feature a plethora of jumpers as well as two pairs of dedicated power PTH pins to configure how to power your QwiicBus circuit. Let's take a closer look at the three options available for powering the QwiicBus.

Important! When using alternate power configurations make sure to double check the jumpers on all EndPoints and MidPoints on your QwiicBus are set properly per the instructions below. Any QwiicBus boards or other Qwiic devices on your bus can be damaged if the circuit is assembled improperly.

Default - Entire System at 3.3V

In this configuration, the entire system is powered at 3.3V and the buck regulator(s) on the MidPoint(s) are unpowered. On the MidPoint(s), the Bypass jumper is CLOSED and both sides of the PSEL jumper are OPEN. 3.3V is provided either from your development board or single-board computer through the Qwiic connector or the 3.3V pin on the primary EndPoint.

Take note, in this configuration where all power is provided over the CAT-6/Ethernet cables, your total current draw will for attached devices will be limited to ~550mA with standard CAT-6/Ethernet cables due to the physical constraints of the wires inside. Anything beyond 550mA runs the risk of damaging the wires and can create a fire hazard.

The 3.3V supply voltage is then transferred from the initial EndPoint over the CAT-6/Ethernet cables in your QwiicBus system. Note that over long lengths of wire, you will see voltage drop and devices further down your QwiicBus chain may misbehave if the voltage drops below their operating range. Refer to the formula and links in the Ethernet Cables subsection above for calculating the voltage drop in your circuit.

Alternate 1 - VCC1 at 5V

While the default 3.3V configuration should work just fine for shorter QwiicBus chains, we found the PCA9615 functions better when powered with 5V. Powering VCC1 with 5V also allows us to also use the buck regulator on the MidPoint to source up to 3A@3.3V to devices connected to the MidPoint. Using this configuration requires adjusting both the EndPoint and MidPoint as well as multiple power supplies.

First and most importantly, the Bypass jumper on each MidPoint must be OPEN. On each MidPoint, adjust the PSEL jumper to the "1" side (see image below).

SparkFun QwiicBus Hookup Guide

It is also strongly recommended to OPEN the 0-1 jumper on the primary / first EndPoint to isolate VCC (VDDA) from VCC1 (VDDB) but leave the 0-1 jumper on the terminating EndPoint CLOSED. Leaving the 0-1 jumper closed will send 5V to any Qwiic devices attached to your terminating / last EndPoint.

SparkFun QwiicBus Hookup Guide

With the jumpers adjusted and your QwiicBus circuit assembled including any peripheral devices attached to your MidPoint(s), connect your 5V source to the VCC1 and GND PTH pins on the primary EndPoint. If the 0-1 jumper is opened, 3.3V should be provided over the Qwiic connectors or through the 3.3V PTH pin to power VCC (VDDA) on the primary EndPoint.

Alternate 2 - VCC2 at 3.8V to 36V

For this configuration, we use two separate voltages to power the EndPoints and MidPoint(s). First and most importantly, the Bypass jumper on each MidPoint must be OPEN. Adjust the PSEL jumper to the "2" position on each MidPoint.

SparkFun QwiicBus Hookup Guide

If you plan to power VCC1 with 5V it is recommended to OPEN the 0-1 jumper on the primary EndPoint to isolate VCC from VCC1. As covered above, we recommend leaving the 0-1 jumper CLOSED on the terminating EndPoint.

After adjusting the jumpers and assembling your QwiicBus circuit including any peripheral devices attached to your MidPoint(s), connect 3.8V to 36V to the VCC2 and GND2 PTH pins on the primary EndPoint. 3.3V for the first EndPoint should be provided from the microcontroller/SBC via the Qwiic connectors or a dedicated source through the 3.3V PTH pin.

Alternate 3 - VCC1 at 5V and VCC2 at 6V to 36V

This advanced configuration uses multiple power supply to allow for optimal performance of the QwiicBus over very long distances with multiple MidPoints. As mentioned above, we have found the QwiicBus operates best over long distances at 5V (particularly VDDB @5V). In this configuration, VCC1 is powered with 5V and VCC2 is powered with 6V-36V. Before connecting power supplies, a few jumpers must be adjusted.

First, the Bypass jumper on each MidPoint must be OPEN. Set the PSEL jumper on all MidPoints to the "2" position. The 0-1 jumper on the primary EndPoint is OPEN and the 0-1 jumper on the terminating EndPoint is CLOSED. This isolates VDDA and VDDB on the first EndPoint so the Qwiic connectors on the first EndPoint are at 3.3V. As we mentioned before, the Qwiic connectors and 3.3V PTH pin on the terminating EndPoint will be at 5V so be careful what is connected to that EndPoint.

After adjusting jumpers on all the QwiicBus boards and assembling the rest of your circuit (including connecting any Qwiic devices to MidPoints/EndPoints), connect the 5V power supply to the VCC1 and GND PTH pins and the power supply sourcing 6V to 36V to the VCC2 and GND2 PTH pins to the primary EndPoint.

Assembling the QwiicBus Circuit

Important! Make sure your QwiicBus circuit is not powered when adding or removing devices to your MidPoint(s) and EndPoint. Connecting and disconnecting devices while your QwiicBus is powered can cause voltage spikes and damage the PCA9615.

After taking into consideration how you intend to configure your QwiicBus circuit it's time to assemble it. Adjust the appropriate jumpers (if necessary), connect your controller (Arduino/SBC) to the primary EndPoint along with any Qwiic/I2C devices to the EndPoints and MidPoint(s) and connect the QwiicBus boards to each other with Ethernet cable plugged into the RJ-45 connectors on each board. Once the devices are all connected together, power up the circuit. The photo below shows the QwiicBus assembled in the default configuration (all boards powered with 3.3V) so your circuit may differ.

SparkFun QwiicBus Hookup Guide A completed QwiicBus Kit circuit using a SparkFun RedBoard Qwiic and operating at 3.3V

With everything adjusted and connected properly, that's all you need to assemble your QwiicBus circuit. Go forth and build ridiculously long, wired I2C circuits to your heart's content!

Troubleshooting

Here a few troubleshooting tips for the SparkFun QwiicBus.

I2C Communication

The PCA9615 supports I2C clock speeds up to 1MHz at short distances but as the cable length increases, high clock speeds can become more unreliable. If you find you are losing data or having unreliable communication on your QwiicBus, try reducing the clock speed as a quick software fix. Switching to one of the alternate power configurations can also help boost the reliability over long distances at high clock speeds.

Voltage Drop

Over long distances of cable the voltage may drop below the operating voltage range of the PCA9615 or attached devices. The formula below can help you calculate the voltage drop at different lengths of CAT-5/Ethernet cable and whether or not you will need to use one of the alternate power options:

SparkFun QwiicBus Hookup Guide

I is the current through the object in Amperes and R is the resistance of the wires in Ohms. Most CAT-5/Ethernet cable will have 24AWG internal wires and depending on the quality of the cable will be either copper or aluminum. Refer to a table like this one from PowerStream to determine the resistance in Ω/1000ft or Ω/km to help calculate the approximate voltage drop over your QwiicBus circuit.

Recommended Power-Up/Power-Down Procedure

Remember to power down the QwiicBus circuit before connecting or disconnecting any devices to the chain. Connecting or disconnecting devices to the QwiicBus can damage the PCA9615 on the QwiicBus boards if it is powered on.

Floating VDDB on the Terminating EndPoint

Reminder, when using any of the alternate power configurations, the 0-1 jumper on the primary / first EndPoint should be OPEN but the 0-1 jumper on the terminating / last should be CLOSED to avoid leaving VDDB on the terminating EndPoint floating. Take note that with the 0-1 jumper CLOSED, 5V is sent to the Qwiic connectors and 3.3V PTH pin on the terminating EndPoint.

Terminating Resistors

Related to the above tip, the QwiicBus only functions with controllers (Arduino/SBC/etc.) connected to the EndPoint. As the name may suggest, the EndPoint design includes the required terminating resistors to act as the ends of the QwiicBus. The MidPoint does not include these resistors since they are intended to be inserted in between the EndPoints as nodes.

General Troubleshooting

Need help?

If your product is not working as you expected or you need technical assistance or information, head on over to the SparkFun Technical Assistance page for some initial troubleshooting.

If you don't find what you need there, the SparkFun Forums are a great place to find and ask for help from our Tech Support team and community. If this is your first visit, you'll need to create a Forum Account to search product forums and post questions.

Resources and Going Further

Now that you have your QwiicBus set up and configured to your liking, it's time to start creating some I2C device networks! For more information, take a look at the following links:

QwiicBus EndPoint Links

QwiicBus MidPoint Links

メーカー品番 16988
SPARKFUN QWIICBUS - ENDPOINT
SparkFun Electronics
メーカー品番 COM-18000
SPARKFUN QWIICBUS - MIDPOINT
SparkFun Electronics
メーカー品番 17250
SPARKFUN QWIICBUS KIT
SparkFun Electronics
メーカー品番 15795
SPARKFUN QWIIC PRO MICRO - USB-C
SparkFun Electronics
メーカー品番 15663
SPARKFUN THING PLUS ESP32 WROOM
SparkFun Electronics
メーカー品番 15123
REDBOARD QWIIC ATMEGA328 EVAL BD
SparkFun Electronics
メーカー品番 15444
REDBOARD ARTEMIS
SparkFun Electronics
メーカー品番 SC0193(11)
SBC 1.5GHZ 4 CORE 2GB PI 4 MOD B
Raspberry Pi
メーカー品番 16386
RASPBERRY PI 4 DESKTOP KIT - 4GB
SparkFun Electronics
メーカー品番 14495
QWIIC ADAPTER
SparkFun Electronics
メーカー品番 15794
QWIIC SHIM FOR RASPBERRY PI
SparkFun Electronics
メーカー品番 15945
SPARKFUN QWIIC PHAT V2.0
SparkFun Electronics
メーカー品番 14352
QWIIC SHIELD FOR ARDUINO
SparkFun Electronics
メーカー品番 14427
QWIIC CABLE - 100MM
SparkFun Electronics
メーカー品番 17257
FLEXIBLE QWIIC CABLE - 500MM
SparkFun Electronics
メーカー品番 14456
SOLDERING IRON - 60W (ADJUSTABLE
SparkFun Electronics
メーカー品番 09325
SOLDER LEAD FREE - 100-GRAM SPOO
SparkFun Electronics
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.