Maker.io main logo

PyBadger Event Badge

67

2024-06-04 | By Adafruit Industries

License: See Original Project

Courtesy of Adafruit

Guide by Kattni Rembor

Overview

 

Download PyBadge FeatherWing Snapfit Case

hello_1

You're headed to the next big conference or event. They'll likely ‎provide a badge with your name on it, but what if you could have ‎something better?‎

That's where PyBadger and PyBadge (or PyGamer or CLUE) come in! ‎Use CircuitPython to easily create an interactive conference or event ‎badge. You can display a "Hello My Name Is"-style badge that you ‎can quickly add your name to or customise it entirely. You can ‎generate and display a custom QR code to direct people to your ‎website. You can also display a "business card" with an image, such ‎as your face or company logo, and a string of text, such as your email ‎address.‎

PyBadger also gives you access to the other features on the board, ‎such as the buttons, NeoPixels, light sensor, and accelerometer. You ‎can easily add all kinds of features to your badge if you choose to.‎

CircuitPython's own Blinka is headed to the next Circuit Playground ‎conference and wants to have the coolest badge there. This guide ‎will walk you through Blinka creating an interactive conference ‎badge. Follow along and customise it to fit your needs!‎

badge_2

All you need to follow along is a PyBadge, battery and lanyard, we ‎have a few options for each, so you can deck out in the fanciest style, ‎or go for an affordable-yet-stylish look.‎

Prepare Your Badge

pybadge_3

Adafruit CircuitPython PyBadger makes it easy to create an ‎interactive conference or event badge with PyBadge or PyGamer. ‎Blinka is headed to a fun conference and is excited to create a ‎badge. Let's take a look!

Download PyBadger

Adafruit CircuitPython PyBadger requires the latest CircuitPython ‎and a number of libraries to work.‎

To download CircuitPython, visit the following link for CLUE, ‎PyBadge or PyGamer, depending on what you're using, and ‎download the latest CircuitPython version for your board.‎

Download CircuitPython for CLUE from circuitpython.org

Download CircuitPython for PyBadge from circuitpython.org

Download CircuitPython for PyGamer from circuitpython.org

Next visit the following link and download the library bundle that ‎matches your CircuitPython version.‎

Download the CircuitPython Library Bundle from circuitpython.org

PyBadger requires the following libraries to work. Download the ‎library bundle and unzip the file. Open the folder, find the lib folder ‎within, and open the lib folder. Copy the following folders and files to ‎the lib folder on your CIRCUITPY drive:‎

  • adafruit_bitmap_font
  • adafruit_bus_device
  • adafruit_display_shapes
  • adafruit_display_text
  • adafruit_miniqr.mpy
  • adafruit_pybadger
  • neopixel.mpy

If you are using PyBadge or PyGamer, copy the following library:‎

  • adafruit_lis3dh.mpy

If you are using CLUE, copy the following library:‎

  • adafruit_lsm6ds.mpy
  • adafruit_register

Once you have the listed files and folders copied to the lib folder on ‎your CIRCUITPY drive, you're ready to go!‎

Using PyBadger

Using PyBadger

Using the PyBadger library is easy. Simply import the library.‎

Download File

Copy Code
from adafruit_pybadger import pybadger

Now you have access to all the features PyBadger has to offer, ‎including badge, business card, and QR code creation.‎

Hello My Name Is...‎

First, we'll create a "Hello My Name Is" style badge to display initially.‎

Download File

Copy Code
pybadger.show_badge(name_string="Blinka", hello_scale=2, my_name_is_scale=2, name_scale=3)

nameis_4

To change the badge to display your name, set name_string="Your ‎Name" when you create the badge object.‎

Each of the scales applies to a different line on the badge, ‎e.g., hello_scale applies to the HELLO string on the badge. When using ‎the default font, the above values for hello_scale and my_name_is_scale are ideal. Depending on the length of ‎your name, you'll want to tweak name_scale to allow it to fit properly.‎

Auto-Dim the Display

The display is the part of the badge that uses up the most battery. To ‎help mitigate that, PyBadger includes the ability to auto-dim the ‎display if the badge isn't moving. If you set it down somewhere, it'll ‎use less battery.‎

Download File‎

Copy Code
while True:
pybadger.auto_dim_display()

dim_5

It defaults to dimming after 5 seconds and brightening up again on a ‎fairly small movement threshold of 1.5. If you would like to change ‎either of those, you can do so when adding ‎the auto_dim_display() function to your code. For example, to change it to ‎wait 10 seconds before dimming, and require more movement to ‎brighten up again, you would add the following:‎

Download File

Copy Code
    pybadger.auto_dim_display(delay=10, movement_threshold=20)

The higher the movement_threshold, the more movement it takes to cause ‎the display to return to full brightness.‎

Business Card

Everyone exchanges business cards at conferences. But it means ‎carrying extra things around and trying to remember who gave you ‎the card in the first place. Not anymore! Now you can display a ‎simple business card with your picture, name, and email address. ‎Someone can snap a quick picture of it and have your face and info ‎available for later.‎

Blinka wants to display her name, email and image when pressing ‎button A.‎

Download File

Copy Code
    if pybadger.button.a:
pybadger.show_business_card(image_name="Blinka.bmp", name_string="Blinka", name_scale=2,
email_string_one="blinka@", email_string_two="adafruit.com")

card_6

The show_business_card function requires you to provide a bitmap image ‎name as a string. You can optionally add your name as a string, and ‎up to two lines of an email address (or any other info you'd like to ‎provide!).‎

The badge will continue to display the business card until you tell it ‎to display something else by pressing another button.‎

Images must be in 16-bit or 24-bit BMP format, and ideally 160x128 ‎pixels. Here's the blinka.bmp file if you need to see what the format ‎is:‎

blinkabmp_7

QR Code

Blinka wants to direct other conference attendees to her website. ‎She can easily do that by generating a QR code and having it display ‎when pressing button B.‎

Download File

Copy Code
    elif pybadger.button.b:
pybadger.show_qr_code(data="https://circuitpython.org")

code_8

The show_qr_code function allows you to set its target by setting data= a ‎string with the target info in it. For example, Blinka wants to point to ‎circuitpython.org and so she sets data="https://circuitpython.org".‎

The badge will continue to display the QR code until you tell it to ‎display something else by pressing another button.‎

Return to Hello My Name Is...‎

Blinka needs a way to display the Hello My Name Is part of the ‎badge again after showing off her business card and QR code. So, ‎the last thing included is assigning the start button to display it.‎

Download File

Copy Code
    elif pybadger.button.start:
pybadger.show_badge(name_string="Blinka", hello_scale=2, my_name_is_scale=2, name_scale=3)

return_9

That's all there is to creating a fun, interactive conference or event ‎badge!‎

Full Example Code

Download Project Bundle

Copy Code
# SPDX-FileCopyrightText: 2021 ladyada for Adafruit Industries
# SPDX-License-Identifier: MIT

from adafruit_pybadger import pybadger

pybadger.show_badge(
name_string="Blinka", hello_scale=2, my_name_is_scale=2, name_scale=3
)

while True:
pybadger.auto_dim_display(
delay=10
) # Remove or comment out this line if you have the PyBadge LC
if pybadger.button.a:
pybadger.show_business_card(
image_name="Blinka.bmp",
name_string="Blinka",
name_scale=2,
email_string_one="blinka@",
email_string_two="adafruit.com",
)
elif pybadger.button.b:
pybadger.show_qr_code(data="https://circuitpython.org")
elif pybadger.button.start:
pybadger.show_badge(
name_string="Blinka", hello_scale=2, my_name_is_scale=2, name_scale=3
)

View on GitHub

メーカー品番 4200
ADAFRUIT PYBADGE FEATHER
Adafruit Industries LLC
メーカー品番 3939
ADAFRUIT PYBADGE LC (LOW COST)
Adafruit Industries LLC
メーカー品番 3987
CIRCUIT PLAYGROUND LANYARD
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.