Maker.io main logo

CircuitPython BLE Advertising Beacons

98

2024-02-21 | By Adafruit Industries

License: See Original Project Bluetooth / BLE

Courtesy of Adafruit

Guide by John Park

Overview

Mmmmm, bacon.....‎

What?‎

Oh. Beacons? Yes, beacons!‎

bacon_1

Beacons are low power, low-cost Bluetooth LE devices that can be ‎used for a very simple job: to advertise a URL to users running an ‎app on their mobile device within range of the device!‎

Technically, beacons can also be used for a few different scenarios ‎where a localized, wireless data broadcast is desirable, such as ‎indoor location tracking, point of sales/marketing, and experience ‎personalization.‎

We'll create two version -- first, a simple beacon that can run on any ‎CircuitPython capable nRF52840 board. Second, a custom version for ‎the CLUE board that also shows QR codes and allows you to scroll ‎among multiple beacon URL choices to advertise!‎

Parts

All you need to advertise your own BLE beacons is any Adafruit ‎Bluefruit nRF52840 board:‎

You'll also want a USB cable for programming it and power, or you ‎can use a LiPoly battery for remote powering.‎

Additionally, you'll need a mobile device running an Eddystone ‎beacon discovery app, such as Physical Web:‎

Understanding BLE Advertising ‎Beacons

beacon_2

Bluetooth LC beacons are low power devices that are used to ‎broadcast a tiny amount of data to any device that's listening. This ‎often takes the form of a mobile device running an app, such as ‎Physical Web, which can read the beacon's advertising broadcast ‎and display a URL the user can then visit.‎

There are two primary BLE beacon standards: Apple's iBeacon, and ‎Google's Eddystone. In this guide, we'll use the Eddystone standard ‎to create a beacon that advertises a website URL (which you can ‎customize to any URL you like.)‎

Advertising

When an Eddystone beacon is running, it transmits a packet of ‎information that includes a Unique Identifier (UID), and another ‎packet of information that includes a website URL.‎

Note, this data is transmitted with no need for connecting, pairing, or ‎bonding with a mobile device. The beacon is pretty much just always ‎sitting there yelling, "Hey! I'm a beacon! This is my name, and this is ‎a URL I think you should visit!"‎

Other Uses

This guide focuses solely on using beacons to advertise a URL, ‎however there are a few other common uses for beacons. These ‎include indoor navigation, tracking (such as lost key finders like Tile), ‎and interaction notifications, such as interactive museum tours.‎

Simple Advertising Beacons

simple_3

CircuitPython Setup

For our simple beacon example, we'll use the ItsyBitsy nRF52840. ‎We'll show you how to set it up with the proper libraries and code to ‎use on the Itsy, but you can apply these instructions to the Feather ‎nRF52840, Circuit Playground Bluefruit, or CLUE boards as well by ‎downloading the appropriate version of CircuitPython for those ‎boards.‎

CircuitPython for ItsyBitsy nRF52840 ‎Express

CircuitPython is a derivative of MicroPython designed to simplify ‎experimentation and education on low-cost microcontrollers. It ‎makes it easier than ever to get prototyping by requiring no upfront ‎desktop software downloads. Simply copy and edit files on ‎the CIRCUITPY drive to iterate.‎

Set up CircuitPython Quick Start!

Follow this quick step-by-step for super-fast Python power :)‎

Download the latest version of CircuitPython for this board via ‎CircuitPython.org

Further Information

For more detailed info on installing CircuitPython, check ‎out Installing CircuitPython.‎

Click the link above and download the latest UF2 file.‎

Download and save it to your desktop (or wherever is handy).‎

download_4

Plug your Itsy nRF52840 into your computer using a known-good ‎USB cable.‎

A lot of people end up using charge-only USB cables and it is very ‎frustrating! So, make sure you have a USB cable you know is good ‎for data sync.‎

In the image, the Reset button is indicated by the magenta arrow, ‎and the BTLE status LED is indicated by the green arrow.‎

Double-click the Reset button on your board (magenta arrow), and ‎you will see the BTLE LED (green arrow) will pulse quickly then ‎slowly blue. If the DotStar LED turns red, check the USB cable, try ‎another USB port, etc.‎

If double-clicking doesn't work the first time, try again. Sometimes it ‎can take a few tries to get the rhythm right!‎

plug_5

You will see a new disk drive appear called ITSY840BOOT.‎

Drag the adafruit_circuitpython_etc.uf2 file to ITSY840BOOT.‎

drag_6

drag_7

The LED will flash. Then, the ITSY840BOOT drive will disappear, and ‎a new disk drive called CIRCUITPY will appear.‎

That's it, you're done! :)‎

done_8

Simple Beacon Code in CircuitPython

Text Editor

Adafruit recommends using the Mu editor for using your ‎CircuitPython code with Adafruit boards. You can get more info ‎in this guide.‎

Alternatively, you can use any text editor that saves files.‎

CircuitPython Libraries & Code.py

To use with CircuitPython, you need to first install a few libraries, into ‎the lib folder on your CIRCUITPY drive. Then you need to ‎update code.py with the example script.‎

Thankfully, we can do this in one go. In the example below, click ‎the Download Project Bundle button below to download the ‎necessary libraries and the code.py file in a zip file. Extract the ‎contents of the zip file, open the directory examples/ and then click ‎on the directory that matches the version of CircuitPython you're ‎using and copy the contents of that directory to ‎your CIRCUITPY drive.‎

Your CIRCUITPY drive should now look similar to the following ‎image:‎

drive_9

Download Project Bundle

Copy Code
# SPDX-FileCopyrightText: 2021 ladyada for Adafruit Industries
# SPDX-License-Identifier: MIT

"""This example broadcasts our Mac Address as our Eddystone ID and a link to the Adafruit Discord
server."""

import time

import adafruit_ble
from adafruit_ble_eddystone import uid, url

radio = adafruit_ble.BLERadio()

# Reuse the BLE address as our Eddystone instance id.
eddystone_uid = uid.EddystoneUID(radio.address_bytes)
eddystone_url = url.EddystoneURL("https://adafru.it/discord")

while True:
# Alternate between advertising our ID and our URL.
radio.start_advertising(eddystone_uid)
time.sleep(0.5)
radio.stop_advertising()

radio.start_advertising(eddystone_url)
time.sleep(0.5)
radio.stop_advertising()

time.sleep(4)

View on GitHub

Code Explainer

Libraries

Here's how this code works. First, we import ‎the time and adafruit_ble libraries.‎

Then, we import uid and url from the adafruit_ble_eddystone library. These ‎two give us the capability to advertise a unique identifier (UID) and a ‎website URL.‎

Download File

Copy Code
import time

import adafruit_ble
from adafruit_ble_eddystone import uid, url

Radio & Eddystone Setup

Next, we'll create an instance of the BLERadio() and then create a ‎variable for the eddystone_uid. This is the unique ID that is used to ‎differentiate beacons when multiple of them are present. We can re-‎use the BLE radio.address_bytes as our UID.‎

We'll also create a variable for the website URL we want to be ‎advertised from our beacon, eddystone_url.‎

In this case, we are using https://adafru.it/discord as the beacon ‎URL, but you can swap in a URL of your choosing. Just be careful it ‎isn't too long -- anything under 18 characters will work, otherwise ‎you can use a URL shortener service, such as bit.ly.‎

Download File

Copy Code
radio = adafruit_ble.BLERadio()

# Reuse the BLE address as our Eddystone instance id.
eddystone_uid = uid.EddystoneUID(radio.address_bytes)
eddystone_url = url.EddystoneURL("https://adafru.it/discord")

You may get away with a longer URL than you think you should -- ‎this is because for certain common URL prefixes ('https://www.' for ‎example) and domains ('.com', '.org', etc.) we substitute them for a ‎single non-printing byte.‎

Advertising

With setup complete, the main, ever-repeating loop of the code now ‎takes over. Here, we alternate between advertising the beacon's UID ‎and the beacon's URL, pause for four seconds, and repeat.‎

Download File

Copy Code
while True:
# Alternate between advertising our ID and our URL.
radio.start_advertising(eddystone_uid)
time.sleep(0.5)
radio.stop_advertising()

radio.start_advertising(eddystone_url)
time.sleep(0.5)
radio.stop_advertising()

time.sleep(4)

Usage

To use it, simply power up the beacon and then launch your Physical ‎Web app (or another beacon-aware app) on your mobile device. ‎You'll see the app scan for beacons.‎

When the beacon is found, you will see some info about it, including ‎a clickable link to take you to the advertised URL.‎

Any icons and descriptive text are scraped from the website itself, ‎and not part of the data delivered by the beacon.‎

usage_10

That's all there is to it! Next, we'll create a more sophisticated version ‎on the CLUE.‎

CLUE Beacon

clue_11

First, set up CircuitPython on the CLUE following the instructions on ‎this page.‎

Libraries

Next, install the libraries needed. This guide page will show you ‎where to download them.‎

You'll need the following libraries for this project:

  • adafruit_bitmap_font
  • adafruit_ble
  • adafruit_ble_eddystone
  • adafruit_bus_device
  • adafruit_display_shapes
  • adafruit_display_text
  • adafruit_pybadger
  • adafruit_register
  • adafruit_lis3mdl.mpy
  • adafruit_lsm6ds.mpy
  • adafruit_miniqr.mpy
  • neopixel.mpy

Clue Libraries

Text Editor

Adafruit recommends using the Mu editor for using your ‎CircuitPython code with the Feather boards. You can get more info ‎in this guide.‎

Alternatively, you can use any text editor that saves files.‎

Image Files and Code.py

This project uses a couple of .bmp image files -- you can get them by ‎downloading the Project Zip link in the embed below. Unzip the ‎downloaded zip archive and then drag the two image files to your ‎CLUE board's CIRCIUTPY drive.‎

Copy the code shown below, paste it into Mu. Save the code from Mu ‎to the CLUE's CIRCUITPY drive as code.py.‎

Download Project Bundle

Copy Code
# SPDX-FileCopyrightText: 2020 John Park for Adafruit Industries
#
# SPDX-License-Identifier: MIT

"""
Eddystone Beacon for CLUE
This example broadcasts our Mac Address as our Eddystone ID and a link to a URL of your choice.
Hold the A button to display QR code, use B button to pick URL from the list.
"""

import time
from adafruit_pybadger import pybadger
import adafruit_ble
from adafruit_ble_eddystone import uid, url

radio = adafruit_ble.BLERadio()

# Reuse the BLE address as our Eddystone instance id.
eddystone_uid = uid.EddystoneUID(radio.address_bytes)

# List of URLs to broadcast here:
ad_url = [("https://circuitpython.org", "CirPy"),
("https://adafru.it/discord","DISCORD"),
("https://forums.adafruit.com", "Forums"),
("https://learn.adafruit.com", "Learn")
]
pick = 0 # use to increment url choices

pybadger.play_tone(1600, 0.25)
pybadger.show_business_card(image_name="cluebeacon.bmp")

while True:
pybadger.auto_dim_display(delay=3, movement_threshold=4)
eddystone_url = url.EddystoneURL(ad_url[pick][0])

if pybadger.button.a and not pybadger.button.b: # Press button A to show QR code
pybadger.play_tone(1200, 0.1)
pybadger.brightness = 1
pybadger.show_qr_code(data=ad_url[pick][0]) # Tests QR code
time.sleep(0.1) # Debounce

elif pybadger.button.b and not pybadger.button.a: # iterate through urls to broadcast
pybadger.play_tone(1600, 0.2)
pick = (pick + 1) % len(ad_url)
pybadger.brightness = 1
pybadger.show_business_card(image_name="bg.bmp", name_string=ad_url[pick][1], name_scale=5,
email_string_one="", email_string_two=ad_url[pick][0])
time.sleep(0.1)

elif pybadger.button.a and pybadger.button.b:
pybadger.play_tone(1000, 0.2)
pybadger.brightness = 1
pybadger.show_business_card(image_name="cluebeacon.bmp")
time.sleep(0.1)

# Alternate between advertising our ID and our URL.
radio.start_advertising(eddystone_uid)
time.sleep(0.5)
radio.stop_advertising()

radio.start_advertising(eddystone_url)
time.sleep(0.5)
radio.stop_advertising()

time.sleep(1)

View on GitHub

projects_cluebacon

How It Works

Like the simple example before, we will import libraries for time, ble, ‎and eddystone support. We will also import the adafruit_pybadger library ‎which makes it convenient to use the buttons, speaker, and screen ‎on the CLUE.‎

Download File

Copy Code
import time
from adafruit_pybadger import pybadger
import adafruit_ble
from adafruit_ble_eddystone import uid, url

Setup

We'll set up the radio and eddystone_uid as before, but this time instead of ‎a single URL, we'll create a list of few to pick through.‎

This is a list of tuples, which each entry containing both a URL and a ‎‎"nice name".‎

The pick variable will be used to select a URL from the list when the B ‎button is pressed.‎

Download File

Copy Code
radio = adafruit_ble.BLERadio()

# Reuse the BLE address as our Eddystone instance id.
eddystone_uid = uid.EddystoneUID(radio.address_bytes)

# List of URLs to broadcast here:
ad_url = [("https://circuitpython.org", "CirPy"),
("https://adafru.it/discord","DISCORD"),
("https://forums.adafruit.com", "Forums"),
("https://learn.adafruit.com", "Learn")
]
pick = 0 # use to increment url choices

We'll use the pybadger.play_tone() command to beep the on-board ‎speaker, and the pybadger.show_business_card() command to display a .bmp ‎image.‎

Download File

Copy Code
pybadger.play_tone(1600, 0.25)
pybadger.show_business_card(image_name="cluebeacon.bmp")

Main Loop

In the main loop of the program, we will set the display to auto dim ‎after three seconds and set the movement threshold so you can ‎shake it a little to wake up the CLUE and undim it.‎

The eddystone_url is set to the first one in the list.‎

Download File

Copy Code
pybadger.auto_dim_display(delay=3, movement_threshold=4)
eddystone_url = url.EddystoneURL(ad_url[pick][0])

Buttons

When the A button is pressed by itself, ‎the pybadger.show_qr_code() command is run, displaying the automatically ‎generated QR code image for the currently selected URL.‎

Download File

Copy Code
if pybadger.button.a and not pybadger.button.b:  # Press button A to show QR code
pybadger.play_tone(1200, 0.1)
pybadger.brightness = 1
pybadger.show_qr_code(data=ad_url[pick][0]) # Tests QR code
time.sleep(0.1) # Debounce

When the B button is pressed, the next URL in the list is selected, ‎and this info is displayed on the screen using ‎the pybadger.show_business_card() command.‎

Download File

Copy Code
elif pybadger.button.b and not pybadger.button.a:  # iterate through urls to broadcast
pybadger.play_tone(1600, 0.2)
pick = (pick + 1) % len(ad_url)
pybadger.brightness = 1
pybadger.show_business_card(image_name="bg.bmp", name_string=ad_url[pick][1], name_scale=5,
email_string_one="", email_string_two=ad_url[pick][0])
time.sleep(0.1)

When both A and B buttons are pressed at the same time, the ‎display returns to the initial screen image.‎

Download File

Copy Code
elif pybadger.button.a and pybadger.button.b:
pybadger.play_tone(1000, 0.2)
pybadger.brightness = 1
pybadger.show_business_card(image_name="cluebeacon.bmp")
time.sleep(0.1)

Beacon Advertising

Finally, we have the beacon advertising code, just as with the simple ‎example. The beacon UID is advertised, then the URL is, and this ‎repeats every second.‎

Download File

Copy Code
# Alternate between advertising our ID and our URL.
radio.start_advertising(eddystone_uid)
time.sleep(0.5)
radio.stop_advertising()

radio.start_advertising(eddystone_url)
time.sleep(0.5)
radio.stop_advertising()

time.sleep(1)

CLUE Beacon Usage

Power up the CLUE and you'll see the welcome screen.‎

clue_12

Pick Beacon Advertisement

Press the B button to pick a URL from your list. There is a small beep ‎when the button press is recognized -- you may need to hold it for a ‎second first.‎

clue_13

The current beacon name and URL will be displayed.‎

clue_14

QR Code

Press the A button to go to QR code mode. This is great for any users ‎without a BLE beacon app who want to use their camera to scan the ‎URL instead.‎

code_15

Here is the auto generated QR code. All made in CircuitPython!‎

code_16

You can press the B button to switch to the other URLs which will ‎change the beacon advertisements almost instantly.‎

NOTE: Depending on the beacon app you're running, you may need ‎to refresh or delete the beacon cache in order to see the changed ‎advertisement URL show up.‎

switch_17

メーカー品番 4481
ITSYBITSY NRF52840 EXPRESS BLE
Adafruit Industries LLC
メーカー品番 4500
CLUE NRF52840 EXPRESS
Adafruit Industries LLC
メーカー品番 4062
ADAFRUIT FEATHER NRF52840 EXPRES
Adafruit Industries LLC
メーカー品番 4333
CIRCUIT PLAYGROUND BLUEFRUIT BLE
Adafruit Industries LLC
メーカー品番 592
CABLE A PLUG TO MCR B PLUG 3'
Adafruit Industries LLC
メーカー品番 1865
EDGE-LAUNCH SMA CONNECTOR FOR 1.
Adafruit Industries LLC
メーカー品番 1443
16MM ILLUMINATED PUSHBUTTON - GR
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.