Maker.io main logo

MicroMod ESP32 Processor Board Hookup Guide

111

2024-08-06 | By SparkFun Electronics

License: See Original Project Wifi Wireless ESP32 MicroMod Qwiic

Courtesy of SparkFun

Guide by ALEX THE GIANT, ELL C

Introduction

Introducing the SparkFun MicroMod ESP32 Processor Board! This bad boy pops an M.2 connector ‎onto the ESP32 so you can take advantage of all that lovely ESP32 power with any of our MicroMod ‎carrier boards. Grab yourself an ESP32 MicroMod Processor Board and let's dive in!‎

 

Required Materials

In addition to your ESP32 Processor Board, you'll need a carrier board to get started. Here we use ‎the Input and Display Carrier Board, but there are a number of others you can choose from.‎

You'll also need a USB-C cable to connect the Carrier to your computer and if you want to add ‎some Qwiic breakouts to your MicroMod project you'll want at least one Qwiic cable to connect it all ‎together. Below are some options for both of those cables:‎

Depending on which Carrier Board you choose, you may need a few extra peripherals to take full ‎advantage of them. Refer to the Carrier Boards' respective Hookup Guides for specific peripheral ‎recommendations.‎

Suggested Reading

The SparkFun MicroMod ecosystem is a unique way to allow users to customize their project to ‎their needs. Do you want to send your weather data via a wireless signal? There's a MicroMod ‎processor for that. Looking to instead maximize efficiency and processing power? You guessed it, ‎there's a MicroMod processor for that. If you are not familiar with the MicroMod system, take a look ‎here:‎

micromod_1

MicroMod Ecosystem

We recommend taking a look through the following tutorials if you are not familiar with the concepts ‎covered in them:‎

Hardware Overview

In this section we'll cover what's included on the MicroMod ESP32 Processor Board.‎

M.2 Connector

All of our MicroMod Processor boards come equipped with the M.2 MicroMod Connector, which ‎leverages the M.2 standard and specification to allow you to install your MicroMod Processor board ‎on your choice of carrier board.‎

front_2

M2 Connector from the Front

back_3

M2 Connector from the Back

Espressif ESP32

Ahhh, the Espressif ESP32. It's one of the most unique microcontrollers on the market. In its native ‎form, it has a laundry list of features. On the MicroMod Processor Board, we include the following:‎

  • Dual-core Tensilica LX6 microprocessor
  • Up to 240MHz clock frequency
  • ‎520kB internal SRAM
  • Integrated 802.11 B/G/N WiFi transceiver
  • ‎2.7 to 3.6V operating range‎
  • ‎500µA sleep current under hibernation
  • ‎10-electrode capacitive touch support
  • Hardware accelerated encryption (AES, SHA2, ECC, RSA-4096)‎
  • ‎16MB Flash Storage‎

espressif_4

Stat LED

stat_5

Wireless Antenna

Need wireless? The Espressif chip provides a WiFi transceiver which sends and receives data ‎through a 2.4GHz Antenna.‎

chip_6

PinOut Notes

The ESP32 MicroMod has a few quirks. The ESP32's GPIO pins provide a lot of flexibility with what ‎each pin can be used for. Whether it's I2C, I2S, SPI, UART, or PWM, the ESP32 MicroMod can do ‎just about everything! However, with that flexibility and a fixed number of GPIO pins, the ESP32 ‎isn't able to do it all at the same time. Below is a list of protocols the ESP32 supports, but pay close ‎attention to the pins used, because some pins are assigned to two or possibly three functions.‎

Strapping Pins

One of the unique aspects of the ESP32 is the strapping pins. When the ESP32 comes out of reset, ‎or as power is supplied, there are a few pins which control the behavior of the board. For a detailed ‎description of these pins, check out the ESP32 Boot Mode Selection page on Espressif‎'s GitHub ‎page. As a summary the strapping pins are:‎

GPIO 0

Having GPIO 0 pulled low as the ESP32 comes out of reset will enter the serial bootloader. ‎Otherwise, the board will run the program stored in flash. On the MicroMod Processor, this pin is ‎pulled high externally through a 10k resistor and is connected to the boot button on the carrier ‎boards, which can pull the pin low.‎

GPIO 2‎

Having GPIO 2 pulled high as the ESP32 comes out of reset will prevent the board from entering ‎the serial bootloader. On the MicroMod Processor, this pin is connected to the status LED (active ‎high) and does not interfere with the board from being able to enter the serial bootloader.‎

GPIO 12‎

If driven high, the flash voltage (VDD_SDIO) is set to 1.8V. If unconnected or pulled low, ‎VDD_SDIO is set to 3.3V. The flash IC used on the MicroMod Processor has a minimum voltage ‎of 2.7V, which would create a brownout condition and might corrupt the data stored to the flash, or ‎simply prevent the program from running. On the ESP32 MicroMod Processor, this pin is ‎connected to PWM1.‎

GPIO 15‎

If driven low, the boot messages printed by the ROM bootloader (at 115200 baud) are silenced. If ‎unconnected or driven high, the messages will be printed as they normally are. On the ESP32 ‎MicroMod Processor, this pin is connected to G0.‎

I2C

We love us some I2C! We've broken out two I2C buses, which can be used with our Qwiic system. ‎The main I2C bus has dedicated GPIO pins 21/22 connected to MicroMod pads 12/14, along with a ‎dedicated interrupt pin connected to GPIO pin 4, which is connected to pad 16 of the MicroMod ‎connector.‎

If you need a second I2C bus, the ESP32 uses GPIO pins 25/26 (pads 42/44 on the MicroMod) for ‎SCL1 and SDA1.‎

Note: The secondary I2C bus is shared with G1 and G2, as well as the I2S bus pins for ‎AUD_LRCLK and AUD_BCLK.‎

UART

The ESP32 Processor has two UARTs available. The primary UART has dedicated GPIO pins 1 and ‎‎3 which can be used for programming as well as printing debug messages to a terminal window. ‎These GPIO pins aren't directly broken out, but instead are converted to USB which is connected ‎to MicroMod pads 3 and 5.‎

The second UART is connected GPIO pins 16 and 17 (pads 19 and 17 on the MicroMod) for RX1 ‎and TX1.‎

Note: The secondary UART is shared with G3 and G4, as well as the I2S bus pins for AUD_OUT, ‎and AUD_IN.‎

GPIO/BUS

The MicroMod connector supports a total of 12 general purpose IO pins, 7 of which are used on ‎the ESP32 Processor, on top of the 6 dedicated pins. The dedicated pins are just that, and are not ‎shared with any other pin, unlike the general-purpose pins which may be shared with other pins. ‎The pins used are:‎

Dedicated Pins

  • A0 - GPIO pin 34, pad 34 on the MicroMod (Input Only!)‎
  • A1 - GPIO pin 35, pad 38 on the MicroMod (Input Only!)
  • D0 - GPIO pin 14, pad 10 on the MicroMod
  • D1 - GPIO pin 27, pad 18 on the MicroMod
  • PWM0 - GPIO pin 13, pad 32 on the MicroMod
  • PWM1 - GPIO pin 12, pad 47 on the MicroMod

General Purpose IO pins

  • G0 - GPIO pin 15, pad 40 on the MicroMod
  • G1 - GPIO pin 25, pad 42 on the MicroMod - Shared with the I2S bus, and secondary I2C bus
  • G2 - GPIO pin 26, pad 44 on the MicroMod - Shared with the I2S bus, and secondary I2C bus
  • G3 - GPIO pin 17, pad 46 on the MicroMod - Shared with the I2S bus, and secondary UART
  • G4 - GPIO pin 16, pad 48 on the MicroMod - Shared with the I2S bus, and secondary UART
  • G5 - GPIO pin 32, pad 73 on the MicroMod - Shared with the 32KHz RTC crystal
  • G6 - GPIO pin 33, pad 71 on the MicroMod - Shared with the 32KHz RTC crystal.‎

AUDIO

The ESP32 Processor supports audio using the I2S standard. The pins used are:‎

  • AUD_OUT - GPIO pin 17, pad 56 on the MicroMod, this is the digital audio output
  • AUD_IN - GPIO pin 16, pad 54 on the MicroMod, this is the digital audio input
  • AUD_LRCLK - GPIO pin 25, pad 52 on the MicroMod. Officially called "word select", and also ‎known as "frame sync"
  • AUD_BCLK - GPIO pin 26, pad 50 on the MicroMod. Officially called "continuous serial clock, ‎and also known as the "bit clock"‎

Note: The I2S bus is shared with the secondary UART, secondary I2C bus, and general-purpose ‎pins G1-G4.‎

SPI

The MicroMod standard supports two Serial Peripheral Interface (SPI) buses, but because of the ‎limited GPIO pins here, only the primary SPI bus is used. This primary SPI bus is dedicated to the ‎following pins:‎

  • SCK - This is the clock pin, which is connected to GPIO 18, or MicroMod pad 57
  • SDO - This is the serial data output of the ESP32, which is connected to GPIO 23, or ‎MicroMod pad 59
  • SDI - This is the serial data input of the ESP32, which is connected to GPIO 19, or MicroMod ‎pad 61
  • ‎#CS - This is the chip select pin, which is connected to GPIO 5, or MicroMod pad 55

Note: You may not recognize the COPI/CIPO labels for SPI pins. SparkFun is working to move ‎away from using MISO/MOSI to describe signals between the controller and the peripheral. Check ‎out this page for more on our reasoning behind this change.‎

ESP32 MicroMod Processor Pin Functionality

function_7

ESP32 PROCESSOR BOARD PINOUT TABLE

esp32-processor-board-pinout-table_8

MICROMOD GENERAL PINOUT TABLE

microod-general-pinout-table_9

MICROMOD GENERAL PIN DESCRIPTIONS

micromod-general-pin-descriptions_10

Board Dimensions

The board measures 22mm x 22mm, with 15mm to the top notch and 12mm to the E key. For more ‎information regarding the processor board physical standards, head on over to the Getting Started ‎with MicroMod tutorial and check out the Hardware Overview section.‎

dimensions_11

The overall thickness of the MicroMod ESP32 Processor Board is ~2.67mm. The height of the ‎tallest component (ESP32 labeled as "U2" in the board file) on the Processor side is ~0.90mm. The ‎PCB thickness is ~0.80mm. The height of the tallest component (transistor labeled as "Q2" in the ‎board file) is about ~0.97mm.‎

Hardware Hookup

To get started with the ESP32 Processor Board, you'll need a carrier board. Here we are using the ‎MicroMod Input and Display Carrier Board. Align the top key of the MicroMod ESP32 Processor ‎Board to the screw terminal of the Input and Display Carrier Board and angle the board into the ‎socket. Insert the board at an angle into the M.2 connector.‎

Note: There is no way to insert the processor backward since the key prevents it from mating with ‎the M.2 connector and as an extra safeguard to prevent inserting a processor that matches the key, ‎the mounting screw is offset so you will not be able to secure an improperly connected processor ‎board.

angle_12

The Processor Board will stick up at an angle, as seen here:‎

socket_13

Once the board is in the socket, gently hold the MicroMod Processor Board down and tighten the ‎screw with a Phillip's head.‎

screw_14

Once the board is secure, your assembled MicroMod system should look similar to the image below!‎

assembled_15

Connecting Everything Up

With your processor inserted and secured it's time to connect your carrier board to your computer ‎using the USB-C connector on the Carrier. Depending on which carrier you choose and which ‎drivers you already have installed, you may need to install drivers.‎

Note: If you've never connected a CP2104 device to your computer before, you may need to install ‎drivers for the USB-to-serial converter. Check out our section on How to Install CP2104 Drivers for ‎help with the installation.‎

Software Setup and Programming

Installing the CP2104 USB Driver

Note: Make sure to manually install the driver for the CP210X with the following instructions. The ‎driver that Windows auto-installs will not work with the auto-reset circuit on the board and cause ‎serial uploads to fail.‎

Users will need to install the SiLabs CP2104 Driver, which can be found here: USB to UART Bridge ‎VCP Driver

DOWNLOAD WINDOWS VCP DRIVER (ZIP)‎

DOWNLOAD MAC OSX VCP DRIVER (ZIP)‎

Note: If applicable, make sure you are using the proper driver files for your CPU architecture. This ‎is usually indicated by a folder or file name with "x86" for 32-bit processors or "x64" for 64-bit ‎processors.‎

Arduino IDE

Note: For first-time users, who have never programmed before and are looking to use the Arduino ‎IDE, we recommend beginning with the SparkFun Inventor's Kit (SIK), which includes a simpler ‎board like the Arduino Uno or SparkFun RedBoard and is designed to help users get started ‎programming with the Arduino IDE.‎

Most users may already be familiar with the Arduino IDE, and it's use. However, for those of you ‎who have never heard the name Arduino before, feel free to check out the Arduino website. To get ‎started with using the Arduino IDE, check out our tutorials below:‎

  • Installing an Arduino Library: How do I install a custom Arduino library? It's easy! This ‎tutorial will go over how to install an Arduino library using the Arduino Library Manager. For libraries ‎not linked with the Arduino IDE, we will also go over manually installing an Arduino library.‎
  • What is an Arduino? What is this 'Arduino' thing anyway? This tutorial dives into what an ‎Arduino is and along with Arduino projects and widgets.‎
  • Installing Arduino IDE: A step-by-step guide to installing and testing the Arduino software on ‎Windows, Mac, and Linux.‎
  • Installing Board Definitions in the Arduino IDE: How do I install a custom Arduino ‎board/core? It's easy! This tutorial will go over how to install an Arduino board definition using the ‎Arduino Board Manager. We will also go over manually installing third-party cores, such as the ‎board definitions required for many of the SparkFun development boards.‎

Install Board Definition

Install the latest ESP32 board definitions in the Arduino IDE (must be v1.8.13 or later).‎

installing_16

Installing Board Definitions in the Arduino IDE

How do I install a custom Arduino board/core? It's easy! This tutorial will go over how to install an ‎Arduino board definition using the Arduino Board Manager. We will also go over manually installing ‎third-party cores, such as the board definitions required for many of the SparkFun development ‎boards.‎

Note: For more instructions, users can follow this tutorial on Installing Additional Cores provided by ‎Arduino. Users will also need the .json file for the Espressif Arduino core:‎https://raw.githubusercontent.com/espressif/arduino-esp32/gh-‎pages/package_esp32_index.json

When selecting a board to program in the Arduino IDE, users should select the SparkFun ESP32 ‎MicroMod from the Tools drop down menu (i.e. Tools > Board > ESP32 Arduino > SparkFun ‎ESP32 MicroMod).‎

Arduino Example: Blink

With the SparkFun ESP32 Arduino core installed, you're ready to begin programming. Make sure ‎you have the ESP32 MicroMod board definition selected under your Tools > Board menu.‎

menu_17

Then select your serial port under the Tools > Port menu.‎

port_18

You can also select the Upload Speed: "921600" baud -- the fastest selectable rate -- will get the ‎code loaded onto your ESP32 the fastest but may fail to upload once-in-a-while. (It's still way worth ‎it for the speed increase!)‎

Loading Blink

To make sure your toolchain and board are properly set up, we'll upload the simplest of sketches -- ‎Blink! The STAT LED on the ESP32 Processor Board is perfect for this test. This is also a good ‎time to test out serial communication. Copy and paste the example sketch below into a fresh ‎Arduino sketch:‎

Copy Code
int ledPin = 2;

void setup()
{
pinMode(ledPin, OUTPUT);
Serial.begin(115200);
}

void loop()
{
Serial.println("Hello, world!");
digitalWrite(ledPin, HIGH);
delay(500);
digitalWrite(ledPin, LOW);
delay(500);
}

With everything setup correctly, upload the code! Once the code finishes transferring, open ‎the serial monitor and set the baud rate to 115200. You should see Hello, world!'s begin to fly ‎by. You may also notice that when the ESP32 boots up it prints out a long sequence of debug ‎messages. These are emitted every time the chip resets -- always at 115200 baud.‎

com_19

You should also see some blinking happening on the ESP32 Processor Board! Blink Blink Blink!‎

MicroMod_Input___Display_Carrier_Board_5

If the blue LED remains off, it's probably still sitting in the bootloader. After uploading a sketch, you ‎may need to tap the reset button to get your ESP32 MicroMod to run the sketch.‎

Arduino Example: WiFi

The ESP32 Arduino core includes a handful of WiFi examples, which demonstrate everything ‎from scanning for nearby networks to sending data to a client server. You can find the examples ‎under the File > Examples > WiFi menu.‎

Here's another example using the WiFi library, which demonstrates how to connect to a nearby WiFi ‎network and poll a remote domain (http://example.com/) as a client.‎

Please note: Make sure you are connecting to the 2.4GHz band on your wireless router; the ‎ESP32 is not compatible with 5GHz signals.

Copy Code
#include <WiFi.h>

// WiFi network name and password:
const char * networkName = "YOUR_NETWORK_HERE";
const char * networkPswd = "YOUR_PASSWORD_HERE";

// Internet domain to request from:
const char * hostDomain = "example.com";
const int hostPort = 80;

const int BUTTON_PIN = 0;
const int LED_PIN = LED_BUILTIN;

void setup()
{
// Initilize hardware:
Serial.begin(115200);
pinMode(BUTTON_PIN, INPUT_PULLUP);
pinMode(LED_PIN, OUTPUT);

// Connect to the WiFi network (see function below loop)
connectToWiFi(networkName, networkPswd);

digitalWrite(LED_PIN, LOW); // LED off
Serial.print("Press the Boot button to connect to ");
Serial.println(hostDomain);
}

void loop()
{
if (digitalRead(BUTTON_PIN) == LOW)
{ // Check if button has been pressed
while (digitalRead(BUTTON_PIN) == LOW)
; // Wait for button to be released

digitalWrite(LED_PIN, HIGH); // Turn on LED
requestURL(hostDomain, hostPort); // Connect to server
digitalWrite(LED_PIN, LOW); // Turn off LED
}
}

void connectToWiFi(const char * ssid, const char * pwd)
{
int ledState = 0;

printLine();
Serial.println("Connecting to WiFi network: " + String(ssid));

WiFi.begin(ssid, pwd);

while (WiFi.status() != WL_CONNECTED)
{
// Blink LED while we're connecting:
digitalWrite(LED_PIN, ledState);
ledState = (ledState + 1) % 2; // Flip ledState
delay(500);
Serial.print(".");
}

Serial.println();
Serial.println("WiFi connected!");
Serial.print("IP address: ");
Serial.println(WiFi.localIP());
}

void requestURL(const char * host, uint8_t port)
{
printLine();
Serial.println("Connecting to domain: " + String(host));

// Use WiFiClient class to create TCP connections
WiFiClient client;
if (!client.connect(host, port))
{
Serial.println("connection failed");
return;
}
Serial.println("Connected!");
printLine();

// This will send the request to the server
client.print((String)"GET / HTTP/1.1\r\n" +
"Host: " + String(host) + "\r\n" +
"Connection: close\r\n\r\n");
unsigned long timeout = millis();
while (client.available() == 0)
{
if (millis() - timeout > 5000)
{
Serial.println(">>> Client Timeout !");
client.stop();
return;
}
}

// Read all the lines of the reply from server and print them to Serial
while (client.available())
{
String line = client.readStringUntil('\r');
Serial.print(line);
}

Serial.println();
Serial.println("closing connection");
client.stop();
}

void printLine()
{
Serial.println();
for (int i=0; i<30; i++)
Serial.print("-");
Serial.println();
}

Make sure you fill in the networkName and networkPswd variables with the name (or SSID) and ‎password of your WiFi network! Once you've done that and uploaded the code, open your serial ‎monitor.‎

serial_20

After your ESP32 connects to the WiFi network, it will wait for you to press the "Boot" button on ‎your carrier board. Tapping that will cause the ESP32 to make an HTTP request to example.com. ‎You should see a string of HTTP headers and HTML similar to the screenshot above.‎

Further Examples

With the MicroMod system, the possibilities for examples with all the processor/carrier board are ‎endless, and we just can't cover them all. You'll notice that in this tutorial, we've selected the Input ‎and Display Carrier Board, but have focused our examples on the Esp32 Processor Board. If you're ‎interested in examples specifically for our carrier board, head on over to our SparkFun MicroMod ‎Input and Display Carrier Board Hookup Guide.‎

Troubleshooting

With the MicroMod Processors, you can change out the processors with little to no changes in the ‎code. But because each processor board's architecture is different, the way communication ‎protocols are initialized might be a little bit different. For the ESP32 Processor, the two main ‎protocols are the Universal Asynchronous Receiver Transmitter (UART), aka Serial, and I2C, aka ‎Wire.‎

Secondary Serial/UART Initialization Tips

The UART is initialized with the begin function as:‎

Copy Code
void begin(unsigned long baud, uint32_t config, int8_t rxPin, int8_t txPin, bool invert, unsigned long timeout_ms)

The primary UART works like any other Arduino board being able to initialize and send messages ‎back to your computer over the USB cable using using Serial.begin(115200) for a baud rate of ‎‎115200 as an example. If you wanted to communicate at the same 115200 baud rate on the ‎secondary UART you would initialize Serial1 as:‎

Copy Code
Serial1.begin(115200, SERIAL_8N1, RX1,TX1);

Or if you want to use the GPIO pin numbers instead, it would be:‎

Copy Code
Serial1.begin(115200, SERIAL_8N1, 16, 17);

Secondary I2C Initialization Tips

The Wire bus is initialized with the begin function as:‎

Copy Code
bool begin(int sda, int scl, uint32_t frequency);  // returns true, if successful init of i2c bus

With the primary Wire bus, these pins use the default SCL and SDA pins connected to GPIO pins ‎‎22 and 21 and can be initialized by simply calling Wire.begin(). If you plan on using the secondary ‎Wire bus, you need to provide the pins, and possibly the desired frequnecy if the default 400kHz is ‎too fast. For most applications though you can use:‎

Copy Code
Wire1.begin(SDA1, SCL1);

Or if you wanted to use the GPIO pin numbers, it would be:‎

Copy Code
Wire1.begin(26, 25);

‎Not working as expected and need help?

If you need technical assistance and more information on a product that is not working as you ‎expected, we recommend heading on over to the SparkFun Technical Assistance page for some ‎initial troubleshooting.

SPARKFUN TECHNICAL ASSISTANCE PAGE‎ ‎

If you don't find what you need there, the SparkFun Forums: MicroMod are a great place to find ‎and ask for help. If this is your first visit, you'll need to create a Forum Account to search product ‎forums and post questions.

SPARKFUN FORUMS: MICROMOD

Resources and Going Further

For more information about the MicroMod ESP32 Processor Board, check out the following links:‎

For more information about the SparkFun MicroMod Ecosystem, take a look at the links below:‎

メーカー品番 16781
MICROMOD ESP32 PROCESSOR
SparkFun Electronics
メーカー品番 16885
MICROMOD ATP CARRIER BOARD
SparkFun Electronics
メーカー品番 16985
MICROMOD INPUT/DISPLAY CARRIER
SparkFun Electronics
メーカー品番 16400
MICROMOD MACHINE LEARN CARRIER
SparkFun Electronics
メーカー品番 15081
QWIIC CABLE KIT
SparkFun Electronics
メーカー品番 14427
QWIIC CABLE - 100MM
SparkFun Electronics
メーカー品番 15424
CBL USB2.0 A PLUG TO C PLG 6.56'
SparkFun Electronics
メーカー品番 14743
CABLE A PLUG TO C PLUG 3.28'
SparkFun Electronics
メーカー品番 15631
ARDUINO UNO INVENTOR KIT V4.1
SparkFun Electronics
メーカー品番 A000066
ARDUINO UNO R3 ATMEGA328P BOARD
Arduino
メーカー品番 15123
REDBOARD QWIIC ATMEGA328 EVAL BD
SparkFun Electronics
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.