Maker.io main logo

Getting Started with Badger 2040

712

2022-11-03 | By Pimoroni

License: See Original Project Wearables

Courtesy of Pimoroni

Guide by Pimoroni

Badger 2040 is a low cost, RP2040-powered eInk/ePaper/EPD programmable ‎badge. We've designed it to be an friendly introduction into the myriad joys of ‎eInk , but flexible and expandable enough to be of interest to intrepid RP2040 ‎haxxors- let’s take a look at what it can do.‎

This tutorial will show you how to plug things in, how to get to grips with the ‎built-in demo programs and how to start programming your Badger with ‎MicroPython.‎

What You'll Need

  • A Badger 2040

  • A USB-C cable (for programming)‎

  • Some sort of battery if you want to disconnect Badger from your ‎computer and update the display on the go - we'll discuss a few options ‎and their pros and cons!

  • A computer to program from (Windows, Mac, or Linux/Raspberry Pi)

Batteries

AA AND AAA BATTERIES

The easiest way to supply your Badger with power is via some good old-‎fashioned double or triple A batteries. We like a 2 x AAA setup the best, as ‎the battery pack sticks onto the back of Badger without being too heavy and ‎unwieldy. You'll need a battery holder with a JST-PH connector to be able to ‎plug it in.‎

power_1

2x AAA rechargeable (NiMH) batteries only put out 2.4V which is, strictly ‎speaking, not enough for Badger. However, in our tests it keeps on truckin' ‎down to an input voltage of 2.05V (without the LED), so if you want to use ‎rechargeable batteries that should be fine.‎

ASSEMBLING THE BADGER ACCESSORY KIT

If you have our Badger accessory kit, it will come with some Velcro for ‎sticking the battery pack to the back of Badger. Before you start sticking ‎things down, experiment a little bit with the positioning of the battery pack:‎

  • If you're hanging Badger from a lanyard, you'll want to make sure the ‎battery pack is balanced in the middle to avoid your badge hanging ‎lopsided. We've put our square in the middle of Badger, but if you ‎wanted you could cut it in half and stick half at each end of the battery ‎pack

  • If you have a on/off switch on your battery bank and want to be able to ‎use it, make sure to position it where it's accessible

  • Once you're ready to stick the bits of Velcro down, press em down and ‎then wait 10 minutes for the adhesive to set. Then you're ready to go!‎

kit_2

kit_3

USB BATTERY PACK

USB battery packs are probably a bit heavy for dangling round your neck, but ‎they might be useful for powering Badger from your pocket or your bag, if you ‎don't want to stick a battery pack to Badger itself. You'll need one that's ‎capable of powering low powered devices - a lot of power banks will ‎automatically shut off if really low amounts of current are being drawn.

packs_4

Our fancy new USB-C power banks have a super-secret low power mode - ‎once you've plugged everything in, hold down the button until the blue LEDs ‎light up one at a time. It's now in low power mode - perfect to supply the ‎modest power needs of our Badger friend (you'll need to plug the power bank ‎in to charge to reset it and return it to normal behaviour).‎

LIPO/LIION BATTERIES (WITH CAUTION!)‎

If the person wearing the badge is an adult who knows what they're doing ‎with LiPo batteries, it's possible to power Badger from a LiPo battery (we ‎like this 500mAh one).‎

LiPos like these are squishy and vulnerable, so a solid enclosure or backplate ‎to protect the battery from impacts and damage whilst being worn is ‎essential. We stuck our LiPo to the back of Badger with a Velcro square to ‎stop it from rattling around...‎

battery_5

‎... and 3D printed a backplate, secured in place with M2 nuts and bolts (if ‎you'd like to print one of your own, you can find the STL here!).‎

backplate_6

Alternatively, you could use a hard case LiPo with Badger 2040 - we really like ‎this tiny Galleon one.‎

A few more things you should consider if you're using a LiPo:‎

  • There's no battery protection included on Badger 2040, so you should ‎only use it with LiPo batteries that include internal protection (all ours ‎do)

  • If you've sourced a battery from elsewhere, check that the connector ‎has the red wire going to + and the black wire going to - on our board. ‎Not all batteries have their connectors attached the same way up!‎

  • Unlike some of our other boards, Badger 2040 doesn't have battery ‎charging circuitry onboard. You'll need to plug your battery into an ‎external LiPo charger (like a LiPo Amigo) to charge it

MicroPython and Badger 2040‎

The custom display drivers in our C++/MicroPython build let us do a bunch of ‎cool stuff with the E Ink display. There are simple drawing and text functions ‎to make it straightforward to display things on the display. You can also ‎change how quickly you update the display - faster updates will mean less ‎saturated blacks and more ghosting on your display, so you'll need to decide ‎whether speed or quality is more important for your application (our demos ‎use a variety of update speeds, so you can see how they behave).‎

INSTALLING BADGER FLAVOURED MICROPYTHON

Your Badger will come preloaded with MicroPython and a suite of examples, ‎but for the all the latest features, tweaks and fixes, you should download ‎yourself the newest version.‎

These instructions will assume you're using version 1.18.5 or later (released ‎‎25/03/2022) - there have been quite a few changes so if something's not ‎working as it's should, try updating your MicroPython version!‎

If you're brand new to Raspberry Pi Pico/RP2040s, you might find the step by ‎step instructions in our Getting Started with Raspberry Pi Pico tutorial useful ‎‎- it will show you how to install our custom MicroPython build and goes into ‎more detail about how to use Thonny. Here's a quick TLDR!‎

  • Download the most recent MicroPython .uf2 from the Releases page of ‎our pimoroni-pico Github repository. You'll want the special version for ‎Badger 2040, which has the BadgerOS launcher and demos built in

  • Hold down the BOOT button of Badger 2040, and then press, and ‎release, the RESET button. This will put it into bootloader mode, and it ‎should appear as a drive on your computer called RPI-RP2

  • Copy the .uf2 file to the RPI-RP2 drive - once you've done that Badger ‎‎2040 will reboot running BadgerOS!‎

USING BADGER OS

You can navigate around the launcher using the up and down arrows, and ‎select an example by pressing A, B, or C. To return to the launcher when ‎you're done with an example, press buttons A and C at the same time.‎

Hold BOOT whilst pressing up or down to adjust the font size or hold BOOT ‎whilst pressing A to toggle dark mode.‎

RUNNING BADGER OS ON BATTERY POWER

If you're running version 1.18.5 or later, the launcher and most of the ‎examples now turn off automatically to conserve battery power. Whilst ‎running on battery power the LED will light up when Badger is awake and ‎consuming power and turn off to let you know when the board is asleep. ‎Press any front button to wake it up where you left off or press A and C ‎together to return to the launcher.‎

Programming Badger with Thonny

Once MicroPython is installed, your Badger won't show up as a drive anymore. ‎To program it, you'll need to talk to it through an interpreter - we're using ‎Thonny, which is available for Windows, Mac or Linux.‎

  • Install the latest version of Thonny. We recommend downloading it ‎from the Thonny website as package managers do not always have ‎the newest version

  • Open up Thonny. Make sure the interpreter (shown in the box on the ‎bottom right corner) is set to 'MicroPython (Raspberry Pi Pico)'

  • Plug your Badger into your computer if it's not plugged in ‎already. Because the launcher will already be running, you'll need to ‎stop it with the stop button in Thonny before sending it any instructions

  • After you press stop, you should get something like this a MicroPython ‎prompt that looks something like this. The flashing cursor next to ‎the >>> in the 'Shell' box tells you that Badger 2040 is talking to your ‎computer and is ready to accept instructions! (If you don't get a prompt ‎or if you get an error, you might have interrupted Badger at a weird ‎point in the program, try pressing reset on your Badger and pressing ‎stop again)‎

prompt_7

LIGHTING UP THE ONBOARD LED

As a test that the board is working properly and you have the correct version ‎of MicroPython installed, you can light up the white onboard LED with the ‎following code - enter it line by line in the REPL (that's the bottom 'Shell' box ‎in Thonny).‎

Copy Code
import badger2040
badger = badger2040.Badger2040()

badger.led(255)

‎‎(Those first two lines are boilerplate code that you'll need at the beginning of ‎any code you run on Badger).‎

Let's turn off the LED again, to be tidy!‎

Copy Code
badger.led(0)‎

WRITING TEXT ON THE SCREEN

Here's how to display text on the screen, in its most basic form. You'll need to ‎enter the boilerplate, as before (unless you're still using the same Thonny ‎session).‎

Copy Code
import badger2040
badger = badger2040.Badger2040()

badger.pen(0)
badger.text("Hello Badger", 20, 20)
badger.update()

The rest of the code does this:‎

  • Picks a pen colour to write with - 0 is black and 15 is white. This display ‎will only show black or white, but if you pick a number in between 0 and ‎‎15 it will dither it to approximate a shade of grey

  • Writes text to the screen buffer - the '20, 20' is the x/y co-ordinates of ‎the left middle of the text

  • Updates the E Ink screen (you can draw multiple things to your screen ‎buffer before triggering an update)

code_8

If you try writing more text to the screen, you will find that things you've ‎drawn to the screen buffer will stick around until you overwrite them. To clear ‎the screen and start with a clean slate:‎

Copy Code
badger.pen(15)
badger.clear()

MORE DRAWING FUNCTIONS

There are more functions in the library for changing the font, size, and ‎thickness of text, as well as functions for drawing individual pixels, lines, and ‎rectangles. Check out the function reference for more info!‎

Customising the BadgerOS Examples

When you run them, some of the examples will create their own data files ‎that you can edit. If you don't have it open already, you will want to have the ‎Files window visible, you can do this with View > Files.‎

files_9

The top box can be used to browse the local files in on your computer, and ‎the bottom box shows the files on your Badger. You can copy files from your ‎computer to your Badger by right clicking on them in the top window and ‎choosing 'Upload to/' (or open up a file by clicking on it in the bottom window, ‎and then press 'save' when you're done). When you're finished ‎editing/uploading data files, hit the reset button on your Badger to start the ‎launcher again.‎

The data files are created the first time you run the relevant examples on ‎your Badger, so if you plug in a fresh Badger and start browsing files you ‎won't see them yet.‎

E-READER.PY

This example comes with an excerpt from Wind in the Willows - replace the ‎contents of 'book.txt' with another text file of your choosing for it to show up ‎in the e-reader. You can find more free books (with text versions) at Project ‎Gutenberg!‎

When running the example, you can press A and B to change the font style ‎and size.‎

LIST.PY

To swap the demo checklist with one of your own, edit the contents of ‎checklist.txt. Each list item should be on a separate line.‎

Copy Code
cake
biscuits
bees
mashed potato

badge_10

IMAGE.PY AND ADDING YOUR OWN IMAGES

To get your own images onto Badger using MicroPython, you will first need ‎to convert them into a 1-bit byte array that represents the monochrome ‎image. We've made a Python script that you can run on your computer to ‎take care of the conversion. The script will convert a bmp, jpg, or png image ‎into a black and white 296 x 128, formatted .bin file that Badger can read.‎

Here's a few different ways you can run it!‎

CONVERTING IMAGES FROM A RASPBERRY PI

‎(Or other Linux command line; Ubuntu, Mac, WSL etc.)‎

  • Open up a terminal

  • Download the pimoroni-pico repo to your computer:

git clone ‎https://github.com/pimoroni/pimoroni-pico

  • Navigate to the image converter tool:

cd pimoroni-‎pico/examples/badger2040/image_converter

  • Then, assuming your starting image file is in the same directory as ‎‎'convert.py', you can convert it like this (adding in your own file ‎names):

python3 convert.py --binary --resize image_file_1.png

  • Or convert multiple images like this:

python3 convert.py --binary --resize ‎image_file_1.png image_file_2.png image_file_3.png

  • If you get a 'No module named PIL' error, you might need to

pip3 install ‎pillow, and then try again.‎

install_11

CONVERTING IMAGES FROM WITHIN THONNY

‎(This may be an easier option if you're using Windows)‎

  • Switch your interpreter to 'The same interpreter who runs Thonny ‎‎(default)' using the box at the bottom right. This tells it to use Thonny's ‎full fat version of Python, instead of Badger's version of MicroPython

  • Install PIL (Python Image Library) in Thonny, with Tools > Manage ‎Packages. Search for Pillow, click on it, and then 'Install'

  • Click 'new' and copy and paste the contents of convert.py into the ‎blank tab. 'Save' it somewhere on your computer, ‎named convert.py (you'll probably want it to save it to the same place as ‎the images you want to convert)

  • In the bottom shell box at the Python prompt, you can then run ‎convert.py from within Thonny like this (adding in your own ‎filenames):

%Run convert.py --resize --binary image_file_1.png

  • Make sure you press enter after typing that in - if you press the ‎green run button it will only run the first part of the command

  • Remember to switch your interpreter back to MicroPython (Raspberry ‎Pi Pico) when you're done converting!‎

convert_12

Once you've generated your .bin file, you can copy it to Badger using the Files ‎menu in Thonny:‎

  • Browse to your file in the top 'This computer' window

  • In the bottom box, double click on the images directory on your Badger ‎to open it up

  • Right click on your .bin file in the top window and select 'Upload to ‎‎/images'‎

copy_13

Your new images should show up in the image example after a board reset. ‎For more control over dithering etc. (and a preview of what they're going to ‎look like), try converting your images into 1 bit black and white with a ‎graphics program such as GIMP before running them through the script.‎

new_14

BADGE.PY

To change the text on the name badge example, edit 'badge.txt'. You can ‎double click on badge.txt in the Files menu to open it up in Thonny ‎‎(remember to 'save' the file when you're done).‎

To change the image, you'll need to convert your image as above, with the ‎following changes:‎

  • The name badge image needs to be named 'badge-image.bin' and in ‎the root directory of your Badger alongside badge.txt (not in the ‎‎/images directory)‎

  • This image needs to be exactly 104 pixels in width and 128 pixels in ‎height, so you'll need to resize it with a graphics program ‎like GIMP before you run it through the conversion script. When you ‎come to convert it, don't use the --resize flag as this will stretch it to 296 ‎x 128, instead use

python3 convert.py --binary badge-image.png

  • or from Thonny: %Run convert.py --binary badge-image.png

change_15

Running Your Own Examples

If you want to modify the examples further (or write your own from scratch), ‎you can find the Python code for all the baked in examples (plus a few ‎extras) on Github.‎

The built-in examples won't show up as Python files that you can edit on ‎Badger - you'll need to copy and paste the example code into a new file in ‎Thonny (clicking the raw button first makes it easier to copy) and press the ‎green 'run' button to run it on your Badger.‎

You'll be prompted for a file name to save it with. If you give it the same ‎filename as one of the built-in examples (badge.py, clock.py etc.) the launcher will ‎run your version of the example instead of the built in one. If you want to go ‎back to the original, just delete your copy from Badger.‎

Next Steps

Once you've got to grips with Thonny and our examples, why not add one of ‎our breakouts into the mix to give your Badger some sensor smarts. If your ‎breakout has a Qw/ST connector, you can plug it straight into Badger with ‎a Qw/ST cable (if not, you can use one of these adaptors). There's a list of ‎which of our breakouts are currently supported in our MicroPython build here.‎

As always, drop us a line on Twitter to tell us what you and your Badger get ‎up to - we'd love to know!‎

Troubleshooting

‎'THONNY CAN'T SEE MY BADGER / DEVICE IS BUSY'‎

Double check you've got your interpreter set to 'Raspberry Pi Pico' and check ‎you've pressed 'stop' to stop the launcher from running! You need the >>> ‎prompt to be visible in the 'shell' window to be able to transfer files or send ‎Python instructions to Badger.‎

Please note that you only need to hold down the BOOT button whilst putting ‎Badger into bootloader mode so you can copy MicroPython to it, you don't ‎need it to be in bootloader mode after that (unless you want to upload new ‎firmware).‎

'THE BATTERY INDICATOR IN THE LAUNCHER ISN'T WORKING!'‎

The battery icon in the top left of the launcher uses voltage values that are ‎reasonable for a LiPo battery, so if you're using AA/AAA batteries it might ‎show as empty, even when there's plenty of juice left. To make the battery ‎icon represent your battery situation better, save your own copy ‎of launcher.py to your Badger and alter the min/max values to something ‎more appropriate - something like this should work better for 2 x (non-‎rechargeable) AAAs:‎

Copy Code
MAX_BATTERY_VOLTAGE = 3.2
MIN_BATTERY_VOLTAGE = 2.0

If you want to know more about how you can use Badger to monitor the ‎voltage from your battery, check out this example.‎

HOW DO I FACTORY RESET?‎

If you need to delete all your programs from Badger's flash memory and start ‎again from scratch, you can do that by downloading this special .uf2 file and ‎copying it to your Badger whilst it's in bootloader mode. Once you've done ‎that, you'll need to copy the Badger MicroPython image across again.‎

You may also find clearing the flash to be useful if you encounter problems ‎after upgrading to the newest version of MicroPython - just make sure you ‎save any code you've been working on to your computer first!‎

That's all folks!‎

メーカー品番 PIM607
BADGER 2040
Pimoroni Ltd
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.