Marlow Mini-Harvester and Linear Tech Eval Board

Green is the color of the day. Everyone is looking for the most organic, most efficient, most economical, most environmentally friendly options to drive their world. The world is now concerned about the environment and global warming and trying to move more toward the use of renewable energy.

If you’re on board with this type of thinking and don’t know where to start, check out the Linear Technology DC2042A evaluation board for evaluation of piezoelectric, thermoelectric, and solar cell energy harvesters, as well as diode voltage drop harvesting. We’ve paired this with the Marlow TEG Mini-Harvester EHA-PA1AN1-R03 for a demo on just how they work together. These two devices paired together make a great place to start with energy harvesting. The board will take the input voltage of any of these harvesters and provide a regulated output voltage of 3.3 VDC.

For further information check out the following links:

Energy Harvester EEiki Post - http://www.eewiki.net/display/projects/Marlow+Industries+Inc.+-+Evergen+TEG+Mini-Harvester

Evaluation Board EEWiki Post  - http://www.eewiki.net/display/projects/Linear+Technology+-+Evaluation+Board+for+Energy+Harvesting

If you have any questions you can also check out our corresponding TechForum posts –

Energy Harvester - https://forum.digikey.com/t/thermo-electric-generator-energy-harvesting/1120

Eval Board - https://forum.digikey.com/t/dc2042a-nd-evaluation-board/1118

著者について

DigiKeyのアソシエートアプリケーションエンジニアリング技術者であるTravis Weesner氏は、2008年よりDigiKeyに勤務し、現在は世界中のお客様に技術支援を提供しています。以前は、半導体のサプライヤプライススペシャリストであり、特にメモリ領域やマイクロコントローラ分野の半導体のアプリケーションについて学びました。Travisはエレクトロニクステクノロジ自動化システムの学位を取得しています。彼の傾向は半導体に向いていますが、センサや自動化が未来の波だと感じています。

More posts by Travis Weesner
 TechForum

Have questions or comments? Continue the conversation on TechForum, Digi-Key's online community and technical resource.

Visit TechForum