![]()
![]()
![]()
![]()
DigiKeyのカタログにはない幅広い製品ラインアップもご用意しています。当社の審査基準を満たしたサプライヤ製品のみを扱っているので、ご購入は安心です。
ご注文の製品は、通常、ご注文日から1~3日以内にサプライヤから発送されます。別途送料がかかる場合がありますので、予めご了承ください。 実際の発送予定日は、製品ページ、カート、ご注文画面でご確認ください。
Incoterms:CPT(関税 & 適用されるVAT/税は、製品の配送時にお客様のご負担となります。)
詳細はヘルプとサポートをご覧ください
Circuit Playground features an ATmega32u4 micro-processor, just like our popular Flora. It also is round and has alligator-clip pads around it.
If you’re ready to step your Arduino game up from older 8-bit/16MHz microcontrollers, the SparkFun SAMD21 Mini Breakout is a great landing spot. The SAMD21 Mini Breakout is a Pro Mini-sized breakout for the Atmel ATSAMD21G18, a 32-bit ARM Cortex-M0+ processor with 256KB flash, 32KB SRAM, and an operating speed of up to 48MHz.
At the Feather M0's heart is an ATSAMD21G18 ARM Cortex M0+ processor, clocked at 48 MHz and at 3.3V logic, the same one used in the new Arduino Zero. This chip has a whopping 256K of FLASH (8x more than the Atmega328 or 32u4) and 32K of RAM (16x as much)!
The SparkFun 1-Channel LoRa Gateway is a powerful 3-network capable device thanks to an onboard ESP32 WROOM module and an RFM95W LoRa modem. The RFM95W handles the 915MHz band while the ESP32 takes care of Bluetooth and WiFi capabilities. One of the ideal uses is to convert LoRa (Long Range) radio messages into data packets that you can access via the web, but of course the flexibility it offers can be put to many more uses!
It's blue! It's skinny! It's the Arduino Pro! SparkFun's minimal design approach to Arduino. This is a 5V Arduino running the 16MHz bootloader in a super-sleek form factor that will fit easily into your next small project.
The Boron LTE is a powerful LTE CAT-M1/NB1 enabled development board that can act as either a standalone cellular endpoint or LTE enabled gateway for Particle Mesh networks. It is based on the Nordic nRF52840 and has built-in battery charging circuitry so it’s easy to connect a Li-Po and deploy your local network in minutes.
If you’re ready to step up your Arduino game from older 8-bit/16MHz microcontrollers, the SparkFun RedBoard Turbo is a formidable alternative. At its heart, the RedBoard Turbo uses the ATSAMD21G18, which is an ARM Cortex M0+, 32-bit microcontroller that can run at up to 48MHz.
Adafruit seesaw is a near-universal converter framework which allows you to add add and extend hardware support to any I2C-capable microcontroller or microcomputer. Instead of getting separate I2C GPIO expanders, ADCs, PWM drivers, etc, seesaw can be configured to give a wide range of capabilities.
Circuit Playground Express is the next step towards a perfect introduction to electronics and programming. We've taken the original Circuit Playground Classic and made it even better! Not only did we pack even more sensors in, we also made it even easier to program.
The MEGA 2560 is designed for more complex projects. With 54 digital I/O pins, 16 analog inputs and a larger space for your sketch it is the recommended board for 3D printers and robotics projects. This gives your projects plenty of room and opportunities.
ご注文、出荷、配送などに関する情報は、当社ウェブサイトの「ヘルプ & サポート」ページでご確認ください。
DigiKey会員にご登録いただいたお客様は、DigiKeyページの上部にある[ログインまたは登録]ドロップダウンメニューから[ログイン]を選択して会員様専用のアカウント(myDIGIKEY)にログインすることで、ご注文を追跡できます。すでにログイン済みのお客様は、こちらからすべてのご注文をすぐにご確認いただけます。ご注文いただいてから、最新のご注文状況が反映されるまでに12時間かかる場合がございますので、予めご了承ください。
返品をご希望のお客様は、こちらのページにアクセスして、返品手続きを開始してください。
DigiKeyのお客様は、会員登録の有無に関わらず、myListsから価格と在庫状況をリアルタイムで確認することができます。DigiKey会員にご登録いただいたお客様は、見積もりの作成が可能です。
登録ページに進み、必須情報を入力してください。 ご登録内容を送信いただくと、確認の電子メールが届きます。
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
![]()
![]()
![]()
![]()