Maker.io main logo

Introduction to Zephyr Part 8: Multithreading

1,046

2025-04-24 | By ShawnHymel

ESP32

Multithreading is a critical feature in real-time operating systems (RTOS) like Zephyr, enabling developers to execute multiple tasks concurrently. By leveraging multiple threads, you can structure your embedded applications to perform tasks like handling inputs, processing data, and controlling outputs independently, all while ensuring that the system remains responsive and efficient.

In this post, we'll explore the basics of multithreading in Zephyr RTOS through a simple example program. The program demonstrates how to blink an LED and print messages to the console simultaneously by creating and managing threads. By the end of this post, you'll understand how threads work in Zephyr, how to define and configure them, and how to manage their execution.

All code for this Introduction to Zephyr series can be found here: https://github.com/ShawnHymel/introduction-to-zephyr

Hardware Connections

For this demonstration, we will connect an LED to pin 13 on the ESP32-S3-DevKitC. Here is a Fritzing diagram showing all of the connections we will use throughout this series:

Introduction to Zephyr Part 8: Multithreading

Example Application: Blinking and Printing

We will take our simple blink application and divide up the separate activities (blinking LED, printing to the console) into different threads. While this is a trivial example, it shows how to run a separate, concurrent threads in Zephyr.

Project Setup

Create a new project directory structure:

Copy Code
/workspace/apps/08_demo_multithreading/
├─ boards/
│  └─ esp32s3_devkitc.overlay
├─ src/
│  └─ main.c
├─ CMakeLists.txt
└─ prj.conf

CMakeLists.txt:

We will use the same boilerplate CMakeLists.txt file that we’ve been using for most of the series:

Copy Code
cmake_minimum_required(VERSION 3.22.0)‎

find_package(Zephyr REQUIRED HINTS $ENV{ZEPHYR_BASE})‎
project(button_demo)‎

target_sources(app PRIVATE src/main.c)‎
prj.conf ‎
Leave empty.‎

boards/esp32s3_devkitc.overlay

We will use the same overlay file that we had in the first tutorial. It simply assigns pin 13 as an output pin and gives it the alias “my-led.”

Copy Code
/ {
    aliases {
        my-led = &led0;
    };

    leds {
        compatible = "gpio-leds";
        led0: d13 {
            gpios = <&gpio0 13 GPIO_ACTIVE_HIGH>;
        };
    };
};

src/main.c

Here is the complete code for reference:

Copy Code
#include <stdio.h>‎
‎#include <zephyr/kernel.h>‎
‎#include <zephyr/drivers/gpio.h>‎

‎// Sleep settings‎
static const int32_t blink_sleep_ms = 500;‎
static const int32_t print_sleep_ms = 700;‎

‎// Stack size settings‎
‎#define BLINK_THREAD_STACK_SIZE 256‎

‎// Define stack areas for the threads‎
K_THREAD_STACK_DEFINE(blink_stack, BLINK_THREAD_STACK_SIZE);‎

‎// Declare thread data structs‎
static struct k_thread blink_thread;‎

‎// Get LED struct from Devicetree‎
const struct gpio_dt_spec led = GPIO_DT_SPEC_GET(DT_ALIAS(my_led), gpios);‎

‎// Blink thread entry point‎
void blink_thread_start(void *arg_1, void *arg_2, void *arg_3)‎
‎{‎
‎    int ret;‎
‎    int state = 0;‎

‎    while (1) {‎

‎        // Change the state of the pin‎
‎        state = !state;‎

‎        // Set pin state‎
‎        ret = gpio_pin_set_dt(&led, state);‎
‎        if (ret < 0) {‎
‎            printk("Error: could not toggle pin\r\n");‎
‎        }‎

‎        k_msleep(blink_sleep_ms);‎
‎    }‎
‎}‎

int main(void)‎
‎{‎
‎    int ret;‎
‎    k_tid_t blink_tid;‎

‎    // Make sure that the GPIO was initialized‎
‎    if (!gpio_is_ready_dt(&led)) {‎
‎        printk("Error: GPIO pin not ready\r\n");‎
‎        return 0;‎
‎    }‎

‎    // Set the GPIO as output‎
‎    ret = gpio_pin_configure_dt(&led, GPIO_OUTPUT);‎
‎    if (ret < 0) {‎
‎        printk("Error: Could not configure GPIO\r\n");‎
‎        return 0;‎
‎    }‎

‎    // Start the blink thread‎
‎    blink_tid = k_thread_create(&blink_thread,          // Thread struct
‎                                blink_stack,            // Stack
‎                                K_THREAD_STACK_SIZEOF(blink_stack),‎
‎                                blink_thread_start,     // Entry point
‎                                NULL,                   // arg_1‎
‎                                NULL,                   // arg_2‎
‎                                NULL,                   // arg_3‎
‎                                7,                      // Priority‎
‎                                0,                      // Options‎
‎                                K_NO_WAIT);             // Delay

‎    // Do forever‎
‎    while (1) {‎
‎        printk("Hello\r\n");‎
‎        k_msleep(print_sleep_ms);‎
‎    }‎

‎    return 0;‎
‎}‎

Build and Flash

In the Docker container, build the demo application:

Copy Code
cd /workspace/apps/08_demo_multithreading/‎
west build -p always -b esp32s3_devkitc/esp32s3/procpu -- -‎DDTC_OVERLAY_FILE=boards/esp32s3_devkitc.overlay

On your host computer, flash the application (replace with the USB port for your ESP32-S3-DevKitC):

Copy Code
python -m esptool --port "<PORT>" --chip auto --baud 921600 --before default_reset --after hard_reset ‎write_flash -u --flash_size detect 0x0 ‎workspace/apps/08_multithreading_demo/build/zephyr/zephyr.bin ‎

After flashing completes, open a serial port:

Copy Code
python -m serial.tools.miniterm "<PORT>" 115200 ‎

You should see the LED flashing on the board as well as “Hello” being printed to the terminal.

Introduction to Zephyr Part 8: Multithreading

Code Discussion

Defining Thread Stacks

In Zephyr, each thread requires its own stack for storing local variables, function call data, and more. The K_THREAD_STACK_DEFINE macro is used to allocate memory for the stack of the blink_thread:

Copy Code
‎#define BLINK_THREAD_STACK_SIZE 256‎
K_THREAD_STACK_DEFINE(blink_stack, BLINK_THREAD_STACK_SIZE);‎

Here, BLINK_THREAD_STACK_SIZE specifies the size of the stack (in bytes). The stack size should be chosen carefully based on the memory requirements of the thread.

Thread Data Structure

Zephyr uses a k_thread structure to manage thread information, such as its state, priority, and stack pointer. In the program, we declare a k_thread instance for the blink thread:

Copy Code
static struct k_thread blink_thread;‎

GPIO Initialization

As we saw in the first tutorial, the GPIO pin for the LED is defined using the Devicetree specification:

Copy Code
const struct gpio_dt_spec led = GPIO_DT_SPEC_GET(DT_ALIAS(my_led), gpios);‎

The GPIO_DT_SPEC_GET macro retrieves the GPIO device and pin information from the Devicetree alias my_led. This abstraction makes the code portable across different boards with varying GPIO configurations.

Before using the GPIO, the program ensures it is ready and configures it as an output pin:

Copy Code
const struct gpio_dt_spec led = GPIO_DT_SPEC_GET(DT_ALIAS(my_led), gpios);const struct ‎gpio_dt_spec led = GPIO_DT_SPEC_GET(DT_ALIAS(my_led), gpios);const struct gpio_dt_spec led = ‎GPIO_DT_SPEC_GET(DT_ALIAS(my_led), gpios);if (!gpio_is_ready_dt(&led)) {‎
‎    printk("Error: GPIO pin not ready\r\n");‎
‎    return 0;‎
‎}‎

ret = gpio_pin_configure_dt(&led, GPIO_OUTPUT);‎
if (ret < 0) {‎
‎    printk("Error: Could not configure GPIO\r\n");‎
‎    return 0;‎
‎}‎

Blink Thread Function

The blink_thread_start function is the entry point for the blink thread. It toggles the state of the GPIO pin to blink the LED and sleeps for a specified duration:

Copy Code
void blink_thread_start(void *arg_1, void *arg_2, void *arg_3)‎
‎{‎
‎    int ret;‎
‎    int state = 0;‎

‎    while (1) {‎
‎        state = !state;  // Toggle state
‎        ret = gpio_pin_set_dt(&led, state);‎
‎        if (ret < 0) {‎
‎            printk("Error: could not toggle pin\r\n");‎
‎        }‎
‎        k_msleep(blink_sleep_ms);  // Sleep
‎    }‎
‎}‎

The k_msleep function suspends the thread for blink_sleep_ms milliseconds, allowing other threads to execute. Threads that are sleeping are considered to be “unready” in the “waiting state” (see here to read more about thread states).

Thread Creation

The blink thread is created and started in the main function using the k_thread_create API:

Copy Code
blink_tid = k_thread_create(&blink_thread,          // Thread struct
‎                            blink_stack,            // Stack
‎                            K_THREAD_STACK_SIZEOF(blink_stack),‎
‎                            blink_thread_start,     // Entry point
‎                            NULL, NULL, NULL,       // Arguments
‎                            7,                      // Priority‎
‎                            0,                      // Options‎
‎                            K_NO_WAIT);             // Delay
  • &blink_thread: Points to the thread's data structure.
  • blink_stack: The stack memory allocated for the thread.
  • K_THREAD_STACK_SIZEOF(blink_stack): Specifies the size of the stack.
  • blink_thread_start: The function executed by the thread (i.e., the entrypoint of the thread).
  • 7: The thread's priority. Similar to Linux, lower numbers indicate higher priorities. You can read more about thread priorities here. Notice that Zephyr also implements cooperative multitasking where threads must explicitly give up execution (rather than be preempted by other, higher-priority threads). Use negative priority numbers to indicate a cooperative thread (whereas positive numbers indicate preemptive threads).
  • K_NO_WAIT: Starts the thread immediately. You could specify a time here to delay the thread execution start or use K_FOREVER to start the thread manually with k_thread_start().

You can find the Zephyr multithreading API documentation here.

Main Thread

The main function acts as the main thread. After configuring the GPIO and starting the blink thread, it enters an infinite loop that prints messages to the console and sleeps for print_sleep_ms milliseconds:

Copy Code
while (1) {‎
‎    printk("Hello\r\n");‎
‎    k_msleep(print_sleep_ms);‎
‎}‎

The main thread defaults to priority 0 (with preemption enabled) or -1 (with preemption disabled). While this example uses the main thread, you will often find many multithreaded applications simply sleep the main thread after spinning up its various worker threads.

Challenge

Your challenge is to use a message queue to pass data between two threads. One thread should read from your temperature sensor (or other sensor), and the other thread should simply print the sensor value to the console. You can read about message queues here. You are welcome to use the MCP9808 I2C driver we made in lesson 6 or use the official JEDEC JC-42 driver to talk to the MCP9808 sensor (sample here).

My solution for this challenge is found here.

Going Further

Zephyr RTOS offers robust support for multithreading, making it an excellent choice for building responsive and efficient embedded systems. Multithreading is incredibly useful when you need to handle multiple I/O events with latency, such as managing networking connections or responding to user interaction on an interface (graphical or text).

If you would like to dive more into real-time operating system theory (multithreading, queues, mutexes, semaphores, scheduling, etc.), check out our Introduction to RTOS series.

The following official Zephyr documentation can help you dive deeper into multithreading:

メーカー品番 ESP32-S3-DEVKITC-1-N32R8V
ESP32-S3-WROOM-2-N32R8V DEV BRD
Espressif Systems
メーカー品番 3533
GRAPHIC DISPLAY TFT RGB 0.96"
Adafruit Industries LLC
メーカー品番 1782
MCP9808 TEMP I2C BREAKOUT BRD
Adafruit Industries LLC
メーカー品番 3386P-1-103TLF
TRIMMER 10K OHM 0.5W PC PIN TOP
Bourns Inc.
メーカー品番 1825910-6
SWITCH TACTILE SPST-NO 0.05A 24V
TE Connectivity ALCOSWITCH Switches
メーカー品番 CF14JT220R
RES 220 OHM 5% 1/4W AXIAL
Stackpole Electronics Inc
メーカー品番 LTL-4224
LED RED CLEAR T-1 3/4 T/H
Lite-On Inc.
メーカー品番 14284
JUMPER M/M 4" 26AWG 30PCS
SparkFun Electronics
メーカー品番 FIT0096
BREADBRD TERM STRIP 3.20X2.00"
DFRobot
メーカー品番 DH-20M50055
USB AM TO USB MICRO, USB 2.0 - 1
Cvilux USA
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.