Maker.io main logo

XRP Tank Chassis

2026-06-15 | By Robert Doran

License: Attribution 3D Printing Raspberry Pi MCU

The 3D print files for this modified chassis can be found here

The XRP Original files can be found here

This project is a modification to the standard XRP chassis that ships with the kit. I found that the turning accuracy for the standard chassis was difficult, especially when being controlled manually and on different surfaces. The modification stretches the length of the chassis and replaces the caster wheels with free-spinning front and rear wheels. The powered wheels are centered front to back and are slightly dropped. This is a configuration historically used in FIRST Robotics Competition robots before the rise of the swerve drive.

XRP Tank Chassis on a robot

As a mentor of an FRC, I was looking for projects to emulate the larger robots with mechanisms similar to those commonly used in competition. It made sense to have a chassis that would behave similarly to the larger robots. Here is an example robot that uses the tank chassis as a base for a small-scale FRC Rebuilt-style robot. As it is still an XRP component, any mechanisms could be added to the chassis.

メーカー品番 28009
EXPERIENTIAL ROBOTICS PLATFORM (
SparkFun Electronics
メーカー品番 28013
EXPERIENTIAL ROBOTICS PLATFORM (
SparkFun Electronics
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.