Maker.io main logo

Update BlueIO firmware using RaspberryPi

31

2021-09-28 | By Sheikh Shuhad

License: GNU Lesser General Public License Raspberry Pi SBC

The BleuIO comes with a bootloader to allow you to update the firmware or flash your own application to the dongle. To flash the dongle, you will need an image file containing the new firmware or your own application and a host USB loader application.

You can download the latest firmware, and host USB loader from our getting started guide.

This article will explain how to update a BleuIO dongle using a RaspberryPi.

Connect the BleuIO dongle to your Linux / RaspberryPi.

bleuio%20dongle%20on%20raspberry%20pi

To identify which device name the dongle is connected to, you will need to run ls /dev on the terminal.You might need to do it twice, once before you connect the dongle and once after, to be able to identify which one is the device name.

The following screenshot shows devices list before and after connecting the dongle.

devices

BleuIO includes a bootloader that allows you to update the firmware easily. When starting up, the dongle will open a COM port for the bootloader for 10 seconds to allow you to update the firmware (or flash your own application). Afterwards, it will close that port and open a new port for the BleuIO application. 

Now that you know the device name, you can run the following command to update the dongle. 

sudo ./host_usb_updater /dev/ttyACM0 ./example_firmware.img -verbose 

The /dev/ttyACM0 means USB-CDC driver of Linux.

NOTE: The device name may vary and may not be the same as in the picture above.

After running this command successfully, you should see Result: Pass on your terminal.  

success

メーカー品番 SSD005/4-V2W
BLUETOOTH 5 LOW ENERGY USB DONGL
Smart Sensor Devices
メーカー品番 SSD005/4-V2B
BLUETOOTH 5 LOW ENERGY USB DONGL
Smart Sensor Devices
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.