Maker.io main logo

SparkFun MicroMod Input and Display Carrier Board Hookup Guide

55

2024-09-03 | By SparkFun Electronics

License: See Original Project Displays LEDs / Discrete / Modules MicroMod Qwiic

Courtesy of SparkFun

Guide by Alex the Giant, Ell C

Introduction

Introducing the SparkFun MicroMod Input and Display Carrier Board! This nifty little board works ‎with all SparkFun MicroMod processors so you can create your own display with one of a multitude ‎of processors.‎

The carrier board includes 6 APA102 Addressable LEDs, 6 Input Buttons, Onboard Voltage ‎Regulation, 2.4" TFT Display Screen, IO Connector, and a Buzzer. In addition, there's a microSD ‎card slot to store and read data.‎

Let's dive in and see what we can do!‎

 

Required Materials

Like all of our MicroMod Carrier Boards, there is no processor included but instead you can plug in ‎a processor board of your choice to the MicroMod M.2 connector on the carrier. Below are a few ‎options to choose for your processor:‎

You'll also need a USB-C cable to connect the Carrier to your computer and if you want to add ‎some Qwiic breakouts to your MicroMod project you'll want at least one Qwiic cable to connect it all ‎together. Below are some options for both of those cables:‎

Along with a processor and the pertinent cables and accessories, if you want to take full advantage ‎of the features of the Input and Display Carrier Board, you will need a microSD card:‎

  • microSD Card - 16GB (Class 10)

Suggested Reading

The SparkFun MicroMod ecosystem is a unique way to allow users to customize their project to ‎their needs. Do you want to send your data via a wireless signal (e.g., Bluetooth or WiFi)? There's a ‎MicroMod processor for that. Looking to instead maximize efficiency and processing power? You ‎guessed it, there's a MicroMod processor for that. If you are not familiar with the MicroMod system, ‎take a look here:‎

micromod

MicroMod Ecosystem

We also recommend taking a look through the following tutorials if you are not familiar with the ‎concepts covered in them:‎

  • Getting Started with MicroMod: Dive into the world of MicroMod - a compact interface to connect a microcontroller to various ‎peripherals via the M.2 Connector!‎

  • Designing with MicroMod: This tutorial will walk you through the specs of the MicroMod processor and carrier board as well as ‎the basics of incorporating the MicroMod form factor into your own PCB designs!‎

  • MicroMod ESP32 Processor Board Hookup Guide: A short hookup guide to get started with the SparkFun MicroMod ESP32 Processor Board.‎

Hardware Overview

In this section we'll cover the various hardware and sensors included on the MicroMod Input & ‎Display Carrier Board.‎

Common Components

Most SparkFun MicroMod Carriers will have some common components and all MicroMod Carriers ‎will have the keyed M.2 MicroMod Connector to plug your processor into. The photo and list below ‎outline some of the components you can expect on most SparkFun MicroMod Carriers.‎

  • M.2 MicroMod Connector - This special keyed M.2 connector lets you install your MicroMod ‎Processor of choice on your Input & Display Carrier Board

  • USB-C Connector - Connect to your computer to program your Processor and also can ‎provide power to your MicroMod system

  • 3.3V Regulator - Provides a regulated 3.3V and sources up to 1A

  • Qwiic Connector - The standard Qwiic connector so you can add other Qwiic devices to your ‎MicroMod system

  • Boot/Reset Buttons - Push buttons to enter Boot Mode on Processor boards and to Reset ‎your MicroMod circuit. More information needed - LAC

  • microSD Slot - Insert a microSD card for reading and writing data

board_2

Power

The Input and Display Carrier Board takes an input voltage range from 2.7V - 6V via the USB-C ‎connector. We've incorporated a power regulation circuit that caps the voltage for power sensitive ‎circuits and the Qwiic connector.‎

Input & Display Carrier Board Specific Components

ATTiny84‎

We've populated this carrier board with Atmel's ATtiny84 with 8kB of programmable flash. This little ‎guy is preprogrammed to communicate with the processor over I2C to read button presses.‎

tiny_3

TFT Display

‎4DLCD's 24320240-IPS is a color active-matrix LCD module incorporating amorphous silicon TFT ‎‎(Thin Film Transistor). The module display area measures 2.4" and contains 240 x 320 pixels.‎

Note: IPS displays have higher display quality, better colors, and much better viewing angles than ‎their non-IPS counterparts.‎

display_4

LEDs

The Input and Display Carrier Board has 6 Addressable APA102 LEDs.

leds_5

Input Buttons

Button button, who's got the button? We do! We have two input buttons (A and B), and a 5 way ‎switch that allows you to navigate a UI or play an onboard game.

buttons_6

JTAG Debugging

We've populated the JTAG footprint for more advanced users who need breakpoint level ‎debugging. We recommend checking out our JTAG section for the compatible JTAG programmer ‎and debugger.‎

debug_7

Jumpers

jumpers_8

I2C Jumper

If you are daisy chaining multiple Qwiic devices, you will want to cut this jumper; if multiple sensors ‎are connected to the bus with the pull-up resistors enabled, the parallel equivalent resistance could ‎create too strong of a pull-up for the bus to operate correctly. As a general rule of thumb, disable all ‎but one pair of pull-up resistors if multiple devices are connected to the bus. To disable the pull up ‎resistors, use an X-acto knife to cut the joint between the two jumper pads highlighted below.‎

PWR Jumper

Cutting this jumper will disable the "Power" LED on the front of the board.‎

‎3V3CTRL Jumper‎

Many of the MicroMod carrier boards have an RTC backup battery on board and as part of the ‎standardized voltage regulation circuit we include a 3V3 jumper that, when closed, allows you to ‎control the 3V3 control regulator. This shuts down everything on the 3V3 rail, but the battery keeps ‎the processor awake. The Input and Display Carrier Board does not have a backup battery, so this ‎jumper should remain open.‎

BYP Jumper

If you really, really, REALLY need more power, closing this jumper will bypass the 2A fuse. Close at ‎your own risk!‎

Measure Jumper

Want to measure the juice running through your circuits? Cut the trace between these PTH pads in ‎order to measure the current with a Digital Multimeter.‎

PinOuts

Note: You may not recognize the COPI/CIPO labels for SPI pins. SparkFun is working to move ‎away from using MISO/MOSI to describe signals between the controller and the peripheral. Check ‎out this page for more on our reasoning behind this change.‎

INPUT & DISPLAY CARRIER BOARD PINOUT TABLE

table_9

MICROMOD GENERAL PINOUT TABLE

table_10

MICROMOD GENERAL PIN DESCRIPTIONS

table_11

Board Dimensions

The Input and Display Carrier Board measures 3.25 inches by 2.25 inches.

dimensions_12

Hardware Hookup

To get started with the Input and Display Carrier Board, you'll need a processor board. Here we are ‎using the MicroMod ESP32 Processor Board.‎

Align the top key of the MicroMod ESP32 Processor Board to the screw terminal of the Input and ‎Display Carrier Board and angle the board into the socket. Insert the board at an angle into the M.2 ‎connector.‎

Note: There is no way to insert the processor backward since the key prevents it from mating with ‎the M.2 connector and as an extra safeguard to prevent inserting a processor that matches the key, ‎the mounting screw is offset so you will not be able to secure an improperly connected processor ‎board.‎

align_13

The Processor Board will stick up at an angle, as seen here:

stick_14

Once the board is in the socket, gently hold the MicroMod Processor Board down and tighten the ‎screw with a Phillip's head.‎

tighten_15

Once the board is secure, your assembled MicroMod system should look similar to the image below!‎

assembled_16

Connecting Everything Up

With your processor inserted and secured it's time to connect your carrier board to your computer ‎using the USB-C connector on the Carrier. Depending on which carrier you choose and which ‎drivers you already have installed, you may need to install drivers.‎

Note: Make sure that for whatever processor board you choose, you have the correct board ‎definitions installed. ‎

For this particular tutorial, we are using the MicroMod ESP32 Processor Board. Board definitions ‎for this processor board can be found in the Software Setup and Programming section of ‎the MicroMod ESP32 Processor Board Hookup Guide. ‎

If you are using a different processor board, go to our MicroMod Processor Boards landing page, ‎find your processor board, and head on over to that tutorial for help installing your board definition.‎

Software Setup and Programming

Note: This example assumes you are using the latest version of the Arduino IDE on your desktop. ‎If this is your first time using Arduino, please review our tutorial on installing the Arduino IDE. If you ‎have not previously installed an Arduino library, please check out our installation guide.

To get started, you're going to want to get familiar with our HyperDisplay libraries. HyperDisplay is ‎an abstracted library for pretty much any 2D graphics display and has a focus on extensibility. Since ‎the interface is standardized, you can write display applications just once and make them work on ‎many different displays with a few small changes. If you want to go more in depth check out this ‎HyperDisplay tutorial.‎

hyper_17

Everything You Should Know About HyperDisplay

‎This is a tutorial to go in-depth about the SparkFun HyperDisplay Arduino Library.‎

To use HyperDisplay with this carrier board, you will need to have all three of the following libraries ‎installed in your Arduino IDE. You can head on over to the individual GitHub pages to download or ‎simply click the appropriate link for each of the libraries listed below:‎

table_18

HyperDisplay GitHub

HyperDisplay Download

SparkFun HyperDisplay ILI9341 Arduino Library GitHub

SparkFun HyperDisplay ILI9341 Arduino Library Download

HyperDisplay 4DLCD-320240 Arduino Library GitHub

HyperDisplay 4DLCD-320240 Arduino Library Download

Check out this tutorial on how to install an Arduino library if you are unfamiliar.‎

Each of the libraries above contain some examples, however the ones that will actually make your ‎Input and Display Carrier Board light up are contained in the 'HyperDisplay 4DLCD-320240 Arduino ‎Library' -- in case you are wondering, that name comes from the name of the display module that is ‎used on the board. Once your libraries have been installed move on to the next section and try out ‎a few of the examples.‎

Example Code

The HyperDisplay library for the Input and Display Carrier Board is named after the LCD module ‎that it uses - the 4DLCD-320240. If you've properly installed the required libraries, you'll notice a ‎number of examples in File->Examples->SparkFun HyperDisplay 4DLCD-320240. If you haven't ‎already, make sure you've got the following three libraries installed:‎

You will also need to make sure that you have the board definitions for your chosen processor ‎board installed. ‎

For this particular tutorial, we are using the MicroMod ESP32 Processor Board. Board definitions ‎for this processor board can be found in the Software Setup and Programming section of ‎the MicroMod ESP32 Processor Board Hookup Guide.‎

All of the following examples are explained in depth in the Everything You Should Know About ‎HyperDisplay Tutorial. We'll show you a quick overview of each example here, but if you want more ‎information on how these examples and their code work, head on over to the HyperDisplay Tutorial.‎

hyper_17

Everything You Should Know About HyperDisplay

This is a tutorial to go in-depth about the SparkFun HyperDisplay Arduino Library.‎

Note: The display's colors are inverted from the standard ILI9341 driver library. If you're using the ‎HyperDisplay libraries, this is taken care of in the HyperDisplay 4DLCD-320240. But if you prefer ‎using a different ILI9341 library, no hard feelings, but you will have to run that library's invert ‎display function in order for the colors to display like you expect.

Example 1: Display Test

Example one verifies that your display is working and gives you some basic code to draw lines and ‎shapes. To start, go to File->Examples->SparkFun HyperDisplay 4DLCD-320240 and ‎load Example1_DisplayTest. In windows, it will look like this:‎

test_19

Make sure you have the correct board selected, as well as the correct COM port. Your processor ‎board of choice will dictate which board definition you need to load.‎

MicroMod_Input_Display_Carrier_Board_Update_1

Example 2: HyperDisplay Basics

This code walks you through the simplest uses of HyperDisplay so that you can start to write your ‎own code. To start, go to File->Examples->SparkFun HyperDisplay 4DLCD-320240 and ‎load Example2_HyperDisplayBasics.‎

menu_20

As with Example 1, please make sure you have the correct board selected, as well as the correct ‎COM port. Go ahead and upload your code, and you should see something like the following (note ‎that the gif is sped up):‎

MicroMod_Input_Display_Carrier_Board_Update_2

Example 3: Advanced HyperDisplay

Example 3 goes over Color Cycles and the drawing functions currently available in the HyperDisplay ‎drawing functions. For a more in-depth look at the functions available in this example, refer to ‎the Advanced Drawing Functions section of the Everything You Should Know About ‎HyperDisplay tutorial.‎

To start, go to File->Examples->SparkFun HyperDisplay 4DLCD-320240 and ‎load and ‎load Example4_BufferingHyperDisplay.

load_21

As above, please make sure you have the correct board selected, as well as the correct COM port. ‎Go ahead and upload your code. You should see something like the following (note that the gif is ‎sped up):‎ ‎

MicroMod_Input_Display_Carrier_Board_3

Example 4: Buffering HyperDisplay

This last example shows you the basics of how to use the buffering abilities of HyperDisplay. You ‎can get more in-depth discussion of this by referring to the Buffering section of the Everything You ‎Should Know About HyperDisplay tutorial.‎

To start, go to File->Examples->SparkFun HyperDisplay 4DLCD-320240 and ‎load Example4_BufferingHyperDisplay.‎‎

buffering_22

As above, please make sure you have the correct board selected, as well as the correct COM port. ‎Go ahead and upload your code. You should see something along the lines of the following (note ‎that the gif is sped up):‎

MicroMod_Input_Display_Carrier_Board_4

Troubleshooting

Not working as expected and need help? ‎

If you need technical assistance and more information on a product that is not working as you ‎expected, we recommend heading on over to the SparkFun Technical Assistance page for some ‎initial troubleshooting.

SPARKFUN TECHNICAL ASSISTANCE PAGE‎ ‎

If you don't find what you need there, the SparkFun Forums: MicroMod are a great place to find ‎and ask for help. If this is your first visit, you'll need to create a Forum Account to search product ‎forums and post questions.

SPARKFUN FORUMS: MICROMOD

Resources and Going Further

For more information about the MicroMod Input and Display Carrier, check out the following links:‎

For more information about the SparkFun MicroMod Ecosystem, take a look at the links below:‎

メーカー品番 16985
MICROMOD INPUT/DISPLAY CARRIER
SparkFun Electronics
メーカー品番 16781
MICROMOD ESP32 PROCESSOR
SparkFun Electronics
メーカー品番 16401
MICROMOD ARTEMIS PROCESSOR
SparkFun Electronics
メーカー品番 16791
MICROMOD SAMD51 PROCESSOR
SparkFun Electronics
メーカー品番 15081
QWIIC CABLE KIT
SparkFun Electronics
メーカー品番 15424
CBL USB2.0 A PLUG TO C PLG 6.56'
SparkFun Electronics
メーカー品番 14743
CABLE A PLUG TO C PLUG 3.28'
SparkFun Electronics
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.