Maker.io main logo

Simple Raspberry Pi Robot

281

2024-11-05 | By Adafruit Industries

License: See Original Project Robot Kits Raspberry Pi SBC

Courtesy of Adafruit

Guide by Tony DiCola

Overview

robot_1

This is a fun project to build a simple robot using the Raspberry Pi ‎and Adafruit's awesome robot chassis kit. This robot is one of the ‎simplest robots you can build and uses two DC motors to control a ‎pair of wheels. A swivel caster in the front holds the robot up, and ‎the Raspberry Pi with motor HAT controls the motors. ‎

There are no sensors or other inputs to the robot, it will just follow a ‎set of instructions in Python code that tell the robot how to ‎move. Use this project as a starting point for your own amazing ‎Raspberry Pi robot projects! You could add sensors to detect objects ‎around the Pi, add a camera to get a robot's eye view of the world, or ‎even connect the robot to web services that control its actions--‎there's almost no limit to what you can do with this amazing robot!‎

To build this project it will help to familiarize yourself with using the ‎Raspberry Pi. Follow these great learn Raspberry Pi guides to learn ‎the basics. You will also want to review the motor HAT guide, and ‎skim the Bluefruit LE feather robot guide to learn more about the ‎robot chassis.‎

Text editor powered by tinymce.‎

Hardware

parts_2

Parts

You'll need the following parts to build this robot:‎

Raspberry Pi Setup

You'll want to make sure your Raspberry Pi is running the latest ‎version of the Raspbian Jessie operating system. In addition, the Pi ‎will need access to the internet through a wired or wireless network ‎connection so it can download necessary software.‎

If you're new to the Raspberry Pi be sure to follow a few getting ‎started guides to learn how to load an operating system on the ‎Pi, setup a wired or wireless network connection, and connect to its ‎command line terminal.‎

Motor HAT

Start the project by following the motor HAT guide to assemble and ‎test the HAT. Make sure you can install the motor HAT software and ‎test each DC motor to verify it spins. It's much easier to troubleshoot ‎issues with the HAT and motors when it's outside the robot chassis!‎

Once you've assembled and checked the motor HAT works, continue ‎on to learn how to put together the robot.‎

Text editor powered by tinymce.‎

Assembly

Follow the steps below to build the robot. It will help to also skim ‎the Bluefruit LE feather robot guide to see more pictures of ‎assembling the robot chassis. There are a few small differences in ‎the assembly of the Pi robot that will be noted below.‎

Start by screwing the DC motors to the back of the chassis (i.e., the ‎end farther away from the angled front). Make sure the motors have ‎the same orientation, with the side that the wire exits facing forward.‎

Next screw in the caster to the center mounting holes.‎

Assemble the wheels by stretching the tires onto the hubs, then ‎push the wheel into place on the motor head and screw it in.‎

You can feed the DC motor wires up through the angled mounting ‎slots in the chassis.‎

assembly_3

Flip the robot over so it stands on its wheels.‎

Cut out a small square of cardboard that's about the same size as ‎the Raspberry Pi. This cardboard will protect the bottom of the Pi ‎from touching the metal robot chassis and shorting out. It's very ‎important to prevent the bottom of the Pi from touching the ‎metal chassis or you could damage the Pi!‎

Screw the top plate standoffs into the mounting holes near the ‎center of the chassis (flanking where the angled mounting slots ‎meet).‎

assembly_4

Place the Pi on the cardboard and position it so the Pi's rear ‎mounting holes (near the USB ports) are directly above the long ‎mounting slot at the back of the chassis. Use the #4-40 machine ‎screws and nuts to screw through the Pi and cardboard to securely ‎hold the Pi in place.‎

assembly_5

If you aren't using Pi HAT standoffs to hold the motor HAT place a ‎piece of electrical tape across the HDMI connector side of the ‎Pi. This will help prevent the motor HAT from getting pushed down ‎into the connectors and shorting out. If you are using the standoffs, ‎you can place them over the front mounting holes of the Pi (not ‎shown).‎

assembly_6

If you haven't already done so, click here to head over to the Motor ‎Hat assembly instructions!‎

Push the motor HAT into place on the Pi's GPIO connector. Screw ‎down the standoffs if being used to hold the HAT.

assembly_7

Connect the DC motors to the motor HAT as shown to the left.

The left (or 'driver side' for US/right side of the road drivers) DC motor ‎should be connected to port M1 on the motor HAT. The right (or ‎‎'passenger side') DC motor should be connected to port M2 on the ‎motor HAT. ‎

The black motor wire connects to the left screw terminal of the port, ‎and the red motor wire connects to the right screw terminal of the ‎port. The middle GND screw terminal is unused.‎

assembly_8

Connect the 4x AA battery pack red wire to the +/positive power ‎screw terminal on the HAT, and the black wire to the -/negative ‎power screw terminal.‎

Finish the robot by screwing the top plate firmly to the standoffs in ‎the center. Use double sided foam tape or electrical tape to hold the ‎‎4xAA battery pack to the top plate, and the USB battery pack to the ‎front of the robot.‎

assembly_9

Woo hoo, that's all there is to building the bot! Your robot should ‎look something like the pictures to the left.‎

Continue on to learn about simple Python software to make the ‎robot move.‎

assembly_10

assembly_11

Text editor powered by tinymce.‎

Software

The software for this project is actually included in the Adafruit ‎CircuitPython MotorKit library examples. There's ‎a motorkit_robot_test.py script that tells the robot to move forward, ‎backward, and turn in different directions. This script uses a little ‎helper class in motorkit_robot.py that talks to the motor HAT and ‎exposes simple functions to move the robot.‎

Make sure you've followed the motor HAT guide software installation.‎

Download Example Files

The installation of the library does not include the examples. So, you ‎will want to grab those manually. You can use the links below to ‎download them. Be sure to save both of these into the same ‎directory.‎

motorkit_robot.py

motorkit_robot_test.py

You can also download the files directly to your device using wget:‎

Copy Code
wget https://raw.githubusercontent.com/adafruit/Adafruit_CircuitPython_MotorKit/master/examples/motorkit_robot.py
wget https://raw.githubusercontent.com/adafruit/Adafruit_CircuitPython_MotorKit/master/examples/motorkit_robot_test.py

Run Example

To run the robot code first make sure the 4x AA battery pack ‎connected to the motor HAT is powered on. Then place the robot on ‎the floor where there are no obstructions around it for a few ‎feet. Remember this is a simple robot that has no sensors to ‎know if it's hitting something or about to fall off a table! Be very ‎careful to ensure the path of the robot is free and safe to travel!‎

When the motorkit_robot_test.py script runs it will instruct the robot to ‎move. So, make sure the coast is clear. When you've ensured the ‎path of the robot is clear run the following command to run the ‎robot code:‎

Copy Code
python3 motorkit_robot_test.py

Be ready to pick up the bot or flip off its motor power supply in ‎case it comes close to hitting something or falling!‎

Woo hoo, you should see the robot start to move around! If you see ‎an error message check that you've followed all of the steps above ‎and in the motor HAT guide to install the software. Try testing each ‎motor individually with the motor HAT guide DC motor test ‎software to make sure they can spin.‎

Note that if the robot spins instead of moving forward you likely have ‎the motors connected incorrectly. Try swapping the order of the ‎connections and testing again. You can flip the robot over and ‎watch the wheels move to check that they both move in the same ‎direction when moving forward, and they move in opposite ‎directions when turning.‎

Customizing

The example is very simple. The real fun comes from writing code to ‎make the robot do what YOU want. Start by making a copy of ‎the motorkit_robot_test.py script and open it in an editor, like nano.‎

Open your script in a text editor and look for these lines:‎

‎Download File

Copy Code
robot.left(0.5, 1)
robot.right(0.5, 1)
robot.steer(0.5, 0.2)
time.sleep(3)
robot.stop()  # Stop the robot from moving.

Those are the basic move commands. You can change those up as ‎you want. Add more, etc.‎

As described in the code comment above them, each takes two ‎parameters. The first one is the speed of the movement. Speed ‎should be a value between 0 and 255. The higher the value the ‎faster the movement. Note that you'll need to start with a value ‎around 75-100 or so to move the motors with enough torque to get ‎the robot started.‎

The second parameter is the amount of time (in seconds) to perform ‎the action. For example, a call to robot.forward(150, 1.0) will move ‎the robot forward at a speed of 150 for 1.0 second.‎

Another way to use the functions is to just pass the first parameter, ‎the speed, to them. This will start the robot moving and then return ‎to your script so you can do other things. For example:‎

Download File

Copy Code
# Spin in place slowly for a few seconds.
robot.right(100)  # No time is specified so the robot will start spinning forever.
time.sleep(2.0)   # Pause for a few seconds while the robot spins (you could do
                  # other processing here though!).
robot.stop()      # Stop the robot from moving.

In the snippet above the robot will start spinning to the right at a ‎speed of 100, then the code will sleep for 2 seconds, and finally stop ‎the robot. Instead of sleeping you could perform other actions ‎though, like reading sensors, talking to web services, etc--the sky is ‎the limit as far as what you can do with the robot & Python code!‎

Text editor powered by tinymce.

メーカー品番 2939
MINI ROBOT ROVER CHASSIS KIT
Adafruit Industries LLC
メーカー品番 2348
DC STEP MTR HAT FOR RASPBERRY PI
Adafruit Industries LLC
メーカー品番 SC1029
SBC 900MHZ 4 CORE 1GB RAM
Raspberry Pi
メーカー品番 SC0563
SBC 1GHZ 1 CORE 512MB RAM
Raspberry Pi
メーカー品番 SC0562
SBC 1GHZ 1 CORE 512MB RAM
Raspberry Pi
メーカー品番 2336
BRASS M2.5 STANDOFFS FOR PI HATS
Adafruit Industries LLC
メーカー品番 830
BATTERY HOLDER AA 4 CELL LEADS
Adafruit Industries LLC
メーカー品番 153
JUMPER WIRE M TO M VARIOUS
Adafruit Industries LLC
メーカー品番 136
LADYADAS ELECTRONICS TOOLKIT
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.