Maker.io main logo

Qualia S3 Space Clock

125

2024-03-19 | By Adafruit Industries

License: See Original Project Displays LCD / TFT

Courtesy of Adafruit

Guide by Liz Clark

Overview

David Bowie asked if there was life on Mars, but what about time? ‎With this project, you can easily switch between viewing your local ‎time on Earth and coordinated Mars time (MTC) on a beautiful round ‎‎720x720 display housed in a retro space-themed orb enclosure.‎

 

The display shows a classic analog clock face for viewing the time. ‎Hour and minute hands are created with vectorio polygons in ‎CircuitPython.‎

display_1

An arcade button mounted to the back of the clock lets you switch ‎between Earth and Mars time.‎

button_2

Inspired by mid-century modern clocks, this 3D printed enclosure ‎embodies a space-age retro aesthetic. The base features beautiful ‎curves that blend the neck to the wide base. The display is mounted ‎to a spherical dome that's tilted 15 degrees for the best viewing ‎angle. The display can swivel slightly, allowing the user to adjust it.‎

3d_3

The base features an opening for the USB-C port, two user buttons, ‎and a reset button.‎

base_4

Prerequisite Guides

Take a moment to review the following guides to learn more about ‎the products.‎

Parts

parts_5

Hardware

Required screws and nuts for assembly.‎

  • ‎4x M2.5 x 6mm long pan head machine screw‎

hardware_6

hardware_7

Circuit Diagram

The diagram below provides a general visual reference for wiring of ‎the components once you get to the Assembly page. This diagram ‎was created using the software package Fritzing.‎

Adafruit Library for Fritzing

Adafruit uses the Adafruit's Fritzing parts library to create circuit ‎diagrams for projects. You can download the library or just grab ‎individual parts. Get the library and parts from GitHub - Adafruit ‎Fritzing Parts.‎

diagram_8

Wired Connections

The Qualia ESP32-S3 is powered by a 5V 1A USB power supply.‎

  • The arcade button connects to the Qualia ESP32-S3 using a 3-‎pin JST Stemma cable.‎

CircuitPython

CircuitPython is a derivative of MicroPython designed to simplify ‎experimentation and education on low-cost microcontrollers. It ‎makes it easier than ever to get prototyping by requiring no upfront ‎desktop software downloads. Simply copy and edit files on ‎the CIRCUITPY drive to iterate.‎

CircuitPython Quickstart

Follow this step-by-step to quickly get CircuitPython running on your ‎board.‎

This microcontroller requires the latest unstable ‎‎(development) release of CircuitPython. Click below to visit the ‎downloads page on circuitpython.org for your board. Then, ‎Browse S3 under Absolute Newest.‎

Download the latest version of CircuitPython for this board via ‎circuitpython.org

Click the link above to download the latest CircuitPython UF2 file.‎

Save it wherever is convenient for you.‎

file_9

The Qualia S3 does not have a RGB status LED.‎

board_10

Plug your board into your computer, using a known-good data-sync ‎cable, directly, or via an adapter if needed.‎

Double-click the reset button (highlighted in red above), and you ‎will see the RGB status LED(s) turn green (highlighted in green ‎above). If you see red, try another port, or if you're using an adapter ‎or hub, try without the hub, or different adapter or hub.‎

This board does not have a Neopixel, so you will need to just double ‎tap the reset button.‎

For this board, tap reset and wait about a half a second and then tap ‎reset again.‎

Some boards may not have a UF2 bootloader installed. If double-‎clicking does not work, follow the instructions on the "Install UF2 ‎Bootloader" page in this guide.‎

If double-clicking doesn't work the first time, try again. Sometimes it ‎can take a few tries to get the rhythm right!‎

A lot of people end up using charge-only USB cables and it is very ‎frustrating! Make sure you have a USB cable you know is good for ‎data sync.‎

You will see a new disk drive appear called TFT_S3BOOT.‎‎

‎Drag the adafruit_circuitpython_etc.uf2 file to TFT_S3BOOT.‎

drag_11

drag_12

The BOOT drive will disappear, and a new disk drive ‎called CIRCUITPY will appear.

‎That's it!‎

boot_13

Create Your settings.toml File

CircuitPython works with WiFi-capable boards to enable you to ‎make projects that have network connectivity. This means working ‎with various passwords and API keys. As of CircuitPython 8, there is ‎support for a settings.toml file. This is a file that is stored on ‎your CIRCUITPY drive, which contains all of your secret network ‎information, such as your SSID, SSID password and any API keys for ‎IoT services. It is designed to separate your sensitive information ‎from your code.py file so you are able to share your code without ‎sharing your credentials.‎

CircuitPython previously used a secrets.py file for this purpose. ‎The settings.toml file is quite similar.‎

Your settings.toml file should be stored in the main directory of your ‎CIRCUITPY drive. It should not be in a folder.‎

CircuitPython settings.toml File

This section will provide a couple of examples of what ‎your settings.toml file should look like, specifically for CircuitPython ‎WiFi projects in general.‎

The most minimal settings.toml file must contain your WiFi SSID ‎and password, as that is the minimum required to connect to WiFi. ‎Copy this example, paste it into your settings.toml, and update:‎

  • your_wifi_ssid

  • your_wifi_password

Download File

Copy Code
CIRCUITPY_WIFI_SSID = "your_wifi_ssid"
CIRCUITPY_WIFI_PASSWORD = "your_wifi_password"

Many CircuitPython network-connected projects on the Adafruit ‎Learn System involve using Adafruit IO. For these projects, you ‎must also include your Adafruit IO username and key. Copy the ‎following example, paste it into your settings.toml file, and update:‎

  • your_wifi_ssid

  • your_wifi_password

  • your_aio_username

  • your_aio_key

Download File

Copy Code
CIRCUITPY_WIFI_SSID = "your_wifi_ssid"
CIRCUITPY_WIFI_PASSWORD = "your_wifi_password"
ADAFRUIT_AIO_USERNAME = "your_aio_username"
ADAFRUIT_AIO_KEY = "your_aio_key"

Some projects use different variable names for the entries in ‎the settings.toml file. For example, a project might ‎use ADAFRUIT_AIO_ID in the place of ADAFRUIT_AIO_USERNAME. If you run into ‎connectivity issues, one of the first things to check is that the ‎names in the settings.toml file match the names in the code.‎

Not every project uses the same variable name for each entry in the ‎settings.toml file! Always verify it matches the code.‎

settings.toml File Tips

Here is an example settings.toml file.‎

Download File

Copy Code
# Comments are supported
CIRCUITPY_WIFI_SSID = "guest wifi"
CIRCUITPY_WIFI_PASSWORD = "guessable"
CIRCUITPY_WEB_API_PORT = 80
CIRCUITPY_WEB_API_PASSWORD = "passw0rd"
test_variable = "this is a test"
thumbs_up = "\U0001f44d"

In a settings.toml file, it's important to keep these factors in mind:‎

  • Strings are wrapped in double quotes; ex: "your-string-here"‎

  • Integers are not quoted and may be written in decimal with ‎optional sign (+1, -1, 1000) or hexadecimal (0xabcd).‎

    • Floats, octal (0o567) and binary (0b11011) are not supported.‎

  • Use \u escapes for weird characters, \x and \ooo escapes are not ‎available in .toml files

    • Example: \U0001f44d for 👍 (thumbs up emoji) ‎and \u20ac for € (EUR sign)‎

  • Unicode emoji, and non-ASCII characters, stand for themselves ‎as long as you're careful to save in "UTF-8 without BOM" format‎ ‎ ‎‎ ‎

When your settings.toml file is ready, you can save it in your text ‎editor with the .toml extension.‎

settings_14

Accessing Your settings.toml Information ‎in code.py

In your code.py file, you'll need to import the os library to access ‎the settings.toml file. Your settings are accessed with ‎the os.getenv() function. You'll pass your settings entry to the function ‎to import it into the code.py file.‎

Download File

Copy Code
import os

print(os.getenv("test_variable"))

code_15

In the upcoming CircuitPython WiFi examples, you'll see how ‎the settings.toml file is used for connecting to your SSID and ‎accessing your API keys.‎

Code the Clock

Once you've finished setting up your Qualia ESP32-S3 with ‎CircuitPython, you can access the code and necessary libraries by ‎downloading the Project Bundle.‎

To do this, click on the Download Project Bundle button in the ‎window below. It will download to your computer as a zipped folder.‎

Download Project Bundle

Copy Code
# SPDX-FileCopyrightText: 2023 Liz Clark for Adafruit Industries
#
# SPDX-License-Identifier: MIT

# Written by Liz Clark (Adafruit Industries) with OpenAI ChatGPT v4 Aug 3rd, 2023 build
# https://help.openai.com/en/articles/6825453-chatgpt-release-notes

# https://chat.openai.com/share/63cbe4c6-007f-4934-a458-a9c8a521620e
# https://chat.openai.com/share/674c0f13-bc78-4d1e-be79-3bc777e29991

import time
from math import pi, cos, sin
import os
import ssl
import wifi
import socketpool
import adafruit_requests
import board
from adafruit_ticks import ticks_ms, ticks_add, ticks_diff
import vectorio
import displayio
from adafruit_io.adafruit_io import IO_HTTP
from jepler_udecimal import Decimal
import keypad
from adafruit_display_text import label
from adafruit_bitmap_font import bitmap_font
from adafruit_qualia.graphics import Graphics, Displays

# timezone offset for calculating mars time
timezone = -5

key = keypad.Keys((board.A0,), value_when_pressed=False, pull=True)

wifi.radio.connect(os.getenv("CIRCUITPY_WIFI_SSID"), os.getenv("CIRCUITPY_WIFI_PASSWORD"))
print(f"Connected to {os.getenv('CIRCUITPY_WIFI_SSID')}")

aio_username = os.getenv('ADAFRUIT_AIO_USERNAME')
aio_key = os.getenv('ADAFRUIT_AIO_KEY')

context = ssl.create_default_context()
pool = socketpool.SocketPool(wifi.radio)
requests = adafruit_requests.Session(pool, context)
io = IO_HTTP(aio_username, aio_key, requests)

earth_bitmap = displayio.OnDiskBitmap("/earth.bmp")
mars_bitmap = displayio.OnDiskBitmap("/mars.bmp")

graphics = Graphics(Displays.ROUND40, default_bg=None, auto_refresh=True)

earth_grid = displayio.TileGrid(earth_bitmap, pixel_shader=earth_bitmap.pixel_shader)
earth_group = displayio.Group()
earth_group.append(earth_grid)

mars_grid = displayio.TileGrid(mars_bitmap, pixel_shader=mars_bitmap.pixel_shader)
mars_group = displayio.Group()
mars_group.append(mars_grid)

def center(grid, bitmap):
    # center the image
    grid.x -= (bitmap.width - graphics.display.width) // 2
    grid.y -= (bitmap.height - graphics.display.height) // 2

center(mars_grid, mars_bitmap)
center(earth_grid, earth_bitmap)

graphics.display.root_group = mars_group

# pointer using vectorio, first the hub
pointer_pal = displayio.Palette(4)
pointer_pal[0] = 0xff0000
pointer_pal[1] = 0x000000
pointer_pal[2] = 0x0000ff
pointer_pal[3] = 0xffffff
pointer_hub = vectorio.Circle(pixel_shader=pointer_pal, radius=26, x=0, y=0)
pointer_hub.x = graphics.display.width // 2
pointer_hub.y = graphics.display.height // 2

# minute hand
mw = 23
mh = 225
min_points = [(mw,0), (mw,-mh), (-mw,-mh), (-mw,0)]
min_hand = vectorio.Polygon(pixel_shader=pointer_pal, points=min_points, x=0,y=0)
min_hand.x = graphics.display.width // 2
min_hand.y = graphics.display.height // 2
mars_group.append(min_hand)
earth_group.append(min_hand)
# hour hand
hw = 25
hh = 175
hour_points = [(hw,0), (hw,-hh), (-hw,-hh), (-hw,0)]
hour_hand = vectorio.Polygon(pixel_shader=pointer_pal, points=hour_points,
                             x=0, y=0, color_index=1)
hour_hand.x = graphics.display.width // 2
hour_hand.y = graphics.display.height // 2
mars_group.append(hour_hand)
earth_group.append(hour_hand)

# add numbers to the clock face
def calculate_number_position(number, center_x, center_y, radius):
    angle = (360 / 12) * (number - 3)  # -3 adjusts the angle to start at 12 o'clock
    rad_angle = pi * angle / 180
    if number >=8:
        x = int(center_x + cos(rad_angle) * radius-40)
    x = int(center_x + cos(rad_angle) * radius)
    y = int(center_y + sin(rad_angle) * radius)
    return x, y

clock_face_numbers = {i: calculate_number_position(i, graphics.display.width // 2,
                        graphics.display.height // 2, 300) for i in range(1, 13)}

font_file = "/Roboto-Regular-47.pcf"

for i in range(1, 13):
    mars_c = vectorio.Circle(pixel_shader=pointer_pal, radius=30, x=clock_face_numbers[i][0]+12,
                             y=clock_face_numbers[i][1], color_index=1)
    earth_c = vectorio.Circle(pixel_shader=pointer_pal, radius=30, x=clock_face_numbers[i][0]+12,
                             y=clock_face_numbers[i][1], color_index=3)
    if i >= 10:
        mars_c.x = mars_c.x + 14
        earth_c.x = earth_c.x + 14
    mars_group.append(mars_c)
    earth_group.append(earth_c)
    text = str(i)
    font = bitmap_font.load_font(font_file)

    mars_text = label.Label(font, text=text, color=0xFFFFFF)
    earth_text = label.Label(font, text=text, color=0x000000)
    mars_text.x = clock_face_numbers[i][0]
    mars_text.y = clock_face_numbers[i][1]
    earth_text.x = clock_face_numbers[i][0]
    earth_text.y = clock_face_numbers[i][1]
    mars_group.append(mars_text)
    earth_group.append(earth_text)

mars_group.append(pointer_hub)
earth_group.append(pointer_hub)

# get time from adafruit io
# called once an hour in the loop
def update_time():
    print("time")
    now = io.receive_time()
    return now

def convert_time(the_time):
    h = the_time[3]
    if h >= 12:
        h -= 12
        a = "PM"
    else:
        a = "AM"
    if h == 0:
        h = 12
    return h, a

# get mars time
def mars_time():
    dt = io.receive_time()
    print(dt)
    utc_offset = 3600 * -timezone
    tai_offset = 37
    millis = time.mktime(dt)
    unix_timestamp = millis + utc_offset

    # Convert to MSD
    msd = (unix_timestamp + tai_offset) / Decimal("88775.244147") + Decimal("34127.2954262")
    print(msd)
    # Convert MSD to MTC
    mtc = (msd % 1) * 24
    mtc_hours = int(mtc)
    mtc_minutes = int((mtc * 60) % 60)
    mtc_seconds = int(((mtc * 3600)) % 60)

    print(f"Mars Time: {mtc_hours:02d}:{mtc_minutes:02d}:{mtc_seconds:02d}")
    return mtc_minutes, mtc_hours

def time_angle(m, the_hour):
    m_offset = 25 if 12 <= m < 18 or 42 <= m < 48 else 5
    h_offset = 25 if 2 <= the_hour % 12 < 4 or 8 <= the_hour % 12 < 10 else 5
    # Adjusted angle calculation for minute hand
    theta_minute = 360 - (m / 60) * 360
    theta_hour = ((the_hour / 12) + (m / (12 * 60))) * 360
    # Calculate coordinates for minute hand (mirrored)
    minute_x = -int(cos(pi * (theta_minute - 90) / 180) * mh)
    minute_y = int(sin(pi * (theta_minute + 90) / 180) * mh)
    hour_x = int(cos(pi * (theta_hour - 90) / 180) * hh)
    hour_y = int(sin(pi * (theta_hour + 90) / 180) * hh)
    min_hand.points = [(mw, 0), (minute_x + m_offset, -minute_y),
                       (minute_x - m_offset, -minute_y), (-mw, 0)]
    hour_hand.points = [(hw, 0), (hour_x + h_offset, -hour_y),
                        (hour_x - h_offset, -hour_y), (-hw, 0)]

clock_timer = 1 * 1000
clock_clock = ticks_ms()
clock = update_time()
hour, am_pm = convert_time(clock)
tick = clock[5]
minute = clock[4]
mars_min, mars_hour = mars_time()
show_earth = True

time_angle(minute, hour)

while True:
    event = key.events.get()
    # swap between earth or mars time
    if event:
        if event.pressed:
            print("updating display")
            show_earth = not show_earth
    # update background image
    # change minute hand color depending on background
    if show_earth:
        if min_hand.color_index != 2:
            time_angle(minute, hour)
            graphics.display.root_group = earth_group
            min_hand.color_index = 2
            pointer_hub.color_index = 2
    else:
        if min_hand.color_index != 0:
            time_angle(mars_min, mars_hour)
            graphics.display.root_group = mars_group
            min_hand.color_index = 0
            pointer_hub.color_index = 0
    # use ticks for timekeeping
    # every minute update clock hands
    # recheck IO time every hour
    if ticks_diff(ticks_ms(), clock_clock) >= clock_timer:
        tick += 1
        if tick > 59:
            tick = 0
            minute += 1
            if minute > 59:
                clock = update_time()
                hour, am_pm = convert_time(clock)
                tick = clock[5]
                minute = clock[4]
            print(f"{hour}:{minute:02} {am_pm}")
            mars_min, mars_hour = mars_time()
            if show_earth:
                time_angle(minute, hour)
            else:
                time_angle(mars_min, mars_hour)
        clock_clock = ticks_add(clock_clock, clock_timer)

View on GitHub

Upload the Code and Libraries to the Qualia ‎ESP32-S3‎

After downloading the Project Bundle, plug your Qualia ESP32-S3 ‎into the computer's USB port with a known good USB data+power ‎cable. You should see a new flash drive appear in the computer's File ‎Explorer or Finder (depending on your operating system) ‎called CIRCUITPY. Unzip the folder and copy the following items to ‎the Qualia ESP32-S3's CIRCUITPY drive.‎

  • lib folder

  • code.py

  • earth.bmp

  • mars.bmp

  • Roboto-Regular-47.pcf‎

Your Qualia ESP32-S3 CIRCUITPY drive should look like this after ‎copying the lib folder, earth.bmp file, mars.bmp file, Roboto-‎Regular-47.pcf file and the code.py file.‎

drive_16

Install the udecimal Library from the ‎Community Bundle

This project uses one additional library from the Community Bundle: ‎the jepler_udecimal library. You'll need to download the Community ‎Bundle and copy the /jepler_udecimal library folder to ‎your /lib folder or use circup to install with:‎

circup install jepler-circuitpython-udecimal

Add Your settings.toml File

As of CircuitPython 8.0.0, there is support for Environment Variables. ‎Environment variables are stored in a settings.toml file. Similar ‎to secrets.py, the settings.toml file separates your sensitive ‎information from your main code.py file. Add your settings.toml file ‎as described in the Create Your settings.toml File page earlier in this ‎guide. You'll need to include ‎your ADAFRUIT_AIO_USERNAME, ADAFRUIT_AIO_KEY, CIRCUITPY_WIFI_SSID and CIRCUITPY_WIFI_PASSWORD.‎

Download File

Copy Code
CIRCUITPY_WIFI_SSID = "your-ssid-here"
CIRCUITPY_WIFI_PASSWORD = "your-ssid-password-here"
ADAFRUIT_AIO_USERNAME = "your-io-username-here"
ADAFRUIT_AIO_KEY = "your-io-key-here"

How the CircuitPython Code Works

At the top of the code, you'll edit the timezone variable to equal ‎your UTC time zone offset. This is used when calculating Mars time ‎‎(MTC).‎

Download File

Copy Code
# timezone offset for calculating mars time
timezone = -5

After that, pin A0 is setup as a keypad object. Pressing the button ‎attached to this pin will switch the display between Earth and Mars ‎time. Then, the board connects to your WiFi SSID and Adafruit IO.‎

Download File

Copy Code
key = keypad.Keys((board.A0,), value_when_pressed=False, pull=True)

wifi.radio.connect(os.getenv("CIRCUITPY_WIFI_SSID"), os.getenv("CIRCUITPY_WIFI_PASSWORD"))
print(f"Connected to {os.getenv('CIRCUITPY_WIFI_SSID')}")

aio_username = os.getenv('ADAFRUIT_AIO_USERNAME')
aio_key = os.getenv('ADAFRUIT_AIO_KEY')

context = ssl.create_default_context()
pool = socketpool.SocketPool(wifi.radio)
requests = adafruit_requests.Session(pool, context)
io = IO_HTTP(aio_username, aio_key, requests)

Graphics

The display is instantiated with the Qualia Graphics library. Then, the ‎Earth and Mars are loaded as OnDiskBitmap's. Display groups are created ‎for each planet.‎

Download File

Copy Code
earth_bitmap = displayio.OnDiskBitmap("/earth.bmp")
mars_bitmap = displayio.OnDiskBitmap("/mars.bmp")

graphics = Graphics(Displays.ROUND40, default_bg=None, auto_refresh=True)

earth_grid = displayio.TileGrid(earth_bitmap, pixel_shader=earth_bitmap.pixel_shader)
earth_group = displayio.Group()
earth_group.append(earth_grid)

mars_grid = displayio.TileGrid(mars_bitmap, pixel_shader=mars_bitmap.pixel_shader)
mars_group = displayio.Group()
mars_group.append(mars_grid)

def center(grid, bitmap):
    # center the image
    grid.x -= (bitmap.width - graphics.display.width) // 2
    grid.y -= (bitmap.height - graphics.display.height) // 2

center(mars_grid, mars_bitmap)
center(earth_grid, earth_bitmap)

graphics.display.root_group = mars_group

vectorio shapes are used for the clock face graphics. A circle is ‎created for the center of the display for the minute and hour hands ‎to fan out from.‎

Download File

Copy Code
# pointer using vectorio, first the hub
pointer_pal = displayio.Palette(4)
pointer_pal[0] = 0xff0000
pointer_pal[1] = 0x000000
pointer_pal[2] = 0x0000ff
pointer_pal[3] = 0xffffff
pointer_hub = vectorio.Circle(pixel_shader=pointer_pal, radius=26, x=0, y=0)
pointer_hub.x = graphics.display.width // 2
pointer_hub.y = graphics.display.height // 2

The minute and hour hands are polygon shapes. The clock hands are ‎added to both display groups.‎

Download File

Copy Code
# minute hand
mw = 23
mh = 225
min_points = [(mw,0), (mw,-mh), (-mw,-mh), (-mw,0)]
min_hand = vectorio.Polygon(pixel_shader=pointer_pal, points=min_points, x=0,y=0)
min_hand.x = graphics.display.width // 2
min_hand.y = graphics.display.height // 2
mars_group.append(min_hand)
earth_group.append(min_hand)
# hour hand
hw = 25
hh = 175
hour_points = [(hw,0), (hw,-hh), (-hw,-hh), (-hw,0)]
hour_hand = vectorio.Polygon(pixel_shader=pointer_pal, points=hour_points,
                             x=0, y=0, color_index=1)
hour_hand.x = graphics.display.width // 2
hour_hand.y = graphics.display.height // 2
mars_group.append(hour_hand)
earth_group.append(hour_hand)

The clock face numbers are placed around the perimeter of the ‎circular display. These coordinates are calculated with ‎the calculate_number_position() function. In a for loop, vectorio circles are ‎created to act as a background for the clock numbers. The clock ‎numbers are added as text labels. There are two instances of these ‎circle and number pairs created for the display groups. The colors ‎differ between the two to better complement the planet ‎backgrounds.‎

Download File

Copy Code
# add numbers to the clock face
def calculate_number_position(number, center_x, center_y, radius):
    angle = (360 / 12) * (number - 3)  # -3 adjusts the angle to start at 12 o'clock
    rad_angle = pi * angle / 180
    if number >=8:
        x = int(center_x + cos(rad_angle) * radius-40)
    x = int(center_x + cos(rad_angle) * radius)
    y = int(center_y + sin(rad_angle) * radius)
    return x, y

clock_face_numbers = {i: calculate_number_position(i, graphics.display.width // 2,
                        graphics.display.height // 2, 300) for i in range(1, 13)}

font_file = "/Roboto-Regular-47.pcf"

for i in range(1, 13):
    mars_c = vectorio.Circle(pixel_shader=pointer_pal, radius=30, x=clock_face_numbers[i][0]+12,
                             y=clock_face_numbers[i][1], color_index=1)
    earth_c = vectorio.Circle(pixel_shader=pointer_pal, radius=30, x=clock_face_numbers[i][0]+12,
                             y=clock_face_numbers[i][1], color_index=3)
    if i >= 10:
        mars_c.x = mars_c.x + 14
        earth_c.x = earth_c.x + 14
    mars_group.append(mars_c)
    earth_group.append(earth_c)
    text = str(i)
    font = bitmap_font.load_font(font_file)

    mars_text = label.Label(font, text=text, color=0xFFFFFF)
    earth_text = label.Label(font, text=text, color=0x000000)
    mars_text.x = clock_face_numbers[i][0]
    mars_text.y = clock_face_numbers[i][1]
    earth_text.x = clock_face_numbers[i][0]
    earth_text.y = clock_face_numbers[i][1]
    mars_group.append(mars_text)
    earth_group.append(earth_text)

Time Functions

The internet time is retrieved using the io.receive_time() function. This ‎returns a struct_time timestamp in the same time zone as your IP ‎address.‎

Download File

Copy Code
# get time from adafruit io
# called once an hour in the loop
def update_time():
    print("time")
    now = io.receive_time()
    return now

The convert_time() function is used to convert the struct_time from 24 hour ‎to 12-hour time.‎

Download File

Copy Code
def convert_time(the_time):
    h = the_time[3]
    if h >= 12:
        h -= 12
        a = "PM"
    else:
        a = "AM"
    if h == 0:
        h = 12
    return h, a

The mars_time() function converts the current time to the Unix ‎timestamp and calculates coordinated Mars time (MTC). This ‎function makes use of the jepler_udecimal library. This library is a ‎subset of the CPython Decimal library, which is designed for ‎arithmetic and greater accuracy over float numbers. CircuitPython ‎does not have an accurate enough float accuracy for this calculation ‎otherwise.‎

A more in-depth explanation on calculating Mars time with ‎CircuitPython can be found in this Playground Note.‎

Download File

Copy Code
# get mars time
def mars_time():
    dt = io.receive_time()
    print(dt)
    utc_offset = 3600 * -timezone
    tai_offset = 37
    millis = time.mktime(dt)
    unix_timestamp = millis + utc_offset

    # Convert to MSD
    msd = (unix_timestamp + tai_offset) / Decimal("88775.244147") + Decimal("34127.2954262")
    print(msd)
    # Convert MSD to MTC
    mtc = (msd % 1) * 24
    mtc_hours = int(mtc)
    mtc_minutes = int((mtc * 60) % 60)
    mtc_seconds = int(((mtc * 3600)) % 60)

    print(f"Mars Time: {mtc_hours:02d}:{mtc_minutes:02d}:{mtc_seconds:02d}")
    return mtc_minutes, mtc_hours

The time_angle() function calculates the angle of the minute and hour ‎hand polygon shapes by updating their coordinates.‎

Download File

Copy Code
def time_angle(m, the_hour):
    m_offset = 25 if 12 <= m < 18 or 42 <= m < 48 else 5
    h_offset = 25 if 2 <= the_hour % 12 < 4 or 8 <= the_hour % 12 < 10 else 5
    # Adjusted angle calculation for minute hand
    theta_minute = 360 - (m / 60) * 360
    theta_hour = ((the_hour / 12) + (m / (12 * 60))) * 360
    # Calculate coordinates for minute hand (mirrored)
    minute_x = -int(cos(pi * (theta_minute - 90) / 180) * mh)
    minute_y = int(sin(pi * (theta_minute + 90) / 180) * mh)
    hour_x = int(cos(pi * (theta_hour - 90) / 180) * hh)
    hour_y = int(sin(pi * (theta_hour + 90) / 180) * hh)
    min_hand.points = [(mw, 0), (minute_x + m_offset, -minute_y),
                       (minute_x - m_offset, -minute_y), (-mw, 0)]
    hour_hand.points = [(hw, 0), (hour_x + h_offset, -hour_y),
                        (hour_x - h_offset, -hour_y), (-hw, 0)]

The Loop

In the loop, if the button attached to A0 is pressed, then the display ‎swaps to either show the Earth time or Mars time. When the display ‎swaps, the background images changes, the clock hand colors ‎change, and the associated time is displayed.‎

Download File

Copy Code
while True:
    event = key.events.get()
    # swap between earth or mars time
    if event:
        if event.pressed:
            print("updating display")
            show_earth = not show_earth
    # update background image
    # change minute hand color depending on background
    if show_earth:
        if min_hand.color_index != 2:
            time_angle(minute, hour)
            graphics.display.root_group = earth_group
            min_hand.color_index = 2
            pointer_hub.color_index = 2
    else:
        if min_hand.color_index != 0:
            time_angle(mars_min, mars_hour)
            graphics.display.root_group = mars_group
            min_hand.color_index = 0
            pointer_hub.color_index = 0

Time Keeping

After the initial time fetch, ticks are used to keep time. Every minute, ‎the angle of the clock hands is updated. Every hour, Adafruit IO is ‎pinged to update the time to keep ticks accurate.‎

Download File

Copy Code
# use ticks for timekeeping
    # every minute update clock hands
    # recheck IO time every hour
    if ticks_diff(ticks_ms(), clock_clock) >= clock_timer:
        tick += 1
        if tick > 59:
            tick = 0
            minute += 1
            if minute > 59:
                clock = update_time()
                hour, am_pm = convert_time(clock)
                tick = clock[5]
                minute = clock[4]
            print(f"{hour}:{minute:02} {am_pm}")
            mars_min, mars_hour = mars_time()
            if show_earth:
                time_angle(minute, hour)
            else:
                time_angle(mars_min, mars_hour)
        clock_clock = ticks_add(clock_clock, clock_timer)

CAD Files

‎3D Printed Parts‎

STL files for 3D printing are oriented to print "as-is" on FDM style ‎machines. Parts are designed to 3D print without any support ‎material using PLA filament. Original design source may be ‎downloaded using the links below.‎

printed_17

Parts List

  • Back Dome

  • Base

  • Bottom Cover

  • Display Mount

  • Display Frame

  • Dome Cover

  • Front Frame

  • Neck Collar

list_18

Download CAD source

Download STLs.zip

 

Build Volume

The parts require a 3D printer with a minimum build volume.‎

  • ‎132mm (X) x 132mm (Y) x 102mm (Z)‎

volume_19

CAD Assembly

The 4in round display press fits into the display mount. The display ‎mount snap fits into the front frame. The display frame snap fits over ‎the 4in round display. The back dome and front frame snap fit ‎together. The button is panel mounted to the dome cover. The base ‎and back dome are connected using the neck collar. The Qualia ‎ESP32-S3 board is secured to the bottom cover using four M2.5 x ‎‎6mm long screws. The bottom cover snap fits onto the bottom of the ‎base. The 4in round display is connected to a 40-pin FPC extension ‎board and ribbon cable that connects to the Qualia ESP32-S3 board.‎

lcds___displays_CAD

Design Source Files

The project assembly was designed in Fusion 360. This can be ‎downloaded in different formats like STEP, STL and more. Electronic ‎components like Adafruit's boards, displays, connectors and more ‎can be downloaded from the Adafruit CAD parts GitHub Repo.

project_21

Wiring Assembly

JST Cable for Button

Get the 3-pin JST cable ready to solder to the 24mm arcade button.‎

wiring_22

Setup JST Cable

Remove the red wire from the cable using wire cutters. The arcade ‎button only needs two wires (black and white.)‎

wiring_23

Solder Cable

Attach the wires to the two terminals on the buttons switch. Polarity ‎does not have to match.‎

cable_24

cable_25

Button Labels

The buttons switch terminals are fitted inside the gray colored ‎plastic housing.‎

button_26

Wired Button

Take a moment to test the 3-pin JST cable by plugging it into the JST ‎port on the Qualia ESP32-S3 board. ‎

Disconnect the button from the board when finished testing.‎

button_28

button_27

FPC Extension

Get the 40-pin FPC extension board and ribbon cable ready to ‎connect to the 4in round display.‎

fpc_28

Connect Ribbon Cables

Carefully lift the two latches on the FPC extension board to open ‎them.‎

Insert the 40-pin ribbon cable into one of the connectors with the ‎blue side facing up.‎

Push ribbon cable to fully seat into the connector then gently press ‎down on latch to close.‎

Insert ribbon cable from the 4in round display into the remaining ‎connector on the FPC extension board. Press down to close latch.‎

ribbon_29

ribbon_30

Install Display to Mount

Get the Display Mount part and 4in round display ready.‎

Carefully place the display into the recess in the 3D printed display ‎mount with the edges lined up.‎

Flip the display ribbon cable so it lays flat against the back. ‎

Gently press the edges of the display into the lip of the 3D printed ‎display mount.‎

install_31

install_32

Install Display Frame

Get the 3D printed display frame ready.‎

Insert the display frame underneath the three clips on the inside of ‎the display mount.‎

The display frame can be flexed to sit flush over the display and ‎under the three clips.‎

frame_33

frame_34

Front Frame

Get the 3D printed front frame ready.‎

Orient the two parts so the notches and keys are lined up. ‎

front_35

Install Display to Front Frame

Carefully insert the display assembly into the front frame with the ‎keys fitted into the notches.‎

Gently press down on all edges so the display frame sits flush with ‎the front frame.‎

front_36

front_37

Secured Display

Take a moment to check the display is secured to the front frame.‎

secured_38

Dome Parts

Get the neck collar, back dome, and base parts ready.‎

dome_39

Install Dome to Base

Line up the hole with the neck of the base and place the back dome ‎onto the base.‎

Press the neck collar into the hole of the base to secure the back ‎dome and base.‎

base_40

base_41

Installed Neck Collar

Take a moment to check the orientation of the neck collar. The side ‎notches should be lined up perpendicularly. ‎

neck_42

Install Front to Dome

Line up the side keys on the front frame with the notches on the ‎back dome.‎

Insert the displays FPC ribbon cable through the back dome.‎

Press the two parts together so they snap fit closed.‎

install_43

install_44

Install Ribbon Cable

Insert the FPC ribbon cable from the display into the neck collar.‎

Pull the FPC ribbon cable through the base.‎

cable_45

cable_46

Dome Cover

Get the arcade button and dome cover ready.‎

Remove the nut from the button by unscrewing it.‎

cover_47

Panel Mount Button

Insert the arcade button into the back cover with the actuator facing ‎the flush surface.‎

Fasten the included nut to secure the button to the back cover.‎

panel_48

Install Button Cable

Insert the 3-pin JST cable from the arcade button through the ‎opening in the neck collar and pull it through the base.‎

jst_49

Snap Fit Cover

Press fit the dome cover into the back dome to snap fit closed.‎

snap_50

snap_51

Connect Display Cable

Insert the FPC ribbon cable from the display into the connector on ‎the Qualia ESP32-S23 board.‎

insert_52

Connect Button Cable

Plug in the 3-pin JST cable from the arcade button to the port on the ‎side of the Qualia ESP32-S3 board.‎

port_53

Base Cover

Get the base cover and Qualia ESP32-S3 board ready.‎

Orient the Qualia ESP32-S3 board face down, bottom up and line up ‎the mounting holes with base cover's built in standoffs. ‎

orient_54

Secure Qualia ESP32-S3‎

Use 4x M2.5 x 6mm long machine steel screws to secure the Qualia ‎ESP32-S3 board to the base cover.‎

secure_55

secure_56

Install Base Cover

Orient the base cover with the base so the port and buttons on the ‎Qualia ESP32-S3 board line up with the opening.‎

Firmly press the base cover into the base to snap fit close.‎

close_57

close_58

USB Power

Use a 5V 1A power supply and USB-C cable to power on the clock.‎

usb_59

メーカー品番 5800
EVAL BOARD FOR ESP32-S3
Adafruit Industries LLC
メーカー品番 5793
GRAPHIC DISPLAY TFT RGB 4"
Adafruit Industries LLC
メーカー品番 3429
SWITCH PUSH SPST-NO WHT 10MA 5V
Adafruit Industries LLC
USB TO 2.1MM MALE BARREL JACK CA
メーカー品番 2697
USB TO 2.1MM MALE BARREL JACK CA
Adafruit Industries LLC
メーカー品番 5153
CABLE A PLUG TO C PLUG 3.28'
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.