Maker.io main logo

Overdrive Guitar Effects Pedal

253

2018-07-31 | By Bantam Tools

License: GNU Lesser General Public License Milling Machines

Courtesy of Bantam Tools

The Overdrive Effects Pedal was designed by Eddie Serratos for Bantam Tools.

This project shows you how to make your very own effects stompbox! We'll go through the steps of downloading the .brd file, loading the file into our software, milling the board on the Bantam Tools Desktop PCB Milling Machine, and soldering the components. This is a great tutorial for those new to milling printed circuit boards (PCBs) or for those who want practice soldering components to the board as a part of a larger assembly.

Tools, Materials, Parts, and Files

TOOLS

MATERIALS

Circuit Board Components

OVERDRIVE PEDAL KIT

FILES

We'll start of by downloading a .brd file that was made in EAGLE, loading it into Bantam Tools Desktop Milling Machine Software, and milling a single-sided circuit board.

Step 1: Download the .brd file and set up your material

If you haven't already, connect your computer to the milling machine with a USB cable, turn the milling machine on, and opening the Bantam Tools Desktop Milling Machine Software.

You'll be prompted to home your machine. Press the Start Homing button.

Press the Start Homing button

Install the 1/32" flat end mill into the milling machine, then click on the Tool "Change" button. If you've never done this before, read more about the process in our Inserting and Locating a Tool guide.

click on the Tool “Change” button

Select the 1/32" flat end mill from the "New tool" drop-down menu and click Continue. A new prompt window will pop up asking to verify tool position. Your machine will move the end mill to the right.

Make sure there's no material under the end mill and that the spoilboard is free of debris. Click the Locate Tool button.

The end mill will slowly descend until it encounters the spoilboard. Once it touches the spoilboard, it'll briefly pause, then retract upwards. This act of touching-off on the spoilboard lets the software know where the end mill's tip is located in space.

You're now ready to load your material.

In the software menu that's located at the top of the screen, select Machine -> Rapid to loading. The spoilboard should now be toward the front of the machine and ready for material loading.

Measure the thickness of your double-sided tape in millimeters using your digital caliper, and enter that number into the Material Placement (Z) field.

enter thickness into the Material Placement (Z) field

Apply the tape to the back of a single-sided PCB blank. Make sure the tape doesn't overlap, otherwise your z-axis will be slightly higher than intended. Be sure to cover as much of the back of the material as possible. Then place the PCB blank at the bottom-right edge of the spoilboard.

Apply the tape to the back of a single-sided PCB blank

Select "Single-Sided FR-1" as your material type. The dimensions of the board should automatically default to the properties of a new board.

It's always a good idea to use a digital caliper to measure the thickness (Z-axis) of your PCB blank. Sometimes a board can be a little thicker than normal, and it's important to enter this value into the Material Thickness (Z) field of the software.

Select “Single-Sided FR-1” as your material type

Now we're ready to load the overdrive pedal.brd file into the software. Click the Open File button and select your .brd file from its saved location.

Click the Open File button

Step 2: Look at the software preview and mill the board

When looking at the preview, if you see any warnings or red on the board, it means that the end mill you've selected to cut the board is too large to mill those areas. This is usually because your components or traces are too close together relative to the size of your cutting tool. To fix this, you'll need to either select a smaller cutting tool, or open the .brd file in EAGLE and edit the layout to create sufficient space for the end mill to fit.

However, in the instance of the .brd file we're milling here, as you can see in the image below, the board is free of any red markings and warnings. Because we see no red warnings, we know that the end mill we've chosen is small enough to successfully mill the board. This means we're ready to mill our board.

Move the Parts to Mill slider to the "bottom" setting and select your 1/32" flat end mill. You can click on the Traces, Holes, and Outline to get an idea of exactly what the machine is going to mill.

Now that our end mill is installed, our material is attached to the spoilboard, and our .brd file is set up in the software, we're ready to mill the board. We have only one file loaded, so we can click either the Start Milling button or the Mill All Visible button; in this instance they both do the same thing and cut our file.

Always stay by your milling machine while it completes the job!

the board is free of any red markings and warnings

After the milling machine finishes cutting the board, use a scraper to remove the PCB from the spoilboard. Here's what your board should look like.

what your board should look like

You now have a circuit board that's ready to be populated with components!

Step 3: Place the components and solder them to the board

We'll place the components in their appropriate places on the circuit board and solder them to the board.

This is what the board will look like when we're done soldering the components onto it.

what the board looks like when we’re done soldering

Notice that the parts are sitting on the side of the PCB that does not have the copper coating.

This is what the other side of the board looks like when finished.

what the other side of the board looks like

The .brd file we're using was created in EAGLE. When placing the components, we can refer to the .brd file as it's viewed in EAGLE to see where the parts should go, as shown in the image below.

The blue lines indicate the traces; notice that they're the mirror image of the traces on the milled PCB board. In other words, if you horizontally flip the image on the left (the .brd file as viewed in EAGLE), then you'll get the image on the right (the PCB board). This is helpful to keep in mind when placing the components on the board.

refer to the .brd file as it

Now let's place our components on the board. The diagram below shows where each of the components goes. Some of the components need one leg to go in a specific hole. Other components, like the resistors, don't have polarity and so the legs can go in either hole. If you're interested in learning more about polarity, this SparkFun guide is a good resource.

diagram shows where each of the components goes

After you've placed the components in their appropriate place, the copper side of the PCB will look something like this.

copper side of the PCB will look something like this

Now it's time to solder the legs to the board. If you're new to soldering, check out Adafruit's Soldering Guide. Once you're done soldering, use diagonal cutters to cut the legs off.

Next, we'll prepare our enclosure to hold the circuit board.

Step 4: Drill the enclosure

The enclosure that we're using for our pedal is the 1590B. It doesn't come with holes for the components to fit into, so we'll add those now.

Start by printing out the 1590B enclosure template on paper and cutting it out along the outside edge.

Print out the 1590B enclosure template on paper

Fold the flaps down along the center rectangle edge, then tape the edges together.

Fold the flaps down along the center rectangle edge

Place your enclosure inside your drilling template.

Tape the template onto the enclosure so that it doesn't move when you're drilling. You'll have an easier time drilling the holes in the correct location if the paper doesn't move.

Tape the template onto the enclosure

We'll be using a stepper bit attached to a drill press to make our holes. This is the specific stepper bit we used, and we liked it because it has diameters in 1mm increments, ranging from 4mm to 12mm. When using a stepper bit, keep drilling downward until the stepper bit diameter matches the diameter on the drilling template.

If you don't have access to stepper bits, you can use regular drill bits intended to drill into metal; however, it won't be possible to get exact hole diameters.

Use the following as reference when using regular drill bits:

  • 3PDT switch: 12mm stepper bit = 1/2" drill bit (~12.7mm hole)

  • DC power jack: 12mm stepper bit = 1/2" drill bit (~12.7mm hole)

  • Input/output jacks: 10mm stepper bit = 3/8" drill bit (~9.5mm hole)

  • Potentiometers: 7mm stepper bit = 5/16" drill bit (~7.9mm hole)

  • LED: 6mm stepper bit = 1/4" drill bit (~6.35mm hole)

If you don't have a drill press a hand drill will do, but remember that a steady hand goes a long way.

Notice that we've taped our paper template to the metal enclosure so the paper doesn't move.

Drill your enclosure holes.

tape the paper template to the metal enclosure

Drill your enclosure holes

When you've drilled all the holes, look to see if there are any sharp edges or burrs. If you find any, use a scouring pad to smooth the edges.

This is what the enclosure looks like once all the holes have been drilled.

What the enclosure looks like once holes are drilled

Step 5: Add hardware and components

Lay out all your hardware.

Lay out all your hardware

Here's where all the parts will be placed.

Here

Begin by inserting the DC power jack, the B50K potentiometer, and the A100K potentiometer.

Tighten the nut on each component just enough so they don't move, but leave them loose enough so that you can still move the components. This makes soldering much easier because you can spin the components if needed.

Next insert the 3PDT switch, the mono jack (the pedal's output), and the stereo jack (the pedal's input).

When looking down at the open enclosure, be sure that the stereo jack is on the left and the mono jack is on the right.

Again, tighten the components just enough to hold them in place, but not so tightly that they can't be moved.

Notice that we have not inserted the LED and bezel into place. We're going to do a bit of soldering before adding the LED and bezel.

Step 6: Solder the components

If you're new to soldering or would like a refresher, check out Adafruit's Soldering Guide.

Begin by soldering the positive wire from the battery clip into the DC power jack.

Solder +wire from battery clip to DC power jack

Soldering +wire from battery clip into DC power jack

Next, solder the wire that will connect to the 3PDT switch and a ground wire. So far, your enclosure should look like the image below.

your enclosure should look like the image

Put some masking tape below the potentiometers to prevent your circuit board from touching the enclosure and becoming grounded. It's not always necessary, but we recommend adding it just to be safe!

Put some masking tape below the potentiometers

The 3DPT switch has nine lugs. Use the image below as a reference for how each lug is numbered. From this point forward, we'll refer to each lug on the 3DPT switch by the number assigned to it.

reference for how each lug is numbered

Solder a wire from lug 3 to lug 9 on the 3DPT switch.

Solder a wire from lug 3 to lug 9 on the 3DPT switch

For the mono output jack, the picture below shows how the lugs are numbered. In the next step, we'll solder to lug 2 on the mono output jack.

how the lugs are numbered

Solder a wire from lug 8 on the 3DPT to lug 2 on the mono output jack.

Solder wire from lug 8 on 3DPT to lug 2 on monojack

For the stereo input jack, the picture below shows how the lugs are numbered. Next, we'll solder to lug 1 on the stereo input jack.

how the lugs are numbered

Solder the negative battery wire to lug 1 on the stereo input jack.

Solder negative battery wire to lug 1 on stereo jack

Solder a wire from lug 2 of the 3PDT switch to lug 3 of the stereo input jack.

Solder wire from lug2 of 3PDT to lug3 of stereo jack

Next, we'll solder to the positive and negative leg of the LED. The longer leg of the LED is the positive leg, and the shorter leg is the negative leg.

solder to the positive and negative leg of the LED

Solder a resistor to the positive leg of the LED. Cut the positive leg of the LED so it's shorter. Then cut the leg of the resistor so it's shorter too, and solder them together. The image below shows how this should look.

Next, cut the negative leg of the LED and solder a wire to it. This wire will serve as the resistor's ground wire.

Solder a resistor to the positive leg of the LED

Keep in mind that in a project like this one, where the pedal is powered by a battery, the value of the resistor used with the LED will affect the battery life. A lower resistor value that allows the LED to burn at its brightest will drain the battery more quickly. A higher resistor value that keeps the LED more dim will prolong battery life. We're using a 56K resistor, which is a high enough value that the LED won't burn too brightly and so the battery won't prematurely be drained.

Use some heat shrink tubes on your connections and you should have something that looks like the image below.

should have something that looks like this

Insert the LED bezel into the enclosure from the top side of the enclosure. Then insert the LED into the bezel from the inside of the enclosure.

Next, cut the positive wire and solder it to lug 5 of the 3PDT switch.

Cut positive wire/solder to lug 5 of 3PDT switch

Insert the negative wire from your LED into lug 2 of the stereo input jack (on the left) but don't solder it yet.

Next, insert the negative wire from the DC power jack into lug 1 of the mono output jack (on the right) but don't solder it yet.

Then route the positive wire from the power jack along the edge of the enclosure and leave it near the 3PDT switch for later use.

Notice that the area with the tape is clear of wires and that the wires are being run along the edge of the enclosure. While this isn't essential for the pedal to work correctly, it's good practice to keep your wires nice and tidy.

it’s good practice to keep your wires nice and tidy

Next, we'll solder our circuit board to both potentiometers, the A100K and the B50K. As a reference for where to solder the components, look at the .brd file as viewed in EAGLE (below).

.brd file as viewed in EAGLE

The lugs on the potentiometers are labeled as shown below.

lugs on the potentiometers are labeled as shown

Begin by soldering the B50K (gain) potentiometer to the board.

First, solder Gain-1 to lug 1 of the potentiometer.

Next, solder Gain-2 to lug 2 of the potentiometer.

Finally, solder Gain-3 to the lug 3 of the potentiometer.

Refer to the board diagram to see where Gain-1, Gain-2, and Gain-3 are located.

soldering the B50K (gain) potentiometer to the board

Refer to the board diagram

where Gain-1, Gain-2, and Gain-3 are located

where Gain-1, Gain-2, and Gain-3 are located

Now solder the A100K potentiometer to the board.

First, solder the Vol-1 wire from the circuit board to lug 1 of the A100K (volume) potentiometer.

Next, solder the Vol-2 wire to lug 2.

Finally, solder the Vol-3 wire to lug 3.

solder the A100K potentiometer to the board

solder the A100K potentiometer to the board

Position your board into the enclosure, route the input (green) wire toward the 3PDT switch, and solder it to lug 1 on the 3PDT switch.

Position your board into the enclosure

A few steps ago, you inserted the negative wire from your LED into lug 2 of the stereo input jack. Now run the negative (black) wire from the circuit board and insert it into lug 2 of the stereo input jack.

Next, cut some hookup wire long enough to reach lug 1 of the mono output jack.

You should now have three wires going into lug 2 of the stereo input jack. Solder these three wires into lug 2.

Solder these three wires into lug 2

From a few steps ago, the negative wire from the DC power jack should be in lug 1 of the mono output jack. Insert the hookup wire from lug 2 of the stereo input jack from the previous step, and solder the two wires into the lug.

solder the two wires into the lug

Next, insert the positive (red) wire from the circuit board and the positive wire from the power jack into lug 4 of the 3PDT switch and solder them.

Finally, insert the output wire (blue) from the circuit board into lug 7 of the 3PDT switch and solder.

Insert wire from circuit board to 3PDT switch/solder

Remember how earlier we left the input/output jacks, potentiometers, DC power jack, and 3PDT switch only partially tightened? Now you can tighten all.

Now you can tighten all

Add the knobs to the potentiometers and test your pedal!

Plug your guitar into the pedal, and then connect the pedal to an amp. Congratulations, you just milled your very own overdrive guitar effect pedal!

This is what your completed pedal looks like.

completed pedal

Troubleshooting

If the pedal doesn't work, check your soldering connections one by one. Make sure that there isn't a cold solder joint or loose wire. If you have a multimeter, use it to make sure that the joints aren't cold. If you haven't used a multimeter before, check out SparkFun's How to Use a Multimeter guide.

If you have any questions, don't hesitate to contact us at support@bantamtools.com. We're here to help. And if you do make the effects pedal, be sure to share it with us. We'd love to see it!

File Downloads:

メーカー品番 TL1004
END MILL CARBIDE 0.031"
Bantam Tools
メーカー品番 MT1004
PROTO BRD COPPER CLAD 5X4" 25PC
Bantam Tools
メーカー品番 FX1016
TAPE DBL COATED/SIDED WHITE
Bantam Tools
メーカー品番 SEK470M016ST
CAP ALUM 47UF 20% 16V RADIAL TH
Cornell Dubilier Knowles
メーカー品番 UPW1C470MDD
CAP ALUM 47UF 20% 16V RADIAL TH
ニチコン
メーカー品番 QYX2A473JTP
CAP FILM 0.047UF 5% 100VDC RAD
ニチコン
メーカー品番 UFW1C101MDD
CAP ALUM 100UF 20% 16V RADIAL TH
ニチコン
メーカー品番 1N4148 A0G
DIODE STANDARD 100V 150MA DO35
Taiwan Semiconductor Corporation
メーカー品番 1N5817-TP
DIODE SCHOTTKY 20V 1A DO41
MCC (Micro Commercial Components)
メーカー品番 MFR-25FBF52-100R
RES 100 OHM 1% 1/4W AXIAL
YAGEO
メーカー品番 CFR-25JB-52-3K3
RES 3.3K OHM 5% 1/4W AXIAL
YAGEO
メーカー品番 MFR-25FBF52-1M
RES 1M OHM 1% 1/4W AXIAL
YAGEO
メーカー品番 MFR-25FBF52-1K
RES 1K OHM 1% 1/4W AXIAL
YAGEO
メーカー品番 CFR-25JB-52-2M2
RES 2.2M OHM 5% 1/4W AXIAL
YAGEO
メーカー品番 CFR-25JB-52-240R
RES 240 OHM 5% 1/4W AXIAL
YAGEO
メーカー品番 MFR-25FBF52-200R
RES 200 OHM 1% 1/4W AXIAL
YAGEO
メーカー品番 11
CONN JACK MONO 6.35MM PNL MNT
Switchcraft Inc.
メーカー品番 12B
CONN JACK STEREO 6.35MM PNL MNT
Switchcraft Inc.
メーカー品番 232
BATT CONNECTOR SNAP 9V 4" LEADS
Keystone Electronics
メーカー品番 PJ-011A
CONN PWR JACK 2X5.5MM SOLDER
Same Sky (Formerly CUI Devices)
メーカー品番 P160KNP-0EC15A100K
POT 100K OHM 1/10W PLASTIC LOG
TT Electronics/BI
メーカー品番 P160KNP-0QD20B50K
POT 50K OHM 1/5W PLASTIC LINEAR
TT Electronics/BI
メーカー品番 FS57003PLT2B2M1QEH
SWITCH PUSHBUTTON 3PDT 1A 9V
E-Switch
メーカー品番 151031SS04000
LED RED DIFFUSED 3MM ROUND T/H
Würth Elektronik
メーカー品番 C-103-SR
LED HOLDER CLIP & RING T-1 FLANG
Bivar Inc.
メーカー品番 1900-H
KNOB SERRATED 0.250" PHENOLIC
Davies Molding, LLC
メーカー品番 C2003A.12.05
HOOK-UP SOLID 24AWG 300V YLW 5'
Encore Wire
メーカー品番 KSP2222ABU
TRANS NPN 40V 0.6A TO-92-3
onsemi
メーカー品番 13839
STOMP BOX ALUM 4.41"L X 2.4"W
SparkFun Electronics
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.