Maker.io main logo

MicroMod Asset Tracker Carrier Board Hookup Guide

125

2024-11-12 | By SparkFun Electronics

License: See Original Project Cellular GPS Wireless Arduino MicroMod Qwiic

Courtesy of SparkFun

Guide by El Duderino, PaulZC

Introduction

The MicroMod Asset Tracker Carrier Board provides you with a toolkit to monitor and track the ‎location of your assets. Do you want to know where your assets are at all times? Or maybe you just ‎want an update if an asset is moved? If so, this is the product for you!‎

Built around the u-blox SARA-R510M8S module, the MicroMod Asset Tracker Carrier Board offers ‎Secure Cloud LTE-M data communication for multi-regional use and has an integrated u-blox M8 ‎GNSS receiver for accurate positioning information.‎

Want to be able to communicate directly with the SARA-R5 over USB-C, without needing a ‎Processor Board? Or want to upgrade the SARA firmware? The included Asset Tracker Update ‎Tool lets you do just that. The Asset Tracker requires a Nano SIM for LTE-M connectivity. You can ‎use the included Hologram eUICC SIM card or choose one from your preferred service provider if ‎you prefer.‎

The Asset Tracker will work with any of our MicroMod Processor Boards, but because the asset ‎tracker offers so many features and can be configured in different ways, some processor boards ‎may be a better choice for your application than others. Please see “Choosing a Processor Board” ‎below for more details.‎

The SARA-R5 supports many different forms of data communication from full TCP/IP sockets and ‎packet switched data, through HTTP Get/Put/Post, FTP (the SARA has a built-in file system), Ping, ‎to good old SMS text messaging!‎

The Asset Tracker has an integrated ICM-20948 Inertial Measurement Unit for 9-Degree of ‎Freedom orientation and movement detection. Want to send a message if your asset is moved? ‎The asset tracker can do that! It also has a built-in digital microphone and so can send an alert as ‎soon as a noise is detected too. Want to add a light sensor? The Qwiic connector will let you do that.‎

Want to use the Asset Tracker to log data during a journey or shipping? It has a built-in micro-SD ‎card socket for data logging. Power options include both USB-C and LiPo battery (with built-in ‎charging and battery fuel gauge), but you can provide power via a breakout pin too.‎

We’ve provided a full set of examples to get you up and running quickly and our SARA-R5 Arduino ‎Library does all of the heavy lifting for you.‎

Required Materials

In addition to the MicroMod Asset Tracker Carrier Board, you’ll need a processor board to get ‎started. Depending on which features of the SARA-R5 you want to use, some of our processor ‎boards may be a better choice for your application. Please see “Choosing a Processor Board” ‎below for more details.‎

You'll also need a USB-C cable to connect the Carrier to your computer and if you want to add ‎some Qwiic breakouts to your MicroMod project you'll want at least one Qwiic cable to connect it all ‎together. Below are some options for both of those cables:‎

You can power the Asset Tracker via USB-C but for portable applications you'll need a single-cell ‎LiPo battery too. Here are some examples:‎

You'll also need LTE and GNSS antennas. There are many to choose from, but here are some ‎recommendations:‎

Note: The SMA connections are standard polarity: the connector on the Asset Tracker is female, ‎the antenna connection needs to be standard male. Antennas with reverse-polarity connectors are ‎not suitable for the Asset Tracker.‎

Recommended Tools

You will need a screwdriver to tighten the screw between the processor board and carrier board.‎

Suggested Reading

If you are not familiar with the MicroMod ecosystem, we recommend reading here for an overview. ‎We recommend reading here for an overview if you decide to take advantage of the Qwiic ‎connector.‎

micromod_1

MicroMod Ecosystem

qwiic_2

Qwiic Connect System

Finally, if you aren't familiar with the following concepts you may want to check out a few of these ‎tutorials before continuing.‎

Serial Communication: Asynchronous serial communication concepts: packets, signal levels, ‎baud rates, UARTs and more!‎

Installing an Arduino Library: How do I install a custom Arduino library? It's easy! This ‎tutorial will go over how to install an Arduino library using the Arduino Library Manager. For libraries ‎not linked with the Arduino IDE, we will also go over manually installing an Arduino library.‎

Logic Levels: Learn the difference between 3.3V and 5V devices and logic levels.‎

Getting Started with MicroMod: Dive into the world of MicroMod - a compact interface to ‎connect a microcontroller to various peripherals via the M.2 Connector!‎

Hardware Overview

The MicroMod Asset Tracker has a lot going on so buckle up. In this section we'll cover the various ‎components and hardware included on the Asset Tracker.‎

Common Components

Most SparkFun MicroMod Carriers will have some common components and all MicroMod Carriers ‎will have the keyed M.2 MicroMod Connector to plug your processor into. The photo and list below ‎outline some of the components you can expect on most SparkFun MicroMod Carriers.‎

  • M.2 MicroMod Connector - This special keyed M.2 connector lets you install your MicroMod ‎Processor of choice on your Asset Tracker Carrier Board.‎

  • USB-C Connector - Connect to your computer to program your Processor and also can ‎provide power to your MicroMod system.‎

  • ‎3.3V Regulator - Provides a regulated 3.3V and sources up to 1A.‎

  • Qwiic Connector - The standard Qwiic connector so you can add other Qwiic devices to your ‎MicroMod system.‎

  • Boot/Reset Buttons - Push buttons to enter Boot Mode on Processor boards and to Reset ‎your MicroMod circuit.‎

  • microSD Slot - Insert a microSD card for reading and writing data.‎

  • RTC Battery - We've included a 3V Lithium Rechargeable Battery as a backup power source ‎for the Processor Board Real Time Clock (if present).‎

components_3

u-blox SARA-R510M8S

The heart of the Asset Tracker is the SARA-R510M8S module from u-blox. This module ‎does so much, it is difficult to know where to begin!

ublox_4

Note: The MicroMod Asset Tracker uses the "00B" product version of the SARA-R5 module ‎‎(specifically the SARA-R510M8S-00B-00). LTE NB-IoT Radio Access Technology, and the LTE ‎FDD bands: 66, 71, 85 are not supported by this version. Refer to the SARA-R5 datasheet for ‎more information.‎

Designed to last an IoT lifetime, this module is 5G-ready with the u-blox UBX-R5 chipset. It has ‎built-in end-to-end security with hardware-based root of trust inside a discrete secure element. It ‎provides a full security suite with foundation, design, and end-to-end security, as well as access ‎control. The built-in u blox M8 GNSS receiver provides accurate and reliable positioning, always ‎and everywhere. It is optimized for ultra-low power consumption and critical firmware updates can ‎be delivered and services enabled via uFOTA (Firmware Over the Air). There. We told you it did a ‎lot!‎

The SARA-R5 supports many different forms of data communication from full TCP/IP sockets and ‎packet switched data, through HTTP Get/Put/Post, FTP (the SARA has a built-in file system), Ping, ‎to good old SMS text messaging! The built-in GNSS receiver provides NMEA format data, and our ‎library looks after the parsing for you.‎

The connection between the SARA-R5 and the MicroMod Processor Board is serial (3.3V UART) ‎but again, with this module being so clever, it can communicate over two serial interfaces at the ‎same time. Want your LTE data on one interface and your GNSS data on a separate interface? It ‎can do that too!‎

Note: Only some of our MicroMod Processors fully support dual serial interfaces. If this is an ‎important feature for you, please see the "Choosing a Processor Board" section below for more ‎details.‎

LTE and GNSS connections are via separate, robust SMA connectors. Switchable 3.3V power for ‎an active antenna is available on the GNSS connector. The Asset Tracker includes a socket for a ‎Nano SIM.‎

If you need to, you can manually turn the SARA off by pushing and holding the SARA On button. ‎The SARA will disconnect from the network before going into low power sleep. Press the button ‎briefly to turn the SARA back on again.‎

ICM-20948 IMU

The Asset Tracker carries the same ICM-20948 9-Degree of Freedom Inertial Measurement Unit ‎as OpenLog Artemis. It can provide fast accelerometer, gyro and magnetometer data and can be ‎configured for “Wake on Motion” too. We have a WOM example ready to go. It has a built-in ‎temperature sensor too.‎

icm_5

Digital Microphone

Thieves are wily these days. When attempting to steal your asset, one of the first things they will do ‎is cover or break the antenna (if they can see it). The built-in SPH0641 digital microphone can be ‎used to send an alert as soon as the Asset Tracker hears the thieves coming!‎

digital_6

Battery Charging and Monitoring Circuit

Since many applications for the Asset Tracker involve a battery-powered circuit, the board includes ‎both the MCP73831 LiPo battery charger and the MAX17048 battery fuel gauge. The MCP7381 ‎Single cell charge management IC can deliver a charge current up to 500mA. The MAX17048 is a ‎low-power I2C fuel gauge to monitor your battery's remaining charge.‎

battery_7

Plated Through-Hole (PTH) Connections

GPIO PTHs

We've broken out dedicated PTHs for digital, analog, pulse width modulation (PWM), I2C and SPI ‎along the sides of the Asset Tracker Carrier Board. You may also notice that we've included a ‎ground rail next to the digital, analog and PWM pins.‎

plated_8

Power PTHs

We've also provided PTHs for monitoring and accessing the following power circuits:‎

  • VIN - The power rail fed by USB-C and/or the LiPo battery.‎

  • ‎3.3V - The regulated 3.3V rail which feeds most of the components on the board. You can ‎measure the 3.3V current draw using the MEAS pins (see below).‎

  • VCCIO - This is the 1.8V rail generated by the SARA-R5. We use it to power ‎the 1.8V to 3.3V level shifters for the UART and I2C connections.‎

  • ‎1.8V - This is the 1.8V rail which powers the IMU. You can disable it by pulling the MicroMod ‎G4 digital pin LOW.‎

  • RST - Pull this low to reset the MicroMod Processor and the SARA-R5.‎

power_8a

SARA-R5 PTHs

The following SARA-R5 I/O connections are also broken out to PTH headers:‎

  • NI - This is the SARA's Network Indicator signal. It will be low (0V) when the network is ‎available, and high (3.3V) when the network is not available.‎

  • TP - This is the Timing Pulse (1PPS) signal and is connected to SARA GPIO6/TP. It will pulse ‎low and high when the SARA is receiving a GNSS signal, and the timing pulse has been ‎enabled. Please see Example11 for more details.‎

  • SARA USB D-/D+/DET - These PTHs provide access to the SARA's diagnostic USB port. This ‎connection is only used to access the SARA's trace log. You cannot (currently) upgrade the ‎SARA via this interface. Please consult the SARA R5 Integration Manual for more details.‎

  • SARA I2C - These 3.3V (level-shifted) PTHs can be used to access the SARA's I2C bus. Some ‎models of the SARA-R5 use I2C to communicate with an external GNSS module. As the SARA-‎R510M8S has GNSS built-in, it is unclear what you might want to use them for. But we've ‎been diligent and have broken them out anyway!‎

pths_9

SWD Programming Pins

An unpopulated JTAG footprint is available for more advanced users who need breakpoint level ‎debugging. Note that this is not populated so you will need a compatible header and compatible ‎JTAG programmer to connect.‎

pins_10

Solder Jumpers

If you have never worked with solder jumpers and PCB traces before or would like a quick ‎refresher, check out our How to Work with Solder Jumpers and PCB Traces tutorial for detailed ‎instructions and tips.‎

On the rear of the board, you will find a large number of jumpers which you can use to connect and ‎disconnect several of the connections between the SARA and the MicroMod Processor:‎

jumpers_11

The tables below outline all of the jumpers on the Asset Tracker along with brief descriptions of ‎their functionality.‎

  • SOLDER JUMPERS (STANDARD)‎

table_12

  • SOLDER JUMPERS (ADVANCED)‎

table_8a

MicroMod Pinout

Wondering what the pins are that are broken out on the MicroMod Asset Tracker Carrier Board? ‎The tables below outline the Asset Tracker pinout as well as the general MicroMod pinout. ‎Remember to compare the pins against your Processor Board to determine which pins are available.‎

Note: You may not recognize the COPI/CIPO labels for SPI pins. SparkFun is working to move ‎away from using MISO/MOSI to describe signals between the controller and the peripheral. Check ‎out this page for more on our reasoning behind this change.‎

  • MICROMOD ASSET TRACKER PINOUT TABLE

table_13

  • MICROMOD GENERAL PINOUT TABLE

header

table_14

  • MICROMOD GENERAL PIN DESCRIPTIONS

table_15

Board Dimensions

The Asset Tracker Carrier Board measures 3.0 inches by 3.0 inches (76.2mm x 76.2mm) and has ‎four mounting holes that fit a 4-40 screw.‎

board_16

Choosing a Processor Board

As you can see from the Jumpers section above, there are some things to consider when choosing ‎a MicroMod Processor Board to go with your Asset Tracker.‎

The MicroMod M.2 connector pinout is very comprehensive and some of the processor chips on ‎our MicroMod Processor Boards just don't have enough I/O pins to let us allocate one to every M.2 ‎pin. So, on those boards we share the pins. For example, on the ESP32 Processor Board, you will ‎see that the UART TX1 pin is shared with the G3 I/O pin and the AUD_OUT pin. We do that so that ‎you can use that pin for TX1 or G3 or AUD_OUT. And for most users and most Carrier Boards, ‎that's perfectly fine. However, since the SARA-R5 has so many pins that we need to connect to, the ‎sharing of TX1 and G3 causes a small problem. We need TX1 to communicate with the SARA, and ‎G3 would normally be used to enable power for the ICM-20948 IMU. We get round that by ‎including a normally open split pad jumper on G3 and making the IMU power circuit default to on. ‎Simple!‎

So, you can use any SparkFun MicroMod Processor in the Asset Tracker, but if you need complete ‎access to all of the pins then here are the restrictions:‎

ESP32 Processor

TX1 is shared with G3. This means you cannot close the G3 split pad to enable control of the IMU ‎Power. The IMU power will need to be always on.‎

RX1 is shared with G4. This means you cannot close the G4 split pad to access the SARA Ring ‎Indicator / Clear to Send 2 pin.‎

AUD_LRCLK is shared with G1. G1 controls the micro-SD power and AUD_LRCLK is connected to ‎the digital microphone. If you want to use the microphone, you will need to open the G1 split pad ‎jumper. The micro-SD power will default to on.‎

AUD_BCLK is shared with G2. G2 can be used to turn the SARA-R5 on/off and AUD_BCLK is ‎connected to the digital microphone. If you want to use the microphone, you will need to open the ‎G2 jumper. You won’t then be able to have the processor turn the SARA on and off. The SARA ‎always powers on automatically when power is connected, so no worries there, and the SARA On ‎button is there if you need it.‎

Artemis Processor

The Artemis Processor does not support the M.2 TX2 and RX2 pins. This means you cannot use ‎the Artemis to talk to the SARA using any of the dual-UART variants (called variants 2, 3 and 4 in ‎the SARA-R5 System Integration Manual). This means you cannot, for example, use UART 1 for ‎your LTE traffic and UART 2 for your GNSS data. That's all. You can do everything over a single ‎UART anyway.‎

nRF5280 Processor

The nRF52840 Processor Board supports all of the pins used by the Asset Tracker. There are no ‎restrictions for this Processor Board.‎

SAMD51 Processor

The SAMD51 Processor Board does not support RTS1 and CTS1 and so you will not be able to ‎perform hardware handshaking when using the UART. Serial buffers are so large these days that ‎you probably won’t even notice this restriction, but it is something to be aware of.‎

RP2040 Processor

AUD_LRCLK is shared with CTS1. This means that if you want to use hardware handshaking for ‎the UART communication, you won’t be able to use the digital microphone.‎

Likewise, AUD_BCLK is shared with RTS1, again preventing you from using the microphone and ‎hardware handshaking at the same time.‎

I2C_INT is shared with TX2. This means that you cannot use the ICM-20948 IMU interrupt and ‎SARA DTR / TXD2 simultaneously. You can open the ICM_INT split pad to isolate the IMU interrupt ‎signal.‎

G4, G5, G6, and G7 are shared with the SPI connections SPI_SCK, SPI_COPI, SPI_CIPO and ‎SPI_CS. This should not be an issue for you, but it does mean you cannot close the G4-G7 ‎jumpers to enable access to: SARA_RI, SARA_INT, SARA is On, and SARA_DSR.‎

STM32 Processor

The STM32 Processor Board does not support RTS1 and CTS1 and so you will not be able to ‎perform hardware handshaking when using the UART. Serial buffers are so large these days that ‎you probably won’t even notice this restriction, but it is something to be aware of.‎

The STM32 Processor Board does not support the M.2 TX2 and RX2 pins. This means you cannot ‎use the STM32 to talk to the SARA using any of the dual-UART variants (called variants 2, 3 and 4 ‎in the SARA-R5 System Integration Manual). You cannot, for example, use UART 1 for your LTE ‎traffic and UART 2 for your GNSS data.‎

G7 is not supported on the STM32 Processor Board. This should not be an issue for you, but it ‎does mean you cannot access the SARA is On signal.‎

Hardware Assembly

Now that we are familiar with the hardware on the Asset Tracker Carrier Board, it's time to assemble ‎it with your chosen MicroMod Processor and get it connected to your computer.‎

Inserting Your Processor

With the M.2 MicroMod connector, connecting your processor board is a breeze. Simply match up ‎the key on your processor's beveled edge connector to the key on the M.2 connector. At a 45° ‎angle, insert the processor board to the M.2 connector. The processor board will stick up at an ‎angle as seen here:‎

insert_17

Once the board is in the socket, gently press the Processor down, grab the set screw and tighten it ‎with a Phillip's head screwdriver:‎

press_18

With the Processor secure, your assembled MicroMod Asset Tracker system should look similar to ‎the image below!‎

secure_19

Note There is technically no way to insert the Processor backwards since the key prevents from ‎mating with the M.2 connector. As an extra safeguard to prevent inserting a Processor improperly ‎or with a poor connection, the mounting screw will not match up if the Processor is not plugged in ‎entirely.‎

Connecting Everything Up

Now is a good time to insert the Nano SIM from your service provider. Make sure the orientation ‎matches the symbol on the PCB; the edge with the trimmed corner is inserted first.‎

The LTE and GNSS connections simply screw on to the appropriate SMA connectors. Make sure ‎you check the labeling on the board and connect them the right way round. (LTE is on the Left.)‎

connect_20

With your processor inserted and secured it's time to connect your MicroMod Asset Tracker Carrier ‎Board to your computer using the USB-C connector. Depending on which processor you choose ‎and which drivers you already have installed, you may need to install drivers for your board. Refer ‎to your Processor's Hookup Guide for detailed instructions on how to install them.‎

Software Setup

Note: The software examples assume you are using the latest version of the Arduino IDE on your ‎computer. If this is your first time using Arduino, please review our tutorial on Installing the Arduino ‎IDE. If you have not previously installed an Arduino library, please read through our Arduino Library ‎Installation Guide.

Note: Make sure that for whichever MicroMod Processor you choose, you have the correct board ‎definitions installed.

‎The Asset Tracker examples will run on any SparkFun MicroMod Processor Board (PB) but each ‎PB has a slightly different sequence to follow when uploading and running code. For example, ‎some require a press of the Boot button and others do not. Head over to our MicroMod Processor ‎Boards landing page, find your Processor, and read through its tutorial for help installing your board ‎definition and how to upload the code.‎

We have prepared a complete set of examples showing you how to use all of the features on the ‎Asset Tracker. However, the examples need access to several Arduino Libraries before they will ‎run correctly and so you need to install those too.‎

Installing the MicroMod Asset Tracker Carrier Board Examples

The Asset Tracker examples live on GitHub in the Asset Tracker repository and you will find them in ‎the Examples folder. You can download the complete repository from GitHub as a single .ZIP file by ‎clicking the button below:‎

SPARKFUN MICROMOD ASSET TRACKER EXAMPLES (ZIP)‎

Unzip the .ZIP file and copy all 22 examples to a suitable folder on your computer. We recommend ‎putting them in your Arduino folder.‎

You will see that each example comprises three files. E.g., for Example1:‎

  • AssetTracker_Example1_Blink.ino is the actual example code

  • AssetTrackerPins.h contains the pin definitions to allow each Processor to work correctly with ‎the Asset Tracker

  • AssetTrackerPins.ino contains useful ‘housekeeping’ functions that do things like turn on the ‎SD or IMU power. They are in a separate file to make them easier to update when we add new ‎processor boards and to avoid cluttering up the main example code.‎

When it is time to open and try Example1 select the AssetTracker_Example1_Blink.ino file first. ‎The other two will open automatically as they are in the same folder.‎

SparkFun u-blox SARA-R5 Arduino Library

The SparkFun u-blox SARA-R5 Arduino Library lives on GitHub too and you can either install it ‎using the Arduino Library Manager, or you can install it manually.‎

If you want to install the library using the Arduino Library Manager, then search for ‘SparkFun u-‎blox SARA-R5’.‎

Alternatively, you can download a .ZIP of the library by clicking the button below:‎

SPARKFUN U-BLOX SARA-R5 ARDUINO LIBRARY

Additional Libraries

Once you have the u-blox SARA-R5 library installed, most (but not all) of the examples will work ‎correctly. To allow the full set to run, you also need to install the following libraries:‎

You can install them using the Arduino Library manager by searching for their respective names. ‎Alternatively, you can download the .ZIP for each of them by clicking the buttons below:‎

SPARKFUN ICM-20948 ARDUINO LIBRARY

SPARKFUN MAX1704X FUEL GAUGE ARDUINO LIBRARY

‎[SPARKFUN QWIIC POWER SWITCH ARDUINO LIBRARY

SPARKFUN MICRO OLED ARDUINO LIBRARY

SDFAT LIBRARY

Arduino Examples

Once you have the MicroMod Asset Tracker Carrier Board examples and all of the required libraries ‎installed, it is finally time to run your first example!‎

Example 1: Blink

Baby steps… Example1 checks that you can communicate with the MicroMod Processor Board, ‎compile and upload code successfully.‎

Navigate to the location the Asset Tracker Examples repository downloaded to and open the ‎Examples folder. In that folder you'll find all the examples. Navigate to Example1 and open the file ‎called AssetTracker_Example1_Blink.ino in the Arduino IDE or copy the code below into a blank ‎sketch, select your Board and Port and click "Upload".‎

Copy Code
#include "AssetTrackerPins.h" // Include the Asset Tracker pin and port definitions

#define SERIAL_PORT Serial // This is the console serial port - change this if required

#include <SparkFun_u-blox_SARA-R5_Arduino_Library.h> //Click here to get the library: http://librarymanager/All#SparkFun_u-blox_SARA-R5_Arduino_Library

// Create a SARA_R5 object to use throughout the sketch. Pass it the power pin number.
SARA_R5 assetTracker(SARA_PWR);

void setup()
{
  initializeAssetTrackerPins(); // Initialize the pins and ports (defined in AssetTrackerPins.ino)
}

void loop()
{
  digitalWrite(LED_BUILTIN, !digitalRead(LED_BUILTIN)); // Flash the STAT LED at 0.5Hz (Read-Invert-Write)
  delay(1000);
}

All Example1 does is blink the STAT LED on the Processor Board. That's all it does. Yes, really. But ‎it proves that you have the correct Processor Board selected and that code compilation and upload ‎works. The good stuff comes in the following examples.‎

Example 2: IMU

Example2 demonstrates how to get readings from the ICM-20948 Inertial Measurement Unit on the ‎Asset Tracker. Open AssetTracker_Example2_IMU.ino and upload to the Processor Board. Now ‎open the Serial Monitor or a terminal emulator and connect to the Processor Board at 115200 Baud. ‎If all is well, you should see the following:‎

ex2_21

Click Send or hit Enter and you should then see the following, followed by lots of lovely IMU data ‎scrolling up the screen:‎

click_22

The things to look out for are a 980 milli-g Acceleration in Z - if your board is horizontal. That's ‎gravity. You will also see a reading of the Earth's magnetic field on one or more of the ‎Magnetometer (Compass) axes, but the value will depend on your local Angle Of Magnetic ‎Declination and Inclination. (Strange but true: the strongest magnetic field points downward into the ‎ground in many places.)‎

Example 3: µSD Card

Example3 uses Bill Greiman's SdFat library to print a directory of all the files on your microSD card.‎

The usual restrictions apply we recommend disconnecting the power to your Asset Tracker before ‎removing or inserting the µSD card. Removing the card while powered can cause data corruption.‎

Example 4: MAX17048 Fuel Gauge

Example 4 demonstrates how to use the MAX17048 Fuel Gauge to read the battery charge status.‎

Example 5: Qwiic

Example5 demonstrates how to use the Qwiic bus to talk to an external sensor attached to the Qwiic ‎connector. The example assumes that you have a Qwiic Power Switch attached, but you can adapt ‎the code to use whichever Qwiic board you have available. The Qwiic I2C bus is called Wire on the ‎Asset Tracker.‎

Example 6: I/O Pins

Example6 demonstrates how to configure the D0, D1, A0, A1, PWM0, and PWM1 Input / Output ‎pins.‎

Example 7: GNSS Antenna Power

Example7 is where we communicate with the SARA-R5 for the first time. The power for the active ‎GNSS antenna is controlled by the SARA GPIO2 pin. When the SARA is on and GPIO2 is high, ‎the 3.3V antenna power is enabled. We need to instruct the SARA to enable GPIO2 and set it high ‎via the UART interface.‎

The example code calls enableGNSSAntennaPowr(); and disableGNSSAntennaPower(); which do ‎the heavy lifting for you. Those functions are defined in AssetTrackerPins.in and in turn call the ‎SARA-R5 library:‎

Copy Code
assetTracker.setGpioMode(assetTracker.GPIO2, assetTracker.GPIO_OUTPUT, 1); // Enable

and

Copy Code
assetTracker.setGpioMode(assetTracker.GPIO2, assetTracker.GPIO_OUTPUT, 0); // Disable

There is no indicator LED to tell you if the antenna power is on. You can, if you wish, use a digital ‎multimeter to probe carefully on the center pin of the GNSS SMA connector. You will see voltage ‎toggling between 3.3V and 0V.‎

Important! When probing the GNSS SMA connector be very careful to avoid static discharge. A ‎grounding strap is recommended to prevent damaging the antenna and board from static discharge.‎

This example demonstrates that serial communication is taking place between the Processor Board ‎and the SARA-R5.‎

Example 8: External SPI

Example8 shows how to use the SPI Breakout Plated-Through Holes (PTHs) on the left edge of the ‎board. The example assumes you have a SparkFun Micro OLED Display connected, but you can ‎adapt the code to talk to whichever SPI board you have available. The SPI port is called SPI on the ‎Asset Tracker.‎

Example 9: VIN

Example9 demonstrates how to read the VIN bus voltage using the resistor divider on the Asset ‎Tracker. The function readVIN() in AssetTrackerPins.ino automatically converts the Analog To ‎Digital Converter result into voltage correctly for the different Processor Boards.‎

Example 10: IMU Wake-On-Motion

Example10 demonstrates how the ICM-20948 IMU can be configured to detect motion or an impact. ‎This example could be a key part of your final asset-tracking code.‎

Example 11: GNSS GPRMC

Example11 demonstrates how to read the Asset Tracker’s location using the u-blox M8 GNSS ‎receiver built into the SARA-R5. The GNSS generates an NMEA GPRMC data stream and our ‎SARA-R5 library does the heavy lifting for you, extracting the latitude and longitude etc. as numbers.‎

Example 12: Identification

Example12 is the first example which communicates with the LTE part of SARA-R5. The example ‎reads data from the SARA including its ID, firmware version, serial number, IMEI and subscriber ‎number. The subscriber number - if present - comes from the SIM. This example demonstrates that ‎the SIM is inserted correctly.‎

Example 13: Network Information

Example13 is the first example which checks that the SARA is receiving an LTE signal. The code ‎prints the received signal strength, registration status and data “context ID”. The SARA reads your ‎operator details from the SIM and uses those when registering on the network.‎

It is important that you run examples 13, 14 and 17 in order as each plays a role in making sure the ‎SARA's data connection is configured correctly.‎

Example 14: Register Operator

Example14 shows if you are already connected to a network and gives you the opportunity to ‎register on a different network (if one is available and if your SIM supports this). You can use this ‎example to list all of the LTE operators the SARA can detect, but you will only be able to connect to ‎networks supported by your SIM.‎

Example 15: Receive SMS

For many applications, good old Short Message Service text messaging is a good solution. ‎Example15 demonstrates how to read and print any existing text messages in the SARA's memory. ‎The code will then wait for a new message to arrive and will print it when it does.‎

Incoming messages are automatically marked as read once they have been printed by the code. ‎You can force the code to print all the messages in memory by commenting the line which says:‎

Copy Code
if (unread == "REC UNREAD") // Only print new (previously-unread) messages.

com5_23

Example 16: Send SMS

Example16 demonstrates how to send an SMS message to another phone or Asset Tracker. The ‎code will ask for the destination number, followed by the message. If you are using the Arduino IDE ‎Serial Monitor, you can type these into the text box at the top of the window and then click Send or ‎press Enter. If you are using a terminal emulator, type the number and then press Enter (or add a ‎newline / line feed character (“\n” or 0x0A)) to end the message.‎

Example 17: Packet Switched Data

Example17 is an important example as it configures the “Context Identifier” for your mobile data ‎connection. The SARA will read details of the data context from the network and SIM and you can ‎confirm which one you want to use. The first context may be blank; select one that shows a ‎sensible name and IP address for your service provider. In the screenshots below, we select ‎option 1:‎

ex17_24

com5_25

The code provides a warning that “deactivate profile failed”. We see this because the SARA needs ‎to disconnect from a profile before it can connect to a new one, and in this case, this failed because ‎there was no profile active. Don’t worry about this warning, it is just there for information. The ‎example shows that our connection was successful by displaying the Internet Protocol (IP) address ‎the SARA has been allocated by the service operator.‎

Example 18: Ping

Example18 tests the SARA's data connection by performing one of the oldest and shortest data ‎transfers going… A ping!‎

The code will ask for the name of the server you want to ping. www.google.com is a good choice, ‎but www.sparkfun.com works too! If the ping is successful, you will see the time it took for the ‎ping to do a round trip in milliseconds.‎

ex18_26

If the ping is not successful, one option to find out why is to uncomment the line which says:‎

Copy Code
assetTracker.enableDebugging(SERIAL_PORT); // Uncomment this line to enable helpful debug messages

This enables a bunch of helpful debug messages that print in the Serial Monitor or your terminal ‎emulator window. After uncommenting the above line, upload the code again.‎

Look for any messages that include +UUPINGER:. That will give you the cause of the PING ERror. ‎The SARA-R5 AT Command Reference contains the full list of Ping error codes in Appendix A.10.‎

For example, error 8 means that the SARA “Cannot resolve host” which is usually a sign that a ‎Domain Name Server (DNS) is not available. Error 17 indicates “Packet Switched Data connection ‎not established”. If you see errors like this, please make sure you ran examples 13, 14, 17 and 18 ‎in order. Each builds on the previous example.‎

Example 19: ThingSpeak

Example19 demonstrates how to send data to ThingSpeak using HTTP POST or GET.‎

Prior to using this example, you need to complete the following steps:‎

  • Create a ThingSpeak User Account here

  • Create a new Channel by selecting Channels --> My Channels --> New Channel

  • Note the Write API Key and copy/paste it into myWriteAPIKey in the example code.‎

The example code reads the temperature from the Asset Tracker IMU and POSTs it to ThingSpeak. ‎It will be added to your ThingSpeak channel as "Field 1".‎

Note: The IMU temperature is always a few degrees warmer than ambient as it is inside a nice ‎warm chip busy running accelerometer, gyro and compass sensors!‎

If you open your serial monitor at 115200 baud the code prints out over serial the data sent to ‎ThingSpeak:‎

serial_27

Check your ThingSpeak channel and you should see data posted to it similar to the screenshot ‎below:‎

channel_28

Examples 20-22: Production Tests‎

Examples 20 - 22 are the ones we use using Asset Tracker production tests to check if the SARA’s ‎I/O pins are connected correctly. We’ve included them as you might find them useful if you want to ‎control the pins on the SARA. The examples use the SARA’s +UTEST mode to control the pins. ‎Please consult the SARA-R5 AT Command Reference for further details.‎

Troubleshooting

In this section we'll go over a few troubleshooting tips for common snags and questions using the ‎MicroMod Asset Tracker Carrier Board.‎

LTE Network Availability

The SARA-R5 supports LTE-M and NB-IoT data communication for multi-regional use. Please ‎check the LTE signal availability for your area before purchasing a SARA-R5 product and selecting ‎an LTE service provider / operator.‎

Data Connectivity

When working through the data connectivity examples, it is important that you run examples 13, 14 ‎and 17 in order, before moving on to example 18 or 19. Each example builds on the last and ‎together they configure the SARA’s data connection correctly.‎

TP (1PPS) Pin and LED

At the time of writing, we are shipping the SARA-R5 on the Asset Tracker with firmware version ‎‎02.06 on it. 02.06 contains a feature (which is just a polite name for a bug!) which means the 1 ‎Pulse-Per-Second from the GNSS does work, but the pulse is only ~3 microseconds wide and ‎cannot be adjusted. Handy huh? u-blox are aware of this - in fact, we told them about it - and a fix is ‎coming but they haven’t added it yet. We will keep an eye out for it and update this section once the ‎fix is released.‎

Just to complicate matters, 3 microseconds is too short for the buffer FET and LED connected to ‎the timing pulse to respond. So, we regret that you cannot currently use the TP PTH. We will share ‎the fix with you as soon as we have it. The SARA firmware is easy to update using the Asset ‎Tracker Firmware Update Tool.‎

NB/IoT Compatibility

The SparkFun MicroMod Asset Tracker uses the "00B" product version of the SARA-R5 module ‎‎(specifically the SARA-R510M8S-00B-00). LTE NB-IoT Radio Access Technology, and the LTE ‎FDD bands: 66, 71, 85 are not supported by this version.‎

General Troubleshooting Help

Not working as expected and need help?

If you need technical assistance and more information on a product that is not working as you ‎expected, we recommend heading on over to the SparkFun Technical Assistance page for some ‎initial troubleshooting.

SPARKFUN TECHNICAL ASSISTANCE PAGE

If you don't find what you need there, the SparkFun Forums: MicroMod are a great place to find ‎and ask for help. If this is your first visit, you'll need to create a Forum Account to search product ‎forums and post questions.

SPARKFUN FORUMS: MICROMOD

Resources and Going Further

Now that you've successfully got your MicroMod Asset Tracker Carrier Board up and running with ‎your Processor Board, it's time to incorporate it into your own tracking project! For more information, ‎check out the resources below:‎

MicroMod Asset Tracker Carrier Documentation:‎

u-blox SARA-R5 LTE-M / NB-IoT module Documentation:‎

MicroMod Documentation:‎

Users looking to update the firmware on their Asset Tracker Carrier Board using the MicroMod ‎Update Tool should read through our MicroMod Update Tool Hookup Guide:‎

micromod_29

MicroMod Update Tool Hookup Guide

Follow this guide to learn how to use the MicroMod Update Tool to interact directly with the UART ‎on the MicroMod Asset Tracker's SARA-R5. Using this board, you can talk directly to the module ‎using u-blox's m-center software as well as update the firmware using EasyFlash.‎

メーカー品番 17272
MICROMOD ASSET TRACKER CARRIER
SparkFun Electronics
メーカー品番 17725
MICROMOD SARA-R5 UPDATE TOOL
SparkFun Electronics
メーカー品番 16781
MICROMOD ESP32 PROCESSOR
SparkFun Electronics
メーカー品番 16401
MICROMOD ARTEMIS PROCESSOR
SparkFun Electronics
メーカー品番 16984
SPARKFUN MICROMOD NRF52840 PROCE
SparkFun Electronics
メーカー品番 16791
MICROMOD SAMD51 PROCESSOR
SparkFun Electronics
メーカー品番 15081
QWIIC CABLE KIT
SparkFun Electronics
メーカー品番 17259
FLEXIBLE QWIIC CABLE - 100MM
SparkFun Electronics
メーカー品番 15424
CBL USB2.0 A PLUG TO C PLG 6.56'
SparkFun Electronics
メーカー品番 14743
CABLE A PLUG TO C PLUG 3.28'
SparkFun Electronics
メーカー品番 15192
GNSS MULTI-BAND MAGNETIC MOUNT A
SparkFun Electronics
メーカー品番 13003
GRAPHIC DISPLAY OLED BLUE 0.66"
SparkFun Electronics
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.