Maker.io main logo

Making an Automatic Rotary Zen Garden!

199

2024-08-09 | By Will Siffer

License: Attribution

 

Motivation to relax

When it comes to Zen gardens, I have never really played with them much or thought much of using them. Recently, I was scrolling through social media and saw a project where someone had an automatic Zen garden that used a 3d printer to draw in sand. After some Google searching, I saw some other makers who made similar ones that were rotational. That is where I got the idea that I could practice basic motor control and create this project that goes through my whole design process from beginning to end. 

 

What I ordered from DigiKey

I included a parts list at the bottom of this post, but the key to this project is the 555 timer, the potentiometer, and the motor.

  1. The 555 timer allows me to generate a signal that could control the motor without writing ANY software or programming ANY controllers.

  2. The potentiometer serves as a way to adjust the speed of the motor in real-time.

  3. The motor is ideal for this use since it is a 90-degree output from the original input shaft, and it is geared down to spin at much lower speeds.

The schematic! Featuring DigiKey's Scheme-it design software:

 

 

Here is the schematic I am following for this project. As you can see, it is pretty simple and can be made on a simple breadboard or Digikey Solderful breadboard like I will be doing. The key here is adding the diode across the motor facing the positive connection. As a motor spins, it builds up magnetic energy and electrical energy in the form of a magnetic field. Under normal conditions, this isn't a problem, in fact, it's necessary. Unfortunately, when the power is removed from the motor, it creates a large changing electric field and thus a large change in current. This change of current builds up and results in a large voltage spike that almost always damages the control electronics. From there, this schematic is pretty straightforward and can be made on any small breadboard. Feel free to give it a shot yourself.

Once I assembled the circuit, I used the oscilloscope and power supply to measure the circuit. In my video above, I encourage you to take a look at my explanation of the circuit. In the video, I discuss how the circuit works and give a visual!

Designing the enclosure:

The next step of the project is to design the controller. Since I have a 3d printer, I am able to print off iterations of the design and change things as I go. This is the part of the project I encourage you to make your own little twist to; here are some examples!

  • I made my rake have 2 different patterns that offset each other in the video; can you make yours flat on one side?

  • What other patterns can you make with your rake?

  • I thought it could be fun to design a rake that wasn't flat, maybe it would be cool to have an S-shaped one! Could you use a different motor to make the sand garden spin even slower?

  • How else can you be creative?

My overall design process is as follows for the enclosure:

  • Design the motor so I have something to work off of.

  • Design the upper part of the enclosure that will hold the sand.

  • Design a way for the sand to not fall down into the motor.

  • Design a way to hold the circuit board and to hold the power cord.

The beauty of this project is its simplicity. I encourage you to make it your own if you decide to make it yourself. You could even use the circuit to control a motor for different projects!

I hope this project inspired you to start a weekend project of your own. All in all, it took about 3 days of work for me to finish this project, so I would say it's doable for someone to complete in a pretty short time. If you decide to make this or something similar, I would recommend you use it as a project where you design it mostly yourself. It's great to work through your design process sometimes and challenge yourself in new ways.

Until next time, my name is Will, and I hope you have a great time making.

メーカー品番 3801
GEARMOTOR 120 RPM 3-6V BI-METAL
Adafruit Industries LLC
メーカー品番 NE555P
IC OSC SINGLE TIMER 100KHZ 8-DIP
Texas Instruments
メーカー品番 PTN16-D100115K1B1
POT 100K OHM 1/8W CARBON LINEAR
Same Sky (Formerly CUI Devices)
メーカー品番 IRF510PBF
MOSFET N-CH 100V 5.6A TO220AB
Vishay Siliconix
メーカー品番 VEL05US060-US-JA
AC/DC WALL MOUNT ADAPTER 6V 5W
XP Power
メーカー品番 1N4001RLG
DIODE STANDARD 50V 1A AXIAL
onsemi
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.