Maker.io main logo

Make Halloween Shine: Spooky Floating Candles from LED Torch Kits!

50

2024-10-10 | By Kitronik Maker

License: See Original Project LEDs / Discrete / Modules

Courtesy of Kitronik

Guide by Kitronik Maker

Happy Halloween 2023 from Kitronik! For those of you celebrating, we are bringing ‎you a magical make that will have your home, office or classroom feeling like a ‎haunted house! ‎

Follow along with Emma's step by step instructions and make your own spooky ‎candles. Please share with us any you make so we can share them on social ‎media too.‎

We Have Used (Per Candle):‎

  • ‎1 x Yellow Flickering Candle LED

  • ‎1 x LED Torch Kit with Battery

  • Hot Glue Gun

  • Hot Glue Sticks

  • Sheets of A4 Card

  • Sticky Tape. (We used White PVC Tape for Colour)‎

  • Fishing Line or other less visible threads for hanging

  • Scissors

    • Optional:‎

      • Polymorph for forming a Flame Shape.‎

How We Made Them:‎

STEP 1 – BUILDING THE TORCH KIT:‎

building_1

Solder together your Torch Kit, leaving out the white LED. Save this for another ‎project!‎

STEP 2 – CONNECT THE FLICKER LED:‎

connect_2

Solder in its place a Flickering Candle LED - these are awesome to have in your ‎toolkit for atmospheric makes like this!‎

STEP 3 – PREPARING THE CANDLES FOR LATER STEPS:‎

preparing_3

For hanging the candles later, tie fishing line securely through the top mounting ‎hole and up between the legs of the LED.‎

STEP 4 – (OPTIONAL) POLYMORPH:‎

step4_4

Melt some polymorph in boiled water and form a flame shape over the LED and ‎incorporate the fishing line into it, ensuring the candle hangs from its centre. ‎Polymorph is translucent and will diffuse the light from the LED, but it’s important ‎that you don’t make it too thick so that the light can still be seen well.‎

STEP 5 – MAKING THE CANDLE BODY:‎

making_5

Noting the size of the board, roll up your card to form the body of the candle. Make ‎a note of where the board will want to sit inside and cut a hole in the card where the ‎switch will be.‎

STEP 6 – TAPE IT:‎

tapeit_6

Secure the rolled card by wrapping it with tape.‎

‎ ‎STEP 7 – HOT GLUE:

hot_7

Using the hot glue, coat the outside of the card thinly to mimic the appearance of ‎wax, leaving the switch hole open.‎

STEP 8 – PLACING BOARD & SWITCH:‎

Insert the board, with a little glue on the sides to hold it in place. Make sure the ‎switch is able to poke through the hole you cut for it.‎

‎ ‎STEP 9 – CAP THE BASE:

cap_8

Add a cap to the top and bottom, using discs of card (one with a hole and a slit for ‎the LED) to support another thin layer of glue.‎

‎ ‎STEP 10 – DECORATION:‎

decoration_9

Add details to your candle! You can form shapes like droplets on a heat-resistant ‎mat, and then use the tip of your hot glue gun to melt the top of them onto the ‎candle. You can also use your glue gun to make creepy cobwebs by flicking it ‎quickly over the heat-resistant mat, perfect to dress these for Halloween! You can ‎also paint them, or even do this entire make using brightly coloured hot glue, or ‎even glittery hot glue!‎

  • ‎ ‎Make sure you don't miss out on other exciting maker news by signing up ‎for our newsletter here.‎

‎©Kitronik Ltd – You may print this page & link to it but must not copy the page or part thereof ‎without Kitronik's prior written consent.‎

メーカー品番 2114
LED TORCH KIT WITH BATTERY
Kitronik Ltd.
メーカー品番 TC/TC-Q-LT GEN II
HOT MELT TC/TC-Q LOW TEMP
3M
メーカー品番 3748-V-O-Q-5/8"X8"
HOT MELT ADHESV 5/8"X8" 1=1STICK
3M
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.