Maker.io main logo

Intro to Embedded Linux Part 2 - Yocto Project

6,076

2021-09-20 | By ShawnHymel

License: Attribution Single Board Computers

In the previous tutorial, we demonstrated how you can create a custom Linux image for a single board computer using Buildroot. This time, we switch to the Yocto Project.

The Yocto Project is a collection of tools and metadata (configuration files) used to generate custom Linux images. It offers more control than Buildroot, but it can be cumbersome to learn and use.

See here if you would like to watch this tutorial in video format:

 

Required Hardware

I will try to explain what is happening at each step in these tutorials so that you can generalize the instructions to almost any single board computer (assuming the board is supported by the build system). However, for the demonstration, I will be using the following platform:

STM32MP157D-DK1

You will also need an SD card. The STM32MP157D-DK1 kit should come with an SD card. In addition, you will need a USB-C power supply capable of supplying 5V, 3A.

Required Software

You will need Linux for this project, as all of the tools we are using must be run in Linux. I will show steps that work in Ubuntu and Linux Mint (and likely other flavors of Debian), but you can probably get almost any Linux distro to work. LiveCD, dual-booting, Windows Subsystem for Linux (WSL), and pre-made Docker images will also likely work.

I recommend using one of the distributions listed here, as they are known to work with the Yocto Project.

The Yocto Project requires at least 50 GB of harddrive space to download and build source files.

I also recommend using a fairly modern computer with at least 4GB of RAM. While you can probably build a Linux image in a Raspberry Pi, expect it to take a very long time.

Definitions

Terminology in the Yocto Project can be a little confusing. These definitions should help you along the way:

  • OpenEmbedded: build system and community

  • The Yocto Project: umbrella project and community

  • Metadata: files containing information about how to build an image

  • Recipe: file with instructions to build one or more packages

  • Layer: directory containing grouped metadata (start with “meta-”)

  • Board support package (BSP): layer that defines how to build for board (usually maintained by vendor)

  • Distribution: specific implementation of Linux (kernel version, rootfs, etc.)

  • Machine: defines the architecture, pins, buses, BSP, etc.

  • Image: output of build process (bootable and executable Linux OS)

Install Dependencies

Run the following to install dependencies on your host computer:

Copy Code
sudo apt update
sudo apt upgrade
sudo apt install -y bc build-essential chrpath cpio diffstat gawk git texinfo wget gdisk python3 python3-pip

You will also need the following to build the image for the STMP32MP1:

Copy Code
sudo apt install -y libssl-dev

Because the Yocto Project tools rely on the “python” command, you will likely need to alias “python” to “python3.” Edit your .bashrc file:

Copy Code
vi ~/.bashrc

Scroll to the bottom and add the following to a new line (press ‘a’ to append new text):

Copy Code
alias python=python3

Save and exit (‘esc’ followed by entering “:wq”). Re-run the .bashrc script to update your shell:

Copy Code
source ~/.bashrc

Check your Python version:

Copy Code
python --version

It should say something like “Python 3.8.xxx.” 

Donwload Layers

Download the Yocto Project poky reference distribution:

Copy Code
mkdir -p ~/Projects/yocto
cd ~/Projects/yocto
git clone git://git.yoctoproject.org/poky.git
cd poky

You will want your poky layer branch to match the branches of all other third-party layers you download (such as the STM32MP1 BSP). You can view the available poky release names here: https://wiki.yoctoproject.org/wiki/Releases. We’re going to have all layers be on the “dunfell” branch.

Copy Code
git checkout dunfell

Next, you’ll want to download the STM32MP board support package (BSP) as a separate layer:

Copy Code
cd ~/Projects/yocto
git clone git://github.com/STMicroelectronics/meta-st-stm32mp
cd meta-st-stm32mp
git checkout dunfell

We checkout the dunfell branch so that it matches the branch name of the poky layer.

View the readme to see what other layers are needed for this particular BSP:

Copy Code
less README

In there, you can see that we need the meta-openembedded layer. Specifically, we need the meta-oe and meta-python layers in the meta-openembedded layer (I only found this out by looking at the errors reported during the build process).

Copy Code
cd ~/Projects/yocto
git clone git://github.com/openembedded/meta-openembedded.git
cd meta-openembedded
git checkout dunfell

View the readme to see if there are any dependencies we need to download for meta-openembedded:

Copy Code
less README

You should not need to install any other layers to build our initial image for the STM32MP157D-DK1.

Configure Build

We start by creating a build environment (to give us access to tools like “bitbake”). Note that the oe-init-build-env script will create an initial “build-mp1” folder and automatically change directories to it.

Copy Code
cd ~/Projects/yocto
source poky/oe-init-build-env build-mp1
cd build-mp1

You can view the layers that will be included in the build with the following:

Copy Code
bitbake-layers show-layers

You should only have the default poky layers to start. We need to edit bblayers.conf in our build to add the necessary STM32MP BSP and dependency layers:

Copy Code
vi conf/bblayers.conf

Update the BBLAYERS variable to be the following (change <username> to your actual username):

Copy Code
BBLAYERS ?= “ \
  /home/<username>/Projects/yocto/poky/meta \
  /home/<username>/Projects/yocto/poky/meta-poky \
  /home/<username>/Projects/yocto/poky/meta-yocto-bsp \
  /home/<username>/Projects/yocto/meta-openembedded/meta-oe \
  /home/<username>/Projects/yocto/meta-openembedded/meta-python \
  /home/<username>/Projects/yocto/meta-st-stm32mp \
  “

Save and exit. Check the layers again with:

Copy Code
bitbake-layers show-layers

You can view the available machine names and settings in ~/Projects/yocto/meta-st-stm32mp/conf/machine. We’ll use “stm32mp1” for our build. To do this, edit local.conf:

Copy Code
vi conf/local.conf

Change the MACHINE variable to the following (comment out the “qemu” emulator and add “stm32mp1” as the machine):

Copy Code
#MACHINE ??= “qemux86-64”
MACHINE = “stm32mp1”

If you are working with a low-end machine (less than ~4GB of RAM), you might run into this error at the end of the build process:

Copy Code
xz: Memory usage limit is too low for the given filter setup.
xz: 1,250 MiB of memory is required. The limit is 918 MiB

This is because the xz compression tool looks at physical RAM when determining the limit, regardless of any swap partition you might have. If you are working with less than 4 GB of RAM, I recommend setting up a swap partition with 8 GB of RAM. You then need to force xz to see that swap partition by setting its memory limit to be higher. We can pass this argument to xz in local.conf by adding the following line (e.g. after you set the MACHINE variable):

Copy Code
# Configure xz (for low-end host machines with low RAM and lots of swap)
XZ_DEFAULTS = ”--memlimit=1500MiB”

Save and exit.

Configure Kernel

Now that your build system is set up, you can make changes to the kernel. To do that, enter:

Copy Code
bitbake -c menuconfig virtual/kernel

Note that the first time you run bitbake for a particular build, it will take some time parsing all the required metadata. This could take an hour or more, depending on your host computer, so be patient.

After it finishes, you should be presented with a menu:

Yocto Project kernel menuconfig

You can change various kernel settings. However, we will leave everything at their defaults for now, so just select Exit and press ‘enter’.

Build Image

The time has come to actually build your image! We need to choose an image to build. I recommend looking through the available images here that are supported by the default poky installation. You’re welcome to use one of them.

Vendors may also provide additional images. For example, ST maintains OpenSTLinux, which is a separate layer used to build different distributions for ST boards. It contains some libraries like qt, which are great for creating graphical interfaces. However, we won’t need any of those extra packages, so we’ll skip adding the OpenSTLinux layer and just focus on the bare minimum, which is provided by the core-image-minimal image.

Once you have everything configured to your liking, just run the following command:

Copy Code
bitbake core-image-minimal

The first time you build an image with bitbake, it will likely take many hours (my first build took around 5-6 hours). One big advantage of the Yocto Project is that it builds everything in stages and layers. If you make any changes (e.g. add a layer, change to a different image, tweak kernel settings), subsequent builds will take far less time. This speeds up development process when you are trying to add low-level support in Linux.

If you see any errors, read them carefully! Missing .h files probably means you’re missing a package, so find a way to install it (e.g. apt install). The great news is that the build process will pick up where it left off, so you won’t need to build from scratch again.

If you need to start over (e.g. you press ‘ctrl + c’ or something gets corrupted/tainted), you can run the following:

Copy Code
bitbake -c cleanall core-image-minimal

If you really want to clean out everything (because something still is not working after calling bitbake cleanall), you can simply delete the tmp folder in your build (e.g. build-mp1) folder:

Copy Code
rm -rf tmp

Once building is complete, you can find all of the output images in the deploy folder:

Copy Code
ls tmp/deploy/images/stm32mp1

We will construct a bootable SD card using some of these image files in the next tutorial.

Recommended Reading

The following material should help you as you continue your embedded Linux journey:

ST has a great workshop series on the STM32MP1 where you can learn more about the hardware, drivers, Linux, etc.

Robert Nelson at Digi-Key maintains a great series of getting started guides with Yocto for various boards that you can view here.

メーカー品番 STM32MP157D-DK1
DISCOVERY STM32MP157D EVAL BRD
STMicroelectronics
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.