Maker.io main logo

How To Make A Custom LED Picture Frame

25

2022-08-18 | By Kitronik Maker

License: See Original Project

Emma shows you how to make a custom LED picture frame, using our LED picture ‎frame kit. Although there is quite a sizable parts list, the step-by-step instructions ‎should make it a breeze.‎

As always, the DXF file is freely downloadable and can be used as is or tweaked to ‎suit your needs. Let's get stuck in!‎

You Will need:‎

Frame Parts:‎

  • A 3mm material of your choice for the frame - we used American Walnut ‎Veneered MDF
  • ‎2mm Laser Compatible MDF
  • ‎4mm Laser Compatible MDF
  • ‎0.8mm Clear Polypropylene
  • ‎8 x 5mm LEDs of your choice (We used 3527)‎
  • Lengths of red and black wire
  • A hinge with appropriate screws for the stand
  • ‎2 x 6mm M3 Pan Head Screws‎

Electronics enclosure:‎

  • ‎3mm Black Acrylic
  • ‎4 x 12mm M3 Pan Head Screws
  • ‎4 x M3 Hex Nuts
  • ‎4 x 6mm Plastic Spacers
  • A length of heat shrink tubing
  • ‎3 x AA Batteries‎

‎How To Make A Custom LED Picture Frame:‎

custom_1

Once you've got all of the parts/materials you'll need, grab the DXF. You can either ‎go straight to your laser cutter or load it into your favourite CAD software for some ‎tweaking.‎‎ ‎

Step 1: To the Laser Cutter:‎

laser_2

Cut out the DXF, using the above image as a guide. The parts that you want to ‎keep are shaded in. Cut the Thicker frame pieces from your veneered MDF, the ‎thin spacer rectangles from 2mm MDF, the back and stand from 5mm MDF, the ‎blue rectangle from clear polypropylene, the small tabs from the same veneered ‎material as the frame, and the small enclosure from 3mm black acrylic.‎‎ ‎

Step 2: Soldering the LEDs:‎

solder_3

Solder together your LEDs in carefully in right-angled groups of four, positive leg to ‎positive leg and negative leg to negative leg, so they are in parallel. Make sure to ‎account for the shape of the frame and make sure the LEDs fit out of the holes in ‎the frame. Attach one colour of wire (we used red) to the positive side of each set, ‎and another (we used black) to the negative. Then connect each of the same ‎colour together.‎‎

‎Step 3: Assembling and Mounting the Kit:‎

assemble_4

Assemble your kit using the kit instructions, and mount it into the enclosure as per ‎the above image:‎‎ ‎

Step 4: Assembling the Back:‎

back_5

Assemble the back by attaching the stand to the back panel. This can be done in ‎any way you feel is appropriate.‎‎ ‎

Step 5: Assembling the Frame: ‎

frame_6

Assemble the back of the frame as shown, screwing the tabs into place. Glue the ‎spacer to the inside of this piece.‎‎ ‎

Step 6: Final Assembly: ‎

final_7

Make an electronics sandwich! Stick together the four front pieces, allow to dry, ‎and push the LEDs into the holes. Find where the wire will exit and cut a little piece ‎out of the MDF spacer accordingly. Now glue the front, LEDs still inserted, down ‎on to the spacer. Clamp until dry, slot in your Polypropylene window and photo, pop ‎on the back and you’re done!‎‎

‎One of the best sources of new Kitronik information is our Newsletter. To make ‎sure you always know what's going on, sign up for our newsletter here! The ext. ‎one's a good one, don't miss it!‎

‎©Kitronik Ltd – You may print this page & link to it but must not copy the page or part thereof ‎without Kitronik's prior written consent.‎

メーカー品番 3527
LED RGB DIFFUSED 5MM T/H
Kitronik Ltd.
メーカー品番 EN91
BATTERY ALKALINE 1.5V AA
Energizer Battery Company
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.