Maker.io main logo

Getting Started with PicoVision

143

2024-02-08 | By Pimoroni

License: See Original Project Raspberry Pi SBC

Courtesy of Pimoroni

Guide by Pimoroni

PicoVision is a powerful digital video stick for bold audio-visual adventures. It ‎uses two RP2040 chips (one as a CPU and one as a GPU) and you can plug it ‎in to just about any HDMI display. Here's how to make it do some stuff!‎

This beginner friendly tutorial will cover:‎

  • how to plug everything in
  • how to get to navigate our launcher and examples
  • how to get talking to PicoVision with MicroPython and Thonny
  • how to make it run DOOM (important!)‎

What you'll need

  • A PicoVision or PicoVision + Accessory Kit
  • A HDMI display of some sort
  • Some powered speakers (if you want to make noise)
  • A USB keyboard (if you want to play DOOM).‎

If you didn't get the accessory kit, you'll need

Assembling the PicoVision Accessory Kit

Here's what you get in the Accessory Kit:‎

kit_1

To get started, plug one end of the HDMI cable into a spare HDMI connector ‎on your monitor or TV. The other end plugs into the HDMI shaped connector ‎on PicoVision (it's labelled DV, for legal reasons.)

board_2

The USB cable goes from your computer to the micro-USB port on the Pico W, ‎this is how we'll provide it with power and also how we'll program the board. ‎If you're just checking out the pre-loaded examples and aren't planning on ‎programming the board just yet you could plug it into any convenient USB ‎power source (perhaps your TV has one?).‎

vision_3

That's all you need to plug in to get started, set aside the microSD card and ‎the cursed accessory injector cable for later :)‎

Using the launcher (PicoVisiOS)‎

PicoVision comes with MicroPython, examples, and a launcher pre-installed ‎for your comfort and convenience.‎

Once you've connected up both the HDMI cable and USB power, hopefully ‎you'll see our launcher on your display (there's a short delay whilst the GPU ‎firmware fires up). If you don't, double check that you've got your TV or ‎monitor set to the correct HDMI channel. If that doesn't help, try hitting ‎PicoVision's reset button in case something's gone awry on startup. The blue ‎ACT light should pulse whenever the RP2040 GPU is happy and doing its ‎thing.‎

Once you're up and going, you can navigate up and down the launcher with ‎the A and X buttons. Press Y to run an example.‎

Hit RESET when you're done with an example and want to return to the menu. ‎Note that the RESET button cuts power to both CPU and GPU, so your ‎monitor might flicker/ reset momentarily as it loses connection.‎

Talking to PicoVision with Thonny

To program PicoVision (or to edit the files on it), you'll need to talk to it ‎through an interpreter - we're using Thonny, which is available for Windows, ‎Mac, or Linux.‎

  • Install the latest version of Thonny. We recommend downloading it ‎from the Thonny website as package managers do not always have ‎the newest version.‎
  • Open up Thonny. Make sure the interpreter (shown in the box on the ‎bottom right corner) is set to 'MicroPython (Raspberry Pi Pico)'.‎
  • Plug your PicoVision into your computer if it's not plugged in already. ‎Because PicoVision is busy running the launcher program, main.py will ‎already be running, you may need to interrupt it with the stop button in ‎Thonny before sending it any instructions. In recent versions of Thonny, ‎there's an option to interrupt running programs automatically - if you ‎want to turn that on it's under Tools > Options > Interpreter > Interrupt ‎working program on connect.
  • After you press stop, you should get a MicroPython prompt that looks ‎something like this. The >>> in the 'Shell' box tells you that PicoVision is ‎talking to your computer and is ready to accept instructions.‎

prompt_4

If you're having trouble using Thonny to communicate with your board, ‎there's some troubleshooting suggestions at the link below:‎

EDITING FILES

Using Thonny, you can open up the .py example files on the device and edit ‎them. To see the files on your board, you will need to have the Files window ‎visible - if you can't see it, you can make it show up with View > Files.‎

edit_5

The top box can be used to browse the local files in on your computer, and ‎the bottom box shows the files on your board. If you want to transfer files to ‎‎(or from) your board, right click on the file you want to copy and select ‎‎'upload to /' or 'download to /'.‎

ADDING YOUR WI-FI CREDENTIALS

Some of the examples (like Seafax) need to connect to the internet to do ‎anything fun. To connect to your wi-fi network PicoVision will need to know ‎your wireless network details - these will be stored in a file ‎called secrets.py which should already exist on your board.‎

Double click on it in the Files window to open it up and edit in your network's ‎SSID and password - both SSID and password should be between quote ‎marks "like this". Note that SSID and password are case sensitive!‎

add_6

Once that's done, click the save icon in the toolbar to save your changes.‎

Hit the RESET button on the board to reload the launcher - if you got your ‎credentials correct hopefully now the wireless examples should be able to ‎connect to the internet!‎

RUNNING EXAMPLES THROUGH THONNY

You can run any of the .py example files stored on PicoVision by double ‎clicking on them in the Files window to open them up and then pressing the ‎green run button in Thonny. Running files like this instead of through the ‎launcher has the advantage that you can view any console messages and ‎errors that your code produces - this is very useful when writing your own ‎code.‎

Writing Your Own Code

Perhaps you'd like to try that now? Here's how to do some basic stuff with ‎PicoVision.‎

HELLO WORLD

Here's a basic example you can run to get some text on your display, quick ‎stat! Copy and paste it into a new tab in Thonny and press the green run ‎button.‎

Copy Code
from picovision import PicoVision, PEN_RGB555

display = PicoVision(PEN_RGB555, 640, 480)

WHITE = display.create_pen(255, 255, 255)

display.set_pen(WHITE)
display.text("Hello PicoVision!", 0, 0, 640, 4)
display.update()

You'll need to specify a few things when setting up your PicoVision display. ‎

Firstly, the pen type - we're using PEN_RGB555 which is 16 bit / 32k colour. ‎You'll also need to specify the width and height of your display (here's we're ‎using 640 x 480 pixels). You'll want to set these to a resolution that your ‎monitor is capable of supporting.‎

Note that higher resolutions (and larger pen types) are slower to refresh, so ‎you might need to experiment with these a bit to find the best settings for ‎your application.‎

We've added some convenient shortcuts for common pen type/resolution ‎combos, so as an alternative you could do this:

Copy Code
from modes import VGA

display = VGA()

WHITE = display.create_pen(255, 255, 255)

display.set_pen(WHITE)
display.text("Hello PicoVision!", 0, 0, 640, 4)
display.update()

Click here to find out more about pen types and modes.‎

Here's what the rest of the code does:‎

create_pen creates a pen colour for us to draw with. The numbers specify the ‎RGB colour on a scale between 0 and 255 - in this case white. We then ‎specify what colour we want to draw with set_pen.‎

text writes text to the screen buffer. When using a bitmap font, the '0, 0' is the ‎x/y co-ordinates of the top left of the text. '640' is when text will start ‎wrapping onto the next line (so needs to be the width of the screen in most ‎cases). The final number '4' is the scale of the text, reduce or increase it to ‎shrink or embiggen!

update updates the screen. You can of course draw multiple things to the ‎screen buffer before triggering an update.‎

The default font is bitmap6, which is all uppercase and a little small and blocky. ‎Check out the other hello world examples in the /basic directory for ‎examples of how to change the font and how to use fancy new vector fonts ‎👀

USING THE BUTTONS

Here's a simple demo of how to read the buttons on PicoVision. Note that the ‎Y button is wired to the CPU / Pico W - this means you can read it with ‎standard MicroPython machine commands. Buttons A and X are wired to the ‎GPU / RP2040 so you'll need to read them slightly differently (using your ‎PicoVision display class):‎

Copy Code
from picovision import PicoVision, PEN_RGB555
import machine
import time

display = PicoVision(PEN_RGB555, 640, 480)

button_y = machine.Pin(9, machine.Pin.IN, machine.Pin.PULL_UP)

print("Press a button!")

while True:
if button_y.value() == 0:
print("Y is pressed")
time.sleep(0.5)
if display.is_button_x_pressed():
print("X is pressed")
time.sleep(0.5)
if display.is_button_a_pressed():
print("A is pressed")
time.sleep(0.5)

MAKING NOISE

We've ported some of the synth functions that we wrote for our Space ‎Unicorn boards to PicoVision - here's a simple demo of how you can use ‎these functions to play notes.‎

The audio jack on PicoVision outputs unamplified line level audio, so you'll ‎need to connect it to powered speakers or similar to hear noise.‎

How to play DOOM

Okay, on to serious business!‎

Here's how you can run Doom on PicoVision to thrill, impress and awe your ‎lovely nerdy friends.‎

FORMATTING THE SD CARD

Our SD cards come with Raspberry Pi OS pre-installed on them, so you'll ‎probably want to format it before use so that you don't have a load of ‎unnecessary files cluttering up the place and causing confusion.

‎Raspberry Pi Imager (available for Windows, MacOS or Linux) is a nice way ‎of doing this as it get rids of any partitions for you as well as formatting the ‎SD card in a Pico-friendly format. After you've downloaded and installed it, ‎click on the 'CHOOSE OS' button, and scroll down to the bottom of the list till ‎you get to the 'Erase' option.‎

format_8

Connect the microSD card to your computer (if you have a laptop with a ‎SD/microSD sized slot this is easy, otherwise you may need to use a USB ‎card reader). Click the 'CHOOSE STORAGE' button, choose your SD card, and ‎then click 'WRITE' to start the format.‎

DOWNLOADING THE FILES

Head over to our pal Mike's fork of rp2040-doom to download the files.‎

First of all, you'll need to download the data file doom1.whx (this is the ‎shareware DOOM1.WAD compiled into a Pico-friendly compressed format). ‎Here's a direct link:‎

Once you've downloaded it, this file then needs to be copied to your ‎PicoVision's SD card.‎

Then head to the releases page to download the firmware to run on the Pico ‎W:‎

The zip file you need to download is called something like rp2040-doom-vx.x-‎vision.zip . Unzip it somewhere on your computer.‎

Hold down the BOOTSEL button and tap RESET to put your board into ‎bootloader/DFU mode. You should see a new drive called RPI-RP2 pop up on ‎your computer. Copy doom_tiny_usb.uf2 across to this drive (the board will reboot ‎once you've done that).‎

CONNECTING THE CABLES

Locate the accessory injector cable that we set aside earlier. Plug a USB ‎keyboard into the USB-A port (that's the big rectangular end). Plug the micro-‎USB cable that's plugged into your computer into the cable's micro-USB ‎socket. You can then connect the micro-USB plug on the accessory injector ‎to the power connector on PicoVision.‎

If you want to hear noise, connect the 3.5mm audio jack on PicoVision up to ‎some powered speakers.‎

If all of that went to plan, your PicoVision now should be running Doom. You ‎can play the game with your USB keyboard - just remember that it's cursor ‎keys to move around, we didn't have WASD back then :)‎

PUTTING IT BACK TO HOW IT WAS

Once you're done with playing Doom, you might want to get MicroPython ‎back. You can download the most recent MicroPython .uf2 from the ‎PicoVision releases page:‎

As before, hold down the BOOTSEL button, and tap RESET to put your board ‎into bootloader/DFU mode. Copy the MicroPython .uf2 across to this drive - ‎after it's restarted, you should be able to talk to it with Thonny once again.‎

Next Steps

Hopefully, you should now feel equipped to start writing your own PicoVision ‎programs - as always, drop us a line on social media and let us know how ‎you're getting on! If you're reading this before 17 November 2023, do ‎consider entering our demoscene competition - there's some sizable pirate ‎gift cards to be won.‎

That's all folks!

メーカー品番 PIM372
GRAPHIC DISPLAY TFT WHITE 8"
Pimoroni Ltd
メーカー品番 KEY0104
BLACK USB KEYBOARD
Pimoroni Ltd
メーカー品番 SC0358
CBL HDMI-A M TO MCR HDMI-D M 1M
Raspberry Pi
メーカー品番 PIM631
GALACTIC UNICORN PICO W
Pimoroni Ltd
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.