Maker.io main logo

DIY Circuit Playground Shields

22

2018-01-17 | By Adafruit Industries

License: See Original Project Breadboards Circuit Playground

Courtesy of Adafruit

Guide by Dave Astels

Overview

The CircuitPlayground and CircuitPlayground Express are great boards for learning with. This is largely due to the abundance of sensors and actuators built into the design.

While there is a pile of builtin hardware, it doesn't include everything. Fortunately it does have several useful connections run out to the alligator clip pads around the edge of the board. That means you can connect to it using alligator clip jumpers, like one of these:

Small Alligator Clip Test Lead (set of 12)

Small Alligator Clip Test Lead (set of 12)

Small Alligator Clip to Male Jumper Wire Bundle

Small Alligator Clip to Male Jumper Wire Bundle - 12 Pieces

Construction

Trace the outline and hole placement of the CircuitPlayground onto a piece of prototyping board, then carefully drill the holes to match those on the CircuitPlayground. This is a bit tricky with the prototyping board, but it just has to be close enough.

This prototype is mean to mount the CircuitPlayground onto a breadboard so put a couple 14-pin header strips in the center at DIP-14 spacing.

This prototype is mean to mount the CircuitPlayground

The next step is to add wires. Start by soldering them to the header pins on the other side of the board, clipping them so as to leave plenty of length beyond the holes.

Red for 3.3v & 5v, black for ground, blue of everything else. Mostly this was to make sure you know how everything was oriented when it comes time to mount the CircuitPlayground.

Red for 3.3v & 5v, black for ground

Once all wires are in place, strip the insulation off the ends, starting just inside the corresponding hole.

strip the insulation off the ends

Bend the ends to go around the bolts that will eventually go through the holes. I found it useful to use a longer bolt of the same size (M3 in my case) to bend the wire around. Trim off any excess wire.

Bend the ends to go around the bolts

The next step is to mount the standoffs using a matching bolt, sandwiching each wire loop between a standoff and the board..

I used hex standoffs that take M3 bolts. It's a good size for this application and the hex shape makes it easy to grab when it's time to tighten things.

I used 10mm standoffs because I happened to find some quickly. For future work I ordered a bunch of 6mm ones since 10mm of space is excessive. You can find the spacers in various lengths. Just be sure to get bolts that are short enough to fit when screwed into each end of the standoff (keeping in mind the thickness of the board on each side.

You need 14 standoffs and 28 bolts.

14 standoffs and 28 bolts

Don't tighten them all the way; you'll want to be able to adjust them when mounting the CircuitPlayground. Put each bolt through a hole from below and screw the standoff onto it. Again, don't snug it up, just finger tight.

Do not tighten them all the way

Finally add the CircuitPlayground board, using the remaining bolts. Once all the bolts are in place, tighten everything. If you used hex standoffs, it's easy to grab one with needlenose pliers while tightening the bolts on either end of it.

add the CircuitPlayground board

Now you can plug your CircuitPlayground into a breadboard and start building without worrying about clips popping off or wires getting pulled out.

メーカー品番 3000
CIRC PLAYGROUND CLASS ATMEGA32U4
Adafruit Industries LLC
メーカー品番 3333
CIRCUIT PLAYGROUND EXPRESS
Adafruit Industries LLC
PANEL MOUNT 1K POTENTIOMETER (BR
メーカー品番 1789
PANEL MOUNT 1K POTENTIOMETER (BR
Adafruit Industries LLC
メーカー品番 3255
TEST LEAD GATOR TO TIP PLUG 6"
Adafruit Industries LLC
メーカー品番 2443
SHLDR SCREW RND HEAD HEX #4-40
Keystone Electronics
メーカー品番 MPMS 003 0005 PH
MACH SCREW PAN PHILLIPS M3X0.5
BFirst Industrial
メーカー品番 8022
BREADBOARD GENERAL PURPOSE NPTH
Vector Electronics
メーカー品番 PREC014SAAN-RC
CONN HEADER VERT 14POS 2.54MM
Sullins Connector Solutions
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.