Maker.io main logo

Circuit Playground PZ-1 Pizza Box DJ Controller

51

2016-09-26 | By Adafruit Industries

License: See Original Project Circuit Playground

Courtesy of Adafruit

Guide by John Park

Overview

 

circuit playground

 

DJ Controller

DJ software is fun to use -- who doesn't like to get the crowd bumping? -- but controlling it from a laptop keyboard isn't. So, DJ software is often controlled with a peripheral device that has buttons, knobs, sliders, and turntables for a more natural feel. But you don't need to invest in one, you can build your own: the Circuit Playground PZ-1!

Circuit Playground PZ-1: Pizza Box DJ Controller

Make Your Own

You can build your own DJ controller using any microcontroller that speaks MIDI, including the Circuit Playground. All of the buttons and sensors on the Circuit Playground can be used to trigger MIDI signals that will tell your DJ software what to do. In this project uses the two buttons and eight capacacitive pads, but you could easily modify it to also utilize the accelerometer, temperature sensor, light sensor, and microphone if you like!

Circuit Playground PZ-1: Pizza Box DJ Controller

Paint Your Interface

The Circuit Playground sending MIDI commands is the brains of the operation, but you'll also want an intuitive interface. So design your own using conductive paint! You can paint any pattern you like, running a different conductive paint circuit trace from each capacitive pad on the Circuit Playground. If you want to create precise designs, mask with tape, or create a stencil.

Circuit Playground PZ-1: Pizza Box DJ Controller

Parts 

Materials and Tools

  • Cardboard 12" pizza box (prefereably new, non-greasy)
  • Mylar stencil blank sheets, 12"x12", 7 mil thick
  • Painter's tape
  • Spray adhesive (optional)
  • Utility knife
  • Stencil brush (any size from 2 - 6)

Software

You can use your Circuit Playground PZ-1 with nearly any DJ software. Here are some popular choices:

  • Mixxx (OSX, Windows, & Linux) [Note: Free and open source]
  • Traktor (OSX, & Windows)
  • Serato DJ (OSX, & Windows)

DJ software will usually include an interface for mapping MIDI commands. It can also be helpful to diagnose your MIDI stream with a utility such as:

  • MIDI Monitor for OSX
  • MIDI-OX for Windows
  • KMIDIMon for Linux

Prep the Circuit Playground

Before you get started on making the PZ-1, make sure you've been through the basic tutorials on using the Circuit Playground. You'll need to have installed the Arduino IDE, added the Circuit Playground board to Arduino, and added the Circuit Playground library. This excellent guide, Introducing Circuit Playground and Circuit Playground lesson #0 will show you how to do all of that and get you going.

Circuit Playground PZ-1: Pizza Box DJ Controller

Plug your Circuit Playground into your computer now, and launch the Arduino IDE. Double check that you've selected the board and port as in the Lesson #0 tutorial and are ready to upload code.

USB MIDI with Teensy Core

There are a few different ways to have the Circuit Playground speak MIDI over USB to your computer. For this project you'll install the Circuit Playground Teensy Core board environment called TeeOnArdu into your Arduino IDE.

Add the Teensy Core by clicking Tools > Board > Board Manager... in the Arduino IDE, and then clicking in the search field (it says Filter your search...) and typing Adafruit TeeOnArdu. Click on the board entry and then click the Install button.

How to Use It

  • In the Arduino IDE, select the new entry under Tools > Board > Circuit Playground (TeensyCore)
  • Then, select Tools > USB Type > MIDI
  • To upload new sketches you just have to double-press the reset button on the Circuit Playground each time you hit the upload button
  • If you decide to use your Circuit Playground as a regular Circuit Playground again, just select it under Tools > Board > Circuit Playground and upload an Arduino sketch like Blink File > Examples > Basics > Digital > Blink. The first time you have to double-press the reset button, but after that your Circuit Playground behaves like out of the box. 

PZ-1 Pizza Box DJ Code MIDI Over USB

Adding the Teensy code to your Arduino environment allows you to use the excellent MIDI over USB commands in your sketches.

You can transmit MIDI messages from your Circuit Playground using a few different commands. (Here's more detailed info from the PJRC Teensy page.) For our needs, the most commons ones are:

Copy Code
usbMIDI.sendNoteOn(note, velocity, channel)
usbMIDI.sendNoteOff(note, velocity, channel)
usbMIDI.sendControlChange(control, value, channel)

You can test out a basic sketch to see if things are all working.

Copy Code
#include <Adafruit_CircuitPlayground.h>

void setup() {
CircuitPlayground.begin();
}

void loop() {
/************* TEST BOTH BUTTONS */
if (CircuitPlayground.leftButton()) {
CircuitPlayground.redLED(HIGH);
usbMIDI.sendNoteOn(60, 127, 0); // 60 = C4 velocity 127 (max)
delay(100);
usbMIDI.sendNoteOff(60, 0, 0);
CircuitPlayground.redLED(LOW);
}
if (CircuitPlayground.rightButton()) {
CircuitPlayground.redLED(HIGH);
usbMIDI.sendNoteOn(61, 127, 0);
delay(100);
usbMIDI.sendNoteOff(61, 0, 0);
CircuitPlayground.redLED(LOW);
}

// dont listen to any incoming MIDI!
while (usbMIDI.read()) {
}
}

Copy that code into your Arduino IDE and then upload it to the Circuit Playground (TeensyCore). Make sure you are in MIDI mode (Tools > USB type > MIDI) and have the correct port selected for your Circuit Playground.

Once uploaded, launch your MIDI monitor software and a music application such as Garage Band. When you press the left and right buttons on the Circuit Playground you should hear see the C4 note indicated in the data stream and hear a C.

DJ Software MIDI Commands Control Change

Instead of playing musical notes, you'll be sending more generic MIDI commands from the Circuit Playground and then configuring your DJ software to use them. The MIDI Control Change command can be used to send numbered controls and their values.

For example, usbMIDI.sendControlChange(12, 127, 1) will send a MIDI command number 12 with a value of 127 over channel 1. You can configure your DJ software to listen for command number 12 on channel 1 and when the value sent is 127, it can raise the volume fader on deck B to full volume. You can stream a series of values from 0-to-127 over that command number 12 and depending on the capacative pad reading on your Circuit Playground that is triggering that MIDI command, you and raise and lower the volume.

PZ-1 Code

Here is the Circuit Playground PZ-1 Pizza Box DJ code. Copy it and paste it into a new Arduino sketch.

Copy Code
//Circuit Playground PZ-1 Pizza Box DJ
// by John Park
// a.k.a. DJ Sternocleidomastoid
// for Adafruit Industries
// MIT License
///////////////////////////////////////////////////////////////////////////////
// MIDI controller for Traktor, Mixxx and other DJ software
// Uses Circuit Playground (Teensy Core) to send MIDI over
// USB
//
// MIDI controller command mapping must be set up in your DJ software, check
// below for MIDI signal outputs
///////////////////////////////////////////////////////////////////////////////

#include <Adafruit_CircuitPlayground.h>
#include <Wire.h>
#include <SPI.h>

///////////////////////////////////////////////////////////////////////////////
//MIDI CC (change control) assignments
const int CHANNEL = 14; //MIDI channel
const int LEFT_BUTTON_CC = 4; //Play/Pause Deck A
const int RIGHT_BUTTON_CC = 19; //MIDI CC for left button: FX 1 On
const int CAP1_CONTROL = 1; //Select/Set Store Hotcue 2 (1 is load point)
const int CAP0_CONTROL = 0; //Left fader mixes Deck B volume down
const int CAP2_CONTROL = 2; //Delete hotcue 2 point
const int CAP3_CONTROL = 3; //Remix Trigger 6-1 or Loop Size /2
const int CAP12_CONTROL = 12; //Right fader mixes Deck A volume down
const int CAP6_CONTROL = 6; //Scratch (jog turn) Deck B
const int CAP9_CONTROL = 9; //Play/Pause Deck B
const int CAP10_CONTROL = 10; //Remix Trigger 6-4 or Loop Set 4 bar

int leftButtonState = 0;
int rightButtonState = 0;
int leftButtonLastState = 0;
int rightButtonLastState = 0;
int cap0State = 0;
int cap0LastState = 0;
int cap1State = 0;
int cap1LastState = 0;
int cap2State = 0;
int cap2LastState = 0;
int cap3State = 0;
int cap3LastState = 0;
int cap12State = 0;
int cap12LastState = 0;
int cap6State = 0;
int cap6LastState = 0;
int cap9State = 0;
int cap9LastState = 0;
int cap10State = 0;
int cap10LastState = 0;
bool cap1ON = false; //prevents off command from being spewed
bool cap12ON = false; //prevents off command from being spewed
bool cap6ON = false; //prevents off command from being spewed

const int CAPMIN = 25; //lowest value that's considered an intentional touch to minimize crosstalk
const int CAPSLOP = 0; //value of capacitive pad variance that's considered noise


///////////////////////////////////////////////////////////////////////////////
//mic_meter code
// To keep the display 'lively,' an upper and lower range of volume
// levels are dynamically adjusted based on recent audio history, and
// the graph is fit into this range.
#define FRAMES 8
uint16_t lvl[FRAMES], // Audio level for the prior #FRAMES frames
avgLo = 6, // Audio volume lower end of range
avgHi = 512, // Audio volume upper end of range
sum = 256 * FRAMES; // Sum of lvl[] array
uint8_t lvlIdx = 0; // Counter into lvl[] array
int16_t peak = 0; // Falling dot shows recent max
int8_t peakV = 0; // Velocity of peak dot

///////////////////////////////////////////////////////////////////////////////
void setup() {
CircuitPlayground.begin();
CircuitPlayground.setBrightness(30); //make brighter for performance, up to 255
CircuitPlayground.clearPixels();
for(uint8_t i=0; i<FRAMES; i ) lvl[i] = 256;

}

///////////////////////////////////////////////////////////////////////////////
// COLOR TABLES for animation ----------------------------------------------

const uint8_t PROGMEM
reds[] = { 0x9A, 0x75, 0x00, 0x00, 0x00, 0x65, 0x84, 0x9A, 0xAD, 0xAD },
greens[] = { 0x00, 0x00, 0x00, 0x87, 0xB1, 0x9E, 0x87, 0x66, 0x00, 0x00 },
blues[] = { 0x95, 0xD5, 0xFF, 0xC3, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00 },
gamma8[] = { // Gamma correction improves the appearance of midrange colors
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
0x01, 0x01, 0x01, 0x01, 0x01, 0x01, 0x01, 0x01, 0x01, 0x01, 0x01, 0x01,
0x02, 0x02, 0x02, 0x02, 0x02, 0x02, 0x02, 0x02, 0x03, 0x03, 0x03, 0x03,
0x03, 0x03, 0x04, 0x04, 0x04, 0x04, 0x05, 0x05, 0x05, 0x05, 0x05, 0x06,
0x06, 0x06, 0x06, 0x07, 0x07, 0x07, 0x08, 0x08, 0x08, 0x09, 0x09, 0x09,
0x0A, 0x0A, 0x0A, 0x0B, 0x0B, 0x0B, 0x0C, 0x0C, 0x0D, 0x0D, 0x0D, 0x0E,
0x0E, 0x0F, 0x0F, 0x10, 0x10, 0x11, 0x11, 0x12, 0x12, 0x13, 0x13, 0x14,
0x14, 0x15, 0x15, 0x16, 0x16, 0x17, 0x18, 0x18, 0x19, 0x19, 0x1A, 0x1B,
0x1B, 0x1C, 0x1D, 0x1D, 0x1E, 0x1F, 0x1F, 0x20, 0x21, 0x22, 0x22, 0x23,
0x24, 0x25, 0x26, 0x26, 0x27, 0x28, 0x29, 0x2A, 0x2A, 0x2B, 0x2C, 0x2D,
0x2E, 0x2F, 0x30, 0x31, 0x32, 0x33, 0x34, 0x35, 0x36, 0x37, 0x38, 0x39,
0x3A, 0x3B, 0x3C, 0x3D, 0x3E, 0x3F, 0x40, 0x41, 0x42, 0x44, 0x45, 0x46,
0x47, 0x48, 0x49, 0x4B, 0x4C, 0x4D, 0x4E, 0x50, 0x51, 0x52, 0x54, 0x55,
0x56, 0x58, 0x59, 0x5A, 0x5C, 0x5D, 0x5E, 0x60, 0x61, 0x63, 0x64, 0x66,
0x67, 0x69, 0x6A, 0x6C, 0x6D, 0x6F, 0x70, 0x72, 0x73, 0x75, 0x77, 0x78,
0x7A, 0x7C, 0x7D, 0x7F, 0x81, 0x82, 0x84, 0x86, 0x88, 0x89, 0x8B, 0x8D,
0x8F, 0x91, 0x92, 0x94, 0x96, 0x98, 0x9A, 0x9C, 0x9E, 0xA0, 0xA2, 0xA4,
0xA6, 0xA8, 0xAA, 0xAC, 0xAE, 0xB0, 0xB2, 0xB4, 0xB6, 0xB8, 0xBA, 0xBC,
0xBF, 0xC1, 0xC3, 0xC5, 0xC7, 0xCA, 0xCC, 0xCE, 0xD1, 0xD3, 0xD5, 0xD7,
0xDA, 0xDC, 0xDF, 0xE1, 0xE3, 0xE6, 0xE8, 0xEB, 0xED, 0xF0, 0xF2, 0xF5,
0xF7, 0xFA, 0xFC, 0xFF };
///////////////////////////////////////////////////////////////////////////////


///////////////////////////////////////////////////////////////////////////////
void loop() {

//Sound activated lights
uint8_t i, r, g, b;
uint16_t minLvl, maxLvl, a, scaled;

a = CircuitPlayground.mic.peak(10); // 10 ms of audio
sum -= lvl[lvlIdx];
lvl[lvlIdx] = a;
sum = a; // Sum of lvl[] array
minLvl = maxLvl = lvl[0]; // Calc min, max of lvl[]...
for(i=1; i<FRAMES; i ) {
if(lvl[i] < minLvl) minLvl = lvl[i];
else if(lvl[i] > maxLvl) maxLvl = lvl[i];
}

// Keep some minimum distance between min & max levels,
// else the display gets "jumpy."
if((maxLvl - minLvl) < 40) {
maxLvl = (minLvl < (512-40)) ? minLvl 40 : 512;
}
avgLo = (avgLo * 7 minLvl 2) / 8; // Dampen min/max levels
avgHi = (maxLvl >= avgHi) ? // (fake rolling averages)
(avgHi * 3 maxLvl 1) / 4 : // Fast rise
(avgHi * 31 maxLvl 8) / 32; // Slow decay

a = sum / FRAMES; // Average of lvl[] array
if(a <= avgLo) { // Below min?
scaled = 0; // Bargraph = zero
} else { // Else scale to fixed-point coordspace 0-2560
scaled = 2560L * (a - avgLo) / (avgHi - avgLo);
if(scaled > 2560) scaled = 2560;
}
if(scaled >= peak) { // New peak
peakV = (scaled - peak) / 4; // Give it an upward nudge
peak = scaled;
}

uint8_t whole = scaled / 256, // Full-brightness pixels (0-10)
frac = scaled & 255; // Brightness of fractional pixel
int whole2 = peak / 256, // Index of peak pixel
frac2 = peak & 255; // Between-pixels position of peak
uint16_t a1, a2; // Scaling factors for color blending

for(i=0; i<10; i ) { // For each NeoPixel...
if(i <= whole) { // In currently-lit area?
r = pgm_read_byte(&reds[i]), // Look up pixel color
g = pgm_read_byte(&greens[i]),
b = pgm_read_byte(&blues[i]);
if(i == whole) { // Fraction pixel at top of range?
a1 = (uint16_t)frac 1; // Fade toward black
r = (r * a1) >> 8;
g = (g * a1) >> 8;
b = (b * a1) >> 8;
}
} else {
r = g = b = 0; // In unlit area
}
// Composite the peak pixel atop whatever else is happening...
if(i == whole2) { // Peak pixel?
a1 = 256 - frac2; // Existing pixel blend factor 1-256
a2 = frac2 1; // Peak pixel blend factor 1-256
r = ((r * a1) (0x84 * a2)) >> 8; // Will
g = ((g * a1) (0x87 * a2)) >> 8; // it
b = ((b * a1) (0xC3 * a2)) >> 8; // blend?
} else if(i == (whole2-1)) { // Just below peak pixel
a1 = frac2 1; // Opposite blend ratios to above,
a2 = 256 - frac2; // but same idea
r = ((r * a1) (0x84 * a2)) >> 8;
g = ((g * a1) (0x87 * a2)) >> 8;
b = ((b * a1) (0xC3 * a2)) >> 8;
}
CircuitPlayground.strip.setPixelColor(i,
pgm_read_byte(&gamma8[r]),
pgm_read_byte(&gamma8[g]),
pgm_read_byte(&gamma8[b]));
}
CircuitPlayground.strip.show();

peak = peakV;
if(peak <= 0) {
peak = 0;
peakV = 0;
} else if(peakV >= -126) {
peakV -= 2;
}

if( lvlIdx >= FRAMES) lvlIdx = 0;

///////////////////////////////////////////////////////////////////////////////
//BUTTONS
//
//read the buttons
leftButtonState = (CircuitPlayground.leftButton());
//not pressed = 0, pressed = 1
rightButtonState = (CircuitPlayground.rightButton());

//Left Button
//compare current button states to previous button states
if(leftButtonState != leftButtonLastState){ //the state has changed
if(leftButtonState == 1){ //went from off to on, it's pressed
usbMIDI.sendControlChange(LEFT_BUTTON_CC, 1, CHANNEL); //send MIDI note ON command
CircuitPlayground.redLED(HIGH); //turn on the red LED
}
else{ //the button went from on to off, it isn't pressed
usbMIDI.sendControlChange(LEFT_BUTTON_CC, 0, CHANNEL); //send MIDI note OFF
CircuitPlayground.redLED(LOW); //turn off the red LED
}
leftButtonLastState = leftButtonState; //toggle
}


//Right Button
if(rightButtonState != rightButtonLastState){
if(rightButtonState == 1){
usbMIDI.sendControlChange(RIGHT_BUTTON_CC, 1, CHANNEL);
CircuitPlayground.redLED(HIGH);
}
else{
usbMIDI.sendControlChange(RIGHT_BUTTON_CC, 0, CHANNEL);
CircuitPlayground.redLED(LOW);
}
rightButtonLastState = rightButtonState;
}
///////////////////////////////////////////////////////////////////////////////
//Cap sense pads
//
//read the capacative pads
int cap1 = CircuitPlayground.readCap(1);
int cap0 = CircuitPlayground.readCap(0);
int cap2 = CircuitPlayground.readCap(2);
int cap3 = CircuitPlayground.readCap(3);
int cap12 = CircuitPlayground.readCap(12);
int cap6 = CircuitPlayground.readCap(6);
int cap9 = CircuitPlayground.readCap(9);
int cap10 = CircuitPlayground.readCap(10);



//cap1 Crossfader Deck B

if(cap1 > CAPMIN){
cap1State=1;
}
else{
cap1State=0;
}
if(cap1State != cap1LastState){
if(cap1State==1){
usbMIDI.sendControlChange(CAP1_CONTROL, 127, CHANNEL);
CircuitPlayground.redLED(HIGH);
}
else {
usbMIDI.sendControlChange(CAP1_CONTROL, 0, CHANNEL);
CircuitPlayground.redLED(LOW);
}
cap1LastState = cap1State;
}

//cap0
if(cap0 > CAPMIN){
cap0State=1;
}
else{
cap0State=0;
}
if(cap0State != cap0LastState){
if(cap0State==1){
usbMIDI.sendControlChange(CAP0_CONTROL, 1, CHANNEL);
CircuitPlayground.redLED(HIGH);
}
else {
usbMIDI.sendControlChange(CAP0_CONTROL, 0, CHANNEL);
CircuitPlayground.redLED(LOW);
}
cap0LastState = cap0State;
}

//cap2
if(cap2 > CAPMIN){
cap2State=1;
}
else{
cap2State=0;
}
if(cap2State != cap2LastState){
if(cap2State==1){
usbMIDI.sendControlChange(CAP2_CONTROL, 1, CHANNEL);
CircuitPlayground.redLED(HIGH);
}
else {
usbMIDI.sendControlChange(CAP2_CONTROL, 0, CHANNEL);
CircuitPlayground.redLED(LOW);
}
cap2LastState = cap2State;
}

//cap3
if(cap3 > CAPMIN){
cap3State=1;
}
else{
cap3State=0;
}
if(cap3State != cap3LastState){
if(cap3State==1){
usbMIDI.sendControlChange(CAP3_CONTROL, 1, CHANNEL);
CircuitPlayground.redLED(HIGH);
}
else {
usbMIDI.sendControlChange(CAP3_CONTROL, 0, CHANNEL);
CircuitPlayground.redLED(LOW);
}
cap3LastState = cap3State;
}

//cap12 Crossfader Deck B

if(cap12 > CAPMIN){
cap12State=1;
}
else{
cap12State=0;
}
if(cap12State != cap12LastState){
if(cap12State==1){
usbMIDI.sendControlChange(CAP12_CONTROL, 127, CHANNEL);
CircuitPlayground.redLED(HIGH);
}
else {
usbMIDI.sendControlChange(CAP12_CONTROL, 0, CHANNEL);
CircuitPlayground.redLED(LOW);
}
cap12LastState = cap12State;
}

//cap6
if (cap6>CAPMIN){
int cap6NewVal = map(CircuitPlayground.readCap(6),0,200,0,127);
if (abs(cap6 - cap6NewVal>CAPSLOP)) {
cap6 = cap6NewVal;
usbMIDI.sendControlChange(CAP6_CONTROL, cap6, CHANNEL);
CircuitPlayground.redLED(HIGH);
cap6ON = true;
}
else{
if (cap6ON==true){
usbMIDI.sendControlChange(CAP6_CONTROL, 0, CHANNEL); //send a 0
CircuitPlayground.redLED(LOW);
cap6ON=false;
}
}
}
//cap9
if(cap9 > CAPMIN){
cap9State=1;
}
else{
cap9State=0;
}
if(cap9State != cap9LastState){
if(cap9State==1){
usbMIDI.sendControlChange(CAP9_CONTROL, 1, CHANNEL);
CircuitPlayground.redLED(HIGH);
}
else {
usbMIDI.sendControlChange(CAP9_CONTROL, 0, CHANNEL);
CircuitPlayground.redLED(LOW);
}
cap9LastState = cap9State;
}

//cap10
if(cap10 > CAPMIN){
cap10State=1;
}
else{
cap10State=0;
}
if(cap10State != cap10LastState){
if(cap10State==1){
usbMIDI.sendControlChange(CAP10_CONTROL, 1, CHANNEL);
CircuitPlayground.redLED(HIGH);
}
else {
usbMIDI.sendControlChange(CAP10_CONTROL, 0, CHANNEL);
CircuitPlayground.redLED(LOW);
}
cap10LastState = cap10State;
}


// MIDI Controllers should discard incoming MIDI messages.
while (usbMIDI.read()) {
}
}

 

You can download the code with the button below. Once downloaded, unzip it and place the directory in your Arduino sketches directory.

PZ1PizzaBoxDF.zip

Customize the Code

You can see in the top of the sketch there are variables for the different MIDI control change commands. These numbers can be changed, but they correspond to the Circuit Playground pins for convenience. These are the MIDI control change numbers you'll need to know when mapping the PZ-1 to your DJ software. The comments show how I'm mapping them in Traktor.

The sketch also contains the Circuit Playground example sketch mic_meter to handle the sweet sound-reactive NeoPixel lighting effects.

Map It

Once you've uploaded the code, verify it is sending the commands by opening your MIDI monitoring software. When you choose the Circuit Playground as MIDI input and press the buttons and pads, you'll see the number, value, and channel data streaming in the utility.

Launch your DJ software and head to the MIDI controller configuration area (usually in the preferences). Here you can refer to the help for particular software you're using to assign each MIDI control change signal from the PZ-1 to the desired software command.

Circuit Playground PZ-1: Pizza Box DJ Controller

Here is a sample mapping that pairs the Circuit Playground PZ-1 with Traktor Pro 2 from Native Instruments.

PZ1_Traktor_mapping.tsi.zip

Conductive Painting

Circuit Playground PZ-1: Pizza Box DJ Controller

Cardboard Canvas

Corrugated cardboard makes a pretty good surface for this project. You can usually get a clean, empty box from a local pizza place if you ask nicely, or buy them in bulk online.

A 12" pizza box is a good size for this controller.

Circuit Playground PZ-1: Pizza Box DJ Controller

Other Materials

Mylar stencil blanks are available online or at art/graphics supply stores. They come in a convenient 12" x 12" size, an 7 mil is a good thickness for this.

You'll also want a hobby knife, masking tape, and some spray adhesive to keep the stencil mask from lifting up while painting.

Circuit Playground PZ-1: Pizza Box DJ Controller

Stencil Design

Your Circuit Playground's capacative pads need to touch the circuit, so that's a good starting point for your design. If you'd like to create the PZ-1 exactly as seen here, download the file below and either print it on regular printer paper to trace, or cut it on a CNC or laser cutter.

PZ-1_DJ_Stencil.svg

Circuit Playground PZ-1: Pizza Box DJ Controller

Use the Stencil

Once you've cut your stencil, you can spray the back side lightly with spray adhesive to help prevent it from lifting up from the cardboard while painting. You'll also want to use masking tape around the edges.

Paint the circuit by loading your stencil brush with conductive paint and then tapping it from above. This vertical tapping helps keep the paint inside the lines, vs strokes which tend to leak underneath as the bristles find the gaps.

Work your way across the entire surface.

Circuit Playground PZ-1: Pizza Box DJ Controller

Circuit Playground PZ-1: Pizza Box DJ Controller

Circuit Playground PZ-1: Pizza Box DJ Controller

Once you've finished, savor the exciting reveal! Lift of your stencil and admire the beautiful results!

Circuit Playground PZ-1: Pizza Box DJ Controller

Circuit Playground PZ-1: Pizza Box DJ Controller

Circuit Playground PZ-1: Pizza Box DJ Controller

Circuit Playground PZ-1: Pizza Box DJ Controller

Circuit Playground PZ-1: Pizza Box DJ Controller

Mount the Circuit Playground

Adding your Circuit Playground to the controller is simple. You'll dab a bit of conductive paint on each of the copper touch pads on the bottom side of the Circuit Playground, then carefully set it down on the corresponding painted trace pads on your cardboard. You can add a bit more paint inside the pads running up to the topside and back over to the outside of the board -- this will not only act as a conductive trace, but also keep the board "glued" down to the controller.

Circuit Playground PZ-1: Pizza Box DJ Controller

ircuit Playground PZ-1: Pizza Box DJ Controller

ircuit Playground PZ-1: Pizza Box DJ Controller

ircuit Playground PZ-1: Pizza Box DJ Controller

Rock the Crowd

Circuit Playground PZ-1: Pizza Box DJ Controller

You're ready to let the PZ-1 take control of your DJ software. Plug the controller into your laptop with the USB cable.

ircuit Playground PZ-1: Pizza Box DJ Controller

ircuit Playground PZ-1: Pizza Box DJ Controller

You can keep the box unfolded and flat, or fold it up.

Circuit Playground PZ-1: Pizza Box DJ Controller

Circuit Playground PZ-1: Pizza Box DJ Controller

What's the time? It is time to DJ.

Circuit Playground PZ-1: Pizza Box DJ Controller

Once you've rocked the crowd all the way out and back, and everyone has gone home for a good night's rest, fold up your PZ-1 and go deliver some delicious tracks at the next party! (Yes, sometimes the next party is in your workshop.)

Circuit Playground PZ-1: Pizza Box DJ Controller

Circuit Playground PZ-1: Pizza Box DJ Controller

メーカー品番 3000
CIRC PLAYGROUND CLASS ATMEGA32U4
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.