Maker.io main logo

Cat TV with Raspberry Pi

409

2024-03-03 | By bekathwia

License: See Original Project Raspberry Pi SBC

 

becky-stern-cat-tv-02 

Today we’re building a mini television for cats. My cat Benchley loves watching TV. It’s really a mini computer ‎since I’m using a Raspberry Pi to play YouTube on a little HDMI screen. Let’s get started.‎

Materials and supplies:‎

becky-stern-cat-tv-04

For this project, I’m using a display gifted to me by Elecrow. It’s a five-inch LCD with capacitive touch and ‎comes with an HDMI cable for video and audio and a USB cable for power and touchscreen input. ‎

becky-stern-cat-tv-05

It works with my Raspberry Pi 5 out of the box, so I just plugged in both cables, as well as a USB speaker, ‎keyboard, and mouse.‎

becky-stern-cat-tv-06

Then I created a first draft of the 3D printed enclosure, which has to fit the screen and speaker next to each ‎other.‎

becky-stern-cat-tv-07

To use the speaker as the audio output, I right clicked on the audio setting in the upper right and selected my ‎USB device from the list. If it’s not there, you may have to do a few command line steps to install support for ‎USB audio. I installed Pulseaudio, restarted my Pi, and it worked straight away.‎

To develop the enclosure a bit further, I played around with speaker grille patterns and settled on this ‎segmented pattern with circles coming partway through. I think it’s giving vintage vibes, and this marble-effect ‎PLA is super classy. I test fit the components inside.‎

I used an HDMI cable that has smaller connectors than usual, so it didn’t add bulk to the size of the enclosure.‎

enclosure

Once I was confident my basic shape would hold and fit all my components, I started playing around with the ‎exterior shape and also wanted to add some ventilation holes because the Raspberry Pi runs pretty hot. I used ‎the honeycomb shape generator in Tinkercad to make grids of holes that are too small for my cat to reach ‎through.‎

I printed this final version of the enclosure in sparkly black PLA on my smooth build plate so the front of the TV ‎would be super flat.‎

Then I test fit the components once again, holding them in place with tape so I could test it with Benchley to see ‎if any changes were needed.‎

I’m just loading Birder King on YouTube in the Pi’s web browser and setting it to full screen. Benchley was super ‎interested, and even went around back to see if he could find any birds and squirrels inside the TV.‎

I discovered that the touch screen was a bit of a problem, as the cats would paw the screen and pause the ‎video. So, I replaced the screen’s USB cable with a charge-only cable, disabling the data connection for the ‎touch screen.‎

becky-stern-cat-tv-09

Then I installed the screen more permanently with some screws and the speaker and Pi with hot glue. You can ‎set up your hot glue fast if you hit it with a little canned air.‎

becky-stern-cat-tv-01

Finally, I brought the finished TV to the living room to see what Benchley and his brother Hamlet think about the ‎final result. They love it!‎

becky-stern-cat-tv-10

becky-stern-cat-tv-08

メーカー品番 SC0445
AC/DC WALL MNT ADAPTER 5.1V 15W
Raspberry Pi
メーカー品番 DIS00005R
GRAPHIC DISPLAY
Elecrow
メーカー品番 3548
STRAIGHT HDMI PLUG ADAPTER
Adafruit Industries LLC
メーカー品番 3557
RIGHT ANGLE (R BEND) MICRO HDMI
Adafruit Industries LLC
メーカー品番 3561
CABLE JUMPER 7.87"
Adafruit Industries LLC
メーカー品番 3369
MINI EXTERNAL USB STEREO SPEAKER
Adafruit Industries LLC
メーカー品番 SC0167
RED USB KEYBOARD
Raspberry Pi
メーカー品番 SC0442
RASPBERRY PI MOUSE RED
Raspberry Pi
メーカー品番 SC1148
HEATSINK ALUMINUM
Raspberry Pi
メーカー品番 ENDER-3 V2
32-Bit Mainboard 3D Printer
Creality 3D
メーカー品番 RM-PL0321
POLYMAKER POLYTERRA PLA FILAMENT
LulzBot
メーカー品番 32614
POCKET PRECISION 4-IN-1 SCREWDRI
Klein Tools, Inc.
メーカー品番 110049634
GF 232 GENERAL PURPOSE GLUE STIC
Steinel America
メーカー品番 3903-B-4-50
TAPE DUCT BLACK 4"X50YDS
3M (TC)
メーカー品番 SC1431
SBC 2.4GHZ 4 CORE 4GB PI 5
Raspberry Pi
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.