Maker.io main logo

Build a USB Game Controller with Arduino Uno R4

2026-05-11 | By Rinme Tom

License: General Public License Arduino

Gaming controllers are a great example of how physical inputs are translated into digital commands. In this project, you’ll build a simple USB Arduino game controller using the Arduino Uno R4, a two-axis joystick, and four push buttons.

When connected to your computer, the Arduino appears as a standard USB keyboard. Moving the joystick sends arrow-key inputs, while the buttons act as custom keys such as W, A, S, and D. Because most PC games already support keyboard controls, the controller works immediately without installing drivers or additional software.

This project is ideal for beginners who want to learn about USB HID (Human Interface Device) communication and build a practical gaming accessory.

Arduino Game Controller

Why Use Arduino as a Game Controller?

Boards with native USB support, such as the Arduino Uno R4, can emulate keyboards, mice, and other HID devices. That means your microcontroller can send keystrokes directly to a PC over USB.

This approach offers several advantages:

  • No drivers required

  • Compatible with most PC games

  • Fully customizable controls

  • Simple hardware design

  • Easy to expand with more buttons or LEDs

Many makers on Reddit recommend using boards with native USB HID support for controller projects because they work as standard input devices across Windows, Linux, and macOS.

Parts Required

To build this controller, you will need:

The joystick provides analog X and Y position data, and the buttons provide digital inputs for additional game actions.

How the Controller Works

The joystick outputs two analog voltages:

  • X-axis controls left and right movement

  • Y-axis controls up and down movement

The Arduino reads these values and compares them to preset thresholds. When the joystick moves beyond those limits, the board sends the corresponding arrow-key press to the computer.

Each push button is connected to a digital input pin configured with INPUT_PULLUP. When a button is pressed, the pin goes LOW, and the Arduino sends a keyboard character.

Hardware Set Up

Wiring Overview

Joystick Connections

  • VCC → 5V

  • GND → GND

  • VRx → A0

  • VRy → A1

Push Buttons

  • Button 1 → D2

  • Button 2 → D3

  • Button 3 → D4

  • Button 4 → D5

  • Other terminal of each button → GND

No external resistors are needed because the internal pull-up resistors are enabled in software.

Pin Mapping

The joystick and buttons are mapped to the following keyboard inputs:

  • Left → Left Arrow

  • Right → Right Arrow

  • Up → Up Arrow

  • Down → Down Arrow

  • Button 1 → W

  • Button 2 → A

  • Button 3 → S

  • Button 4 → D

You can change these key assignments to match your favorite game.

Circuit Diagram

Arduino Code

Copy Code
#include <Keyboard.h>

// Joystick pins
const int joyX = A0;
const int joyY = A1;

// Button pins
const int buttonPins[4] = {2, 3, 4, 5};

// Dead zone thresholds
const int LOW_TH = 350;
const int HIGH_TH = 670;

// Button key mapping
const char buttonKeys[4] = {'w', 'a', 's', 'd'};

void setup() {
  for (int i = 0; i < 4; i++) {
    pinMode(buttonPins[i], INPUT_PULLUP);
  }

  delay(3000);          // Allow time for USB enumeration
  Keyboard.begin();
}

void loop() {
  int x = analogRead(joyX);
  int y = analogRead(joyY);

  // Horizontal movement
  if (x < LOW_TH)
    Keyboard.press(KEY_LEFT_ARROW);
  else
    Keyboard.release(KEY_LEFT_ARROW);

  if (x > HIGH_TH)
    Keyboard.press(KEY_RIGHT_ARROW);
  else
    Keyboard.release(KEY_RIGHT_ARROW);

  // Vertical movement
  if (y < LOW_TH)
    Keyboard.press(KEY_UP_ARROW);
  else
    Keyboard.release(KEY_UP_ARROW);

  if (y > HIGH_TH)
    Keyboard.press(KEY_DOWN_ARROW);
  else
    Keyboard.release(KEY_DOWN_ARROW);

  // Button handling
  for (int i = 0; i < 4; i++) {
    if (digitalRead(buttonPins[i]) == LOW)
      Keyboard.press(buttonKeys[i]);
    else
      Keyboard.release(buttonKeys[i]);
  }

  delay(10);
}

Understanding the Dead Zone

Analog joysticks rarely sit at exactly their center value. Small fluctuations can cause unwanted movement if every reading is treated as input.

The dead zone solves this by defining a neutral range:

  • Values below 350 trigger movement in one direction

  • Values above 670 trigger movement in the opposite direction

  • Values in between are ignored

Adjust these thresholds if your joystick drifts when untouched.

Full set up

Testing the Controller

  1. Upload the code to your Arduino Uno R4.

  2. Connect the board to your PC.

  3. Open a text editor.

  4. Move the joystick and press buttons.

You should see the arrow keys and W/A/S/D characters appear.

Once confirmed, open any game that supports keyboard controls and map the keys as needed.

Playing Games

Applications

This controller works well for:

  • Retro games

  • Arcade emulators

  • Platformers

  • Fighting games

  • Educational projects

  • Custom control panels

Because it behaves like a keyboard, it is compatible with virtually any game that accepts keyboard input.

Troubleshooting

Controller Not Detected

Make sure you are using an Arduino board with native USB support and that the Keyboard.h library is included.

Random Movement

Increase the dead zone thresholds.

Buttons Trigger Constantly

Verify that one side of each button is connected to ground.

Keys Stay Pressed

Check for loose wiring or missing Keyboard.release() calls.

Ideas for Upgrades

Once the basic controller is working, you can expand the design by adding:

  • More action buttons

  • Turbo-fire functionality

  • RGB LEDs

  • Vibration feedback

  • Wireless connectivity

  • 3D-printed enclosure

What You Learn

This project demonstrates several useful embedded systems concepts:

  • Reading analog and digital inputs

  • USB HID communication

  • Keyboard emulation

  • Debouncing and dead zones

  • Human-machine interface design

Final Thoughts

Building a custom USB game controller is a fun and practical way to explore how hardware interacts with software. With only a handful of components, you can create a plug-and-play controller that works with thousands of PC games.

Whether you are reliving retro gaming memories or experimenting with custom input devices, the Arduino Uno R4 makes it easy to turn your ideas into a fully functional controller.

メーカー品番 ABX00087
ARDUINO UNO R4 WIFI
Arduino
メーカー品番 ABX00080
ARDUINO UNO R4 MINIMA
Arduino
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.