Maker.io main logo

Bluetooth Cycling Speed & Cadence Sensor Display with Clue

75

2020-04-16 | By Adafruit Industries

License: See Original Project

Courtesy of Adafruit

Guide by John Park

Overview

Learn to read cycling speed and cadence sensor data over Bluetooth LE and display data on your CLUE board's screen!

Using our Bluefruit libraries and CircuitPython, it's now possible to connect to multiple devices, in the case of separate speed and cadence sensors, as well as dual sensor devices that present as a single BLE peripheral.

 

 

The adafruit_clue library is used to help keep things simple, so you can write the wheel and crank revolution text to the display without diving into complicated display code.

In a future project, we'll cover the math needed to convert these raw revolution values into speed and cadence like you'll see on a typical bike computer or cycling app. This project will get you familiar with reading and displaying data directly onto the CLUE.

Parts

magnets_1

magnets_2

magnets_3

Cycling Speed & Cadence Sensor

Bluetooth LE compatible, such as the Wahoo Fitness Blue SC. This type of device is two sensors in one package and typically reads speed and cadence revolutions based on a pair of magnets affixed to a spoke and crank.

You can also use individual speed and/or cadence sensors that use an IMU rather than a magnet to sense revolutions, such as the Wahoo RPM Speed and RPM Cadence.

Be sure that your sensors use Bluetooth LE and not Ant+ or some other radio standard. (Some use both, which is fine.)

Understanding BLE

Bluetooth_2

BLE Basics

To understand how we communicate between the MagicLight Bulb and the Circuit Playground Bluefruit (CPB), it's first important to get an overview of how Bluetooth Low Energy (BLE) works in general.

The nRF52840 chip on the CPB uses Bluetooth Low Energy, or BLE. BLE is a wireless communication protocol used by many devices, including mobile devices. You can communicate between your CPB and peripherals such as the Magic Light, mobile devices, and even other CPB boards!

There are a few terms and concepts commonly used in BLE with which you may want to familiarize yourself. This will help you understand what your code is doing when you're using CircuitPython and BLE.

Two major concepts to know about are the two modes of BLE devices:

  • Broadcasting mode (also called GAP for Generic Access Profile)

  • Connected device mode (also called GATT for Generic ATTribute Profile).

GAP mode deals with broadcasting peripheral advertisements, such as "I'm a device named LEDBlue-19592CBC", as well as advertising information necessary to establish a dedicated device connection if desired. The peripheral may also be advertising available services.

GATT mode deals with communications and attribute transfer between two devices once they are connected, such as between a heart monitor and a phone, or between your CPB and the Magic Light.

GAP_4

Bluetooth LE Terms

GAP Mode

Device Roles:

  • Peripheral - The low-power device that broadcasts advertisements. Examples of peripherals include: heart rate monitor, smart watch, fitness tracker, iBeacon, and the Magic Light. The CPB can also work as a peripheral.

  • Central - The host "computer" that observes advertisements being broadcast by the Peripherals. This is often a mobile device such as a phone, tablet, desktop or laptop, but the CPB can also act as a central (which it will in this project).

Terms:

  • Advertising - Information sent by the peripheral before a dedicated connection has been established. All nearby Central's can observe these advertisements. When a peripheral device advertises, it may be transmitting the name of the device, describing its capabilities, and/or some other piece of data. Central can look for advertising peripherals to connect to and use that information to determine each peripheral's capabilities (or Services offered, more on that below).

GATT Mode

Device Roles:

Server - In connected mode, a device may take on a new role as a Server, providing a Service available to clients. It can now send and receive data packets as requested by the Client device to which it now has a connection.

Client - In connected mode, a device may also take on a new role as Client that can send requests to one or more of a Server's available Services to send and receive data packets.

NOTE: A device in GATT mode can take on the role of both Server and Client while connected to another device.

Terms:

  • Profile - A pre-defined collection of Services that a BLE device can provide. For example, the Heart Rate Profile, or the Cycling Sensor (bike computer) Profile. These Profiles are defined by the Bluetooth Special Interest Group (SIG). For devices that don't fit into one of the pre-defined Profiles, the manufacturer creates their own Profile. For example, there is not a "Smart Bulb" profile, so the Magic Light manufacturer has created their own unique one.

  • Service - A function the Server provides. For example, a heart rate monitor armband may have separate Services for Device Information, Battery Service, and Heart Rate itself. Each Service is comprised of collections of information called Characteristics. In the case of the Heart Rate Service, the two Characteristics are Heart Rate Measurement and Body Sensor Location. The peripheral advertises its services. 

  • Characteristic - A Characteristic is a container for the value, or attribute, of a piece of data along with any associated metadata, such as a human-readable name. A characteristic may be readable, writable, or both. For example, the Heart Rate Measurement Characteristic can be served up to the Client device and will report the heart rate measurement as a number, as well as the unit string "bpm" for beats-per-minute. The Magic Light Server has a Characteristic for the RGB value of the bulb which can be written to by the Central to change the color. Characteristics each have a Universal Unique Identifier (UUID) which is a 16-bit or 128-bit ID.

  • Packet - Data transmitted by a device. BLE devices and host computers transmit and receive data in small bursts called packets.

This guide is another good introduction to the concepts of BLE, including GAP, GATT, Profiles, Services, and Characteristics.

Cycling Speed and Cadence Service

The Bluetooth Special Interest Group has a standardized GATT (Generitt ATTribute Profile) for cycling speed and cadence sensors called the Cycling Speed and Cadence (CSC) profile. (You can see a list of all the GATT services here.)

This defines the commands and data that can be exchanged between bike sensor devices and the client device such as a phone, tablet, or BLE capable microcontroller (like we'll use in our project).

If you want to see how the Bluetooth SIG defines a GATT, such as the Cycling Speed and Cadence Profile.

Even better, run that URL through a code beautifier, such as codebeatify.org for a more human-readable version.

readversion_5

 

Cycling Speed & Cadence Characteristics

The CSC service defines characteristics that can be served from the sensors to a connected device.

CSC Measurement

The most important for most needs is the CSC Measurement characteristic which serves up the following information:

  • Wheel revolutions - used to calculate speed of a known wheel diameter

  • Last wheel event time

  • Crank revolutions -- used to indicate pedaling cadence

  • Last crank event time

Not all Cycling sensor support all of the above characteristics. Some individual sensors will report just speed or just cadence.

Sensor Location

CSC sensors will also include a characteristic for the intended location of the cadence sensor, typically the right crank. This is built into the sensor firmware, not something that the device is determining on the fly!

SC Control Point

The speed/cadence (SC) control point characteristic is used to allow the client device to write control points to the CSC in order to initiate sensor calibration.

nRF Connect View

We can use the nRF Connect app from Nordic on iOS and Android to connect to a CSC sensor and look at the service, characteristics, and data.

Here we see data advertised including the device name, available services, connection parameters, and more.

device_6

CSC Measurement

In this image, we can see the CSC device (WAHOO BLUESC) has been connected, and the Cycling Speed and Cadence characteristic is reporting its data.

CSC_7

Supported Features

By requesting a read of the CSD Feature, we can see that both Wheel Revolution Data and Crank Revolution Data are supported.

feature_8

If we request a read of the Sensor Location characteristic, we receive it as shown here, indicating "Right Crank":

crank_9

CircuitPython on CLUE

CircuitPython is a derivative of MicroPython designed to simplify experimentation and education on low-cost microcontrollers. It makes it easier than ever to get prototyping by requiring no upfront desktop software downloads. Simply copy and edit files on the CIRCUITPY flash drive to iterate.

The following instructions will show you how to install CircuitPython. If you've already installed CircuitPython but are looking to update it or reinstall it, the same steps work for that as well!

Set up CircuitPython Quick Start!

Follow this quick step-by-step for super-fast Python power :)

Download the latest version of

CircuitPython for CLUE from circuitpython.org

download_10

Click the link above to download the latest version of CircuitPython for the CLUE.

Download and save it to your desktop (or wherever is handy).

Adafruit_11

Plug your CLUE into your computer using a known-good USB cable.

A lot of people end up using charge-only USB cables and it is very frustrating! So, make sure you have a USB cable you know is good for data sync.

Double-click the Reset button on the top (magenta arrow) on your board, and you will see the NeoPixel RGB LED (green arrow) turn green. If it turns red, check the USB cable, try another USB port, etc. Note: The little red LED next to the USB connector will pulse red. That's ok!

If double-clicking doesn't work the first time, try again. Sometimes it can take a few tries to get the rhythm right!

clueboot_12

clueboot_13

You will see a new disk drive appear called CLUEBOOT.

Drag the adafruit-circuitpython-clue-etc.uf2 file to CLUEBOOT.

LED_13

The LED will flash. Then, the CLUEBOOT drive will disappear and a new disk drive called CIRCUITPY will appear.

If this is the first time you're installing CircuitPython or you're doing a completely fresh install after erasing the filesystem, you will have two files - boot_out.txt, and code.py, and one folder - lib on your CIRCUITPY drive.

If CircuitPython was already installed, the files present before reloading CircuitPython should still be present on your CIRCUITPY drive. Loading CircuitPython will not create new files if there was already a CircuitPython filesystem present.

That's it, you're done! :)

CLUE CircuitPython Libraries

The CLUE is packed full of features like a display and a ton of sensors. Now that you have CircuitPython installed on your CLUE, you'll need to install a base set of CircuitPython libraries to use the features of the board with CircuitPython.

Follow these steps to get the necessary libraries installed.

Installing CircuitPython Libraries on your CLUE

If you do not already have a lib folder on your CIRCUITPY drive, create one now.

Then, download the CircuitPython library bundle that matches your version of CircuitPython from CircuitPython.org.

Download the latest library

bundle from circuitpython.org

folder_14

The bundle downloads as a .zip file. Extract the file. Open the resulting folder.

drives_15

Open the lib folder found within.

lib_16

Once inside, you'll find a lengthy list of folders and .mpy files. To install a CircuitPython library, you drag the file or folder from the bundle lib folder to the lib folder on your CIRCUITPY drive.

circdrive_17

Copy the following folders and files from the bundle lib folder to the lib folder on your CIRCUITPY drive:

  • adafruit_apds9960

  • adafruit_bmp280.mpy

  • adafruit_bus_device

  • adafruit_clue.mpy

  • adafruit_display_shapes

  • adafruit_display_text

  • adafruit_lis3mdl.mpy

  • adafruit_lsm6ds.mpy

  • adafruit_register

  • adafruit_sht31d.mpy

  • adafruit_slideshow.mpy

  • neopixel.mpy

Your lib folder should look like the image on the left. These libraries will let you run the demos in the CLUE guide.

Code the CLUE in CircuitPython

Libraries

Once your CLUE is set up with CircuitPython and library files in general, we'll add some project specific libraries.

libraries_18

From the library bundle you downloaded in that guide page, transfer any additional libraries shown here onto the CLUE's /lib directory on the CIRCUITPY drive:

  • adafruit_apds9960

  • adafruit_ble

  • adafruit_ble_cycling_speed_and_cadence.py

  • adafruit_bmp280.mpy

  • adafruit_bus_device

  • adafruit_clue.py

  • adafruit_display_notification

  • adafruit_display_shapes

  • adafruit_display_text

  • adafruit_lis3mdl.mpy

  • adafruit_lsm6ds.mpy

  • adafruit_register

  • adafruit_sht31d.mpy

  • neopixel.mpy

  • simpleio.mpy

Text Editor

Adafruit recommends using the Mu editor for using your CircuitPython code with the Feather boards. You can get more info in this guide.

Alternatively, you can use any text editor that saves files.

Code.py

Copy the code shown below, paste it into Mu. Plug your CLUE into your computer via a known good USB cable. In your operating system's file explorer/finder, you should see a new flash drive named CIRCUITPY. Save the code from Mu to the CLUE's CIRCUITPY drive as code.py.

Download: Project Zip or CLUE_cycling_simple.py

Copy Code
"""
Read cycling speed and cadence data from a peripheral using the standard BLE
Cycling Speed and Cadence (CSC) Service.
Works with single sensor (e.g., Wahoo Blue SC) or sensor pair, such as Wahoo RPM
"""

import time
from adafruit_clue import clue
import adafruit_ble
from adafruit_ble.advertising.standard import ProvideServicesAdvertisement
from adafruit_ble.services.standard.device_info import DeviceInfoService
from adafruit_ble_cycling_speed_and_cadence import CyclingSpeedAndCadenceService

clue_data = clue.simple_text_display(title="Cycle Revs", title_scale=1, text_scale=3)

# PyLint can't find BLERadio for some reason so special case it here.
ble = adafruit_ble.BLERadio()    # pylint: disable=no-member


while True:
    print("Scanning...")
    # Save advertisements, indexed by address
    advs = {}
    for adv in ble.start_scan(ProvideServicesAdvertisement, timeout=5):
        if CyclingSpeedAndCadenceService in adv.services:
            print("found a CyclingSpeedAndCadenceService advertisement")
            # Save advertisement. Overwrite duplicates from same address (device).
            advs[adv.address] = adv

    ble.stop_scan()
    print("Stopped scanning")
    if not advs:
        # Nothing found. Go back and keep looking.
        continue

    # Connect to all available CSC sensors.
    cyc_connections = []
    for adv in advs.values():
        cyc_connections.append(ble.connect(adv))
        print("Connected", len(cyc_connections))

    # Print out info about each sensors.
    for conn in cyc_connections:
        if conn.connected:
            if DeviceInfoService in conn:
                dis = conn[DeviceInfoService]
                try:
                    manufacturer = dis.manufacturer
                except AttributeError:
                    manufacturer = "(Manufacturer Not specified)"
                print("Device:", manufacturer)
            else:
                print("No device information")

    print("Waiting for data... (could be 10-20 seconds or more)")
    # Get CSC Service from each sensor.
    cyc_services = []
    for conn in cyc_connections:
        cyc_services.append(conn[CyclingSpeedAndCadenceService])
    # Read data from each sensor once a second.
    # Stop if we lose connection to all sensors.

    while True:
        still_connected = False
        wheel_revs = None
        crank_revs = None
        for conn, svc in zip(cyc_connections, cyc_services):
            if conn.connected:
                still_connected = True
                values = svc.measurement_values
                if values is not None:  # add this
                    if values.cumulative_wheel_revolutions:
                        wheel_revs = values.cumulative_wheel_revolutions
                    if values.cumulative_crank_revolutions:
                        crank_revs = values.cumulative_crank_revolutions

        if not still_connected:
            break
        if wheel_revs:   # might still be None
            print(wheel_revs)
            clue_data[0].text = "Wheel: {0:d}".format(wheel_revs)
            clue_data.show()
        if crank_revs:
            print(crank_revs)
            clue_data[2].text = "Crank: {0:d}".format(crank_revs)
            clue_data.show()
        time.sleep(0.1)

Code Explainer

The code is doing a few fundamental things.

First, it loads the time and board libraries, as well as the necessary libraries to use BLE in general, and the adafruit_ble_cycling_speed_and_cadence library in specific.

We also load the adafruit_clue library so we can take advantage of convenient commands that simplify using the CLUE's display.

The clue_data variable is created to instantiate the CLUE display object for simple text and titles.

We also set up the BLERadio so it can be used to communicate with the sensor.

Download: file

Copy Code
import time
from adafruit_clue import clue
import adafruit_ble
from adafruit_ble.advertising.standard import ProvideServicesAdvertisement
from adafruit_ble.services.standard.device_info import DeviceInfoService
from adafruit_ble_cycling_speed_and_cadence import CyclingSpeedAndCadenceService

clue_data = clue.simple_text_display(title="Cycle Revs", title_scale=1, text_scale=3, num_lines=3)

# PyLint can't find BLERadio for some reason so special case it here.
ble = adafruit_ble.BLERadio()    # pylint: disable=no-member

Connection

Next, we scan for a BLE peripheral device advertising that it has the Cycling Speed & Cadence service.

When it is found, the CLUE will connect to it and then display the device name and other info. These are regular print() statements that show up in the REPL or other serial display, including the CLUE's display.

Download: file

Copy Code
while True:
    print("Scanning...")
    # Save advertisements, indexed by address
    advs = {}
    for adv in ble.start_scan(ProvideServicesAdvertisement, timeout=5):
        if CyclingSpeedAndCadenceService in adv.services:
            print("found a CyclingSpeedAndCadenceService advertisement")
            # Save advertisement. Overwrite duplicates from same address (device).
            advs[adv.address] = adv

    ble.stop_scan()
    print("Stopped scanning")
    if not advs:
        # Nothing found. Go back and keep looking.
        continue

    # Connect to all available CSC sensors.
    cyc_connections = []
    for adv in advs.values():
        cyc_connections.append(ble.connect(adv))
        print("Connected", len(cyc_connections))

    # Print out info about each sensors.
    for conn in cyc_connections:
        if conn.connected:
            if DeviceInfoService in conn:
                dis = conn[DeviceInfoService]
                try:
                    manufacturer = dis.manufacturer
                except AttributeError:
                    manufacturer = "(Manufacturer Not specified)"
                print("Device:", manufacturer)
            else:
                print("No device information")

    print("Waiting for data... (could be 10-20 seconds or more)")
    # Get CSC Service from each sensor.
    cyc_services = []
    for conn in cyc_connections:
        cyc_services.append(conn[CyclingSpeedAndCadenceService])
    # Read data from each sensor once a second.
    # Stop if we lose connection to all sensors.

Receiving Revolution Values

Once connected, we create a pair of variables to store the wheel and crank revolution values as wheel_revs and crank_revs

When we receive values for these two attributes they are displayed on the CLUE screen using the clue_data[].text command, and clue_data.show() to update the display.

Download: file

Copy Code
while True:
        still_connected = False
        wheel_revs = None
        crank_revs = None
        for conn, svc in zip(cyc_connections, cyc_services):
            if conn.connected:
                still_connected = True
                values = svc.measurement_values
                if values is not None:  # add this
                    if values.cumulative_wheel_revolutions:
                        wheel_revs = values.cumulative_wheel_revolutions
                    if values.cumulative_crank_revolutions:
                        crank_revs = values.cumulative_crank_revolutions

        if not still_connected:
            break
        if wheel_revs:   # might still be None
            print(wheel_revs)
            clue_data[0].text = "Wheel: {0:d}".format(wheel_revs)
            clue_data.show()
        if crank_revs:
            print(crank_revs)
            clue_data[2].text = "Crank: {0:d}".format(crank_revs)
            clue_data.show()
        time.sleep(0.1)

Let's check it out in action!

Use the CLUE Cycling Display

display_20

sensors_21

sensors_22

Install Sensors

Follow the manufacturer's directions to install your speed and cadence sensors. Here you can see a single unit with a magnet attached to a rear wheel spoke for wheel revolution sensing, and a crank mounted magnet for cadence sensing.

The unit detects each magnet with a different Hall effect sensor and then sends revolution data over BLE.

clue_23

clue_24

clue_25

clue_26

clue_27

clue_28

Use the CLUE Display

Plug in power to the CLUE, either with a battery pack or over USB.

The CLUE will begin to search for the cycling speed & cadence sensor.

Turn the crank to wake up the sensor in case it has gone into power saving mode.

When the CLUE finds the CSC sensor, they will negotiate a connection.

Now, you can give the wheel a spin and crank the pedal. You'll see the cumulative revolutions of each displayed on the CLUE!

cycle_29

メーカー品番 4500
CLUE NRF52840 EXPRESS
Adafruit Industries LLC
メーカー品番 4191
BATTERY HOLDER AAA 2 CELL LEADS
Adafruit Industries LLC
メーカー品番 EN92
BATTERY ALKALINE 1.5V AAA
Energizer Battery Company
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.