Maker.io main logo

Adding Third Party Boards to the Arduino v1.6.4+ IDE

69

2016-05-06 | By Adafruit Industries

License: See Original Project Circuit Playground

Courtesy of Adafruit

Guide by Todd Treece

Overview

Version 1.6.4 of the Arduino IDE introduced official support for adding third party boards (like the Adafruit Flora and Trinket) to the new Board Manager. This addition is great news, because it allows users to quickly add new boards with the click of a button. Previously the addition of new boards required a cumbersome manual installation process, or in certain cases, the download of a completely separate version of the IDE with the new boards added.

The new Board Manager solves those issues. We had figured out a way to add custom boards in v1.6.3 of the Arduino IDE, but it was not officially supported by Arduino. Thanks to the hard work of Federico Fissore and the Arduino developer community, we can now add new boards just as easily using officially supported methods. Let's get started.

Arduino IDE Setup

The first thing you will need to do is to download the latest release of the Arduino IDE. You will need to be using version 1.6.4 or higher for this guide.

Arduino IDE v1.6.4 Download

After you have downloaded and installed v1.6.4, you will need to start the IDE and navigate to the Preferences menu. You can access it from the File menu in Windows or Linux, or the Arduino menu on OS X.

Navigate to the Arduino preferences menu

A dialog will pop up just like the one shown below.

Preferences Dialog

We will be adding a URL to the new Additional Boards Manager URLs option. The list of URLs is comma separated, and you will only have to add each URL once. New Adafruit boards and updates to existing boards will automatically be picked up by the Board Manager each time it is opened. The URLs point to index files that the Board Manager uses to build the list of available & installed boards.

To find the most up to date list of URLs you can add, you can visit the list of third party board URLs on the Arduino IDE wiki. We will only need to add one URL to the IDE in this example, but you can add multiple URLS by separating them with commas. Copy and paste the link below into the Additional Boards Manager URLs option in the Arduino IDE preferences.

 
Copy Code
https://adafruit.github.io/arduino-board-index/package_adafruit_index.json

 

Additional Boards Manager URLs

Proxy Setting Warning

Here's a short description of each of the Adafruit supplied packages that will be available in the Board Manager when you add the URL:

  • Adafruit AVR Boards - Includes support for Flora, Gemma, Feather 32u4, Trinket, & Trinket Pro.
  • Adafruit SAMD Boards - Includes support for Feather M0
  • Arduino Leonardo & Micro MIDI-USB - This adds MIDI over USB support for the Flora, Feather 32u4, Micro and Leonardo using the arcore project.

Click OK to save the new preference settings. Next we will look at installing boards with the Board Manager.

Installing Boards

Now that you have added the appropriate URLs to the Arduino IDE preferences, you can open the Boards Manager by navigating to the Tools->Board menu.

Tools -> Board Menu

Once the Board Manager opens, click on the category drop down menu on the top left hand side of the window and select Contributed. You will then be able to select and install the boards supplied by the URLs added to the preferences. In the example below, we are installing support for Adafruit AVR Boards, but the same applies to all boards installed with the Board Manager. 

Boards Manager

Next, quit and reopen the Arduino IDE to ensure that all of the boards are properly installed. You should now be able to select and upload to the new boards listed in the Tools->Board menu.

Reopen Tools ->Boards Menu

That's it! Please let us know if you encounter any issues in the Adafruit customer support forums.

メーカー品番 3000
CIRC PLAYGROUND CLASS ATMEGA32U4
Adafruit Industries LLC
メーカー品番 659
FLORA ELECTRONIC PLATFORM V3
Adafruit Industries LLC
メーカー品番 1500
TRINKET 3V ATTINY85 EVAL BRD
Adafruit Industries LLC
メーカー品番 1501
TRINKET 5V ATTINY85 EVAL BRD
Adafruit Industries LLC
メーカー品番 2000
PRO TRINKET 5V ATMEGA328P EVAL
Adafruit Industries LLC
メーカー品番 2010
PRO TRINKET 3V ATMEGA328P EVAL
Adafruit Industries LLC
メーカー品番 2471
ESP8266 HUZZAH BREAKOUT BOARD
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.