Maker.io main logo

Adalight for Circuit Playground

39

2017-04-05 | By Adafruit Industries

License: See Original Project

Courtesy of Adafruit

Guide by Phillip Burgess

Overview

One of my first projects with Adafruit was Adalight, an ambient lighting effect for media PCs, similar to the Ambilight feature of mid-2000s Philips TVs. Basically, matching what's on the screen to a set of background lights to make the display pop!

All the pieces of the Adalight project - a microcontroller, addressable “smart” LEDs and a USB connection — are present today on the diminutive Circuit Playground board. Why not replicate this classic project on today’s affordable hardware?

This small remake is no substitute for the gargantuan Adalight builds that some users have created…but for laptops or small all-in-one PCs, it can be a fun project for a board you may already be learning with. There’s no soldering and no extra power supply this time around!

Here’s what the original Adalight could do:

 

For small screens, and only a few minute's time, we can have a pint-sized version easily working, just some software on your PC and on the Circuit Playground board. If you love it, you can always upgrade to the mega-AdaLight version!

Download & Install

Three pieces of software must be installed to follow this project:

Arduino IDE

If you’ve used Circuit Playground before, the Arduino software is already installed on your system. If not, please read Circuit Playground Lesson #0 for guidance on downloading and installing the software and getting your computer talking to Circuit Playground.

Before continuing, you should know how to upload a sketch (such as the example “Blink” sketch) to the Circuit Playground board. Read through the getting-started guides (such as the one linked above) if this is unfamiliar territory.

Processing IDE

Next, download the Processing IDE from the Processing web site. Processing is a programming language for Windows, Mac and Linux with audiovisual applications in mind. The first section of the Getting Started page explains how to install the software.

The Arduino and Processing IDEs look VERY similar!

Adalight ZIP

Finally, visit the Adalight page on Github and download the ZIP file, or simply use this link to download directly:

Download Adalight ZIP File

After uncompressing the ZIP file, you’ll need to move some files into place.

If you’ve run the Arduino and/or Processing IDEs before, there will be corresponding “Arduino” and “Processing” folders inside your personal “Documents” folder (or “My Documents” in Windows). In that case, move the contents of the Arduino and Processing folders from the Adalight ZIP file into the corresponding document folders.

If the Arduino and Processing folders don’t yet exist on your system, you can just copy these from the Adalight ZIP file to your Documents folder.

The other files and folders in the ZIP file can be ignored. These are for other projects and aren’t essential to its use.

other files and folders in the ZIP file can be ignored

Exit Arduino and Processing IDEs if they’re running

Upload Code to Circuit Playground

Launch the Arduino IDE. From the File menu, select Sketchbook, which should “roll over” to show LEDstream_CircuitPlayground. Select this.

From the Tools menu, select Board, then Adafruit Circuit Playground. If this option is not present in the Board menu, the Circuit Playground software is not correctly installed. Please review the previously-mentiouned tutorials to get this started.

From the Tools menu again, select Serial Port, and then the port corresponding to your Circuit Playground board.

Click the Upload button near the top-left of the window:

Upload Code to Circuit Playground

If all goes well, you should see a “Done Uploading” message in the Arduino window. You won’t see Circuit Playground doing anything yet, but it’s ready and waiting for other software on your computer to connect…

Run the Processing Sketch

Launch the Processing IDE. After a moment, you should see a blue and white window that looks similar to the Arduino IDE, but darker.

From the File menu, select Sketchbook. This pops out a new window, which you should be able to scroll through and find the “Adalight_CircuitPlayground” sketch (if it’s not there, review the installation steps above), then open it.

You can try running it just as-is, but it likely won’t work…you’ll either get a small preview window (that”s a promising start), or it might just completely crash if there are no serial devices attached.

You need to edit the code first to point to the correct serial device number. When the program first starts, it prints out the names of serial devices, starting from #0. If you stop the program very quickly, you can scroll up in the console to see this list…count up from zero until you find the serial port corresponding to the Circuit Playground device (it’ll be the same serial port name you selected in the Arduino IDE). Then run again. If it’s not working, check your counting and try again.

This will be different on every system, so we can’t just tell you what to put there.

Run the Processing Sketch

When it works, you should see the NeoPixels on the Circuit Playground board light up.

What It Does

With the USB port at the bottom, stick Circuit Playground to the back of your screen, facing the wall behind. Blue poster-tack or double-stick foam tape can work…or sometimes even regular clear sticky tape across the face of the board. But DO NOT stick Circuit Playground directly on the back of a metal-bodied device, like an aluminum MacBook, or you’ll get an electrical short…cover the back of the board or use a mounting method that leaves a little space between board and screen.

Mounting the Circuit Playground

ALWAYS leave an air gap between the screen and board

The Processing sketch clones the contents of your screen and sends this data to the Circuit Playground, which then updates the LEDs. Try moving windows around, or play a movie or a game.

The Processing code

The Processing code captures screen shots just as fast as it can. In then divides this image into a 5x5 grid, and takes the averages of each of those squares…

The Processing code

Ten of those squares correspond to the ten NeoPixels on the Circuit Playground board. It’s not all one color…you can actually see motion reflected in the LEDs.

The Processing code

The Processing code doesn’t work with all graphics cards and modes…full-screen video, for example, may be accessing the graphics hardware directly and bypassing the normal frame buffer that Processing works with. (In one case, it works fine with full-screen movies on my NVIDIA-based iMac, but not my Intel Graphics-based MacBook Air…in the latter case, I have to keep the movie in a windowed mode, with the menu bar visible. Ah well.)

There are compatible third-party apps that may work better with full-screen video. The original Adalight guide mentions a couple of options (Lightpack and Boblight) that may fare better in this regard, though they’ll require some initial set-up to define the pixel placement as described above.

メーカー品番 3000
CIRC PLAYGROUND CLASS ATMEGA32U4
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.