Maker.io main logo

3D Printed Illuminated Wand Prop

64

2024-04-30 | By SparkFun Electronics

License: See Original Project 3D Printing

Courtesy of SparkFun

Guide by BBOYHO

Introduction

In this tutorial, we will learn about how to create a theatrical prop for a performance by 3D printing a ‎wand and adding an LED.‎

wand_1

Required Materials

To follow along with this project tutorial, you will need the following materials. You may not need ‎everything though depending on what you have. Add it to your cart, read through the guide, and ‎adjust the cart, as necessary.‎

Tools

You will need a soldering tools, a 3D printer, and ABS filament. A heat gun or hot air rework station ‎is optional for applying heat to heat shrink or if you want to smooth out the edges of hot glue.‎

You will also need:‎

  • Scissors

  • Hot Glue Gun and Glue Sticks

  • Sandpaper or Filer

Suggested Reading

If you aren't familiar with the following concepts, we recommend checking out these tutorials before ‎continuing. The flashlight kit is a good beginning kit to start with if you have not soldered before!‎

  • How to Power a Project: A tutorial to help figure out the power requirements of your project.‎

  • LilyPad Buttons and Switches: Learn about the button and switch offerings in the LilyPad ‎line and how to use them.‎

  • Flashlight Kit: This is an assembly guide for the SparkFun Flashlight Kit, a basic learn to solder ‎kit.‎

‎3D Print It‎

After browsing Thingiverse, the model that I found appealing was “jakereeves” elder wand. Head ‎over to the thing and download the files to print the model of your size. Since the print area is small, ‎you will need to print the part in two pieces.‎

THINGIVERSE: THE ELDER WAND

Understanding Your Circuit

The circuit is simple and consists of an LED, 10Ω resistor, LilyPad switch, and a battery holder. I ‎chose to add a current limiting resistor between the anode (longer leg) of the LED and "+" terminal ‎of the battery holder. The resistor was probably not necessary since a coin cell is not able to source ‎enough current to damage the LED. Nonetheless, a resistor was still added as good practice. The ‎LilyPad switch was added between the cathode (shorter leg) of the LED and the "--" terminal of the ‎battery holder.‎

diagram_2

While the orientation of the switch did not affect the overall functionality of the circuit, I did decided ‎to have the ON side of the LilyPad switch facing toward the LED for the user. Also, the LilyPad coin ‎cell holder was a bit big compared to the size of the wand, so a smaller holder was chosen for the ‎project. There will be markings on the holder to indicate the "+" and "--" terminals with the ‎alternative holder.‎

dim_3

Dimension of LilyPad Coin Cell Holder ‎[PRT-10730]‎

dim_4

Dimension of Coin Cell Holder ‎[DEV-08822]‎

Hardware Hookup

Note: I used a Lulzbot Taz 5 for the print. The Lulzbot Taz 6 should have a sufficient enough area ‎to print the wand pieces.‎

After printing the wand on your 3D printer and removing it from the print area, you will need to ‎remove the raft support under the wand. Carefully remove support using pliers. With my settings, ‎there was also some support printed in the handle that needed to be removed before gluing the ‎two pieces together. When ready, add some hot glue in the dimple of the handle and join the two ‎pieces together.‎

join_5

Tip: If you are using hot glue, try using a hot air rework station to smooth out the rough sections of ‎glue holding the part together. Just try not to apply too much heat as this can warp or melt the wand ‎that was printed with ABS. ‎

tip_6

Once assembled, your wand should look similar to the image below.‎

assembled_7

Let's start on the electronics side of the wand. The super bright white LED was bright but hard to ‎see from all angles. To diffuse the LED and increase the viewing angle of the LED, you will need to ‎sand the epoxy lens. Using sandpaper or file, sand the outside of the LED. Make sure to hold the ‎legs close to the LED to avoid damaging pins coming out of the epoxy lens.‎

sand_8

Wrap a current limiting resistor around one terminal of the LED. In this case, I added a 10Ω resistor ‎to the longer leg of the LED (i.e., +, anode side). Then solder and trim down the remaining terminal ‎with a flush cutter. Make sure to be careful when handling the resistor terminals since they are thin ‎compared to the terminals of the LED.‎

wrap_9

Cut two solid core wires so that they are able to run along the length of the wand. You will want a ‎little extra room to work with the wire. Strip the wire ends and solder one wire to the shorter leg of ‎the LED (i.e. --, cathode side). Then solder the second wire to the other end of the resistor.‎

cut_10

Note: While you can use stranded core wire, solid core wire will hold its shape better compared to ‎stranded wires.‎

Cut some heat shrink to cover the exposed terminals of the LED and resistor. Slide the heat shrink ‎down the wires and over the terminals. Wrap the wires around the wand. You will need to use one ‎hand to hold the wires down as you twist the wires around the wand. Make sure the wires are ‎secure to the wand. If you are satisfied with the length of wires provided for the switch and coin cell ‎holder's "+" terminal, apply heat to the heat shrink.‎

heatstrink_11

Before soldering wires to the switch and the coin cell battery holder, take note of the location of ‎where the components will be added. The switch will go on the top of the wand between grooves ‎shown in the image below. The battery holder will go underneath the wand (where the raft support ‎was removed) between the grooves as shown in the image.‎

location_12

You should have enough wire to add a switch and battery holder. Solder the wire that was from the ‎LED's cathode side (i.e., "-", longer leg) to the terminal adjacent to the ON position. If you are ‎unsure of the polarity, test it out with a coin cell battery or multimeter.‎

solder_13

Tip: The plated through hole on the LilyPad switch was designed to provide enough area for ‎contact when using conductive thread and hold the component against fabric. However, you can ‎still solder to the pad. If necessary, you could hook and clamp the wire down against the hole using ‎pliers. You may need to use a 3rd hand or tape to hold the wire and switch down when soldering ‎the joint.‎

Carefully bend the terminals of the coin cell holder using the end of a wire stripper so that it can fit ‎nicely between the grooves of the wand.‎

bend_14

Strip the other end of the wire that is connected to the resistor and slide the exposed ends of the ‎wire through the top of the "+" terminals through hole. If you are satisfied with the length, solder ‎the wire to the terminal. Then cut and strip another piece of wire to add between the switch's OFF ‎position and the holder's "--" terminal.‎

strip_15

At this point, test out the connections with a coin cell battery or multimeter. Make sure the switch is ‎flipped to the ON position. If you are using a coin cell battery, the battery does not need to be fully ‎inserted in the coin cell holder to light up.‎

Cut some clear heat shrink and slide it over the LED and wand's tip. Apply heat to the heat shrink.‎

heat_16

If you are satisfied with the connections, hot glue the bottom of the switch and coin cell battery ‎holder to the wand. Avoid adding too much hot glue on the coin cell battery holder. If the holder's ‎contacts to the battery are covered, it can interfere with the circuit causing the LED to not light up. ‎Once the hot glue has cooled down, fully insert the coin cell battery into the holder.

glue_17

The wand's handle should look similar to the image below.‎

handle_18

Your fully assembled 3D printed illuminated wand should look similar to the image below!‎

assembled_19

If you have not already, flip the switch to power the LED. Even in a bright room, the diffused LED ‎was still visible!‎

bright_20

Illuminated Wand in Bright Room

low_21

Illuminated Wand in Low Light

Repeat the steps above to make more wands as necessary for all of your wizards!‎

wands_22

Stress Testing in the Field

Rehearsals

How did it go when I handed the illuminated wands over to my students? Well, they did not mind the ‎circuit being wrapped around on the outside of the wand. The kids started saying magical ‎incantations, ran around flicking imaginary balls of energy, and tried making things levitate. As a ‎result, NO ONE WAS FOCUSED. Luckily, I handed them their illuminated wands during their last ‎rehearsal before the fall show. At least they were really in character?

rehearsals_23

rehearsals_24

Show Time!‎

When it came time for the show, everything went as planned. The illuminated wands lasted ‎throughout tech, during the performance, and after the show. Here’s a picture of the team after ‎they went on!‎

show_25

Making it Better

There’s always room for improvement. After the project was completed, I had a few ideas of making ‎the prop more functional. Below are a list of possible upgrades and improvements that could be ‎implemented for future builds.‎

  • Microcontroller and Sensors -- If I had more time, I would have wanted to add a ‎microcontroller and sensors (i.e., an accelerometer and gyro) to each of the wands so that the ‎LED would only turn on based on the gestures.‎

  • Custom 3D Model -- I would have also wanted to design a wand from scratch to include the ‎electronics on the inside similar to the other models found on Thingiverse.‎

Resources and Going Further

For more information related to the project, check out the resources below:‎

メーカー品番 10969
RESISTOR KIT - 1/4W (500 TOTAL)
SparkFun Electronics
メーカー品番 09350
SLIDE SWITCH
SparkFun Electronics
メーカー品番 08022
HOOK-UP SOLID 22AWG BLACK 25'
SparkFun Electronics
メーカー品番 14456
SOLDERING IRON - 60W (ADJUSTABLE
SparkFun Electronics
メーカー品番 10326
HEATERIZER XL-3000 HEAT GUN
SparkFun Electronics
メーカー品番 09163
SOLDER LEAD FREE - 15-GRAM TUBE
SparkFun Electronics
メーカー品番 57818
WIRE STRIPPERS & CUTTERS 7.25"
Wiha
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.