Maker.io main logo

Hacksmith Industries' Jet-Powered Snow Racer Aims for Land Speed Glory

314

2025-03-24 | By The Hacksmith

Microcontrollers

Innovation and adrenaline collide as the popular YouTube channel Hacksmith Industries takes on the challenge of breaking the land speed record for jet-powered sleds. Known for their ambitious engineering projects that bring fictional ideas to life, the Hacksmith team has once again pushed the limits of creativity and technology. This time, their vehicle of choice is a heavily modified GT Snow Racer, fitted with not one, but two KingTech K320 G5 jet engines.

The Concept

The idea behind this record-breaking attempt is both simple and extreme: take a lightweight GT Snow Racer—a classic winter sled—and outfit it with high-performance turbine engines designed for model jets. With each KingTech K320 G5 capable of producing an astounding 140 pounds of thrust, the combined output propels the sled into unprecedented territory.

The team’s goal is not just to break records but to demonstrate the sheer power and potential of jet propulsion in unconventional applications. With their signature mix of ingenuity and hands-on engineering, Hacksmith Industries has transformed a common winter toy into a high-speed ice rocket.

Engineering the Beast

Transforming a standard snow racer into a high-speed rocket on ice requires significant modifications. The original metal frame is reinforced to handle the immense forces at play, while the steering system is upgraded to maintain control at extreme velocities. Custom mounting brackets securely hold the twin jet engines in place, and a sophisticated fuel delivery system ensures a steady burn.

Safety is paramount, with the addition of a drag chute, brakes, and a stability-focused ski setup designed to reduce drag and enhance maneuverability.

Hacksmith Industries' Jet-Powered Snow Racer Aims for Land Speed Glory

Scheme-it detail link

Hacksmith Industries' Jet-Powered Snow Racer Aims for Land Speed Glory

Scheme-it link

The Speed Test

To put the sled to the test, the Hacksmith team selects a snowmobile drag strip as their proving ground. This controlled environment provides a groomed surface designed for high-speed runs, ensuring optimal conditions for testing. The team meticulously prepares for the test run, conducting multiple safety checks and running trial tests at lower speeds before unleashing the full power of the twin jets.

The moment of truth arrives as the engines roar to life, sending plumes of jet exhaust into the cold air. With a deafening scream, the sled accelerates, carving through the ice with astonishing speed. As the sled reaches its peak performance, the onboard cameras capture every thrilling second, ensuring that fans worldwide can witness the spectacle in the full YouTube video.

The Future of Extreme Sled Racing

This attempt is not just about breaking records—it’s about pushing the boundaries of engineering and human daring. If successful, it could pave the way for a new breed of high-speed winter sports, inspiring other engineers, and thrill-seekers to push their own limits.

Hacksmith Industries is no stranger to extreme projects, having built everything from real-life plasma lightsabers to exoskeletons capable of superhuman strength. Their GT Snow Racer Jet project is another testament to their ability to blend engineering expertise with entertainment, educating and inspiring millions of viewers around the world.

With cutting-edge technology and sheer determination, Hacksmith Industries’ GT Snow Racer Jet is set to make history, proving that with the right modifications, even a humble sled can become a speed demon on ice. Fans can follow the entire journey in their YouTube video, where they showcase the design, build process, and high-speed test runs. Whether or not they officially break the record, one thing is certain—this project is an unforgettable showcase of ingenuity, creativity, and pure speed.

メーカー品番 11113
ARDUINO PRO MINI 328 5V/16MHZ
SparkFun Electronics
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.