Maker.io main logo

A Short Review on Thermocouples and What We Use Them For!

289

2024-07-22 | By Andrew Chen

Hi, my name is Andrew! Here, we will be going over thermocouples, their applications, the physics behind them, and what factors you should consider when choosing a thermocouple for your own personal projects.

A Short Review on Thermocouples and What We Use Them For!

In physics, heat has the tendency to evenly distribute itself across a material when there is a temperature gradient. For example, if we have a rod and heat is applied to only one end of the rod, then we can expect the transfer of heat energy to flow from the heat-applied rod to the other end. This principle applies to the individual particles inside the rod as well; electrons are good carriers of thermal energy, especially in metals where there exists a lattice structure. Electrons are able to easily flow from one end to the other, and we can induce this phenomenon by applying some heat.

This is why thermocouple devices are usually made out of metal for easy electron flow from one region to the other. Some common pairs of materials that may be used when creating a thermocouple are iron-constantan (also known as type T) and platinum and rhodium (thermocouples here are considered type S, R, or B depending on the ratio). Depending on the specifics of the applications you are looking for, you may want a thermocouple that is more sensitive to changes in heat or may be more resistant.

A Short Review on Thermocouples and What We Use Them For!

Generally speaking, a thermocouple works by having two different wires made from different metals welded at a particular junction. Voltage is induced when there is a change in the temperature in that particular junction. The science behind this is that different metals have different levels of affinity for heat conduction. So, there will be a difference in temperature between the two wires. This difference induces an EMF that has very practical applications in home appliances, industrial processes, and temperature sensors in thermostats.

A Short Review on Thermocouples and What We Use Them For!

Another common application of thermocouples is in gas stoves/furnaces. Although seemingly very minor, thermocouples also can play a huge safety role. In a residential furnace, the pilot flight generates a flame, which then ignites an emission of natural gas from a valve. A thermocouple will be able to sense the flame and leave the gas valve open; otherwise, the thermocouple can detect a lack of presence of a flame and can be used to close the valve, preventing any unnecessary gas leaks and possible poisoning or explosions.

Due to the different varieties and flavors that thermocouples come in, you may want to design a project where you'll need a specific type of thermocouple that works best for your application. Depending on what you're making, there are a few certain factors to consider when picking out a thermocouple:

  • Thermocouples generally have a rating of a temperature range, and this information is usually pretty easy to find either on the datasheet or on the thermocouple’s product page. Thermocouples with a higher temperature rating are typically made of a high concentration of rhodium, making type S, R, or B thermocouples significantly more costly. Consider the budget of your project and the range you'll most likely operate within.
  • Response time: thermocouples usually come in three different types: exposed, grounded, and ungrounded. If you need a really fast response time from the thermocouple, then you should opt for an exposed junction. However, if you are working with an application where the thermocouple may be coming into contact with chemical corrosion, it's ill-advised to work with an exposed junction. An ungrounded thermocouple is the slowest in response time but can be installed such that it is isolated electronically from the rest of the system.

These are just some factors to consider when picking out the right thermocouple for the specific specs and constraints of your project. If you found this blog post entertaining and informative, please share this post with your friends!

As always,

Andrew

メーカー品番 COM1705
TYPE-K BRAIDED THERMOCOUPLE
Pimoroni Ltd
メーカー品番 GK11M
PROBE TEMP "K" 4' INSULATED LEAD
TPI (Test Products Int)
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.