Maker.io main logo

What is Solder Flux and Why You Should Use It

67,147

2023-04-03 | By Maker.io Staff

Solder / Desoldering Solder

What is Solder Flux and Why You Should Use It

When assembling circuit boards, the tools and solder used are only one part of the equation ‎needed to successfully build reliable and durable electronics. Flux is another crucial ingredient in ‎the recipe to success as it plays a vital role in preparing the electronic components and surface ‎of the PCB, making solder flow more easily, and binding the metal to pads and component legs ‎to help fuse them. This article investigates a few types of flux commonly used in electronics ‎projects.‎

Understanding the Role of Flux When Soldering

Anyone who’s ever tried soldering components to a PCB with untinned pads without flux will ‎know the problems to go along with the process. The solder will hardly stick to the pads or the ‎components, and even if it does, the solder joints are often brittle and of bad quality. That’s often ‎due to a mix of factors. For example, the copper pads on the PCB start to oxidize as soon as ‎they’re exposed to air after the etching process. This thin oxidization layer builds up on the ‎surface, preventing the solder from sticking to the copper properly. Further, different solder formulations may result in the solder having a harder time bonding to the copper or gold-plated ‎legs of components.‎

This is where flux comes in, as this chemical product helps prepare the surfaces on the PCB by ‎removing oxidization and wetting the surface. Further, flux helps create a true metallurgic bond ‎between the PCB’s pads and component legs, ensuring that solder joints won’t crack when ‎exposed to thermal and physical stress. Finally, flux also helps prevent new oxidization from ‎forming during the high heat soldering process which would normally accelerate oxidization.‎

The Three Main Types of Soldering Flux in Electronics

Like solder, you can distinguish the types of flux commonly available for use in electronics ‎assembly by the base chemical used to create the flux. The three main types are rosin-based, ‎no-clean, and water-soluble flux. Alternatively, it’s also possible to classify the flux according to ‎its delivered form, such as a spray, liquid, paste, or core embedded within the solder.‎

The first type, rosin-based flux, is made from pine tree sap and then dissolved in a solvent, ‎usually isopropyl alcohol. The resulting product is slightly acidic, which helps dissolve built-up ‎gunk and oxidization. In this state, the flux is called type-R rosin flux. However, manufacturers ‎can add additional acid activators to make the flux more aggressive and increase its ability to ‎dissolve heavier oxide films, which may be required when soldering at higher temperatures, such ‎as lead-free solder. Depending on the activation level, the flux is categorized into RMA (rosin ‎mildly activated) and RA (rosin activated). Due to its acidic nature, this flux must be cleaned off ‎the PCB after assembly to prevent it from corroding the board over time.‎

What is Solder Flux and Why You Should Use It

No-clean flux is a rosin flux with minimal activation, meaning removing the chemical upon ‎assembly is unnecessary. However, due to the decreased acidity, this type of flux is not as ‎efficient in preparing the surfaces for soldering, and they may not be suitable for working with ‎higher temperatures. While not crucial, cleaning the board after assembly is still recommended, ‎as no-clean flux can leave behind a sticky residue that may attract dust and lead to hardware ‎failures in sensitive components over time.

Finally, water-soluble flux employs synthetic resins to achieve a good middle-ground between ‎no-clean flux and type R flux, as they are still quite corrosive, which leads to a well-prepared, ‎clean soldering surface, yet they are easy to clean up. After assembly, this flux must be rinsed ‎off the board using de-ionized water instead of chemical solvents, which is less messy and more ‎cost-effective. In addition, some water-soluble flux is also (mostly) water-based, which can ‎reduce harmful emissions during the soldering process and is better for workers and the ‎environment.‎

Using the Correct Form of Delivery

What is Solder Flux and Why You Should Use ItMany solder wires have flux embedded in their core. This flux is often no-clean and can be seen ‎evaporating during the soldering process.‎

Most people will seldom need to add additional flux when soldering, as they’ll most likely use a ‎solder that embeds flux in the core of the wire. However, some people prefer adding extra flux in ‎the form of paste to aid them in mounting large components that require high temperatures to ‎solder, like I/O ports and transformers. Further, the use of flux depends on the technique used ‎and the size of the components to solder. For instance, reflow or hot-air soldering of SMD ‎components requires solder paste, which is flux with dissolved solder powder. Further, de-‎soldering usually requires adding extra flux in either liquid or paste form, as the old flux has likely ‎been cleaned off after manufacturing, and the old solder joints will probably have oxidized over ‎time, making removal more difficult without additional flux.‎

Recommended reading for more information about flux:‎

How to Solder with Flux

Solder and Flux

Cleaning PCBs

メーカー品番 CQ4LF-B-R
LIQUID FLUX NO-CLEAN IN 6ML (0.2
Chip Quik Inc.
メーカー品番 CQ4LF
FLUX - NO CLEAN PEN 0.34 OZ
Chip Quik Inc.
メーカー品番 RA891
ROSIN PASTE FLUX (RA) IN 2OZ FLA
Chip Quik Inc.
メーカー品番 CQNTRM
FLUX REMOVER (NON-FLAMMABLE) IN
Chip Quik Inc.
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.