Maker.io main logo

Arduino Launches the Arduino UNO Mini Limited-Edition Board

306

2021-11-29 | By Travis Foss

To celebrate selling over 10 million UNO boards, Arduino has produced a Limited-Edition version of the UNO board, the UNO Mini Limited Edition. The Arduino UNO, which launched back in 2010, has become the board that most commonly represents the Arduino name.

Due to meeting the milestone of 10 million boards sold, Arduino created something super cool to celebrate this milestone. The board they came up with is the UNO Mini Limited Edition.

Arduino Launches the Arduino UNO Mini Limited-Edition Board

The UNO Mini Limited Edition has similar specifications to the original Arduino UNO boards; however, they have added a few updates users are sure to love. One of the first things users will notice is that the USB port has been updated to a USB-C port. The second change users will notice is the footprint is much smaller than the original. With a footprint of 34.2mm x 26.7mm x 8mm, the UNO Mini Limited Edition is a quarter of the size of the most recent version of the UNO boards, the UNO Rev 3.

Arduino Launches the Arduino UNO Mini Limited-Edition Board

These Limited-edition boards come individually numbered, creating an excellent collector item for anyone who loves Arduino products. With all the features that users love, the new UNO Mini Limited Edition will be a collector’s item for years to come.

Arduino Launches the Arduino UNO Mini Limited-Edition Board

UNO Mini Limited-Edition Specs

  • Microcontroller: ATmega328P
  • Operating Voltage: 5V
  • Input Voltage: 6-20V
  • Digital I/O Pins: 14
  • PWM I/O Pins: 6
  • Analog Input Pins: 6
  • Flash Memory: 32KB
  • SRAM: 2 KB
  • EEPROM: 1 KB
  • Clock Speed: 16MHz
  • Dimensions: 34.2mm x 26.7mm x 8mm

The Arduino UNO Mini Limited Edition is available for order today. However, supplies are limited, so order yours by visiting the UNO Mini LE page today.

メーカー品番 A000066
ARDUINO UNO R3 ATMEGA328P BOARD
Arduino
メーカー品番 ABX00062
ARDUINO UNO MINI LE
Arduino
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.