SiWx917 Wireless Pro Kit - Unboxing | DigiKey
Inside the box you’ll find the RD4002A Wireless Pro Kit Mainboard, the SiWG917 Radio Board, a logic analyzer harness, a ribbon cable, two headers, and a battery holder.
https://www.digikey.com/en/products/detail/silicon-labs/SIWX917-PK6031A/21801049
The SiWx917 Wireless Pro Kit features an onboard debugger with a virtual COM port and logic analyzer for application development and debugging. Hardware and peripherals include Ethernet and USB connectivity, humidity and temp sensor, advanced energy monitor, a 20 pin expansion header, and an LCD.
Here, we’ll demonstrate how to commission your module onto a WiFi network. First, plug the radio board into the mainboard. Then, connect the Wireless Pro kit to a computer with the power selection switch in the AEM position.Download the Simplicity Connect app on a mobile device. Then, download Simplicity Studio and install the WiSeConnect 3 extension under the install tab. From the Welcome window, click the start button. Next, check for the latest adapter firmware and confirm the Gecko SDK Suite is selected. Now, create new project and click finish. Connect the device and run the out of box project.
From the Simplicity Connect app, connect to the BLE Configurator and select an access point. The module is now commissioned into the WiFi network.
Learn more: Maker.io - https://www.digikey.com/en/maker DigiKey’s Blog – TheCircuit https://www.digikey.com/en/blog Connect with DigiKey on Facebook https://www.facebook.com/digikey.electronics/ And follow us on X (Formerly Known as Twitter) https://twitter.com/digikey
Part List
| 画像 | メーカー品番 | 商品概要 | 入手可能な数量 | 料金 | 詳細を表示 | |
|---|---|---|---|---|---|---|
![]() | ![]() | SIWX917-PK6031A | PRO KIT SOC WI-FI 6 BLUETOOTH LE | 47 - 即時 | $33,310.00 | 詳細を表示 |