Microchip Technologyが提供するPIC10(L)F32(0,2) Prog Specのデータシート

6‘ ‘MICFIDCHIP PIC10(L)F320/322
2011-2012 Microchip Technology Inc. Advance Information DS41572D-page 1
PIC10(L)F320/322
This document includes the
programming specifications for the
following devices:
1.0 OVERVIEW
The PIC10(L)F320/322 devices are programmed using
In-Circuit Serial Programming™ (ICSP™). This
programming specification applies to the
PIC10(L)F320/322 devices in all packages.
With the exception of memory size and the voltage
regulator, all other aspects of the PIC10(L)F320/322
devices are identical.
1.1 Hardware Requirements
1.1.1 HIGH-VOLTAGE ICSP
PROGRAMMING
In High-Voltage ICSP mode, the device requires two
programmable power supplies: one for VDD and one for
the MCLR/VPP pin.
1.1.2 LOW-VOLTAGE ICSP
PROGRAMMING
In Low-Voltage ICSP mode, the PIC10(L)F320/322
devices can be programmed using a single VDD source
in the operating range. The MCLR/VPP pin does not
have to be brought to a different voltage, but can
instead be left at the normal operating voltage.
1.1.2.1 Single-Supply ICSP Programming
The LVP bit in the Configuration Word enables single-
supply (low-voltage) ICSP programming. The LVP bit
defaults to a ‘1’ (enabled) from the factory. The LVP bit
may only be programmed to ‘0’ by entering the High-
Voltage ICSP mode, where the MCLR/VPP pin is raised
to VIHH. Once the LVP bit is programmed to a ‘0’, only
the High-Voltage ICSP mode is available and only the
High-Voltage ICSP mode can be used to program the
device.
• PIC10F320 • PIC10LF320
• PIC10F322 • PIC10LF322
Note 1: The High-Voltage ICSP mode is always
available, regardless of the state of the
LVP bit, by applying VIHH to the MCLR/
VPP pin.
2: While in Low-Voltage ICSP mode, MCLR
is always enabled, regardless of the
MCLRE bit, and the port pin can no
longer be used as a general purpose
input.
PIC10(L)F320/322 Flash Memory Programming Specification
MCLR MCLR MCLR MCLR
PIC10(L)F320/322
DS41572D-page 2 Advance Information 2011-2012 Microchip Technology Inc.
1.2 Pin Utilization
Five pins are needed for ICSP™ programming. The
pins are listed in Ta b l e 1 - 1 .
TABLE 1-1: PIN DESCRIPTIONS DURING PROGRAMMING
Pin Name
During Programming
Function Pin Type Pin Description
RA1 ICSPCLK I/O Clock Input – Schmitt Trigger Input
RA0 ICSPDAT I/O Data Input/Output – Schmitt Trigger Input
RA3/MCLR/VPP Program/Verify mode P(1) Program Mode Select/Programming Power Supply
VDD VDD P Power Supply
VSS VSS P Ground
Legend: I = Input, O = Output, P = Power
Note 1: To activate the Program/Verify mode, high voltage needs to be applied to MCLR/VPP input. Since the
MCLR /VPP is used for a level source, MCLR/VPP does not draw any significant current.
2011-2012 Microchip Technology Inc. Advance Information DS41572D-page 3
PIC10(L)F320/322
2.0 DEVICE PINOUTS
The pin diagrams for the PIC10(L)F320/322 family are
shown in Figure 2-1 and Figure 2-2. The pins that are
required for programming are listed in Table 1 - 1 and
shown in bold lettering in the pin diagrams.
FIGURE 2-1: 6-PIN DIAGRAM FOR PIC10(L)F320/322
FIGURE 2-2: 8-PIN DIAGRAM FOR PIC10(L)F320/322
SOT-23
1
2
34
5
6
PIC10(L)F320
PIC10(L)F322
RA3/MCLR/V
PP
VDD
RA2
ICSPCLK/RA1
ICSPDAT/RA0
V
SS
PDIP, DFN
1
2
3
45
6
7
8
RA3/MCLR/V
PP
VSS
N/C
RA0/ICSPDAT
ICSPCLK/RA1
N/C
VDD
RA2
PIC10(L)F320
PIC10(L)F322
PIC10(L)F320/322
DS41572D-page 4 Advance Information 2011-2012 Microchip Technology Inc.
3.0 MEMORY MAP
The memory for the PIC10(L)F320/322 devices is
broken into two sections: program memory and
configuration memory. The size of the program
memory and the configuration memory is different
between devices.
FIGURE 3-1: PIC10F320 AND PIC10LF320 PROGRAM MEMORY MAPPING
1FFF
h
2000
h
2080
h
3FFF
h
256 W
Maps to
Program Memory
Configuration Memory
2000h-2080h
User ID Location
User ID Location
User ID Location
User ID Location
Reserved
Reserved
Device ID
Configuration Word 1
Calibration Word 1
Calibration Word 2
Reserved
2000h
2001h
2002h
2003h
2004h
2005h
2006h
2007h
2008h
2009h
Implemented
200Ah-207Fh
0000
h
Maps to
0000h-00FFh
00FFh
2011-2012 Microchip Technology Inc. Advance Information DS41572D-page 5
PIC10(L)F320/322
FIGURE 3-2: PIC10F322 AND PIC10LF322 PROGRAM MEMORY MAPPING
1FFF
h
2000
h
2080
h
3FFF
h
512 W
Maps to
Program Memory
Configuration Memory
2000h-2080h
User ID Location
User ID Location
User ID Location
User ID Location
Reserved
Reserved
Device ID
Configuration Word 1
Calibration Word 1
Calibration Word 2
Reserved
2000h
2001h
2002h
2003h
2004h
2005h
2006h
2007h
2009h
2008h
Implemented
200Ah-207Fh
0000
h
01FF
h
Maps to
0000h-01FFh
AB®
PIC10(L)F320/322
DS41572D-page 6 Advance Information 2011-2012 Microchip Technology Inc.
3.1 User ID Location
A user may store identification information (user ID) in
four designated locations. The user ID locations are
mapped to 2000h-2003h. Each location is 14 bits in
length. Code protection has no effect on these memory
locations. Each location may be read with code
protection enabled or disabled.
3.2 Device ID
The device ID word for the PIC10(L)F320 and the
PIC10(L)F322 is located at 2006h. This location cannot
be erased or modified.
REGISTER 3-1: DEVICEID: DEVICE ID REGISTER(1)
TABLE 3-1: DEVICE ID VALUES
Note: MPLAB® IDE only displays the 7 Least
Significant bits (LSb) of each user ID
location, the upper bits are not read. It is
recommended that only the 7 LSbs be
used if MPLAB IDE is the primary tool
used to read these addresses.
RR RRRR
DEV8 DEV7 DEV6 DEV5 DEV4 DEV3
bit 13 bit 8
RRRRRRRR
DEV2 DEV1 DEV0 REV4 REV3 REV2 REV1 REV0
bit 7 bit 0
Legend:
R = Readable bit P = Programmable bit ‘1’ = Bit is set ‘0’ = Bit is cleared
-n = Value at POR W = Writable bit U = Unimplemented bit,
read as ‘0
x = Bit is unknown
bit 13-5 DEV<8:0>: Device ID bits
These bits are used to identify the part number.
bit 4-0 REV<4:0>: Revision ID bits
These bits are used to identify the revision.
Note 1: This location cannot be written.
DEVICE
DEVICE ID VALUES
DEV<8:0> REV<4:0>
PIC10F320 10 1001 101 x xxxx
PIC10F322 10 1001 100 x xxxx
PIC10LF320 10 1001 111 x xxxx
PIC10LF322 10 1001 110 x xxxx
2011-2012 Microchip Technology Inc. Advance Information DS41572D-page 7
PIC10(L)F320/322
3.3 Configuration Word
The PIC10(L)F320 and PIC10(L)F322 have one
Configuration Word, Configuration Word 1 (2007h).
The individual bits within this Configuration Word are
used to enable or disable device functions such as the
Brown-out Reset, code protection and Power-up Timer.
3.4 Calibration Words
For the PIC10(L)F320 and PIC10(L)F322 devices, the
16 MHz internal oscillator (INTOSC) and the Brown-out
Reset (BOR) are factory calibrated and stored in
Calibration Words 1 and 2 (2008h and 2009h).
The Calibration Words do not participate in erase
operations. The device can be erased without affecting
the Calibration Words.
PWRTE ‘ 256 W Flash memory PlC10F320. 512 W Flash memory PlC10F322. MCLR MCLR MCLR MCLR MCLR MCLR MCLR MCLR MCLR
PIC10(L)F320/322
DS41572D-page 8 Advance Information 2011-2012 Microchip Technology Inc.
REGISTER 3-2: CONFIGURATION WORD 1
U-1 R/P-1 R/P-1 R/P-1 R/P-0 R/P-1
WRT1 WRT0 BORV LPBOREN LVP
bit 13 bit 8
R/P-1 R/P-1 R/P-1 R/P-1 R/P-1 R/P-1 R/P-1 R/P-1
CP MCLRE PWRTE WDTE1 WDTE0 BOREN1 BOREN0 FOSC
bit 7 bit 0
Legend:
R = Readable bit P = Programmable bit U = Unimplemented bit, read as ‘1
0 = Bit is cleared ‘1’ = Bit is set -n = Value when blank or after Bulk Erase
bit 13 Unimplemented: Reads as ‘1
bit 12-11 WRT<1:0>: Flash Memory Self-Write Protection bits
256 W Flash memory: PIC10F320:
11 = Write protection off
10 = 000h to 03Fh write-protected, 040h to 0FFh may be modified by PMCON control
01 = 000h to 07Fh write-protected, 080h to 0FFh may be modified by PMCON control
00 = 000h to 0FFh write-protected, no addresses may be modified by PMCON control
512 W Flash memory: PIC10F322:
11 = Write protection off
10 = 000h to 07Fh write-protected, 080h to 1FFh may be modified by PMCON control
01 = 000h to 0FFh write-protected, 100h to 1FFh may be modified by PMCON control
00 = 000h to 1FFh write-protected, no addresses may be modified by PMCON control
bit 10 BORV: Brown-out Reset Voltage Selection bit
1 = Brown-out Reset Voltage (VBOR) set to 1.9V (LF parts) or 2.4V (F parts)
0 = Brown-out Reset Voltage (VBOR) set to 2.7V
bit 9 LPBOREN: Low-Power Brown-out Reset Enable bit
1 = Low-power Brown-out Reset is enabled
0 = Low-power Brown-out Reset is disabled
bit 8 LVP: Low-Voltage Programming Enable bit
1 = Low-voltage programming enabled. RA3/MCLR/VPP pin function is MCLR.
0 = High Voltage on MCLR/VPP must be used for programming
bit 7 CP: Flash Program Memory Code Protection bit
1 = Code protection off
0 = Code protection on
bit 6 MCLRE: RA3/MCLR/VPP Pin Function Select bit
When LVP = 1, this bit is overridden to ‘1: pin function is MCLR, weak pull-up enabled
1 =RA3/MCLR
/VPP pin function is MCLR; Weak pull-up enabled
0 =RA3/MCLR
/VPP pin function is digital input; MCLR internally disabled; Weak pull-up under
software control
bit 5 PWRTE: Power-up Timer Enable bit
1 = PWRT disabled
0 = PWRT enabled
bit 4-3 WDTE<1:0>: Watchdog Timer Enable bit
11 = WDT enabled, SWDTEN is ignored
10 = WDT enabled while running and disabled in Sleep. SWDTEN is ignored
01 = WDT controlled by the SWDTEN bit in the WDTCON register
00 = WDT disabled. SWDTEN is ignored
2011-2012 Microchip Technology Inc. Advance Information DS41572D-page 9
PIC10(L)F320/322
bit 2-1 BOREN<1:0>: Brown-out Reset Enable bits
11 = Brown-out Reset enabled; SBOREN bit is ignored
10 = Brown-out Reset enabled while running, disabled in Sleep; SBOREN bit is ignored
01 = Brown-out Reset controlled by the SBOREN bit in the BORCON register
00 = Brown-out Reset disabled; SBOREN bit is ignored
bit 0 FOSC: Oscillator Selection bit
1 = EC oscillator from CLKIN
0 = INTOSC oscillator; CLKIN not enabled
MCLR MCLR MCLR MCLR MCLR MCLR PWRTE MCLR
PIC10(L)F320/322
DS41572D-page 10 Advance Information 2011-2012 Microchip Technology Inc.
4.0 PROGRAM/VERIFY MODE
In Program/Verify mode, the program memory and the
configuration memory can be accessed and
programmed in serial fashion. ICSPDAT and
ICSPCLK are used for the data and the clock,
respectively. All commands and data words are
transmitted LSb first. Data changes on the rising edge
of the ICSPCLK and latched on the falling edge. In
Program/Verify mode, both the ICSPDAT and
ICSPCLK are Schmitt Trigger inputs. The sequence
that enters the device into Program/Verify mode
places all other logic into the Reset state. Upon
entering Program/Verify mode, all I/Os are
automatically configured as high-impedance inputs
and the address is cleared.
4.1 Program/Verify Mode Entry and
Exit
There are two different methods of entering Program/
Verify mode:
•VPPFirst entry mode
•V
DD – First entry mode
4.1.1 VPP – FIRST ENTRY MODE
To enter Program/Verify mode via the VPP-first method
the following sequence must be followed:
1. Hold ICSPCLK and ICSPDAT low. All other pins
should be unpowered.
2. Raise the voltage on MCLR from 0V to VIHH.
3. Raise the voltage on VDD from 0V to the desired
operating voltage.
The VPP-first entry prevents the device from executing
code prior to entering Program/Verify mode. For
example, the device will execute code when the
Configuration Word has MCLR disabled (MCLRE = 0),
the power-up time is disabled (PWRTE =0), the
internal oscillator is selected (FOSC =10x), and RA0
and RA1 are driven by the user application. Since this
may prevent entry, VPP-First Entry mode is strongly
recommended. See the timing diagram in Figure 8-2.
4.1.2 VDD – FIRST ENTRY MODE
To enter Program/Verify mode via the VDD-first method,
the following sequence must be followed:
1. Hold ICSPCLK and ICSPDAT low.
2. Raise the voltage on VDD from 0V to the desired
operating voltage.
3. Raise the voltage on MCLR from VDD or below
to VIHH.
The VDD-first method is useful when programming the
device, when VDD is already applied, for it is not
necessary to disconnect VDD to enter Program/Verify
mode. See the timing diagram in Figure 8-1.
4.1.3 PROGRAM/VERIFY MODE EXIT
To exit Program/Verify mode take MCLR to VDD or
lower (VIL). See Figures 8-3 and 8-4.
4.2 Low-Voltage Programming (LVP)
Mode
The Low-Voltage Programming mode allows the
PIC10(L)F320/322 devices to be programmed using
VDD only, without high voltage. When the LVP bit of the
Configuration Word 1 register is set to ‘1’, the low-
voltage ICSP programming entry is enabled. To disable
the Low-Voltage ICSP mode, the LVP bit must be
programmed to ‘0’. This can only be done while in the
High-Voltage Entry mode.
Entry into the Low-Voltage ICSP Program/Verify modes
requires the following steps:
1. MCLR is brought to VIL.
2. A 32-bit key sequence is presented on
ICSPDAT, while clocking ICSPCLK.
The key sequence is a specific 32-bit pattern, ‘0100
1101 0100 0011 0100 1000 0101 0000’ (more
easily remembered as MCHP in ASCII). The device will
enter Program/Verify mode only if the sequence is
valid. The Least Significant bit of the Least Significant
nibble must be shifted in first.
Once the key sequence is complete, MCLR must be
held at VIL for as long as Program/Verify mode is to be
maintained.
For low-voltage programming timing, see Figure 8-7
and Figure 8-8.
Exiting Program/Verify mode is done by no longer
driving MCLR to VIL. See Figure 8-7 and Figure 8-8.
Note: To enter LVP mode, the LSb of the Least
Significant nibble must be shifted in first.
This differs from entering the key
sequence on other parts.
2011-2012 Microchip Technology Inc. Advance Information DS41572D-page 11
PIC10(L)F320/322
4.3 Program/Verify Commands
The PIC10(L)F320 and PIC10(L)F322 devices
implement 10 programming commands, each six bits in
length. The commands are summarized in Table 4 -1.
Commands that have data associated with them are
specified to have a minimum delay of TDLY between the
command and the data. After this delay, 16 clocks are
required to either clock in or clock out the 14-bit data
word. The first clock is for the Start bit and the last clock
is for the Stop bit.
TABLE 4-1: COMMAND MAPPING FOR PIC10(L)F320 AND PIC10(L)F322
4.3.1 LOAD CONFIGURATION
The Load Configuration command is used to access
the configuration memory (user ID locations,
Configuration Word and Calibration Words). The Load
Configuration command sets the address to 2000h and
loads the data latches with one word of data (see
Figure 4-1).
After issuing the Load Configuration command, use the
Increment Address command until the proper address
to be programmed is reached. The address is then pro-
grammed by issuing either the Begin Internally Timed
Programming or Begin Externally Timed Programming
command.
The only way to get back to the program memory
(address 0) is to exit Program/Verify mode or issue the
Reset Address command after the configuration memory
has been accessed by the Load Configuration command.
FIGURE 4-1: LOAD CONFIGURATION
Command
Mapping Data/Note
Binary (MSb … LSb) Hex
Load Configuration x00000 00h 0, data (14), 0
Load Data For Program Memory x00010 02h 0, data (14), 0
Read Data From Program Memory x00100 04h 0, data (14), 0
Increment Address x00110 06h
Reset Address x10110 16h
Begin Internally Timed Programming x01000 08h
Begin Externally Timed Programming x11000 18h
End Externally Timed Programming x010100Ah
Bulk Erase Program Memory x01001 09h Internally Timed
Row Erase Program Memory x10001 11h Internally Timed
Note: Externally timed writes are not supported
for Configuration and Calibration bits. Any
externally timed write to the Configuration
or Calibration Word will have no effect on
the targeted word.
X0 0LSb MSb 0
1234561215 16
ICSPCLK
ICSPDAT
000 0
TDLY
PIC10(L)F320/322
DS41572D-page 12 Advance Information 2011-2012 Microchip Technology Inc.
4.3.2 LOAD DATA FOR PROGRAM
MEMORY
The Load Data for Program Memory command is used to
load one 14-bit word into the data latches. The word
programs into program memory after the Begin Internally
Timed Programming or Begin Externally Timed
Programming command is issued (see Figure 4-2).
FIGURE 4-2: LOAD DATA FOR PROGRAM MEMORY
4.3.3 READ DATA FROM PROGRAM
MEMORY
The Read Data from Program Memory command will
transmit data bits out of the program memory map
currently accessed, starting with the second rising edge
of the clock input. The ICSPDAT pin will go into Output
mode on the first falling clock edge, and it will revert to
Input mode (high-impedance) after the 16th falling edge
of the clock. If the program memory is code-protected
(CP), the data will be read as zeros (see Figure 4-3).
FIGURE 4-3: READ DATA FROM PROGRAM MEMORY
ICSPCLK
ICSPDAT
1234561215 16
X00
LSb MSb 0
010 0
TDLY
1 2 3 4 5 6 1 2 15 16
LSb MSb
TDLY
ICSPCLK
ICSPDAT
Input Input
Output
x
(from Programmer)
X
0
001 0
ICSPDAT
(from Device)
2011-2012 Microchip Technology Inc. Advance Information DS41572D-page 13
PIC10(L)F320/322
4.3.4 INCREMENT ADDRESS
The address is incremented when this command is
received. It is not possible to decrement the address.
To reset this counter, the user must use the Reset
Address command or exit Program/Verify mode and re-
enter it.
If the address is incremented from address 1FFFh, it
will wrap-around to location 0000h. If the address is
incremented from 3FFFh, it will wrap-around to location
2000h.
FIGURE 4-4: INCREMENT ADDRESS
4.3.5 RESET ADDRESS
The Reset Address command will reset the address to
0000h, regardless of the current value. The address is
used in program memory or the configuration memory.
FIGURE 4-5: RESET ADDRESS
X
0
123 45612
ICSPCLK
ICSPDAT
011
3
XXX
TDLY
Next Command
0
Address + 1
Address
X
0
123 4561
2
ICSPCLK
ICSPDAT
011
3
XXX
TDLY
Next Command
1
0000h
N
Address
PIC10(L)F320/322
DS41572D-page 14 Advance Information 2011-2012 Microchip Technology Inc.
4.3.6 BEGIN INTERNALLY TIMED
PROGRAMMING
A Load Configuration or Load Data for Program
Memory command must be given before every Begin
Programming command. Programming of the
addressed memory will begin after this command is
received. An internal timing mechanism executes the
write. The user must allow for the program cycle time,
TPINT, for the programming to complete.
The End Externally Timed Programming command is
not needed when the Begin Internally Timed
Programming is used to start the programming.
The program memory address that is being
programmed is not erased prior to being programmed.
FIGURE 4-6: BEGIN INTERNALLY TIMED PROGRAMMING
4.3.7 BEGIN EXTERNALLY TIMED
PROGRAMMING
A Load Configuration or Load Data for Program
Memory command must be given before every Begin
Programming command. Programming of the
addressed memory will begin after this command is
received. To complete the programming, the End
Externally Timed Programming command must be sent
in the specified time window defined by TPEXT. The
program memory address that is being programmed is
not erased prior to being programmed.
The Begin Externally Timed Programming command
cannot be used for programming the Configuration
Word (see Figure 4-7).
FIGURE 4-7: BEGIN EXTERNALLY TIMED PROGRAMMING
12345612
ICSPCLK
ICSPDAT
3
TPINT
X
1
000XXX
0
Next Command
X
10
123 4561
2
ICSPCLK
ICSPDAT
00 0 110
End Externally Timed Programming
Command
TPEXT
3
2011-2012 Microchip Technology Inc. Advance Information DS41572D-page 15
PIC10(L)F320/322
4.3.8 END EXTERNALLY TIMED
PROGRAMMING
This command is required after a Begin Externally
Timed Programming command is given. This
command must be sent within the time window
specified by TPEXT after the Begin Externally Timed
Programming command is sent.
After sending the End Externally Timed Programming
command, an additional delay (TDIS) is required before
sending the next command. This delay is longer than
the delay ordinarily required between other commands
(see Figure 4-8).
FIGURE 4-8: END EXTERNALLY TIMED PROGRAMMING
4.3.9 BULK ERASE PROGRAM MEMORY
The Bulk Erase Program Memory command performs
two different functions dependent on the current state
of the address.
A Bulk Erase Program Memory command should not
be issued when the address is greater than 2008h.
After receiving the Bulk Erase Program Memory
command, the erase will not complete until the time
interval, T
ERAB, has expired.
FIGURE 4-9: BULK ERASE PROGRAM MEMORY
12345612
ICSPCLK
ICSPDAT
3
TDIS
X
1
010XXX
0
Next Command
Address 0000h-1FFFh:
Program Memory is erased
Configuration Word is erased
Address 2000h-2008h:
Program Memory is erased
Configuration Word is erased
User ID Locations are erased
Note: The code protection Configuration bit
(CP) has no effect on the Bulk Erase
Program Memory command.
123 4561
2
ICSPCLK
ICSPDAT
3
TERAB
X
1
100XXX
0
Next Command
PIC10(L)F320/322
DS41572D-page 16 Advance Information 2011-2012 Microchip Technology Inc.
4.3.10 ROW ERASE PROGRAM MEMORY
This command erases the 16-word row of program
memory pointed to by PC<13:5>. If the program
memory array is protected (CP = 0) or the PC points to
the configuration memory (> 0x2000), the command is
ignored. When the address is 2000h-2008h, the Row
Erase Program Memory command will only erase the
user ID locations, regardless of the Configuration bit
CP setting.
After receiving the Row Erase Program Memory
command, the erase will not be complete until the time
interval, T
ERAR, has expired.
FIGURE 4-10: ROW ERASE PROGRAM MEMORY
123 4561
2
ICSPCLK
ICSPDAT
3
TERAR
X
0
100XXX
1
Next Command
2011-2012 Microchip Technology Inc. Advance Information DS41572D-page 17
PIC10(L)F320/322
5.0 PROGRAMMING ALGORITHMS
The PIC10(L)F320 and PIC10(L)F322 devices have
the capability of storing 16 14-bit words in its data
latches. The data latches are internal to the
PIC10(L)F320 and PIC10(L)F322 devices and are only
used for programming. The data latches allow the user
to program up to 16 program words with a single Begin
Externally Timed Programming or Begin Internally
Timed Programming command. The Load Program
Data or the Load Configuration command is used to
load a single data latch. The data latch will hold the
data until the Begin Externally Timed Programming or
Begin Internally Timed Programming command is
given.
The data latches are aligned with the 5 LSb of the
address. The address at the time the Begin Externally
Timed Programming or Begin Internally Timed
Programming command is given will determine which
location(s) in memory are written. Writes cannot cross
a physical 16-word boundary. For example, attempting
to write from address 0002h-0021h will result in data
being written to 0020h-003Fh.
If more than 16 data latches are written without a Begin
Externally Timed Programming or Begin Internally
Timed Programming command, the data in the data
latches will be overwritten. The following figures show
the recommended flowcharts for programming.
PIC10(L)F320/322
DS41572D-page 18 Advance Information 2011-2012 Microchip Technology Inc.
FIGURE 5-1: DEVICE PROGRAM/VERIFY FLOWCHART
Done
Start
Bulk Erase
Device(3)
Write User IDs
Enter
Programming Mode
Write Program
Memory(1)
Verify User IDs
Write Configuration
Word(2)
Verify Configuration
Word
Exit Programming
Mode
Verify Program
Memory
Note 1: See Figure 5-2.
2: See Figure 5-5.
3: See Figure 5-6.
2011-2012 Microchip Technology Inc. Advance Information DS41572D-page 19
PIC10(L)F320/322
FIGURE 5-2: PROGRAM MEMORY FLOWCHART
Start
Read Data
Program Memory
Data Correct?
Report
Programming
Failure
All Locations
Done?
No
No
Increment
Address
Command
from
Bulk Erase
Program
Yes
Memory(1, 2)
Done
Yes
Note 1: This step is optional if the device has already been erased or has not been previously programmed.
2: If the device is code-protected or must be completely erased, then Bulk Erase the device per Figure 5-6.
3: See Figure 5-3 or Figure 5-4.
Program Cycle
(3)
PIC10(L)F320/322
DS41572D-page 20 Advance Information 2011-2012 Microchip Technology Inc.
FIGURE 5-3: ONE-WORD PROGRAM CYCLE
Begin
Programming
Wait TDIS
Load Data
for
Program Memory
Command
(Internally timed)
Begin
Programming
Wait TPEXT
Command
(Externally timed)
End
Programming
Wait TPINT
Program Cycle
Command
2011-2012 Microchip Technology Inc. Advance Information DS41572D-page 21
PIC10(L)F320/322
FIGURE 5-4: MULTIPLE-WORD PROGRAM CYCLE
Begin
Programming
Wait TPINT
Load Data
for
Program Memory
Command
(Internally timed)
Wait TPEXT
End
Programming
Wait TDIS
Load Data
for
Program Memory
Increment
Address
Command
Load Data
for
Program Memory
Begin
Programming
Command
(Externally timed)
Latch 1
Latch 2
Latch 32
Increment
Address
Command
Program Cycle
Command
Yes Rep Address : 20mm Dara Currecw narw
PIC10(L)F320/322
DS41572D-page 22 Advance Information 2011-2012 Microchip Technology Inc.
FIGURE 5-5: CONFIGURATION MEMORY PROGRAM FLOWCHART
Start
Load
Configuration
Program Cycle(2)
Read Data
Memory Command
Data Correct? Report
Programming
Failure
Address =
2004h?
Data Correct?
Report
Programming
Failure
Yes
No
Yes
Yes
No
Increment
Address
Command
No Increment
Address
Command
Done
One-word
One-word
Program Cycle(2)
(Config. Word)
Increment
Address
Command
Increment
Address
Command
(User ID)
From Program
Read Data
Memory Command
From Program
Program
Bulk Erase
Memory(1)
Data Correct?
Report
Programming
Failure
Yes
No
One-word
Program Cycle(2)
Increment
Address
Command
Read Data
Memory Command
From Program
Note 1: This step is optional if the device is erased or not previously programmed.
2: See Figure 5-3.
2011-2012 Microchip Technology Inc. Advance Information DS41572D-page 23
PIC10(L)F320/322
FIGURE 5-6: ERASE FLOWCHART
Start
Load Configuration
Done
Bulk Erase
Program Memory
Note: This sequence does not erase the Calibration Words.
PIC10(L)F320/322
DS41572D-page 24 Advance Information 2011-2012 Microchip Technology Inc.
6.0 CODE PROTECTION
Code protection is controlled using the CP bit in
Configuration Word 1. When code protection is
enabled, all program memory locations, 0000h-00FFh
for the PIC10(L)F320 and 0000h-01FFh for the
PIC10(L)F322, will read as ‘0’ and further programming
of the program memory is disabled. Program memory
can still be read by user code during program
execution.
The user ID locations and Configuration Word can be
programmed and read out regardless of the code
protection settings.
6.1 Enabling Code Protection
Code protection is enabled by programming the CP bit
in Configuration Word 1 to ‘0’.
6.2 Disabling Code Protection
The only way to disable code protection is to use the
Bulk Erase Program Memory command.
2011-2012 Microchip Technology Inc. Advance Information DS41572D-page 25
PIC10(L)F320/322
7.0 HEX FILE USAGE
In the hex file there are two bytes per program word
stored in the Intel® INH8M hex format. Data is stored
LSB first, MSB second. Because there are two bytes
per word, the addresses in the hex file are 2x the
address in program memory. (Example: The
Configuration Word 1 is stored at 2007h on the
PIC10(L)F320 and PIC10(L)F322. In the hex file this
will be at location 400Eh-400Fh).
7.1 Configuration Word
To allow portability of code, it is strongly recommended
that the programmer is able to read the Configuration
Word and user ID locations from the hex file. If the Con-
figuration Word information was not present in the hex
file, a simple warning message may be issued. Simi-
larly, while saving a hex file, Configuration Word and
user ID information should be included.
7.2 Device ID and Revision
If a device ID is present in the hex file at 400Ch-400Dh
(2006h on the part), the programmer should verify the
device ID (excluding the revision) against the value
read from the part. On a mismatch condition, the
programmer should generate a warning message.
7.3 Checksum Computation
The checksum is calculated by two different methods,
dependent on the setting of the CP Configuration bit.
7.3.1 CODE PROTECTION DISABLED
With the code protection disabled, the checksum is
computed by reading the contents of the PIC10(L)F320
and PIC10(L)F322 program memory locations and
adding up the program memory data, starting at
address 0000h, up to the maximum user addressable
location, 00FFh for the PIC10(L)F320 and 01FFh for
the PIC10(L)F322. Any Carry bit exceeding 16 bits are
neglected. Additionally, the relevant bits of the Config-
uration Word are added to the checksum. All unused
Configuration bits are masked to ‘0’. See Tabl e 7-1 for
Configuration Word mask values.
Example 7-1 through Example 7-4 shown below are for
a blank device and for a device with 00AAh at the first
and last program memory locations.
EXAMPLE 7-1: CHECKSUM COMPUTED WITH CODE PROTECTION DISABLED (PIC10F320),
BLANK DEVICE
TABLE 7-1: CONFIGURATION WORD
MASK VALUES
Device Config. Word 1 Mask
PIC10F320 1FFFh
PIC10LF320 1FFFh
PIC10F322 1FFFh
PIC10LF322 1FFFh
PIC10F320 Sum of Memory addresses 0000h-00FFh(1) FF00h
Configuration Word 1(2) 3FFFh
Configuration Word 1 mask(3) 1FFFh
Checksum = FF00h + (3FFFh and 1FFFh)
= FF00h + 1FFFh
= 1EFFh(4)
Note 1: Sum of Memory addresses = (Total number of program memory address locations) x (3FFFh) = FF00h,
truncated to 16 bits.
2: Configuration Word 1 = all bits are ‘1’; thus, code-protect is disabled.
3: Configuration Word 1 Mask = all bits are set to ‘1’, except for unimplemented bits that are ‘0’.
4: Truncate to 16 bits.
PIC10(L)F320/322
DS41572D-page 26 Advance Information 2011-2012 Microchip Technology Inc.
EXAMPLE 7-2: CHECKSUM COMPUTED WITH CODE PROTECTION DISABLED (PIC10LF320),
00AAh AT FIRST AND LAST ADDRESS
EXAMPLE 7-3: CHECKSUM COMPUTED WITH CODE PROTECTION DISABLED (PIC10F322),
BLANK DEVICE
EXAMPLE 7-4: CHECKSUM COMPUTED WITH CODE PROTECTION DISABLED (PIC10LF322),
00AAh AT FIRST AND LAST ADDRESS
PIC10LF320 Sum of Memory addresses 0000h-00FFh(1) 8056h
Configuration Word 1(2) 3FFFh
Configuration Word 1 mask(3) 1FFFh
Checksum = 8056h + (3FFFh and 1FFFh)
= 8056h + 1FFFh
= A055h(4)
Note 1: Total number of program memory address locations: 00FFh + 1 = 0100h. Then, 0100h - 2 = 00FEh.
Thus, [(00FEh x 3FFFh) + (2 x 00AAh)] = 8056h, truncated to 16 bits.
2: Configuration Word 1 = all bits are ‘1’; thus, code-protect is disabled.
3: Configuration Word 1 Mask = all Configuration Word bits are set to ‘1’, except for unimplemented bits
that are ‘0’.
4: Truncate to 16 bits.
PIC10F322 Sum of Memory addresses 0000h-01FFh(1) FE00h
Configuration Word 1(2) 3FFFh
Configuration Word 1 mask(3) 1FFFh
Checksum = FE00h + (3FFFh and 1FFFh)
= FE00h + 1FFFh
= 1DFFh
Note 1: Sum of Memory addresses = (Total number of program memory address locations) x (3FFFh) = FE00h,
truncated to 16 bits.
2: Configuration Word 1 = all bits are ‘1’; thus, code-protect is disabled.
3: Configuration Word 1 Mask = all bits are set to ‘1, except for unimplemented bits that are ‘0’.
PIC10LF322 Sum of Memory addresses 0000h-01FFh(1) 7F56h
Configuration Word 1(2) 3FFFh
Configuration Word 1 mask(3) 1FFFh
Checksum = 7F56h + (3FFFh and 1FFFh)
= 7F56h + 1FFFh
= 9F55h
Note 1: Total number of program memory address locations: 01FFh + 1 = 0200h. Then, 0200h - 2 = 01FEh.
Thus, [(01FEh x 3FFFh) + (2 x 00AAh)] = 7F56h, truncated to 16 bits.
2: Configuration Word 1 = all bits are ‘1’; thus, code-protect is disabled.
3: Configuration Word 1 Mask = all Configuration Word bits are set to ‘1’, except for unimplemented bits
that are ‘0’.
2011-2012 Microchip Technology Inc. Advance Information DS41572D-page 27
PIC10(L)F320/322
7.3.2 CODE PROTECTION ENABLED
With the program code protection enabled, the
checksum is computed in the following manner: the
Least Significant nibble of each user ID is used to
create a 16-bit value. The masked value of user ID
location 2000h is the Most Significant nibble. This Sum
of user IDs is summed with the Configuration Word (all
unimplemented Configuration bits are masked to ‘0’).
Example 7-5 through Example 7-8 shown below are for
a blank device and for a device with 00AAh at the first
and last program memory locations. Also, see Table 7-1
for Configuration Word mask values with code protection
enabled.
EXAMPLE 7-5: CHECKSUM COMPUTED WITH CODE PROTECTION ENABLED (PIC10F320),
BLANK DEVICE
PIC10F320 Configuration Word 1(2) 3F7Fh
Configuration Word 1 mask(3) 1FFFh
User ID (2000h)(1) 0001h
User ID (2001h)(1) 0007h
User ID (2002h)(1) 000Ah
User ID (2003h)(1) 000Fh
Sum of User IDs(4) = (0001h and 000Fh) << 12 + (0007h and 000Fh) << 8 +
(000Ah and 000Fh) << 4 + (000Fh and 000Fh)
= 1000h + 0700h + 00A0h + 000Fh
= 17AFh
Checksum = (3F7Fh and 1FFFh) + Sum of User IDs
= 1F7Fh + 17AFh
= 372Eh
Note 1: User ID values in this example are random values.
2: Configuration Word 1 = all bits are ‘1’, except the code-protect enable bit.
3: Configuration Word 1 Mask = all Configuration Word bits are set to ‘1’, except for unimplemented bits
which read0’.
4: << = shift left, thus the LSb of the first user ID value is the MSb of the sum of user IDs and so on until
the LSb of the last user ID value becomes the LSb of the sum of user IDs.
PIC10(L)F320/322
DS41572D-page 28 Advance Information 2011-2012 Microchip Technology Inc.
EXAMPLE 7-6: CHECKSUM COMPUTED WITH CODE PROTECTION ENABLED (PIC10F322),
BLANK DEVICE
EXAMPLE 7-7: CHECKSUM COMPUTED WITH CODE PROTECTION ENABLED (PIC10LF320),
00AAh AT FIRST AND LAST ADDRESS
PIC10F322 Configuration Word 1 (2) 3F7Fh
Configuration Word 1 mask(3) 1FFFh
User ID (2000h)(1) 0001h
User ID (2001h)(1) 0007h
User ID (2002h)(1) 000Ah
User ID (2003h)(1) 000Fh
Sum of User IDs(4) = (0001h and 000Fh) << 12 + (0007h and 000Fh) << 8 +
(000Ah and 000Fh) << 4 + (000Fh and 000Fh)
= 1000h + 0700h + 00A0h + 000Fh
= 17AFh
Checksum = (3F7Fh and 1FFFh) + Sum of User IDs
= 1F7Fh + 17AFh
= 372Eh
Note 1: User ID values in this example are random values.
2: Configuration Word 1 = all bits are1’, except the code-protect enable bit.
3: Configuration Word 1 Mask = all Configuration Word bits are set to1’, except for unimplemented bits
which read0’.
4: << = shift left, thus the LSb of the first user ID value is the MSb of the sum of user IDs and so on until
the LSb of the last user ID value becomes the LSb of the sum of user IDs.
PIC10LF320 Configuration Word 1(2) 3F7Fh
Configuration Word 1 mask(3) 1FFFh
User ID (2000h)(1) 0009h
User ID (2001h)(1) 0008h
User ID (2002h)(1) 000Dh
User ID (2003h)(1) 0005h
Sum of User IDs (4) = (0009h and 000Fh) << 12 + (0008h and 000Fh) << 8 +
(000Dh and 000Fh) << 4 + (0005h and 000Fh)
= 9000h + 0800h + 00D0h + 0005h
= 98D5h
Checksum = (3F7Fh and 1FFFh) + Sum of User IDs
= 1F7Fh + 98D5h
= B854h
Note 1: User ID values in this example are random values.
2: Configuration Word 1 = all bits are ‘1’, except the code-protect enable bit.
3: Configuration Word 1 Mask = all Configuration Word bits are set to ‘1’, except for unimplemented bits
which read ‘0’.
4: << = shift left, thus the LSb of the first user ID value is the MSb of the sum of user IDs and so on until
the LSb of the last user ID value becomes the LSb of the sum of user IDs.
2011-2012 Microchip Technology Inc. Advance Information DS41572D-page 29
PIC10(L)F320/322
EXAMPLE 7-8: CHECKSUM COMPUTED WITH CODE PROTECTION ENABLED (PIC10LF322),
00AAh AT FIRST AND LAST ADDRESS
PIC10LF322 Configuration Word 1(2) 3F7Fh
Configuration Word 1 mask(3) 1FFFh
User ID (2000h)(1) 0009h
User ID (2001h)(1) 0008h
User ID (2002h)(1) 000Dh
User ID (2003h)(1) 0005h
Sum of User IDs(4) = (0009h and 000Fh) << 12 + (0008h and 000Fh) << 8 +
(000Dh and 000Fh) << 4 + (0005h and 000Fh)
= 9000h + 0800h + 00D0h + 0005h
= 98D5h
Checksum = (3F7Fh and 1FFFh) + Sum of User IDs
= 1F7Fh + 98D5h
= B854h
Note 1: User ID values in this example are random values.
2: Configuration Word 1 = all bits are1’, except the code-protect enable bit.
3: Configuration Word 1 Mask = all Configuration Word bits are set to1’, except for unimplemented bits
which read0’.
4: << = shift left, thus the LSb of the first user ID value is the MSb of the sum of user IDs and so on until
the LSb of the last user ID value becomes the LSb of the sum of user IDs.
Standard Operating Conditions (unless umsrwiss stated) Supply Voltages and currents PlC1DF320 PlC1DLF320 v Read/Write and Row Erase operations v 7 v v v v E Bulk Erase operations 2.7 7 v v PlC1DF320 PlC1DLF320 v (lCSFCLK. ICSFDAT) input high level 0.8 v 7 7 v v (lCSFCLK. ICSFDAT) input low level 7 7 0.2 v v ICSPDAT output nign level v on] | = a 5 mA, v o : 5v ICSPDAT output low level v +0 6 | : 3 mA‘ v = 5v Programming mods entry and exit Frugramlng mode entry setup trrne ICSPCLK, Frugramlng mode entry nold trrne lCSPCLK. Serial Program/Veri T Cluck Low Pulse width too 7 7 ns T Cluck High Pulse Width too 7 7 ns T Data in setup trrne belure clockv too 7 7 ns i CIockT to data out valid (during a Read Data CluckL to data low-impedance (during a Read CluckL to data high-impedance (during a Read
PIC10(L)F320/322
DS41572D-page 30 Advance Information 2011-2012 Microchip Technology Inc.
8.0 ELECTRICAL SPECIFICATIONS
Refer to device specific data sheet for absolute
maximum ratings.
TABLE 8-1: AC/DC CHARACTERISTICS TIMING REQUIREMENTS FOR PROGRAM/VERIFY
MODE
AC/DC CHARACTERISTICS Standard Operating Conditions (unless otherwise stated)
Operating Temperature +10°C TA +40°C
Sym. Characteristics Min. Type. Max. Units Conditions/
Comments
Supply Voltages and currents
Supply Voltage (VDDMIN, VDDMAX)
PIC10F320
PIC10F322 2.3 — 5.5 V
VDD
PIC10LF320
PIC10LF322 1.8 — 3.6 V
VPEW Read/Write and Row Erase operations VDDMIN —VDDMAX V
VPBE VPBE Bulk Erase operations 2.7 VDDMAX V
Bulk Erase operations
PIC10F320
PIC10F322 2.3 — 5.5 V
PIC10LF320
PIC10LF322 2.3 — 3.6 V
IDDI Current on VDD, Idle ——
1.0 mA
IDDA Current on VDD, program cycle or Bulk Erase in
progress ——
5.0 mA
VIHH
VPP
High voltage on MCLR/VPP for
Program/Verify mode entry 8.0 — 9.0 V
TVHHR MCLR rise time (VDD to VIHH) for
Program/Verify mode entry ——1.0s
IPP Current on MCLR/VPP 600 A
I/O pins
VIH (ICSPCLK, ICSPDAT) input high level 0.8 VDD —— V
VIL (ICSPCLK, ICSPDAT) input low level 0.2 VDD V
VOH
ICSPDAT output high level VDD-0.7
VDD-0.7
VDD-0.7
VDD V
IOH = 3.5 mA, VDD = 5V
IOH = 3 mA, VDD = 3.3V
IOH = 2 mA, VDD = 1.8V
VOL
ICSPDAT output low level
VSS
VSS+0.6
VSS+0.6
VSS+0.6
V
IOH = 8 mA, VDD = 5V
IOH = 6 mA, VDD = 3.3V
IOH = 3 mA, VDD = 1.8V
Programming mode entry and exit
TENTS Programing mode entry setup time: ICSPCLK,
ICSPDAT setup time before VDD or MCLR 100 — — ns
TENTH Programing mode entry hold time: ICSPCLK,
ICSPDAT hold time after VDD or MCLR 250 ——s
Serial Program/Verify
TCKL Clock Low Pulse Width 100 ns
TCKH Clock High Pulse Width 100 ns
TDS Data in setup time before clock100 ns
TDH Data in hold time after clock100 — — ns
TCO Clock to data out valid (during a Read Data
command) 0 — 80 ns
TLZD Clock to data low-impedance (during a Read
Data command) 0 — 80 ns
THZD Clock to data high-impedance (during a Read
Data command) 0 — 80 ns
Standard Operating Conditions (unless omsrwiss stated) Data mpul not dnven to next clock rrrput (delay T Butx Erase cycte time 7 7 5 ms T Row Erase cycte trrne 7 7 2 5 ms 7 7 2 5 ms Program memory Internauy trmeu pmgrammmg operatmn trrne Externally timed programmmg putse |D"C g T g +40% Trme detay tram program to compare (HV Trme detay when exmng
2011-2012 Microchip Technology Inc. Advance Information DS41572D-page 31
PIC10(L)F320/322
TDLY
Data input not driven to next clock input (delay
required between command/data or command/
command)
1.0 — — s
TERAB Bulk Erase cycle time 5 ms
TERAR Row Erase cycle time 2.5 ms
TPINT Internally timed programming operation time
2.5
5
ms
ms
Program memory
Configuration fuses
TPEXT Externally timed programming pulse 1.0 2.1 ms 10°C TA +40°C
Program memory
TDIS Time delay from program to compare (HV
discharge time) 100 — s
TEXIT Time delay when exiting
Program/Verify mode 1—s
TABLE 8-1: AC/DC CHARACTERISTICS TIMING REQUIREMENTS FOR PROGRAM/VERIFY
MODE (CONTINUED)
AC/DC CHARACTERISTICS Standard Operating Conditions (unless otherwise stated)
Operating Temperature +10°C TA +40°C
Sym. Characteristics Min. Type. Max. Units Conditions/
Comments
PIC10(L)F320/322
DS41572D-page 32 Advance Information 2011-2012 Microchip Technology Inc.
8.1 AC Timing Diagrams
FIGURE 8-1: PROGRAMMING MODE
ENTRY – VDD FIRST
FIGURE 8-2: PROGRAMMING MODE
ENTRY – MCLR/VPP FIRST
FIGURE 8-3: PROGRAMMING MODE
EXIT – MCLR/VPP LAST
FIGURE 8-4: PROGRAMMING MODE
EXIT – VDD LAST
FIGURE 8-5: CLOCK AND DATA
TIMING
TENTH
VDD
TENTS
ICSPDAT
ICSPCLK
VIHH
VIL
MCLR/VPP
is
at VDD
TENTH
ICSPDAT
ICSPCLK
VDD
TENTS
MCLR/VPP
VIHH
VIL
TEXIT
MCLR/VPP
VDD
ICSPDAT
ICSPCLK
VIHH
VIL
TEXIT
VDD
ICSPDAT
ICSPCLK
VIHH
VIL
MCLR/VPP
is at VDD
as
ICSPCLK
TCKH TCKL
TDH
TDS
ICSPDAT
Output
TCO
ICSPDAT
ICSPDAT
ICSPDAT
TLZD
THZD
Input
as
from Input
from Output
to Input
to Output
mm 7777777 mm 77777 W1 ” n “ SW fl Lil—X -CS$ \ 33 3) “ ‘L/i P F“ l—\ /—\ m—V rflflfl _C$i
2011-2012 Microchip Technology Inc. Advance Information DS41572D-page 33
PIC10(L)F320/322
FIGURE 8-6: COMMAND-PAYLOAD TIMING
FIGURE 8-7: LVP ENTRY (POWERING UP)
FIGURE 8-8: LVP ENTRY (POWERED)
123 4561215 16
X0LSb MSb 0
TDLY
Command Next
Command
Payload
ICSPCLK
ICSPDAT
XXXXX
TCKLTCKH
33 clocks
012... 31
TDH
TDS
TENTH
LSb of Pattern MSb of Pattern
VDD
MCLR
ICSPCLK
ICSPDAT
TENTS
TCKH TCKL
33 Clocks
Note 1: Sequence matching can start with no edge on MCLR first.
0 1 2 ... 31
TDH
TDS
TENTH
LSb of Pattern MSb of Pattern
VDD
MCLR
ICSPCLK
ICSPDAT
PIC10(L)F320/322
DS41572D-page 34 Advance Information 2011-2012 Microchip Technology Inc.
APPENDIX A: REVISION HISTORY
Revision A (03/2011)
Initial release of this document.
Revision B (05/2011)
Added sections 1.1.1, 1.1.2 and 1.1.2.1; Updated
Figures 2-1 and 2-2; Updated Table 3-1; Updated
Registers 3-1 and 3-2; Other minor corrections.
Revision C (10/2011)
Updated Examples 7-1 to 7-8; Updated Electrical
Specifications; Other minor corrections.
Revision D (03/2012)
Added new section 4.2, Low-Voltage Programming
(LVP) mode; Added Note to section 4.3.1; Added
Figures 8-7 and 8-8.
YSTEM
2011-2012 Microchip Technology Inc. Advance Information DS41572D-page 35
Information contained in this publication regarding device
applications and the like is provided only for your convenience
and may be superseded by updates. It is your responsibility to
ensure that your application meets with your specifications.
MICROCHIP MAKES NO REPRESENTATIONS OR
WARRANTIES OF ANY KIND WHETHER EXPRESS OR
IMPLIED, WRITTEN OR ORAL, STATUTORY OR
OTHERWISE, RELATED TO THE INFORMATION,
INCLUDING BUT NOT LIMITED TO ITS CONDITION,
QUALITY, PERFORMANCE, MERCHANTABILITY OR
FITNESS FOR PURPOSE. Microchip disclaims all liability
arising from this information and its use. Use of Microchip
devices in life support and/or safety applications is entirely at
the buyer’s risk, and the buyer agrees to defend, indemnify and
hold harmless Microchip from any and all damages, claims,
suits, or expenses resulting from such use. No licenses are
conveyed, implicitly or otherwise, under any Microchip
intellectual property rights.
Trademarks
The Microchip name and logo, the Microchip logo, dsPIC,
KEELOQ, KEELOQ logo, MPLAB, PIC, PICmicro, PICSTART,
PIC32 logo, rfPIC and UNI/O are registered trademarks of
Microchip Technology Incorporated in the U.S.A. and other
countries.
FilterLab, Hampshire, HI-TECH C, Linear Active Thermistor,
MXDEV, MXLAB, SEEVAL and The Embedded Control
Solutions Company are registered trademarks of Microchip
Technology Incorporated in the U.S.A.
Analog-for-the-Digital Age, Application Maestro, chipKIT,
chipKIT logo, CodeGuard, dsPICDEM, dsPICDEM.net,
dsPICworks, dsSPEAK, ECAN, ECONOMONITOR,
FanSense, HI-TIDE, In-Circuit Serial Programming, ICSP,
Mindi, MiWi, MPASM, MPLAB Certified logo, MPLIB,
MPLINK, mTouch, Omniscient Code Generation, PICC,
PICC-18, PICDEM, PICDEM.net, PICkit, PICtail, REAL ICE,
rfLAB, Select Mode, Total Endurance, TSHARC,
UniWinDriver, WiperLock and ZENA are trademarks of
Microchip Technology Incorporated in the U.S.A. and other
countries.
SQTP is a service mark of Microchip Technology Incorporated
in the U.S.A.
All other trademarks mentioned herein are property of their
respective companies.
© 2011-2012, Microchip Technology Incorporated, Printed in
the U.S.A., All Rights Reserved.
Printed on recycled paper.
ISBN: 9781620761571
Note the following details of the code protection feature on Microchip devices:
Microchip products meet the specification contained in their particular Microchip Data Sheet.
Microchip believes that its family of products is one of the most secure families of its kind on the market today, when used in the
intended manner and under normal conditions.
There are dishonest and possibly illegal methods used to breach the code protection feature. All of these methods, to our
knowledge, require using the Microchip products in a manner outside the operating specifications contained in Microchip’s Data
Sheets. Most likely, the person doing so is engaged in theft of intellectual property.
Microchip is willing to work with the customer who is concerned about the integrity of their code.
Neither Microchip nor any other semiconductor manufacturer can guarantee the security of their code. Code protection does not
mean that we are guaranteeing the product as “unbreakable.
Code protection is constantly evolving. We at Microchip are committed to continuously improving the code protection features of our
products. Attempts to break Microchip’s code protection feature may be a violation of the Digital Millennium Copyright Act. If such acts
allow unauthorized access to your software or other copyrighted work, you may have a right to sue for relief under that Act.
Microchip received ISO/TS-16949:2009 certification for its worldwide
headquarters, design and wafer fabrication facilities in Chandler and
Tempe, Arizona; Gresham, Oregon and design centers in California
and India. The Company’s quality system processes and procedures
are for its PIC® MCUs and dsPIC® DSCs, KEELOQ® code hopping
devices, Serial EEPROMs, microperipherals, nonvolatile memory and
analog products. In addition, Microchip’s quality system for the design
and manufacture of development systems is ISO 9001:2000 certified.
QUALITY MANAGEMENT S
YSTEM
CERTIFIED BY DNV
== ISO/TS 16949 ==
6‘ MICROCHIP AMERICAS ASIA/PACIFIC ASIA/PACIFIC EUROPE
DS41572D-page 36 Advance Information 2011-2012 Microchip Technology Inc.
AMERICAS
Corporate Office
2355 West Chandler Blvd.
Chandler, AZ 85224-6199
Tel: 480-792-7200
Fax: 480-792-7277
Technical Support:
http://www.microchip.com/
support
Web Address:
www.microchip.com
Atlanta
Duluth, GA
Tel: 678-957-9614
Fax: 678-957-1455
Boston
Westborough, MA
Tel: 774-760-0087
Fax: 774-760-0088
Chicago
Itasca, IL
Tel: 630-285-0071
Fax: 630-285-0075
Cleveland
Independence, OH
Tel: 216-447-0464
Fax: 216-447-0643
Dallas
Addison, TX
Tel: 972-818-7423
Fax: 972-818-2924
Detroit
Farmington Hills, MI
Tel: 248-538-2250
Fax: 248-538-2260
Indianapolis
Noblesville, IN
Tel: 317-773-8323
Fax: 317-773-5453
Los Angeles
Mission Viejo, CA
Tel: 949-462-9523
Fax: 949-462-9608
Santa Clara
Santa Clara, CA
Tel: 408-961-6444
Fax: 408-961-6445
Toronto
Mississauga, Ontario,
Canada
Tel: 905-673-0699
Fax: 905-673-6509
ASIA/PACIFIC
Asia Pacific Office
Suites 3707-14, 37th Floor
Tower 6, The Gateway
Harbour City, Kowloon
Hong Kong
Tel: 852-2401-1200
Fax: 852-2401-3431
Australia - Sydney
Tel: 61-2-9868-6733
Fax: 61-2-9868-6755
China - Beijing
Tel: 86-10-8569-7000
Fax: 86-10-8528-2104
China - Chengdu
Tel: 86-28-8665-5511
Fax: 86-28-8665-7889
China - Chongqing
Tel: 86-23-8980-9588
Fax: 86-23-8980-9500
China - Hangzhou
Tel: 86-571-2819-3187
Fax: 86-571-2819-3189
China - Hong Kong SAR
Tel: 852-2401-1200
Fax: 852-2401-3431
China - Nanjing
Tel: 86-25-8473-2460
Fax: 86-25-8473-2470
China - Qingdao
Tel: 86-532-8502-7355
Fax: 86-532-8502-7205
China - Shanghai
Tel: 86-21-5407-5533
Fax: 86-21-5407-5066
China - Shenyang
Tel: 86-24-2334-2829
Fax: 86-24-2334-2393
China - Shenzhen
Tel: 86-755-8203-2660
Fax: 86-755-8203-1760
China - Wuhan
Tel: 86-27-5980-5300
Fax: 86-27-5980-5118
China - Xian
Tel: 86-29-8833-7252
Fax: 86-29-8833-7256
China - Xiamen
Tel: 86-592-2388138
Fax: 86-592-2388130
China - Zhuhai
Tel: 86-756-3210040
Fax: 86-756-3210049
ASIA/PACIFIC
India - Bangalore
Tel: 91-80-3090-4444
Fax: 91-80-3090-4123
India - New Delhi
Tel: 91-11-4160-8631
Fax: 91-11-4160-8632
India - Pune
Tel: 91-20-2566-1512
Fax: 91-20-2566-1513
Japan - Osaka
Tel: 81-66-152-7160
Fax: 81-66-152-9310
Japan - Yokohama
Tel: 81-45-471- 6166
Fax: 81-45-471-6122
Korea - Daegu
Tel: 82-53-744-4301
Fax: 82-53-744-4302
Korea - Seoul
Tel: 82-2-554-7200
Fax: 82-2-558-5932 or
82-2-558-5934
Malaysia - Kuala Lumpur
Tel: 60-3-6201-9857
Fax: 60-3-6201-9859
Malaysia - Penang
Tel: 60-4-227-8870
Fax: 60-4-227-4068
Philippines - Manila
Tel: 63-2-634-9065
Fax: 63-2-634-9069
Singapore
Tel: 65-6334-8870
Fax: 65-6334-8850
Taiwan - Hsin Chu
Tel: 886-3-5778-366
Fax: 886-3-5770-955
Taiwan - Kaohsiung
Tel: 886-7-536-4818
Fax: 886-7-330-9305
Taiwan - Taipei
Tel: 886-2-2500-6610
Fax: 886-2-2508-0102
Thailand - Bangkok
Tel: 66-2-694-1351
Fax: 66-2-694-1350
EUROPE
Austria - Wels
Tel: 43-7242-2244-39
Fax: 43-7242-2244-393
Denmark - Copenhagen
Tel: 45-4450-2828
Fax: 45-4485-2829
France - Paris
Tel: 33-1-69-53-63-20
Fax: 33-1-69-30-90-79
Germany - Munich
Tel: 49-89-627-144-0
Fax: 49-89-627-144-44
Italy - Milan
Tel: 39-0331-742611
Fax: 39-0331-466781
Netherlands - Drunen
Tel: 31-416-690399
Fax: 31-416-690340
Spain - Madrid
Tel: 34-91-708-08-90
Fax: 34-91-708-08-91
UK - Wokingham
Tel: 44-118-921-5869
Fax: 44-118-921-5820
Worldwide Sales and Service
11/29/11