11-03-0022 Instruction Sheet Datasheet by Molex

View All Related Products | Download PDF Datasheet
Exlmttol Tool f0! Iha Remuvul of all 2.54mm (.1 [)0 in.) ”KK" Ierminuls
Extractor Tool for the Removal of all 2.54mm (.100 in.) “KK” Terminals
Doc No. 11-03-0022 Release Date: 03-01-05 UNCONTROLLED COPY Page 1 of 1
Revision: C Revision Date: 03-01-05
Extractor Tool
Instruction Sheet
Order No. 11-03-0022
(HT-2759)
For the removal of all 2.54mm (.100 in.) KK Crimp Terminals series in all housings.
Operation:
Individual terminals may be removed from the housing using
this extractor tool.
1. Push the terminal forward in the housing so that the
locking tang is clearly visible.
2. Insert the tool into the interface opening (slot) of the
connector housing on an angle as shown in Figure 1.
3. Rotate the extractor tool into the position shown in
Figure 2. This will depress the locking tang of the
terminal and allow the terminal to be removed by
gently pulling on the wire.
Molex Application Tooling Group
1150 E. Diehl Road
Naperville, IL 60563
Tel:(630) 969-4550
FAX (630) 505-0049
EXTRACTOR
TOOL
TERMINAL
HOUSING
PULL
Figure 2
EXTRACTOR TOOL
TERMINAL
LOCKING TANG
SLOT
PUSH WIRE
Figure 1
HOUSING

Products related to this Datasheet

TOOL EXTRACTION MOLEX .100 TERM