WRx1 Telit Modem Firmware Update Guide - Verizon Datasheet by Digi

View All Related Products | Download PDF Datasheet
Digi Transport® WR11, WR21, and
WR31 Telit Modem Firmware Update
- Verizon
Update Guide
Revision history—90002340
Revision Date Description
A February 2019 Initial release.
B February 2019 Additional edits.
C April 2020 Updated links to the modem firmware.
Trademarks and copyright
Digi, Digi International, and the Digi logo are trademarks or registered trademarks in the United
States and other countries worldwide. All other trademarks mentioned in this document are the
property of their respective owners.
© 2020 Digi International Inc. All rights reserved.
Disclaimers
Information in this document is subject to change without notice and does not represent a
commitment on the part of Digi International. Digi provides this document “as is,” without warranty of
any kind, expressed or implied, including, but not limited to, the implied warranties of fitness or
merchantability for a particular purpose. Digi may make improvements and/or changes in this manual
or in the product(s) and/or the program(s) described in this manual at any time.
Warranty
To view product warranty information, go to the following website:
www.digi.com/howtobuy/terms
Send comments
Documentation feedback: To provide feedback on this document, send your comments to
techcomm@digi.com.
Technical support
Digi Technical Support: Digi offers multiple technical support plans and service packages to help our
customers get the most out of their Digi product. For information on Technical Support plans and
pricing, visit us at www.digi.com/support. For questions or assistance contact Technical Support at
tech.support@digi.com.
Digi Transport® WR11, WR21, and WR31 Telit Modem Firmware Update -
Verizon
2
Contents
Verizon network changes: Digi Transport WR11, WR21, and WR31
Determine if an update is needed
Update the Modem Firmware
Prerequisites 6
Best practices 6
Where to find the updated modem firmware 7
Using the Public Support site method 7
Not using the Public Support site method 7
Updating the modem firmware on your router 7
Method 1: Update the modem firmware using Digi Remote Manager 9
Step 1: Download the updated modem firmware 9
Step 2:Download begins 11
Step 3: Verify that the update was successful 12
Method 2: Update the modem firmware using your WANconnection 13
Step 1: Download the updated modem firmware 13
Step 2:Download begins 14
Step 3: Verify that the update was successful 14
Method 3: Update the modem firmware using alocal LAN connection 16
Step 1: Download the updated modem firmware 16
Step 2:Download begins 16
Step 3: Verify that the update was successful 16
Method 4: Update the modem firmware using aUSB flash drive 18
Step 1: Create the update text file 18
Step 2:Prepare the flash drive 18
Step 3: Perform the update 18
Step 4: Verify that the update was successful 18
Digi Transport® WR11, WR21, and WR31 Telit Modem Firmware Update -
Verizon
3
Verizon network changes: Digi Transport WR11,
WR21, and WR31
This document describes how to update cellular modem firmware to comply with Verizon network
changes occurring on March 30th, 2019.
It applies to Digi TransPort routers containing one of these LTE modems:
nTelit LE910-NAv2 (single SKU, AT&T and Verizon)
nTelit LE910-NA1 (single SKU, AT&T and Verizon)
The affected and correct firmware versions are as follows:
Device SKU
Affected Modem
Firmware
Good Modem
Firmware
Digi TransPort WR11 WR11-M6xx-xxx-xx 20.00.014 / 20.00.524 20.00.015 / 20.00.525
Digi TransPort WR21 WR21-M5xx-xxx-xx 20.00.004 / 20.00.504 20.00.005 / 20.00.505
Digi TransPort WR31 WR31-M5xx-xxx-xx 20.00.004 / 20.00.504 20.00.005 / 20.00.505
Digi Transport® WR11, WR21, and WR31 Telit Modem Firmware Update -
Verizon
4
Um uurnnme WWW command: modemsul 1 Mom: Exam Wizards % Configuration lulwork Ann“, Command: modemslal 7 system Command result Remake Management Socurlty mug-e: so: nde- “nus ox ral-nmry Mn: :1 nu my :7: 1. 5m status: Rum pr'cm‘m’ “mare Carrier 10- Vernon Basic Sign) slrm‘l -7: 4-- Python Rldh new-uh. Lu "annulmem Sip.) quamy (um um do an. as» -99 an. a [Min 3-" I Ilelwork smug am... . m. CQIIIIEC‘IGIIS Cell 10‘- 2:79.}. Velemury Rerunrk: unhon. nun 5mm Dal-1n: vs only :"T‘ “’9 HInuleurnrz um nn ynr unru- v2 Top talkers Mminislralion 20 “You : asuumnns:
Determine if an update is needed
Within the Web User Interface (WebUI), navigate to Administration - Execute a command, and issue
the modem status command: modemstat ?
Note All WebUI Administrative commands can be issued at the Command Line Interface (CLI) using
SSH, Telnet, or serial.
Within the results, the modem firmware version will be listed next to "Firmware:". If this data shows
20.00.**4 or lower, then the modem needs to be updated.
Refer to the image below as a reference:
Digi Transport® WR11, WR21, and WR31 Telit Modem Firmware Update -
Verizon
5
Update the Modem Firmware
Prerequisites
The following is required to complete this update:
nTransPort device firmware (SarOS) must be running 6.1.3.8 or later, but it is strongly
recommended that the device is running 7.0.0.6 or later.
n50 MB of free storage required by the cellular modem firmware file. If storage is low, contact
Tech support for guidance on freeing space on your router.
nTo allow the appropriate files to be placed onto the device, the local FTP server must be
enabled on the TransPort for all methods that do not involve using Digi Remote Manager for
the upgrade: LAN or WAN.
nAll upgrade methods will need the applyAPN.py Python file as part of the upgrade.
nRecord the APN of the SIM card. If you do not know the APN, you can obtain it by running
modemstat ? command from a command line interface. The APN value is in the APN is use
field.
To determine how much space is available on our router:
1. Within the WebUI, navigate to Administration - Execute a command.
2. Issue the directory command: dir
The last line shows the number of Flash Free bytes.
Best practices
When upgrading your cellular module, any momentary loss of power or event that causes the router or
modem to reset can result in an unrecoverable router. The following should be considered when
performing the update:
nDo not remove power during the modem firmware update process.
nTerminate any operation that may interfere with the modem firmware update process,
including:
lPython applications that programmatically control the cellular modem, for example to
reset the modem, to do fail-over or to enable/disable the modem based on custom logic.
lSureLink recovery mechanisms (i.e., link_retries, check_reg, rebootfails) or dual SIM
failover features.
lRouter recovery mechanisms, like the cloud watchdog feature (cloud 0 watchdog).
Digi Transport® WR11, WR21, and WR31 Telit Modem Firmware Update -
Verizon
6
Update the Modem Firmware Where to find the updated modem firmware
Digi Transport® WR11, WR21, and WR31 Telit Modem Firmware Update -
Verizon
7
Where to find the updated modem firmware
Using the Public Support site method
You can find the updated modem firmware by using the Public Support site method of upgrading
firmware, which means you have direct access to ftp1.digi.com.
If your router has access to the Digi public support site (ftp1.digi.com), the update can be done using a
single command.
You can test whether you have access to the Digi Public Support site.
1. Within the WebUI, navigate to Administration - Execute a command.
2. Initiate the ping command: ping ftp1.digi.com
3. If you can resolve and connect to ftp1.digi.com, the ping command will return immediately
and show 100 % success.
Not using the Public Support site method
If you are not using the Public Support site method, the updated modem firmware can be found in the
locations specified below.
You can manually pull the modem firmware, which is then written to your router’s Flash drive, and is
then written from Flash to the modem. After the write is completed, you should delete the binary, as it
is large and does not need to be retained.
Modem: M6 (LE910- NA1)
Modem firmware:
http://ftp1.digi.com/support/firmware/transport/LE910NA1_carrier_firmware/all.bin
File size and current all.bin MD5 checksum:
http://ftp1.digi.com/support/firmware/transport/LE910NA1_carrier_firmware/le910na1.txt
Modem: M5 (LE910 NA-V2)
Modem firmware:
http://ftp1.digi.com/support/firmware/transport/LE910NA_V2_carrier_firmware/all.bin
File size and current all.bin MD5 checksum:
http://ftp1.digi.com/support/firmware/transport/LE910NA_V2_carrier_firmware/le910na2.txt
Python: applyAPN.py
Modem firmware:
ftp://ftp1.digi.com/support/telit/83000128-01.zip
Note All upgrade methods will need the applyAPN.py Python file as part of the upgrade.
Updating the modem firmware on your router
There are three methods shown below that can be used to download modem firmware and update
your router:
Update the Modem Firmware Updating the modem firmware on your router
Digi Transport® WR11, WR21, and WR31 Telit Modem Firmware Update -
Verizon
8
nMethod 1: Update the modem firmware using Digi Remote Manager
nMethod 2: Update the modem firmware using your WANconnection
nMethod 3: Update the modem firmware using alocal LAN connection
nMethod 4: Update the modem firmware using aUSB flash drive
After you have updated the modem firmware, verify that the update was successful.
Note Downloading the firmware over a cellular connection (method 1 and method 2) will result in
roughly 50 MB of data use on your cellular data plan.
mummhuNb—l 11 12 13 14 I ! lm/bin/python I o watches the m of 3 Transport router upon: sarcli I callback function that handles each line from the retrieved file. I Return: False it 9WD criteria is met. otherwise True I won blank lines are appended to line: I and your m here: use:De:ired_nPfl = ‘—
Update the Modem Firmware Method 1: Update the modem firmware using Digi Remote Manager
Digi Transport® WR11, WR21, and WR31 Telit Modem Firmware Update -
Verizon
9
Method 1: Update the modem firmware using Digi Remote
Manager
Step 1: Download the updated modem firmware
If your router has access to Digi’s public support site
For a single device
1. Download the applyAPN.py Python script from the Digi FTP site.
2. Unzip the downloaded file, and edit the applyAPN.py file with the correct APN for your Verizon
plan. The area to edit is shown in the example below:
3. Save the changes to the applyAPN.py script.
4. Within Digi Remote Manager, navigate to Device Management > Schedules.
5. Double-click on the desired device to open the Properties screen.
6. In the Properties screen, click Administration > File Managment, and then click Upload to
place the applyAPN.py file on to the router.
7. Navigate to Administration > Execute a command, and start the Python script by issuing the
command: python applyAPN.py
8. Click Execute a command to initiate the download process using the command: carrier all -
ftp
For multiple devices
1. Download the applyAPN.py Python script from the Digi FTP site.
2. Unzip the downloaded file, and edit the applyAPN.py file with the correct APN for your Verizon
plan. The area to edit is shown in the example below:
mqmméwwr—A 11 12 13 14 IE/uaz/bin/python I f Hatches the m of a Transport router upon sarcli l Callback function that handle: each line from the retrieved file. 1 Return: False if checklimn Criteria is met. otherwise True i Non blank lines are appended to line: I [Add your AP“ here userDesirecLAPfl = "— “Mb W 2 mm, .M ....._ 1;" WW UM, :W...« m. - umm WM... V w. . Thom,"
Update the Modem Firmware Method 1: Update the modem firmware using Digi Remote Manager
Digi Transport® WR11, WR21, and WR31 Telit Modem Firmware Update -
Verizon
10
3. Save the changes to the applyAPN.py script.
4. Within Digi Remote Manager, navigate to Device Management > Schedules.
5. Click New Schedule.
6. Click Upload Files and then click Browse. Navigate to the applyAPN.py file on your hard drive.
7. Click Command Line Interface, and type the command: python applyAPN.py
8. Click Command Line Interface, and type the command: carrier all -ftp
9. De-select the Allow Offline option for all three items added above.
Use the image below as a reference:
Note The task can also be saved using the Save As option at the bottom. This allows the task
to be run again without having to build the task each time.
10. Enter a description in the Description field.
11. Click Schedule >>.
12. On the Scheduler page, choose the Devices,Tags, or Groups to run the update process task
for your selection.
wmqmmaunu 11 12 13 14 I ! Iw/bin/pychon I 0 watches the W of 3 Transport router upon sarcii I Callback function that handle: each line from the retrieved file. I Returns False it We” criteria is met. otherwise True I “on blank lines are appended to line: I and your m hexe nemesiredJum = ~—
Update the Modem Firmware Method 1: Update the modem firmware using Digi Remote Manager
Digi Transport® WR11, WR21, and WR31 Telit Modem Firmware Update -
Verizon
11
Note The TransPort devices must all be of the same type when using this method, for
example, all devices must be WR21s. If the devices are not of the same type and the task is run
on them, it is likely the Digi device will become inoperable after the task completes.
13. Click Run Now to start the process for the selected devices.
Note The Operations tab may show the update process task has completed, but the devices
may not have completed the task. Verification that the update task process has completed on
the devices occurs in Step 3, below.
If your router does not have access to Digi's public support site
1. Download the applyAPN.py Python script from the Digi FTP site.
2. Download the all.bin file for the radio in your device.
3. Unzip the downloaded file, and edit the applyAPN.py file with the correct APN for your Verizon
plan. The area to edit is shown in the example below:
4. Save the changes to the applyAPN.py script.
5. Within Digi Remote Manager, navigate to Device Management > Devices.
6. Double-click on the desired device to open the Properties screen.
7. In Properties screen, click Administration > File Management and then click the Upload icon
to place the all.bin file on to the router.
8. On the same File Management page, click the Upload icon to place the applyAPN.py file onto
the router.
9. Navigate to Administration > Execute a command, and start the Python script with the
command: python applyAPN.py
10. Use Execute a command to initiate the download process using the command: carrier all
Step 2:Download begins
If your Remote Manager WAN connection is through cellular (PPP 1), you will lose connectivity to the
router for 5-10 minutes while the firmware gets written to the modem. The modem will reconnect
when complete.
Update the Modem Firmware Method 1: Update the modem firmware using Digi Remote Manager
Digi Transport® WR11, WR21, and WR31 Telit Modem Firmware Update -
Verizon
12
Note When using Remote Manager for the update, keep the cloud watchdog active. The default
Remote Manager Watchdog will not reset the router unless the router is disconnected for 45 minutes.
See Best Practices for issues when upgrading cellular modem firmware.
Step 3: Verify that the update was successful
1. In the Remote Manager, click on the Device Management tab.
2. Double-click on the target device to display the device properties.
3. Click Refresh at the bottom of the Device page.
4. Click Execute a command.
5. Type in the modem status command: modemstat ?
6. Validate the output shows the updated firmware version. An example is listed below.
mummhuNb—l 11 12 13 14 I ! lm/bin/python I o watches the m of 3 Transport router upon: sarcli I callback function that handles each line from the retrieved file. I Return: False it 9WD criteria is met. otherwise True I won blank lines are appended to line: I and your m hexe' use:De:ired_nPfl = ‘—
Update the Modem Firmware Method 2: Update the modem firmware using your WANconnection
Digi Transport® WR11, WR21, and WR31 Telit Modem Firmware Update -
Verizon
13
Method 2: Update the modem firmware using your
WANconnection
Prerequisite
The local FTP server must be enabled on the TransPort device to allow the appropriate files to be
placed onto the device.
Step 1: Download the updated modem firmware
If your router has access to Digi’s public support site
1. Download the applyAPN.py Python script from the Digi FTP site.
2. Unzip the downloaded file, and edit the applyAPN.py file with the correct APN for your Verizon
plan. The area to edit is shown in the example below:
3. Save the changes to the applyAPN.py script.
4. Using an FTP program such as FileZilla, place the applyAPN.py and all.bin files on the root (/)
directory of the router.
5. In the WebUI, navigate to Administration - Execute a command.
6. Start the Python script with the command: python applyAPN.py
7. Initiate the download process using command: carrier all -ftp
If your router does not have access to Digi's public support site
1. Download the applyAPN.py Python script from the Digi FTP site.
2. Download the all.bin file for the radio in your device.
3. Unzip the downloaded file, and edit the applyAPN.py file with the correct APN for your Verizon
plan. The area to edit is shown in the example below:
mummnuNH 11 12 13 14 I ! Im/bin/python I o watches the m of 3 Transport router upon: sarcli I callback function that handles each line from the retrieved file. I Returns False it W0 criteria is met. otherwise True I won blank lines are appended to line: I and your m hexe' use:De:ired_lum = "—
Update the Modem Firmware Method 2: Update the modem firmware using your WANconnection
Digi Transport® WR11, WR21, and WR31 Telit Modem Firmware Update -
Verizon
14
4. Save the changes to the applyAPN.py script.
5. Using an FTP program such as FileZilla, place the applyAPN.py and all.bin files on the root (/)
directory of the router.
6. Within the WebUI, navigate to Administration - Execute a command, start the Python script
with the command: python applyAPN.py
7. While on the same Execute a command page, initiate the download process using the
command: carrier all
Note See Best Practices for information about common issues when upgrading cellular modem
firmware.
Step 2:Download begins
If your Web UI WAN connection is through cellular (PPP 1), you will lose connectivity to the router for 5-
10 minutes while the firmware gets written to the modem. The modem will reconnect when
complete.
Step 3: Verify that the update was successful
After the upgrade process completes, wait 10 minutes. and re-issue the modem status command:
modemstat ?
This command can be executed in the WebUI under Administration - Execute a command, or at the
CLI via Telnet, SSH, or the serial port.
The updated modem firmware version listed in the Firmware field should be 20.00.**5. An example of
this is shown below:
um mum and gar-“ml mum'- Mum vim... um. Imminent sun-"v rel-mm Aypfik-lhm we mim- IlaMgemenl new sums Conn-alum run-many sum Log Ann-Ivar r p mun so: nooe- mm a: u n. mo n 25-” mm wxm up“: “rung“: .n ‘- Inu- mnmmz m sun-I cum (um um -u a-. mu -n a... am 41.; a mu bull I! ma um.) um... mum, mm Mk: Ian-in: rs only IMF-(mu! um m: L!!! an u lr—ro u..-
Update the Modem Firmware Method 2: Update the modem firmware using your WANconnection
Digi Transport® WR11, WR21, and WR31 Telit Modem Firmware Update -
Verizon
15
Update the Modem Firmware Method 3: Update the modem firmware using alocal LAN connection
Digi Transport® WR11, WR21, and WR31 Telit Modem Firmware Update -
Verizon
16
Method 3: Update the modem firmware using alocal LAN
connection
Prerequisite
The local FTP server must be enabled on the TransPort device to allow the appropriate files to be
placed onto the device.
Step 1: Download the updated modem firmware
If your router has access to Digi’s public support site
1. In the WebUI, navigate to Administration - Execute a command.
2. Initiate the download process using command: carrier all -ftp
If your router does not have access to Digi's public support site
1. Download the all.bin file for the radio in your device.
2. Using an FTP program, such as FileZilla, place the all.bin file on the root (/) directory of the
router.
3. Within the WebUI, navigate to Administration - Execute a command, initiate the download
process using the command: carrier all
Note See Best Practices for information about avoiding events that could prematurely reset your
router.
Step 2:Download begins
Once the entire all.bin file is on the router, the modem will reset to write the image. The cellular
connection will be lost for approximately 5-10 minutes while the firmware gets written to the modem.
Step 3: Verify that the update was successful
After the upgrade process completes, wait 10 minutes. and re-issue the modem status command:
modemstat ?
This command can be executed in the WebUI under Administration - Execute a command, or at the
CLI via Telnet, SSH, or the serial port.
The updated modem firmware version listed in the Firmware field should be 20.00.**5. An example of
this is shown below:
u... mum Wm comm: mum! 7 um Wilt-"1‘ Em mliqur-llml MW Alli-In; "RI-I nun-nae Imminent sundry a" mm mm a: VII-lucky u n. mg 1 2m; _ , um Aypfik [km In!!!“ M‘ up“! “rung“: 4' ‘- mm.- ...x. zen-Mk“: u! Hungarian! mm .511“ (um nu -u an. In! -n an. Inc «1.5 a ham sums "' W" :2” con-muons 1",,” rum-w um... lethu, nun 5...: m, rs only mm "m m. an H 2......5 [pt-m
Update the Modem Firmware Method 3: Update the modem firmware using alocal LAN connection
Digi Transport® WR11, WR21, and WR31 Telit Modem Firmware Update -
Verizon
17
Note If your cellular connection does not come back after the upgrade, it is likely that your Verizon
APN will need to be re-entered. In the WebUI, navigate to Configuration - Network > Interfaces >
Mobile and enter in the APN.
Update the Modem Firmware Method 4: Update the modem firmware using aUSB flash drive
Digi Transport® WR11, WR21, and WR31 Telit Modem Firmware Update -
Verizon
18
Method 4: Update the modem firmware using aUSB flash drive
Step 1: Create the update text file
1. Open a new text file.
2. Copy the following text into the file, making sure to edit the APN_GOES_HERE section with the
actual APN for the Verizon SIM card:
del all.bin
copy u:all.bin all.bin
carrier all
del all.bin
modemcc 0 apn APN_GOES_HERE”
config 0 save
flashleds
3. Save the text file as: autoexec.bat
Step 2:Prepare the flash drive
1. Using a PC, format the flash drive for FAT format to allow the TransPort to read the drive.
2. Download the appropriate all.bin file for the device from the Digi FTP site.
3. Copy the all.bin and autoexec.bat files to the flash drive.
4. Safely eject and remove the flash drive from the PC after the file transfer.
Step 3: Perform the update
1. Power up the router completely by waiting approximately 30 seconds after power is applied.
Note Take note of the standard LED behavior before starting the upgrade, as the LED behavior
will change once the process has completed.
2. Insert the thumb drive and the process will begin.
3. When the process completes, the routers LEDs will start flashing in an alternating pattern.
4. Power the router off.
5. Remove the flash drive.
6. Power the router back on.
Step 4: Verify that the update was successful
After the router powers up, connect to the device, and issue the modem status command: modemstat
?
This command can be executed in the WebUI under Administration > Execute a command, or at the
CLI via Telnet, SSH, or the serial port.
The updated modem firmware version listed in the Firmware field should be 20.00.**5. An example of
this is shown below:
um mum and gar-“ml mum'- Mum vim... um. Imminent sun-"v rel-mm Aypfik-lhm we mim- IlaMgemenl new sums Conn-alum run-many sum Log Ann-Ivar r p mun so: nooe- mm a: u n. mo n 25-” mm wxm up“: “rung“: .n ‘- Inu- mnmmz m sun-I cum (um um -u a-. mu -n a... am 41.; a mu bull I! ma um.) um... mum, mm Mk: Ian-in: rs only IMF-(mu! um m: L!!! an u lr—ro u..-
Update the Modem Firmware Method 4: Update the modem firmware using aUSB flash drive
Digi Transport® WR11, WR21, and WR31 Telit Modem Firmware Update -
Verizon
19

Products related to this Datasheet

CELLULAR ROUTER 4GLTE AT&T VERIZ
CELLULAR ROUTER AT&T VERIZON
CELLULAR ROUTER N AMER LTE/HSPA+
CELLULAR ROUTER N AMER HSPA+/LTE