EFM8UB1-SLSTK2000A Quick Start Guide Datasheet by Silicon Labs

View All Related Products | Download PDF Datasheet
SILICEIN LABS
EFM8 Universal Bee Family
QSG132: EFM8UB1-SLSTK2000A Quick
Start Guide
The EFM8UB1-SLSTK2000A is an excellent starting point to get
familiar with the EFM8 Universal Bee microcontrollers.
The kit contains sensors and peripherals demonstrating some of the MCU's many capa-
bilities. The kit can also serve as a starting point for application development.
KIT CONTENTS
EFM8UB1 Universal Bee Starter Kit Board
1 x mini USB cable
1 x micro USB cable
1 x CR2032 coin cell battery
Getting Started card
silabs.com | Smart. Connected. Energy-friendly. Rev. 0.3
HMme Kmy Hs-s- Shuts-1K” “may... compnmnwh Kuauml . » ”Mm...” sum-Man uum... hum L urn-Amy»... (a hummus—Immun- urn-Amman“. @ lm-nwummum x “mm H mummy..."- Inner-mm u mm—uwu—n Imu-Auw—«I- <3 mun—mm”-="" mmm="" gmz'zfzzr="" "r="" “www.="" .munm.="">
1. Getting Started
Install Simplicity Studio
Simplicity Studio is a free software suite needed to start developing your application. Download the latest version of Simplicity Studio
from the Silicon Labs website:
http://www.silabs.com/simplicity-studio
Note: The board comes pre-loaded with a default application, Space Invaders, to play with while the software downloads.
Set Up Your Kit
1. Provide power to the board by connecting the DBG USB connector to the PC using the provided USB cable.
Note: Some demos that use the device USB may require the second USB cable to be connected. See the demo description for
more information.
Detect Your Device
1. Wait for the J-Link debug adapter to appear in the [Devices] area. The board may take some time to appear due to driver instal-
lations for the debug adapter.
2. Click the J-Link debug adapter or the board information corresponding to the board. This will verify that the installation was suc-
cessful, identify the MCU on the kit hardware, and automatically configure the software tools for use with your device.
QSG132: EFM8UB1-SLSTK2000A Quick Start Guide
Getting Started
silabs.com | Smart. Connected. Energy-friendly. Rev. 0.3 | 1
EFMEBBI Busy Bee Starter KR mm “mm." I mm a_..... u I mm...m.m_ - mum-m...“- mmwm 0 EFMEBBI Busy Bee Starter Kit mm...“- munbflm cover-Inn“ um. EFMOBII CPTOO7B Demo (9 Th'smmple pmjeausesme Ema LCD mdemmmmeuseaL .mmm (D
Run Blinky
Click the [Demos] tile to load the available demos. Select [Rainbow Blinky] and click [Start] to download and run the demo. Follow
the instructions on the kit LCD screen to run the demo.
QSG132: EFM8UB1-SLSTK2000A Quick Start Guide
Getting Started
silabs.com | Smart. Connected. Energy-friendly. Rev. 0.3 | 2
.W Va . mxfisamms 4x5: “Wu“ swam Busy Bee Starter Kn “mm—12w" ”MW XMW mm...“- munbflm cover-Inn“ um. EFMOBBI CPTOO7B Demo (9 Th’smmpk prqea‘ usesme EFMa LCD m denim“ me use 0L
2. Resources
Demos
Demos are a quick and easy way to evaluate a device without compiling or debugging code. Demos can be accessed using the [Get-
ting Started]>[Demos] area in the launcher.
QSG132: EFM8UB1-SLSTK2000A Quick Start Guide
Resources
silabs.com | Smart. Connected. Energy-friendly. Rev. 0.3 | 3
m ~o . m anomm = u 1:! i 1 03 EFMBBBI Busy Bee S‘arter Kit awn-1mm Damn—mum cammlwh humu- “ Mluiwm M ”mm-".1..."- mmmmh—ml EFMCIII ADC Externallnput m mmplo codeubu and mm m analog measuremennfmm nput um using, W Va . W EFMEBBI Busy Bee Starter KR a cum; 1 «Wm cam-m. mm...“ :- mmmm a "mum“- ~W I .mnmw. mnmnmmm
Software Examples
Software examples can be imported, compiled, and downloaded using the [Getting Started]>[Software Examples] area in the launch-
er.
Software Documentation
Software documentation provides more information on the firmware libraries available for the selected device. Access these documents
using the [Documentation] area in the launcher.
QSG132: EFM8UB1-SLSTK2000A Quick Start Guide
Resources
silabs.com | Smart. Connected. Energy-friendly. Rev. 0.3 | 4
EFMEBBI Busy Bee Starter Kit Mrmmt Damnation emu-mm mm. W». . -W. n .u w . {mumm- mm BKDSmA_Ml_s¢hemafic g ~o - w arm EFMEBBI Busy Bee Starter Kit «(m-m. mmmm cmanm um.
Kit Documentation and User’s Guide
Kit documentation like the schematic and detailed board user guide can be found using the [Documentation] area of the launcher.
Application Notes
Application Notes on peripherals and other various topics can be accessed using the [Getting Started]>[Software Examples] area of
the launcher.
QSG132: EFM8UB1-SLSTK2000A Quick Start Guide
Resources
silabs.com | Smart. Connected. Energy-friendly. Rev. 0.3 | 5
.m ~o . om.” as. nujxana EFMEBBI Busy Bee Starter Kit mmm. Dom-Mu. @ MM a." cm... W um-
Community and Support
Have a question? Visit the community by clicking the [Resources]>[Silicon Labs Community] area of the launcher.
QSG132: EFM8UB1-SLSTK2000A Quick Start Guide
Resources
silabs.com | Smart. Connected. Energy-friendly. Rev. 0.3 | 6
SILICON LABS
http://www.silabs.com
Silicon Laboratories Inc.
400 West Cesar Chavez
Austin, TX 78701
USA
Simplicity Studio
One-click access to MCU and
wireless tools, documentation,
software, source code libraries &
more. Available for Windows,
Mac and Linux!
IoT Portfolio
www.silabs.com/IoT
SW/HW
www.silabs.com/simplicity
Quality
www.silabs.com/quality
Support and Community
community.silabs.com
Disclaimer
Silicon Laboratories intends to provide customers with the latest, accurate, and in-depth documentation of all peripherals and modules available for system and software implementers using
or intending to use the Silicon Laboratories products. Characterization data, available modules and peripherals, memory sizes and memory addresses refer to each specific device, and
"Typical" parameters provided can and do vary in different applications. Application examples described herein are for illustrative purposes only. Silicon Laboratories reserves the right to
make changes without further notice and limitation to product information, specifications, and descriptions herein, and does not give warranties as to the accuracy or completeness of the
included information. Silicon Laboratories shall have no liability for the consequences of use of the information supplied herein. This document does not imply or express copyright licenses
granted hereunder to design or fabricate any integrated circuits. The products are not designed or authorized to be used within any Life Support System without the specific written consent
of Silicon Laboratories. A "Life Support System" is any product or system intended to support or sustain life and/or health, which, if it fails, can be reasonably expected to result in significant
personal injury or death. Silicon Laboratories products are not designed or authorized for military applications. Silicon Laboratories products shall under no circumstances be used in
weapons of mass destruction including (but not limited to) nuclear, biological or chemical weapons, or missiles capable of delivering such weapons.
Trademark Information
Silicon Laboratories Inc.® , Silicon Laboratories®, Silicon Labs®, SiLabs® and the Silicon Labs logo®, Bluegiga®, Bluegiga Logo®, Clockbuilder®, CMEMS®, DSPLL®, EFM®, EFM32®,
EFR, Ember®, Energy Micro, Energy Micro logo and combinations thereof, "the world’s most energy friendly microcontrollers", Ember®, EZLink®, EZRadio®, EZRadioPRO®, Gecko®,
ISOmodem®, Precision32®, ProSLIC®, Simplicity Studio®, SiPHY®, Telegesis, the Telegesis Logo®, USBXpress® and others are trademarks or registered trademarks of Silicon Laborato-
ries Inc. ARM, CORTEX, Cortex-M3 and THUMB are trademarks or registered trademarks of ARM Holdings. Keil is a registered trademark of ARM Limited. All other products or brand
names mentioned herein are trademarks of their respective holders.

Products related to this Datasheet

UNIVERSAL BEE STARTR KIT EFM8UB1