JPY | USD

Logic

Devices that have an output which is based on a logical operation performed on the input.

Gates and Inverters Gates and Inverters A semiconductor device used in digital circuits to change the state of the output based on the state of the inputs. Each type of gate has different rules as to what the output will be. Common gate types include AND, OR, NAD, NOR, and NOT (inverter) styles.
View all Gates and Inverters
Gates and Inverters - Multi-function, Configurable Gates and Inverters - Multi-function, Configurable A semiconductor device used in digital circuits to change the state of the output based on the state of the inputs. Items in this family can either have a variety of outputs or be set to provide specific logic outputs.
View all Gates and Inverters - Multi-function, Configurable
Buffers, Drivers, Transceivers Buffers, Drivers, Transceivers Semiconductor devices that are designed to provide isolation, sends or receives logic signals.
View all Buffers, Drivers, Transceivers
Signal Switches, Multiplexers, Decoders Signal Switches, Multiplexers, Decoders Semiconductor devices that are designed to block or reroute logic signals.
View all Signal Switches, Multiplexers, Decoders
Translators, Level Shifters Translators, Level Shifters Semiconductor devices that are designed to provide changes between different logic levels (voltage levels).
View all Translators, Level Shifters
Flip Flops Flip Flops A semiconductor devices designed to store a logic state (bit). The state of these devices remain stable until a trigger pulse is received. Flip-flops are edge sensitive devices. Several types of flip flops exist including D (Delay), JK, and SR (Set Reset).
View all Flip Flops
Counters, Dividers Counters, Dividers A semiconductor device that counts the number of times a state changes or an event occurs or a semiconductor device that is designed to divide an input frequency.
View all Counters, Dividers
Shift Registers Shift Registers A semiconductor device that is composed of multiple flip flops with the output of one being used as the input for the next.
View all Shift Registers
Latches Latches A semiconductor device designed to store a logic state (bit). If the enable is set on the device then the outputs will be constantly changing based on changes in the inputs. Many type of latches exist including D (Delay), SR (Set Reset) and T (Transparent).
View all Latches
Multivibrators Multivibrators A semiconductor that switches between states.
View all Multivibrators
Comparators Comparators A semiconductor devices that is designed to look at different inputs and based on the differences return an output. Different styles are available for that compare difference types of inputs.
View all Comparators
FIFOs FIFOs A semiconductor device that stores data on a first in first out basis.
View all FIFOs
Parity Generators and Checkers Parity Generators and Checkers A semiconductor device that is used to produce and/or check on an extra bit that is transmitted with a signal. this extra bit is used to check for errors that occurred during transmission.
View all Parity Generators and Checkers
Universal Bus Functions Universal Bus Functions Semiconductor devices that are designed to be used in Universal Bus circuits.
View all Universal Bus Functions
Specialty Logic Specialty Logic Devices designed to provide specific or unique logic functions.
View all Specialty Logic